aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorEric Anholt2012-01-03 16:32:18 -0600
committerEric Anholt2012-01-04 16:49:44 -0600
commit683855f65523c978562ead56f9d68f50ffdca1a2 (patch)
tree078e74f9858d18f63d55d23ce3592a15ddfc540d /include/drm/i915_drm.h
parentccbc40340b7b472939a90ae8afc0a82b358ce189 (diff)
downloadexternal-libgbm-683855f65523c978562ead56f9d68f50ffdca1a2.tar.gz
external-libgbm-683855f65523c978562ead56f9d68f50ffdca1a2.tar.xz
external-libgbm-683855f65523c978562ead56f9d68f50ffdca1a2.zip
intel: Add regression tests for batch decode.
The .batch was generated using the dump-a-batch branch of git://people.freedesktop.org/~anholt/mesa using glxgears on gen7 hardware, using INTEL_DEVID_OVERRIDE for non-gen7 (this means that offsets in the buffers for non-gen7 are 0!). The .ref was generated by: ./test_decode tests/gen7-3d.batch -dump. The .sh exists because you can't supply arguments to tests using the simple automake tests driver. Something reasonable could be done using automake's parallel-tests driver (in fact, a previous version of the patch did that), but I was concerned that: 1) The parallel-tests driver is documented to be unstable -- they may change interfaces on us later. 2) The parallel-tests driver hides the output of tests in .log files scattered all over the tree, which was ugly and more painful to work with. v2: Actually add the batch files, add a .gitignore for the *-new.txt files added after failures, and fix failure mode for undetected chipset name. Reviewed-by: Daniel Vetter <daniel.vetter@ffwll.ch> (v1)
Diffstat (limited to 'include/drm/i915_drm.h')
0 files changed, 0 insertions, 0 deletions