diff options
author | Emil Velikov | 2017-02-13 19:34:14 -0600 |
---|---|---|
committer | Emil Velikov | 2017-02-13 19:35:56 -0600 |
commit | f6499b11534450b0f8c2b20529ebedaae924c156 (patch) | |
tree | 37476da3c606b836ce1b50f7a8f5e50820da54d2 /include | |
parent | ec80fd36a752960f28c5c900c8c68e201ce07093 (diff) | |
download | external-libgbm-f6499b11534450b0f8c2b20529ebedaae924c156.tar.gz external-libgbm-f6499b11534450b0f8c2b20529ebedaae924c156.tar.xz external-libgbm-f6499b11534450b0f8c2b20529ebedaae924c156.zip |
headers: add explicit note against local changes in the README
Even with the step by step guide people sometimes get confused.
Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com>
Diffstat (limited to 'include')
-rw-r--r-- | include/drm/README | 2 |
1 files changed, 2 insertions, 0 deletions
diff --git a/include/drm/README b/include/drm/README index a50b02c0..f3cdf5da 100644 --- a/include/drm/README +++ b/include/drm/README | |||
@@ -67,6 +67,8 @@ That said, it's up-to the individual developers to sync with newer version | |||
67 | 67 | ||
68 | When and how to update these files | 68 | When and how to update these files |
69 | ---------------------------------- | 69 | ---------------------------------- |
70 | Note: One should not do _any_ changes to the files apart from the steps below. | ||
71 | |||
70 | In order to update the files do the following: | 72 | In order to update the files do the following: |
71 | - Switch to a Linux kernel tree/branch which is not rebased. | 73 | - Switch to a Linux kernel tree/branch which is not rebased. |
72 | For example: airlied/drm-next | 74 | For example: airlied/drm-next |