diff options
-rw-r--r-- | freedreno/msm/msm_priv.h | 16 | ||||
-rw-r--r-- | freedreno/msm/msm_ringbuffer.c | 38 |
2 files changed, 31 insertions, 23 deletions
diff --git a/freedreno/msm/msm_priv.h b/freedreno/msm/msm_priv.h index 1f44398d..6d670aab 100644 --- a/freedreno/msm/msm_priv.h +++ b/freedreno/msm/msm_priv.h | |||
@@ -40,6 +40,7 @@ | |||
40 | struct msm_device { | 40 | struct msm_device { |
41 | struct fd_device base; | 41 | struct fd_device base; |
42 | struct fd_bo_cache ring_cache; | 42 | struct fd_bo_cache ring_cache; |
43 | unsigned ring_cnt; | ||
43 | }; | 44 | }; |
44 | 45 | ||
45 | static inline struct msm_device * to_msm_device(struct fd_device *x) | 46 | static inline struct msm_device * to_msm_device(struct fd_device *x) |
@@ -72,18 +73,11 @@ struct msm_bo { | |||
72 | struct fd_bo base; | 73 | struct fd_bo base; |
73 | uint64_t offset; | 74 | uint64_t offset; |
74 | uint64_t presumed; | 75 | uint64_t presumed; |
75 | /* in the common case, a bo won't be referenced by more than a single | 76 | /* to avoid excess hashtable lookups, cache the ring this bo was |
76 | * (parent) ring[*]. So to avoid looping over all the bo's in the | 77 | * last emitted on (since that will probably also be the next ring |
77 | * reloc table to find the idx of a bo that might already be in the | 78 | * it is emitted on) |
78 | * table, we cache the idx in the bo. But in order to detect the | ||
79 | * slow-path where bo is ref'd in multiple rb's, we also must track | ||
80 | * the current_ring for which the idx is valid. See bo2idx(). | ||
81 | * | ||
82 | * [*] in case multiple ringbuffers, ie. one toplevel and other rb(s) | ||
83 | * used for IB target(s), the toplevel rb is the parent which is | ||
84 | * tracking bo's for the submit | ||
85 | */ | 79 | */ |
86 | struct fd_ringbuffer *current_ring; | 80 | unsigned current_ring_seqno; |
87 | uint32_t idx; | 81 | uint32_t idx; |
88 | }; | 82 | }; |
89 | 83 | ||
diff --git a/freedreno/msm/msm_ringbuffer.c b/freedreno/msm/msm_ringbuffer.c index 86fc83e0..fbfaefae 100644 --- a/freedreno/msm/msm_ringbuffer.c +++ b/freedreno/msm/msm_ringbuffer.c | |||
@@ -92,6 +92,11 @@ struct msm_ringbuffer { | |||
92 | 92 | ||
93 | int is_growable; | 93 | int is_growable; |
94 | unsigned cmd_count; | 94 | unsigned cmd_count; |
95 | |||
96 | unsigned seqno; | ||
97 | |||
98 | /* maps fd_bo to idx: */ | ||
99 | void *bo_table; | ||
95 | }; | 100 | }; |
96 | 101 | ||
97 | static inline struct msm_ringbuffer * to_msm_ringbuffer(struct fd_ringbuffer *x) | 102 | static inline struct msm_ringbuffer * to_msm_ringbuffer(struct fd_ringbuffer *x) |
@@ -217,21 +222,24 @@ static uint32_t bo2idx(struct fd_ringbuffer *ring, struct fd_bo *bo, uint32_t fl | |||
217 | struct msm_bo *msm_bo = to_msm_bo(bo); | 222 | struct msm_bo *msm_bo = to_msm_bo(bo); |
218 | uint32_t idx; | 223 | uint32_t idx; |
219 | pthread_mutex_lock(&idx_lock); | 224 | pthread_mutex_lock(&idx_lock); |
220 | if (!msm_bo->current_ring) { | 225 | if (msm_bo->current_ring_seqno == msm_ring->seqno) { |
221 | idx = append_bo(ring, bo); | ||
222 | msm_bo->current_ring = ring; | ||
223 | msm_bo->idx = idx; | ||
224 | } else if (msm_bo->current_ring == ring) { | ||
225 | idx = msm_bo->idx; | 226 | idx = msm_bo->idx; |
226 | } else { | 227 | } else { |
227 | /* slow-path: */ | 228 | void *val; |
228 | for (idx = 0; idx < msm_ring->nr_bos; idx++) | 229 | |
229 | if (msm_ring->bos[idx] == bo) | 230 | if (!msm_ring->bo_table) |
230 | break; | 231 | msm_ring->bo_table = drmHashCreate(); |
231 | if (idx == msm_ring->nr_bos) { | 232 | |
232 | /* not found */ | 233 | if (!drmHashLookup(msm_ring->bo_table, bo->handle, &val)) { |
234 | /* found */ | ||
235 | idx = (uint32_t)val; | ||
236 | } else { | ||
233 | idx = append_bo(ring, bo); | 237 | idx = append_bo(ring, bo); |
238 | val = (void *)idx; | ||
239 | drmHashInsert(msm_ring->bo_table, bo->handle, val); | ||
234 | } | 240 | } |
241 | msm_bo->current_ring_seqno = msm_ring->seqno; | ||
242 | msm_bo->idx = idx; | ||
235 | } | 243 | } |
236 | pthread_mutex_unlock(&idx_lock); | 244 | pthread_mutex_unlock(&idx_lock); |
237 | if (flags & FD_RELOC_READ) | 245 | if (flags & FD_RELOC_READ) |
@@ -318,7 +326,7 @@ static void flush_reset(struct fd_ringbuffer *ring) | |||
318 | 326 | ||
319 | for (i = 0; i < msm_ring->nr_bos; i++) { | 327 | for (i = 0; i < msm_ring->nr_bos; i++) { |
320 | struct msm_bo *msm_bo = to_msm_bo(msm_ring->bos[i]); | 328 | struct msm_bo *msm_bo = to_msm_bo(msm_ring->bos[i]); |
321 | msm_bo->current_ring = NULL; | 329 | msm_bo->current_ring_seqno = 0; |
322 | fd_bo_del(&msm_bo->base); | 330 | fd_bo_del(&msm_bo->base); |
323 | } | 331 | } |
324 | 332 | ||
@@ -333,6 +341,11 @@ static void flush_reset(struct fd_ringbuffer *ring) | |||
333 | msm_ring->nr_cmds = 0; | 341 | msm_ring->nr_cmds = 0; |
334 | msm_ring->nr_bos = 0; | 342 | msm_ring->nr_bos = 0; |
335 | 343 | ||
344 | if (msm_ring->bo_table) { | ||
345 | drmHashDestroy(msm_ring->bo_table); | ||
346 | msm_ring->bo_table = NULL; | ||
347 | } | ||
348 | |||
336 | if (msm_ring->is_growable) { | 349 | if (msm_ring->is_growable) { |
337 | delete_cmds(msm_ring); | 350 | delete_cmds(msm_ring); |
338 | } else { | 351 | } else { |
@@ -551,6 +564,7 @@ drm_private struct fd_ringbuffer * msm_ringbuffer_new(struct fd_pipe *pipe, | |||
551 | } | 564 | } |
552 | 565 | ||
553 | list_inithead(&msm_ring->cmd_list); | 566 | list_inithead(&msm_ring->cmd_list); |
567 | msm_ring->seqno = ++to_msm_device(pipe->dev)->ring_cnt; | ||
554 | 568 | ||
555 | ring = &msm_ring->base; | 569 | ring = &msm_ring->base; |
556 | ring->funcs = &funcs; | 570 | ring->funcs = &funcs; |