diff options
-rw-r--r-- | .gitignore | 1 | ||||
-rw-r--r-- | Makefile.am | 6 | ||||
-rw-r--r-- | configure.ac | 10 | ||||
-rw-r--r-- | libkms/Makefile.am | 20 | ||||
-rw-r--r-- | libkms/api.c | 124 | ||||
-rw-r--r-- | libkms/internal.h | 67 | ||||
-rw-r--r-- | libkms/libkms.h | 69 | ||||
-rw-r--r-- | libkms/libkms.pc.in | 10 | ||||
-rw-r--r-- | libkms/vmwgfx.c | 226 | ||||
-rw-r--r-- | libkms/vmwgfx_drm.h | 441 |
10 files changed, 973 insertions, 1 deletions
@@ -42,6 +42,7 @@ libdrm.pc | |||
42 | libdrm_intel.pc | 42 | libdrm_intel.pc |
43 | libdrm_nouveau.pc | 43 | libdrm_nouveau.pc |
44 | libdrm_radeon.pc | 44 | libdrm_radeon.pc |
45 | libkms.pc | ||
45 | libtool | 46 | libtool |
46 | ltmain.sh | 47 | ltmain.sh |
47 | mach64.kld | 48 | mach64.kld |
diff --git a/Makefile.am b/Makefile.am index 41e5a342..ee3ccc70 100644 --- a/Makefile.am +++ b/Makefile.am | |||
@@ -25,6 +25,10 @@ DISTCHECK_CONFIGURE_FLAGS = --enable-nouveau-experimental-api --enable-radeon-ex | |||
25 | pkgconfigdir = @pkgconfigdir@ | 25 | pkgconfigdir = @pkgconfigdir@ |
26 | pkgconfig_DATA = libdrm.pc | 26 | pkgconfig_DATA = libdrm.pc |
27 | 27 | ||
28 | if HAVE_LIBKMS | ||
29 | LIBKMS_SUBDIR = libkms | ||
30 | endif | ||
31 | |||
28 | if HAVE_INTEL | 32 | if HAVE_INTEL |
29 | INTEL_SUBDIR = intel | 33 | INTEL_SUBDIR = intel |
30 | endif | 34 | endif |
@@ -37,7 +41,7 @@ if HAVE_RADEON | |||
37 | RADEON_SUBDIR = radeon | 41 | RADEON_SUBDIR = radeon |
38 | endif | 42 | endif |
39 | 43 | ||
40 | SUBDIRS = . $(INTEL_SUBDIR) $(NOUVEAU_SUBDIR) $(RADEON_SUBDIR) tests include | 44 | SUBDIRS = . $(LIBKMS_SUBDIR) $(INTEL_SUBDIR) $(NOUVEAU_SUBDIR) $(RADEON_SUBDIR) tests include |
41 | 45 | ||
42 | libdrm_la_LTLIBRARIES = libdrm.la | 46 | libdrm_la_LTLIBRARIES = libdrm.la |
43 | libdrm_ladir = $(libdir) | 47 | libdrm_ladir = $(libdir) |
diff --git a/configure.ac b/configure.ac index b8842201..52c591dd 100644 --- a/configure.ac +++ b/configure.ac | |||
@@ -43,6 +43,11 @@ AC_ARG_ENABLE(udev, AS_HELP_STRING([--enable-udev], | |||
43 | [Enable support for using udev instead of mknod (default: disabled)]), | 43 | [Enable support for using udev instead of mknod (default: disabled)]), |
44 | [UDEV=$enableval], [UDEV=no]) | 44 | [UDEV=$enableval], [UDEV=no]) |
45 | 45 | ||
46 | AC_ARG_ENABLE(libkms, | ||
47 | AS_HELP_STRING([--disable-libkms], | ||
48 | [Enable KMS mm abstraction library (default: yes)]), | ||
49 | [LIBKMS=$enableval], [LIBKMS=yes]) | ||
50 | |||
46 | AC_ARG_ENABLE(intel, | 51 | AC_ARG_ENABLE(intel, |
47 | AS_HELP_STRING([--disable-intel], | 52 | AS_HELP_STRING([--disable-intel], |
48 | [Enable support for intel's KMS API (default: auto)]), | 53 | [Enable support for intel's KMS API (default: auto)]), |
@@ -134,6 +139,8 @@ if test "x$UDEV" = xyes; then | |||
134 | AC_DEFINE(UDEV, 1, [Have UDEV support]) | 139 | AC_DEFINE(UDEV, 1, [Have UDEV support]) |
135 | fi | 140 | fi |
136 | 141 | ||
142 | AM_CONDITIONAL(HAVE_LIBKMS, [test "x$LIBKMS" = xyes]) | ||
143 | |||
137 | AM_CONDITIONAL(HAVE_NOUVEAU, [test "x$NOUVEAU" = xyes]) | 144 | AM_CONDITIONAL(HAVE_NOUVEAU, [test "x$NOUVEAU" = xyes]) |
138 | 145 | ||
139 | AM_CONDITIONAL(HAVE_RADEON, [test "x$RADEON" = xyes]) | 146 | AM_CONDITIONAL(HAVE_RADEON, [test "x$RADEON" = xyes]) |
@@ -199,6 +206,8 @@ AC_SUBST(kernel_source) | |||
199 | AC_SUBST(WARN_CFLAGS) | 206 | AC_SUBST(WARN_CFLAGS) |
200 | AC_OUTPUT([ | 207 | AC_OUTPUT([ |
201 | Makefile | 208 | Makefile |
209 | libkms/Makefile | ||
210 | libkms/libkms.pc | ||
202 | intel/Makefile | 211 | intel/Makefile |
203 | intel/libdrm_intel.pc | 212 | intel/libdrm_intel.pc |
204 | radeon/Makefile | 213 | radeon/Makefile |
@@ -215,6 +224,7 @@ AC_OUTPUT([ | |||
215 | echo "" | 224 | echo "" |
216 | echo "$PACKAGE_STRING will be compiled with:" | 225 | echo "$PACKAGE_STRING will be compiled with:" |
217 | echo "" | 226 | echo "" |
227 | echo " libkms $LIBKMS" | ||
218 | echo " Intel API $INTEL" | 228 | echo " Intel API $INTEL" |
219 | echo " Radeon API $RADEON" | 229 | echo " Radeon API $RADEON" |
220 | echo " Nouveau API $NOUVEAU" | 230 | echo " Nouveau API $NOUVEAU" |
diff --git a/libkms/Makefile.am b/libkms/Makefile.am new file mode 100644 index 00000000..d65d6012 --- /dev/null +++ b/libkms/Makefile.am | |||
@@ -0,0 +1,20 @@ | |||
1 | AM_CFLAGS = \ | ||
2 | $(WARN_CFLAGS) \ | ||
3 | -I$(top_srcdir)/include/drm | ||
4 | |||
5 | libkms_la_LTLIBRARIES = libkms.la | ||
6 | libkms_ladir = $(libdir) | ||
7 | libkms_la_LDFLAGS = -version-number 1:0:0 -no-undefined | ||
8 | libkms_la_LIBADD = | ||
9 | |||
10 | libkms_la_SOURCES = \ | ||
11 | api.c \ | ||
12 | vmwgfx.c | ||
13 | |||
14 | libkmsincludedir = ${includedir}/libkms | ||
15 | libkmsinclude_HEADERS = libkms.h | ||
16 | |||
17 | pkgconfigdir = @pkgconfigdir@ | ||
18 | pkgconfig_DATA = libkms.pc | ||
19 | |||
20 | EXTRA_DIST = libkms.pc.in | ||
diff --git a/libkms/api.c b/libkms/api.c new file mode 100644 index 00000000..f15ee70b --- /dev/null +++ b/libkms/api.c | |||
@@ -0,0 +1,124 @@ | |||
1 | /************************************************************************** | ||
2 | * | ||
3 | * Copyright © 2009 VMware, Inc., Palo Alto, CA., USA | ||
4 | * All Rights Reserved. | ||
5 | * | ||
6 | * Permission is hereby granted, free of charge, to any person obtaining a | ||
7 | * copy of this software and associated documentation files (the | ||
8 | * "Software"), to deal in the Software without restriction, including | ||
9 | * without limitation the rights to use, copy, modify, merge, publish, | ||
10 | * distribute, sub license, and/or sell copies of the Software, and to | ||
11 | * permit persons to whom the Software is furnished to do so, subject to | ||
12 | * the following conditions: | ||
13 | * | ||
14 | * The above copyright notice and this permission notice (including the | ||
15 | * next paragraph) shall be included in all copies or substantial portions | ||
16 | * of the Software. | ||
17 | * | ||
18 | * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR | ||
19 | * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, | ||
20 | * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. IN NO EVENT SHALL | ||
21 | * THE COPYRIGHT HOLDERS, AUTHORS AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, | ||
22 | * DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR | ||
23 | * OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE | ||
24 | * USE OR OTHER DEALINGS IN THE SOFTWARE. | ||
25 | * | ||
26 | **************************************************************************/ | ||
27 | |||
28 | |||
29 | #include <errno.h> | ||
30 | #include <stdlib.h> | ||
31 | #include <string.h> | ||
32 | #include "internal.h" | ||
33 | |||
34 | int kms_create(int fd, struct kms_driver **out) | ||
35 | { | ||
36 | return vmwgfx_create(fd, out); | ||
37 | } | ||
38 | |||
39 | int kms_get_prop(struct kms_driver *kms, unsigned key, unsigned *out) | ||
40 | { | ||
41 | switch (key) { | ||
42 | case KMS_MAX_SCANOUT_WIDTH: | ||
43 | case KMS_MAX_SCANOUT_HEIGHT: | ||
44 | case KMS_MIN_SCANOUT_WIDTH: | ||
45 | case KMS_MIN_SCANOUT_HEIGHT: | ||
46 | case KMS_MAX_CURSOR_WIDTH: | ||
47 | case KMS_MAX_CURSOR_HEIGHT: | ||
48 | case KMS_MIN_CURSOR_WIDTH: | ||
49 | case KMS_MIN_CURSOR_HEIGHT: | ||
50 | break; | ||
51 | default: | ||
52 | return -EINVAL; | ||
53 | } | ||
54 | return kms->get_prop(kms, key, out); | ||
55 | } | ||
56 | |||
57 | int kms_destroy(struct kms_driver *kms) | ||
58 | { | ||
59 | free(kms); | ||
60 | return 0; | ||
61 | } | ||
62 | |||
63 | int kms_bo_create(struct kms_driver *kms, const unsigned *attr, struct kms_bo **out) | ||
64 | { | ||
65 | unsigned width = 0; | ||
66 | unsigned height = 0; | ||
67 | enum kms_bo_type type = KMS_BO_TYPE_SCANOUT; | ||
68 | int i; | ||
69 | |||
70 | for (i = 0; attr[i];) { | ||
71 | unsigned key = attr[i++]; | ||
72 | unsigned value = attr[i++]; | ||
73 | |||
74 | switch (key) { | ||
75 | case KMS_WIDTH: | ||
76 | width = value; | ||
77 | break; | ||
78 | case KMS_HEIGHT: | ||
79 | height = value; | ||
80 | break; | ||
81 | case KMS_BO_TYPE: | ||
82 | type = value; | ||
83 | break; | ||
84 | default: | ||
85 | return EINVAL; | ||
86 | } | ||
87 | } | ||
88 | |||
89 | if (width == 0 || height == 0) | ||
90 | return -EINVAL; | ||
91 | |||
92 | return kms->bo_create(kms, width, height, type, attr, out); | ||
93 | } | ||
94 | |||
95 | int kms_bo_get_prop(struct kms_bo *bo, unsigned key, unsigned *out) | ||
96 | { | ||
97 | switch (key) { | ||
98 | case KMS_PITCH: | ||
99 | *out = bo->pitch; | ||
100 | break; | ||
101 | case KMS_HANDLE: | ||
102 | *out = bo->handle; | ||
103 | break; | ||
104 | default: | ||
105 | return -EINVAL; | ||
106 | } | ||
107 | |||
108 | return 0; | ||
109 | } | ||
110 | |||
111 | int kms_bo_map(struct kms_bo *bo, void **out) | ||
112 | { | ||
113 | return bo->kms->bo_map(bo, out); | ||
114 | } | ||
115 | |||
116 | int kms_bo_unmap(struct kms_bo *bo) | ||
117 | { | ||
118 | return bo->kms->bo_unmap(bo); | ||
119 | } | ||
120 | |||
121 | int kms_bo_destroy(struct kms_bo *bo) | ||
122 | { | ||
123 | return bo->kms->bo_destroy(bo); | ||
124 | } | ||
diff --git a/libkms/internal.h b/libkms/internal.h new file mode 100644 index 00000000..f1a2b1cf --- /dev/null +++ b/libkms/internal.h | |||
@@ -0,0 +1,67 @@ | |||
1 | /************************************************************************** | ||
2 | * | ||
3 | * Copyright © 2009 VMware, Inc., Palo Alto, CA., USA | ||
4 | * All Rights Reserved. | ||
5 | * | ||
6 | * Permission is hereby granted, free of charge, to any person obtaining a | ||
7 | * copy of this software and associated documentation files (the | ||
8 | * "Software"), to deal in the Software without restriction, including | ||
9 | * without limitation the rights to use, copy, modify, merge, publish, | ||
10 | * distribute, sub license, and/or sell copies of the Software, and to | ||
11 | * permit persons to whom the Software is furnished to do so, subject to | ||
12 | * the following conditions: | ||
13 | * | ||
14 | * The above copyright notice and this permission notice (including the | ||
15 | * next paragraph) shall be included in all copies or substantial portions | ||
16 | * of the Software. | ||
17 | * | ||
18 | * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR | ||
19 | * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, | ||
20 | * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. IN NO EVENT SHALL | ||
21 | * THE COPYRIGHT HOLDERS, AUTHORS AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, | ||
22 | * DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR | ||
23 | * OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE | ||
24 | * USE OR OTHER DEALINGS IN THE SOFTWARE. | ||
25 | * | ||
26 | **************************************************************************/ | ||
27 | |||
28 | |||
29 | #ifndef INTERNAL_H_ | ||
30 | #define INTERNAL_H_ | ||
31 | |||
32 | #include "libkms.h" | ||
33 | |||
34 | struct kms_driver | ||
35 | { | ||
36 | int (*get_prop)(struct kms_driver *kms, const unsigned key, | ||
37 | unsigned *out); | ||
38 | int (*destroy)(struct kms_driver *kms); | ||
39 | |||
40 | int (*bo_create)(struct kms_driver *kms, | ||
41 | unsigned width, | ||
42 | unsigned height, | ||
43 | enum kms_bo_type type, | ||
44 | const unsigned *attr, | ||
45 | struct kms_bo **out); | ||
46 | int (*bo_get_prop)(struct kms_bo *bo, const unsigned key, | ||
47 | unsigned *out); | ||
48 | int (*bo_map)(struct kms_bo *bo, void **out); | ||
49 | int (*bo_unmap)(struct kms_bo *bo); | ||
50 | int (*bo_destroy)(struct kms_bo *bo); | ||
51 | |||
52 | int fd; | ||
53 | }; | ||
54 | |||
55 | struct kms_bo | ||
56 | { | ||
57 | struct kms_driver *kms; | ||
58 | void *ptr; | ||
59 | size_t size; | ||
60 | size_t offset; | ||
61 | size_t pitch; | ||
62 | unsigned handle; | ||
63 | }; | ||
64 | |||
65 | int vmwgfx_create(int fd, struct kms_driver **out); | ||
66 | |||
67 | #endif | ||
diff --git a/libkms/libkms.h b/libkms/libkms.h new file mode 100644 index 00000000..9cc8ae21 --- /dev/null +++ b/libkms/libkms.h | |||
@@ -0,0 +1,69 @@ | |||
1 | /************************************************************************** | ||
2 | * | ||
3 | * Copyright © 2009 VMware, Inc., Palo Alto, CA., USA | ||
4 | * All Rights Reserved. | ||
5 | * | ||
6 | * Permission is hereby granted, free of charge, to any person obtaining a | ||
7 | * copy of this software and associated documentation files (the | ||
8 | * "Software"), to deal in the Software without restriction, including | ||
9 | * without limitation the rights to use, copy, modify, merge, publish, | ||
10 | * distribute, sub license, and/or sell copies of the Software, and to | ||
11 | * permit persons to whom the Software is furnished to do so, subject to | ||
12 | * the following conditions: | ||
13 | * | ||
14 | * The above copyright notice and this permission notice (including the | ||
15 | * next paragraph) shall be included in all copies or substantial portions | ||
16 | * of the Software. | ||
17 | * | ||
18 | * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR | ||
19 | * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, | ||
20 | * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. IN NO EVENT SHALL | ||
21 | * THE COPYRIGHT HOLDERS, AUTHORS AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, | ||
22 | * DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR | ||
23 | * OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE | ||
24 | * USE OR OTHER DEALINGS IN THE SOFTWARE. | ||
25 | * | ||
26 | **************************************************************************/ | ||
27 | |||
28 | |||
29 | #ifndef _LIBKMS_H_ | ||
30 | #define _LIBKMS_H_ | ||
31 | |||
32 | struct kms_driver; | ||
33 | struct kms_bo; | ||
34 | |||
35 | enum kms_attrib | ||
36 | { | ||
37 | KMS_TERMINATE_PROP_LIST, | ||
38 | KMS_BO_TYPE, | ||
39 | KMS_WIDTH, | ||
40 | KMS_HEIGHT, | ||
41 | KMS_PITCH, | ||
42 | KMS_HANDLE, | ||
43 | KMS_MAX_SCANOUT_WIDTH, | ||
44 | KMS_MAX_SCANOUT_HEIGHT, | ||
45 | KMS_MIN_SCANOUT_WIDTH, | ||
46 | KMS_MIN_SCANOUT_HEIGHT, | ||
47 | KMS_MAX_CURSOR_WIDTH, | ||
48 | KMS_MAX_CURSOR_HEIGHT, | ||
49 | KMS_MIN_CURSOR_WIDTH, | ||
50 | KMS_MIN_CURSOR_HEIGHT, | ||
51 | }; | ||
52 | |||
53 | enum kms_bo_type | ||
54 | { | ||
55 | KMS_BO_TYPE_SCANOUT = (1 << 0), | ||
56 | KMS_BO_TYPE_CURSOR = (1 << 1), | ||
57 | }; | ||
58 | |||
59 | int kms_create(int fd, struct kms_driver **out); | ||
60 | int kms_get_prop(struct kms_driver *kms, unsigned key, unsigned *out); | ||
61 | int kms_destroy(struct kms_driver *kms); | ||
62 | |||
63 | int kms_bo_create(struct kms_driver *kms, const unsigned *attr, struct kms_bo **out); | ||
64 | int kms_bo_get_prop(struct kms_bo *bo, unsigned key, unsigned *out); | ||
65 | int kms_bo_map(struct kms_bo *bo, void **out); | ||
66 | int kms_bo_unmap(struct kms_bo *bo); | ||
67 | int kms_bo_destroy(struct kms_bo *bo); | ||
68 | |||
69 | #endif | ||
diff --git a/libkms/libkms.pc.in b/libkms/libkms.pc.in new file mode 100644 index 00000000..b3cbbf33 --- /dev/null +++ b/libkms/libkms.pc.in | |||
@@ -0,0 +1,10 @@ | |||
1 | prefix=@prefix@ | ||
2 | exec_prefix=@exec_prefix@ | ||
3 | libdir=@libdir@ | ||
4 | includedir=@includedir@ | ||
5 | |||
6 | Name: libkms | ||
7 | Description: Library that abstract aways the different mm interface for kernel drivers | ||
8 | Version: 1.0 | ||
9 | Libs: -L${libdir} -lkms | ||
10 | Cflags: -I${includedir}/libkms | ||
diff --git a/libkms/vmwgfx.c b/libkms/vmwgfx.c new file mode 100644 index 00000000..5030b7e3 --- /dev/null +++ b/libkms/vmwgfx.c | |||
@@ -0,0 +1,226 @@ | |||
1 | /************************************************************************** | ||
2 | * | ||
3 | * Copyright © 2009 VMware, Inc., Palo Alto, CA., USA | ||
4 | * All Rights Reserved. | ||
5 | * | ||
6 | * Permission is hereby granted, free of charge, to any person obtaining a | ||
7 | * copy of this software and associated documentation files (the | ||
8 | * "Software"), to deal in the Software without restriction, including | ||
9 | * without limitation the rights to use, copy, modify, merge, publish, | ||
10 | * distribute, sub license, and/or sell copies of the Software, and to | ||
11 | * permit persons to whom the Software is furnished to do so, subject to | ||
12 | * the following conditions: | ||
13 | * | ||
14 | * The above copyright notice and this permission notice (including the | ||
15 | * next paragraph) shall be included in all copies or substantial portions | ||
16 | * of the Software. | ||
17 | * | ||
18 | * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR | ||
19 | * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, | ||
20 | * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. IN NO EVENT SHALL | ||
21 | * THE COPYRIGHT HOLDERS, AUTHORS AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, | ||
22 | * DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR | ||
23 | * OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE | ||
24 | * USE OR OTHER DEALINGS IN THE SOFTWARE. | ||
25 | * | ||
26 | **************************************************************************/ | ||
27 | |||
28 | |||
29 | #define HAVE_STDINT_H | ||
30 | #define _FILE_OFFSET_BITS 64 | ||
31 | |||
32 | #include <errno.h> | ||
33 | #include <stdlib.h> | ||
34 | #include <string.h> | ||
35 | #include "internal.h" | ||
36 | |||
37 | #include <sys/mman.h> | ||
38 | #include "xf86drm.h" | ||
39 | #include "vmwgfx_drm.h" | ||
40 | |||
41 | struct vmwgfx_bo | ||
42 | { | ||
43 | struct kms_bo base; | ||
44 | uint64_t map_handle; | ||
45 | unsigned map_count; | ||
46 | }; | ||
47 | |||
48 | static int | ||
49 | vmwgfx_get_prop(struct kms_driver *kms, unsigned key, unsigned *out) | ||
50 | { | ||
51 | switch (key) { | ||
52 | case KMS_MAX_SCANOUT_WIDTH: | ||
53 | *out = 2048; | ||
54 | break; | ||
55 | case KMS_MAX_SCANOUT_HEIGHT: | ||
56 | *out = 2048; | ||
57 | break; | ||
58 | case KMS_MIN_SCANOUT_WIDTH: | ||
59 | *out = 1; | ||
60 | break; | ||
61 | case KMS_MIN_SCANOUT_HEIGHT: | ||
62 | *out = 1; | ||
63 | break; | ||
64 | case KMS_MAX_CURSOR_WIDTH: | ||
65 | *out = 64; | ||
66 | break; | ||
67 | case KMS_MAX_CURSOR_HEIGHT: | ||
68 | *out = 64; | ||
69 | break; | ||
70 | case KMS_MIN_CURSOR_WIDTH: | ||
71 | *out = 64; | ||
72 | break; | ||
73 | case KMS_MIN_CURSOR_HEIGHT: | ||
74 | *out = 64; | ||
75 | break; | ||
76 | default: | ||
77 | return -EINVAL; | ||
78 | } | ||
79 | return 0; | ||
80 | } | ||
81 | |||
82 | static int | ||
83 | vmwgfx_destroy(struct kms_driver *kms) | ||
84 | { | ||
85 | free(kms); | ||
86 | return 0; | ||
87 | } | ||
88 | |||
89 | static int | ||
90 | vmwgfx_bo_create(struct kms_driver *kms, | ||
91 | const unsigned width, const unsigned height, | ||
92 | const enum kms_bo_type type, const unsigned *attr, | ||
93 | struct kms_bo **out) | ||
94 | { | ||
95 | struct vmwgfx_bo *bo; | ||
96 | int i, ret; | ||
97 | |||
98 | for (i = 0; attr[i]; i += 2) { | ||
99 | switch (attr[i]) { | ||
100 | case KMS_WIDTH: | ||
101 | case KMS_HEIGHT: | ||
102 | case KMS_BO_TYPE: | ||
103 | break; | ||
104 | default: | ||
105 | return EINVAL; | ||
106 | } | ||
107 | } | ||
108 | |||
109 | bo = calloc(1, sizeof(*bo)); | ||
110 | if (!bo) | ||
111 | return -EINVAL; | ||
112 | |||
113 | { | ||
114 | union drm_vmw_alloc_dmabuf_arg arg; | ||
115 | struct drm_vmw_alloc_dmabuf_req *req = &arg.req; | ||
116 | struct drm_vmw_dmabuf_rep *rep = &arg.rep; | ||
117 | |||
118 | memset(&arg, 0, sizeof(arg)); | ||
119 | req->size = width * height * 4; | ||
120 | bo->base.size = req->size; | ||
121 | bo->base.pitch = width * 4; | ||
122 | bo->base.kms = kms; | ||
123 | |||
124 | do { | ||
125 | ret = drmCommandWriteRead(bo->base.kms->fd, | ||
126 | DRM_VMW_ALLOC_DMABUF, | ||
127 | &arg, sizeof(arg)); | ||
128 | } while (ret == -ERESTART); | ||
129 | |||
130 | if (ret) | ||
131 | goto err_free; | ||
132 | |||
133 | bo->base.handle = rep->handle; | ||
134 | bo->map_handle = rep->map_handle; | ||
135 | bo->base.handle = rep->cur_gmr_id; | ||
136 | bo->base.offset = rep->cur_gmr_offset; | ||
137 | } | ||
138 | |||
139 | *out = &bo->base; | ||
140 | |||
141 | return 0; | ||
142 | |||
143 | err_free: | ||
144 | free(bo); | ||
145 | return ret; | ||
146 | } | ||
147 | |||
148 | static int | ||
149 | vmwgfx_bo_get_prop(struct kms_bo *bo, unsigned key, unsigned *out) | ||
150 | { | ||
151 | switch (key) { | ||
152 | default: | ||
153 | return -EINVAL; | ||
154 | } | ||
155 | } | ||
156 | |||
157 | static int | ||
158 | vmwgfx_bo_map(struct kms_bo *_bo, void **out) | ||
159 | { | ||
160 | struct vmwgfx_bo *bo = (struct vmwgfx_bo *)_bo; | ||
161 | void *map; | ||
162 | |||
163 | if (!bo->map_count) { | ||
164 | map = mmap(NULL, bo->base.size, PROT_READ | PROT_WRITE, | ||
165 | MAP_SHARED, bo->base.kms->fd, bo->map_handle); | ||
166 | |||
167 | if (!map) | ||
168 | return -ENOMEM; | ||
169 | |||
170 | bo->base.ptr = map; | ||
171 | } | ||
172 | |||
173 | bo->map_count++; | ||
174 | *out = bo->base.ptr; | ||
175 | |||
176 | return 0; | ||
177 | } | ||
178 | |||
179 | static int | ||
180 | vmwgfx_bo_unmap(struct kms_bo *_bo) | ||
181 | { | ||
182 | struct vmwgfx_bo *bo = (struct vmwgfx_bo *)_bo; | ||
183 | bo->map_count--; | ||
184 | return 0; | ||
185 | } | ||
186 | |||
187 | static int | ||
188 | vmwgfx_bo_destroy(struct kms_bo *_bo) | ||
189 | { | ||
190 | struct vmwgfx_bo *bo = (struct vmwgfx_bo *)_bo; | ||
191 | struct drm_vmw_unref_dmabuf_arg arg; | ||
192 | |||
193 | if (bo->map_count) { | ||
194 | munmap(bo->base.ptr, bo->base.size); | ||
195 | bo->base.ptr = NULL; | ||
196 | } | ||
197 | |||
198 | memset(&arg, 0, sizeof(arg)); | ||
199 | arg.handle = bo->base.handle; | ||
200 | drmCommandWrite(bo->base.kms->fd, DRM_VMW_UNREF_DMABUF, &arg, sizeof(arg)); | ||
201 | |||
202 | free(bo); | ||
203 | return 0; | ||
204 | } | ||
205 | |||
206 | int | ||
207 | vmwgfx_create(int fd, struct kms_driver **out) | ||
208 | { | ||
209 | struct kms_driver *kms; | ||
210 | |||
211 | kms = calloc(1, sizeof(*kms)); | ||
212 | if (!kms) | ||
213 | return -ENOMEM; | ||
214 | |||
215 | kms->fd = fd; | ||
216 | |||
217 | kms->bo_create = vmwgfx_bo_create; | ||
218 | kms->bo_map = vmwgfx_bo_map; | ||
219 | kms->bo_unmap = vmwgfx_bo_unmap; | ||
220 | kms->bo_get_prop = vmwgfx_bo_get_prop; | ||
221 | kms->bo_destroy = vmwgfx_bo_destroy; | ||
222 | kms->get_prop = vmwgfx_get_prop; | ||
223 | kms->destroy = vmwgfx_destroy; | ||
224 | *out = kms; | ||
225 | return 0; | ||
226 | } | ||
diff --git a/libkms/vmwgfx_drm.h b/libkms/vmwgfx_drm.h new file mode 100644 index 00000000..597ab3c9 --- /dev/null +++ b/libkms/vmwgfx_drm.h | |||
@@ -0,0 +1,441 @@ | |||
1 | /************************************************************************** | ||
2 | * | ||
3 | * Copyright © 2009 VMware, Inc., Palo Alto, CA., USA | ||
4 | * All Rights Reserved. | ||
5 | * | ||
6 | * Permission is hereby granted, free of charge, to any person obtaining a | ||
7 | * copy of this software and associated documentation files (the | ||
8 | * "Software"), to deal in the Software without restriction, including | ||
9 | * without limitation the rights to use, copy, modify, merge, publish, | ||
10 | * distribute, sub license, and/or sell copies of the Software, and to | ||
11 | * permit persons to whom the Software is furnished to do so, subject to | ||
12 | * the following conditions: | ||
13 | * | ||
14 | * The above copyright notice and this permission notice (including the | ||
15 | * next paragraph) shall be included in all copies or substantial portions | ||
16 | * of the Software. | ||
17 | * | ||
18 | * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR | ||
19 | * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, | ||
20 | * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. IN NO EVENT SHALL | ||
21 | * THE COPYRIGHT HOLDERS, AUTHORS AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, | ||
22 | * DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR | ||
23 | * OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE | ||
24 | * USE OR OTHER DEALINGS IN THE SOFTWARE. | ||
25 | * | ||
26 | **************************************************************************/ | ||
27 | |||
28 | #ifndef _VMWGFX_DRM_H_ | ||
29 | #define _VMWGFX_DRM_H_ | ||
30 | |||
31 | #define DRM_VMW_MAX_SURFACE_FACES 6 | ||
32 | #define DRM_VMW_MAX_MIP_LEVELS 24 | ||
33 | |||
34 | #define DRM_VMW_EXT_NAME_LEN 128 | ||
35 | |||
36 | #define DRM_VMW_GET_PARAM 1 | ||
37 | #define DRM_VMW_EXTENSION 2 | ||
38 | #define DRM_VMW_CREATE_CONTEXT 3 | ||
39 | #define DRM_VMW_UNREF_CONTEXT 4 | ||
40 | #define DRM_VMW_CREATE_SURFACE 5 | ||
41 | #define DRM_VMW_UNREF_SURFACE 6 | ||
42 | #define DRM_VMW_REF_SURFACE 7 | ||
43 | #define DRM_VMW_EXECBUF 8 | ||
44 | #define DRM_VMW_ALLOC_DMABUF 9 | ||
45 | #define DRM_VMW_UNREF_DMABUF 10 | ||
46 | #define DRM_VMW_FIFO_DEBUG 11 | ||
47 | #define DRM_VMW_FENCE_WAIT 12 | ||
48 | |||
49 | /*************************************************************************/ | ||
50 | /** | ||
51 | * DRM_VMW_GET_PARAM - get device information. | ||
52 | * | ||
53 | * Currently we support only one parameter: | ||
54 | * | ||
55 | * DRM_VMW_PARAM_FIFO_OFFSET: | ||
56 | * Offset to use to map the first page of the FIFO read-only. | ||
57 | * The fifo is mapped using the mmap() system call on the drm device. | ||
58 | */ | ||
59 | |||
60 | #define DRM_VMW_PARAM_FIFO_OFFSET 0 | ||
61 | |||
62 | /** | ||
63 | * struct drm_vmw_getparam_arg | ||
64 | * | ||
65 | * @value: Returned value. //Out | ||
66 | * @param: Parameter to query. //In. | ||
67 | * | ||
68 | * Argument to the DRM_VMW_GET_PARAM Ioctl. | ||
69 | */ | ||
70 | |||
71 | struct drm_vmw_getparam_arg { | ||
72 | uint64_t value; | ||
73 | uint32_t param; | ||
74 | uint32_t pad64; | ||
75 | }; | ||
76 | |||
77 | /*************************************************************************/ | ||
78 | /** | ||
79 | * DRM_VMW_EXTENSION - Query device extensions. | ||
80 | */ | ||
81 | |||
82 | /** | ||
83 | * struct drm_vmw_extension_rep | ||
84 | * | ||
85 | * @exists: The queried extension exists. | ||
86 | * @driver_ioctl_offset: Ioctl number of the first ioctl in the extension. | ||
87 | * @driver_sarea_offset: Offset to any space in the DRI SAREA | ||
88 | * used by the extension. | ||
89 | * @major: Major version number of the extension. | ||
90 | * @minor: Minor version number of the extension. | ||
91 | * @pl: Patch level version number of the extension. | ||
92 | * | ||
93 | * Output argument to the DRM_VMW_EXTENSION Ioctl. | ||
94 | */ | ||
95 | |||
96 | struct drm_vmw_extension_rep { | ||
97 | int32_t exists; | ||
98 | uint32_t driver_ioctl_offset; | ||
99 | uint32_t driver_sarea_offset; | ||
100 | uint32_t major; | ||
101 | uint32_t minor; | ||
102 | uint32_t pl; | ||
103 | uint32_t pad64; | ||
104 | }; | ||
105 | |||
106 | /** | ||
107 | * union drm_vmw_extension_arg | ||
108 | * | ||
109 | * @extension - Ascii name of the extension to be queried. //In | ||
110 | * @rep - Reply as defined above. //Out | ||
111 | * | ||
112 | * Argument to the DRM_VMW_EXTENSION Ioctl. | ||
113 | */ | ||
114 | |||
115 | union drm_vmw_extension_arg { | ||
116 | char extension[DRM_VMW_EXT_NAME_LEN]; | ||
117 | struct drm_vmw_extension_rep rep; | ||
118 | }; | ||
119 | |||
120 | /*************************************************************************/ | ||
121 | /** | ||
122 | * DRM_VMW_CREATE_CONTEXT - Create a host context. | ||
123 | * | ||
124 | * Allocates a device unique context id, and queues a create context command | ||
125 | * for the host. Does not wait for host completion. | ||
126 | */ | ||
127 | |||
128 | /** | ||
129 | * struct drm_vmw_context_arg | ||
130 | * | ||
131 | * @cid: Device unique context ID. | ||
132 | * | ||
133 | * Output argument to the DRM_VMW_CREATE_CONTEXT Ioctl. | ||
134 | * Input argument to the DRM_VMW_UNREF_CONTEXT Ioctl. | ||
135 | */ | ||
136 | |||
137 | struct drm_vmw_context_arg { | ||
138 | int32_t cid; | ||
139 | uint32_t pad64; | ||
140 | }; | ||
141 | |||
142 | /*************************************************************************/ | ||
143 | /** | ||
144 | * DRM_VMW_UNREF_CONTEXT - Create a host context. | ||
145 | * | ||
146 | * Frees a global context id, and queues a destroy host command for the host. | ||
147 | * Does not wait for host completion. The context ID can be used directly | ||
148 | * in the command stream and shows up as the same context ID on the host. | ||
149 | */ | ||
150 | |||
151 | /*************************************************************************/ | ||
152 | /** | ||
153 | * DRM_VMW_CREATE_SURFACE - Create a host suface. | ||
154 | * | ||
155 | * Allocates a device unique surface id, and queues a create surface command | ||
156 | * for the host. Does not wait for host completion. The surface ID can be | ||
157 | * used directly in the command stream and shows up as the same surface | ||
158 | * ID on the host. | ||
159 | */ | ||
160 | |||
161 | /** | ||
162 | * struct drm_wmv_surface_create_req | ||
163 | * | ||
164 | * @flags: Surface flags as understood by the host. | ||
165 | * @format: Surface format as understood by the host. | ||
166 | * @mip_levels: Number of mip levels for each face. | ||
167 | * An unused face should have 0 encoded. | ||
168 | * @size_addr: Address of a user-space array of sruct drm_vmw_size | ||
169 | * cast to an uint64_t for 32-64 bit compatibility. | ||
170 | * The size of the array should equal the total number of mipmap levels. | ||
171 | * @shareable: Boolean whether other clients (as identified by file descriptors) | ||
172 | * may reference this surface. | ||
173 | * | ||
174 | * Input data to the DRM_VMW_CREATE_SURFACE Ioctl. | ||
175 | * Output data from the DRM_VMW_REF_SURFACE Ioctl. | ||
176 | */ | ||
177 | |||
178 | struct drm_vmw_surface_create_req { | ||
179 | uint32_t flags; | ||
180 | uint32_t format; | ||
181 | uint32_t mip_levels[DRM_VMW_MAX_SURFACE_FACES]; | ||
182 | uint64_t size_addr; | ||
183 | int32_t shareable; | ||
184 | uint32_t pad64; | ||
185 | }; | ||
186 | |||
187 | /** | ||
188 | * struct drm_wmv_surface_arg | ||
189 | * | ||
190 | * @sid: Surface id of created surface or surface to destroy or reference. | ||
191 | * | ||
192 | * Output data from the DRM_VMW_CREATE_SURFACE Ioctl. | ||
193 | * Input argument to the DRM_VMW_UNREF_SURFACE Ioctl. | ||
194 | * Input argument to the DRM_VMW_REF_SURFACE Ioctl. | ||
195 | */ | ||
196 | |||
197 | struct drm_vmw_surface_arg { | ||
198 | int32_t sid; | ||
199 | uint32_t pad64; | ||
200 | }; | ||
201 | |||
202 | /** | ||
203 | * struct drm_vmw_size ioctl. | ||
204 | * | ||
205 | * @width - mip level width | ||
206 | * @height - mip level height | ||
207 | * @depth - mip level depth | ||
208 | * | ||
209 | * Description of a mip level. | ||
210 | * Input data to the DRM_WMW_CREATE_SURFACE Ioctl. | ||
211 | */ | ||
212 | |||
213 | struct drm_vmw_size { | ||
214 | uint32_t width; | ||
215 | uint32_t height; | ||
216 | uint32_t depth; | ||
217 | uint32_t pad64; | ||
218 | }; | ||
219 | |||
220 | /** | ||
221 | * union drm_vmw_surface_create_arg | ||
222 | * | ||
223 | * @rep: Output data as described above. | ||
224 | * @req: Input data as described above. | ||
225 | * | ||
226 | * Argument to the DRM_VMW_CREATE_SURFACE Ioctl. | ||
227 | */ | ||
228 | |||
229 | union drm_vmw_surface_create_arg { | ||
230 | struct drm_vmw_surface_arg rep; | ||
231 | struct drm_vmw_surface_create_req req; | ||
232 | }; | ||
233 | |||
234 | /*************************************************************************/ | ||
235 | /** | ||
236 | * DRM_VMW_REF_SURFACE - Reference a host surface. | ||
237 | * | ||
238 | * Puts a reference on a host surface with a give sid, as previously | ||
239 | * returned by the DRM_VMW_CREATE_SURFACE ioctl. | ||
240 | * A reference will make sure the surface isn't destroyed while we hold | ||
241 | * it and will allow the calling client to use the surface ID in the command | ||
242 | * stream. | ||
243 | * | ||
244 | * On successful return, the Ioctl returns the surface information given | ||
245 | * in the DRM_VMW_CREATE_SURFACE ioctl. | ||
246 | */ | ||
247 | |||
248 | /** | ||
249 | * union drm_vmw_surface_reference_arg | ||
250 | * | ||
251 | * @rep: Output data as described above. | ||
252 | * @req: Input data as described above. | ||
253 | * | ||
254 | * Argument to the DRM_VMW_REF_SURFACE Ioctl. | ||
255 | */ | ||
256 | |||
257 | union drm_vmw_surface_reference_arg { | ||
258 | struct drm_vmw_surface_create_req rep; | ||
259 | struct drm_vmw_surface_arg req; | ||
260 | }; | ||
261 | |||
262 | /*************************************************************************/ | ||
263 | /** | ||
264 | * DRM_VMW_UNREF_SURFACE - Unreference a host surface. | ||
265 | * | ||
266 | * Clear a reference previously put on a host surface. | ||
267 | * When all references are gone, including the one implicitly placed | ||
268 | * on creation, | ||
269 | * a destroy surface command will be queued for the host. | ||
270 | * Does not wait for completion. | ||
271 | */ | ||
272 | |||
273 | /*************************************************************************/ | ||
274 | /** | ||
275 | * DRM_VMW_EXECBUF | ||
276 | * | ||
277 | * Submit a command buffer for execution on the host, and return a | ||
278 | * fence sequence that when signaled, indicates that the command buffer has | ||
279 | * executed. | ||
280 | */ | ||
281 | |||
282 | /** | ||
283 | * struct drm_vmw_execbuf_arg | ||
284 | * | ||
285 | * @commands: User-space address of a command buffer cast to an uint64_t. | ||
286 | * @command-size: Size in bytes of the command buffer. | ||
287 | * @fence_rep: User-space address of a struct drm_vmw_fence_rep cast to an | ||
288 | * uint64_t. | ||
289 | * | ||
290 | * Argument to the DRM_VMW_EXECBUF Ioctl. | ||
291 | */ | ||
292 | |||
293 | struct drm_vmw_execbuf_arg { | ||
294 | uint64_t commands; | ||
295 | uint32_t command_size; | ||
296 | uint32_t pad64; | ||
297 | uint64_t fence_rep; | ||
298 | }; | ||
299 | |||
300 | /** | ||
301 | * struct drm_vmw_fence_rep | ||
302 | * | ||
303 | * @fence_seq: Fence sequence associated with a command submission. | ||
304 | * @error: This member should've been set to -EFAULT on submission. | ||
305 | * The following actions should be take on completion: | ||
306 | * error == -EFAULT: Fence communication failed. The host is synchronized. | ||
307 | * Use the last fence id read from the FIFO fence register. | ||
308 | * error != 0 && error != -EFAULT: | ||
309 | * Fence submission failed. The host is synchronized. Use the fence_seq member. | ||
310 | * error == 0: All is OK, The host may not be synchronized. | ||
311 | * Use the fence_seq member. | ||
312 | * | ||
313 | * Input / Output data to the DRM_VMW_EXECBUF Ioctl. | ||
314 | */ | ||
315 | |||
316 | struct drm_vmw_fence_rep { | ||
317 | uint64_t fence_seq; | ||
318 | int32_t error; | ||
319 | uint32_t pad64; | ||
320 | }; | ||
321 | |||
322 | /*************************************************************************/ | ||
323 | /** | ||
324 | * DRM_VMW_ALLOC_DMABUF | ||
325 | * | ||
326 | * Allocate a DMA buffer that is visible also to the host. | ||
327 | * NOTE: The buffer is | ||
328 | * identified by a handle and an offset, which are private to the guest, but | ||
329 | * useable in the command stream. The guest kernel may translate these | ||
330 | * and patch up the command stream accordingly. In the future, the offset may | ||
331 | * be zero at all times, or it may disappear from the interface before it is | ||
332 | * fixed. | ||
333 | * | ||
334 | * The DMA buffer may stay user-space mapped in the guest at all times, | ||
335 | * and is thus suitable for sub-allocation. | ||
336 | * | ||
337 | * DMA buffers are mapped using the mmap() syscall on the drm device. | ||
338 | */ | ||
339 | |||
340 | /** | ||
341 | * struct drm_vmw_alloc_dmabuf_req | ||
342 | * | ||
343 | * @size: Required minimum size of the buffer. | ||
344 | * | ||
345 | * Input data to the DRM_VMW_ALLOC_DMABUF Ioctl. | ||
346 | */ | ||
347 | |||
348 | struct drm_vmw_alloc_dmabuf_req { | ||
349 | uint32_t size; | ||
350 | uint32_t pad64; | ||
351 | }; | ||
352 | |||
353 | /** | ||
354 | * struct drm_vmw_dmabuf_rep | ||
355 | * | ||
356 | * @map_handle: Offset to use in the mmap() call used to map the buffer. | ||
357 | * @handle: Handle unique to this buffer. Used for unreferencing. | ||
358 | * @cur_gmr_id: GMR id to use in the command stream when this buffer is | ||
359 | * referenced. See not above. | ||
360 | * @cur_gmr_offset: Offset to use in the command stream when this buffer is | ||
361 | * referenced. See note above. | ||
362 | * | ||
363 | * Output data from the DRM_VMW_ALLOC_DMABUF Ioctl. | ||
364 | */ | ||
365 | |||
366 | struct drm_vmw_dmabuf_rep { | ||
367 | uint64_t map_handle; | ||
368 | uint32_t handle; | ||
369 | uint32_t cur_gmr_id; | ||
370 | uint32_t cur_gmr_offset; | ||
371 | uint32_t pad64; | ||
372 | }; | ||
373 | |||
374 | /** | ||
375 | * union drm_vmw_dmabuf_arg | ||
376 | * | ||
377 | * @req: Input data as described above. | ||
378 | * @rep: Output data as described above. | ||
379 | * | ||
380 | * Argument to the DRM_VMW_ALLOC_DMABUF Ioctl. | ||
381 | */ | ||
382 | |||
383 | union drm_vmw_alloc_dmabuf_arg { | ||
384 | struct drm_vmw_alloc_dmabuf_req req; | ||
385 | struct drm_vmw_dmabuf_rep rep; | ||
386 | }; | ||
387 | |||
388 | /*************************************************************************/ | ||
389 | /** | ||
390 | * DRM_VMW_UNREF_DMABUF - Free a DMA buffer. | ||
391 | * | ||
392 | */ | ||
393 | |||
394 | /** | ||
395 | * struct drm_vmw_unref_dmabuf_arg | ||
396 | * | ||
397 | * @handle: Handle indicating what buffer to free. Obtained from the | ||
398 | * DRM_VMW_ALLOC_DMABUF Ioctl. | ||
399 | * | ||
400 | * Argument to the DRM_VMW_UNREF_DMABUF Ioctl. | ||
401 | */ | ||
402 | |||
403 | struct drm_vmw_unref_dmabuf_arg { | ||
404 | uint32_t handle; | ||
405 | uint32_t pad64; | ||
406 | }; | ||
407 | |||
408 | /*************************************************************************/ | ||
409 | /** | ||
410 | * DRM_VMW_FIFO_DEBUG - Get last FIFO submission. | ||
411 | * | ||
412 | * This IOCTL copies the last FIFO submission directly out of the FIFO buffer. | ||
413 | */ | ||
414 | |||
415 | /** | ||
416 | * struct drm_vmw_fifo_debug_arg | ||
417 | * | ||
418 | * @debug_buffer: User space address of a debug_buffer cast to an uint64_t //In | ||
419 | * @debug_buffer_size: Size in bytes of debug buffer //In | ||
420 | * @used_size: Number of bytes copied to the buffer // Out | ||
421 | * @did_not_fit: Boolean indicating that the fifo contents did not fit. //Out | ||
422 | * | ||
423 | * Argument to the DRM_VMW_FIFO_DEBUG Ioctl. | ||
424 | */ | ||
425 | |||
426 | struct drm_vmw_fifo_debug_arg { | ||
427 | uint64_t debug_buffer; | ||
428 | uint32_t debug_buffer_size; | ||
429 | uint32_t used_size; | ||
430 | int32_t did_not_fit; | ||
431 | uint32_t pad64; | ||
432 | }; | ||
433 | |||
434 | struct drm_vmw_fence_wait_arg { | ||
435 | uint64_t sequence; | ||
436 | uint64_t kernel_cookie; | ||
437 | int32_t cookie_valid; | ||
438 | int32_t pad64; | ||
439 | }; | ||
440 | |||
441 | #endif | ||