diff options
Diffstat (limited to 'amdgpu')
-rw-r--r-- | amdgpu/amdgpu.h | 24 | ||||
-rw-r--r-- | amdgpu/amdgpu_cs.c | 115 | ||||
-rw-r--r-- | amdgpu/amdgpu_internal.h | 2 |
3 files changed, 56 insertions, 85 deletions
diff --git a/amdgpu/amdgpu.h b/amdgpu/amdgpu.h index 11a86eff..d010d99c 100644 --- a/amdgpu/amdgpu.h +++ b/amdgpu/amdgpu.h | |||
@@ -882,7 +882,6 @@ int amdgpu_cs_ctx_create(amdgpu_device_handle dev, | |||
882 | * | 882 | * |
883 | * Destroy GPU execution context when not needed any more | 883 | * Destroy GPU execution context when not needed any more |
884 | * | 884 | * |
885 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() | ||
886 | * \param context - \c [in] GPU Context handle | 885 | * \param context - \c [in] GPU Context handle |
887 | * | 886 | * |
888 | * \return 0 on success\n | 887 | * \return 0 on success\n |
@@ -892,13 +891,11 @@ int amdgpu_cs_ctx_create(amdgpu_device_handle dev, | |||
892 | * \sa amdgpu_cs_ctx_create() | 891 | * \sa amdgpu_cs_ctx_create() |
893 | * | 892 | * |
894 | */ | 893 | */ |
895 | int amdgpu_cs_ctx_free(amdgpu_device_handle dev, | 894 | int amdgpu_cs_ctx_free(amdgpu_context_handle context); |
896 | amdgpu_context_handle context); | ||
897 | 895 | ||
898 | /** | 896 | /** |
899 | * Query reset state for the specific GPU Context | 897 | * Query reset state for the specific GPU Context |
900 | * | 898 | * |
901 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() | ||
902 | * \param context - \c [in] GPU Context handle | 899 | * \param context - \c [in] GPU Context handle |
903 | * \param state - \c [out] Reset state status | 900 | * \param state - \c [out] Reset state status |
904 | * | 901 | * |
@@ -909,8 +906,7 @@ int amdgpu_cs_ctx_free(amdgpu_device_handle dev, | |||
909 | * \sa amdgpu_cs_ctx_create() | 906 | * \sa amdgpu_cs_ctx_create() |
910 | * | 907 | * |
911 | */ | 908 | */ |
912 | int amdgpu_cs_query_reset_state(amdgpu_device_handle dev, | 909 | int amdgpu_cs_query_reset_state(amdgpu_context_handle context, |
913 | amdgpu_context_handle context, | ||
914 | enum amdgpu_cs_ctx_reset_state *state); | 910 | enum amdgpu_cs_ctx_reset_state *state); |
915 | 911 | ||
916 | 912 | ||
@@ -924,7 +920,6 @@ int amdgpu_cs_query_reset_state(amdgpu_device_handle dev, | |||
924 | * Allocate memory to be filled with PM4 packets and be served as the first | 920 | * Allocate memory to be filled with PM4 packets and be served as the first |
925 | * entry point of execution (a.k.a. Indirect Buffer) | 921 | * entry point of execution (a.k.a. Indirect Buffer) |
926 | * | 922 | * |
927 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() | ||
928 | * \param context - \c [in] GPU Context which will use IB | 923 | * \param context - \c [in] GPU Context which will use IB |
929 | * \param ib_size - \c [in] Size of allocation | 924 | * \param ib_size - \c [in] Size of allocation |
930 | * \param output - \c [out] Pointer to structure to get information about | 925 | * \param output - \c [out] Pointer to structure to get information about |
@@ -937,8 +932,7 @@ int amdgpu_cs_query_reset_state(amdgpu_device_handle dev, | |||
937 | * \sa amdgpu_cs_free_ib() | 932 | * \sa amdgpu_cs_free_ib() |
938 | * | 933 | * |
939 | */ | 934 | */ |
940 | int amdgpu_cs_alloc_ib(amdgpu_device_handle dev, | 935 | int amdgpu_cs_alloc_ib(amdgpu_context_handle context, |
941 | amdgpu_context_handle context, | ||
942 | enum amdgpu_cs_ib_size ib_size, | 936 | enum amdgpu_cs_ib_size ib_size, |
943 | struct amdgpu_cs_ib_alloc_result *output); | 937 | struct amdgpu_cs_ib_alloc_result *output); |
944 | 938 | ||
@@ -946,8 +940,6 @@ int amdgpu_cs_alloc_ib(amdgpu_device_handle dev, | |||
946 | * If UMD has allocates IBs which doesn’t need any more than those IBs must | 940 | * If UMD has allocates IBs which doesn’t need any more than those IBs must |
947 | * be explicitly freed | 941 | * be explicitly freed |
948 | * | 942 | * |
949 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() | ||
950 | * \param context - \c [in] GPU Context containing IB | ||
951 | * \param handle - \c [in] IB handle | 943 | * \param handle - \c [in] IB handle |
952 | * | 944 | * |
953 | * \return 0 on success\n | 945 | * \return 0 on success\n |
@@ -960,9 +952,7 @@ int amdgpu_cs_alloc_ib(amdgpu_device_handle dev, | |||
960 | * \sa amdgpu_cs_alloc_ib() | 952 | * \sa amdgpu_cs_alloc_ib() |
961 | * | 953 | * |
962 | */ | 954 | */ |
963 | int amdgpu_cs_free_ib(amdgpu_device_handle dev, | 955 | int amdgpu_cs_free_ib(amdgpu_ib_handle handle); |
964 | amdgpu_context_handle context, | ||
965 | amdgpu_ib_handle handle); | ||
966 | 956 | ||
967 | /** | 957 | /** |
968 | * Send request to submit command buffers to hardware. | 958 | * Send request to submit command buffers to hardware. |
@@ -1011,8 +1001,7 @@ int amdgpu_cs_free_ib(amdgpu_device_handle dev, | |||
1011 | * amdgpu_cs_query_fence_status() | 1001 | * amdgpu_cs_query_fence_status() |
1012 | * | 1002 | * |
1013 | */ | 1003 | */ |
1014 | int amdgpu_cs_submit(amdgpu_device_handle dev, | 1004 | int amdgpu_cs_submit(amdgpu_context_handle context, |
1015 | amdgpu_context_handle context, | ||
1016 | uint64_t flags, | 1005 | uint64_t flags, |
1017 | struct amdgpu_cs_request *ibs_request, | 1006 | struct amdgpu_cs_request *ibs_request, |
1018 | uint32_t number_of_requests, | 1007 | uint32_t number_of_requests, |
@@ -1038,8 +1027,7 @@ int amdgpu_cs_submit(amdgpu_device_handle dev, | |||
1038 | * | 1027 | * |
1039 | * \sa amdgpu_cs_submit() | 1028 | * \sa amdgpu_cs_submit() |
1040 | */ | 1029 | */ |
1041 | int amdgpu_cs_query_fence_status(amdgpu_device_handle dev, | 1030 | int amdgpu_cs_query_fence_status(struct amdgpu_cs_query_fence *fence, |
1042 | struct amdgpu_cs_query_fence *fence, | ||
1043 | uint32_t *expired); | 1031 | uint32_t *expired); |
1044 | 1032 | ||
1045 | 1033 | ||
diff --git a/amdgpu/amdgpu_cs.c b/amdgpu/amdgpu_cs.c index 91e6bcfc..4d5b3ecf 100644 --- a/amdgpu/amdgpu_cs.c +++ b/amdgpu/amdgpu_cs.c | |||
@@ -42,8 +42,7 @@ | |||
42 | * | 42 | * |
43 | * \return 0 on success otherwise POSIX Error code | 43 | * \return 0 on success otherwise POSIX Error code |
44 | */ | 44 | */ |
45 | static int amdgpu_cs_create_ib(amdgpu_device_handle dev, | 45 | static int amdgpu_cs_create_ib(amdgpu_context_handle context, |
46 | amdgpu_context_handle context, | ||
47 | enum amdgpu_cs_ib_size ib_size, | 46 | enum amdgpu_cs_ib_size ib_size, |
48 | amdgpu_ib_handle *ib) | 47 | amdgpu_ib_handle *ib) |
49 | { | 48 | { |
@@ -79,7 +78,7 @@ static int amdgpu_cs_create_ib(amdgpu_device_handle dev, | |||
79 | 78 | ||
80 | alloc_buffer.preferred_heap = AMDGPU_GEM_DOMAIN_GTT; | 79 | alloc_buffer.preferred_heap = AMDGPU_GEM_DOMAIN_GTT; |
81 | 80 | ||
82 | r = amdgpu_bo_alloc(dev, | 81 | r = amdgpu_bo_alloc(context->dev, |
83 | &alloc_buffer, | 82 | &alloc_buffer, |
84 | &info); | 83 | &info); |
85 | if (r) | 84 | if (r) |
@@ -98,6 +97,7 @@ static int amdgpu_cs_create_ib(amdgpu_device_handle dev, | |||
98 | return -ENOMEM; | 97 | return -ENOMEM; |
99 | } | 98 | } |
100 | 99 | ||
100 | new_ib->context = context; | ||
101 | new_ib->buf_handle = info.buf_handle; | 101 | new_ib->buf_handle = info.buf_handle; |
102 | new_ib->cpu = cpu; | 102 | new_ib->cpu = cpu; |
103 | new_ib->virtual_mc_base_address = info.virtual_mc_base_address; | 103 | new_ib->virtual_mc_base_address = info.virtual_mc_base_address; |
@@ -114,10 +114,10 @@ static int amdgpu_cs_create_ib(amdgpu_device_handle dev, | |||
114 | * | 114 | * |
115 | * \return 0 on success otherwise POSIX Error code | 115 | * \return 0 on success otherwise POSIX Error code |
116 | */ | 116 | */ |
117 | static int amdgpu_cs_destroy_ib(amdgpu_device_handle dev, | 117 | static int amdgpu_cs_destroy_ib(amdgpu_ib_handle ib) |
118 | amdgpu_ib_handle ib) | ||
119 | { | 118 | { |
120 | int r; | 119 | int r; |
120 | |||
121 | r = amdgpu_bo_cpu_unmap(ib->buf_handle); | 121 | r = amdgpu_bo_cpu_unmap(ib->buf_handle); |
122 | if (r) | 122 | if (r) |
123 | return r; | 123 | return r; |
@@ -162,8 +162,7 @@ static int amdgpu_cs_init_ib_pool(amdgpu_context_handle context) | |||
162 | * | 162 | * |
163 | * \return 0 on success otherwise POSIX Error code | 163 | * \return 0 on success otherwise POSIX Error code |
164 | */ | 164 | */ |
165 | static int amdgpu_cs_alloc_from_ib_pool(amdgpu_device_handle dev, | 165 | static int amdgpu_cs_alloc_from_ib_pool(amdgpu_context_handle context, |
166 | amdgpu_context_handle context, | ||
167 | enum amdgpu_cs_ib_size ib_size, | 166 | enum amdgpu_cs_ib_size ib_size, |
168 | amdgpu_ib_handle *ib) | 167 | amdgpu_ib_handle *ib) |
169 | { | 168 | { |
@@ -210,21 +209,19 @@ static void amdgpu_cs_free_to_ib_pool(amdgpu_context_handle context, | |||
210 | * | 209 | * |
211 | * \return 0 on success otherwise POSIX Error code | 210 | * \return 0 on success otherwise POSIX Error code |
212 | */ | 211 | */ |
213 | static int amdgpu_cs_destroy_ib_pool(amdgpu_device_handle dev, | 212 | static int amdgpu_cs_destroy_ib_pool(amdgpu_context_handle context) |
214 | amdgpu_context_handle context) | ||
215 | { | 213 | { |
216 | int i; | ||
217 | int r; | ||
218 | struct list_head *head; | 214 | struct list_head *head; |
219 | struct amdgpu_ib *next; | 215 | struct amdgpu_ib *next; |
220 | struct amdgpu_ib *storage; | 216 | struct amdgpu_ib *storage; |
217 | int i, r; | ||
221 | 218 | ||
222 | r = 0; | 219 | r = 0; |
223 | pthread_mutex_lock(&context->pool_mutex); | 220 | pthread_mutex_lock(&context->pool_mutex); |
224 | for (i = 0; i < AMDGPU_CS_IB_SIZE_NUM; i++) { | 221 | for (i = 0; i < AMDGPU_CS_IB_SIZE_NUM; i++) { |
225 | head = &context->ib_pools[i]; | 222 | head = &context->ib_pools[i]; |
226 | LIST_FOR_EACH_ENTRY_SAFE(next, storage, head, list_node) { | 223 | LIST_FOR_EACH_ENTRY_SAFE(next, storage, head, list_node) { |
227 | r = amdgpu_cs_destroy_ib(dev, next); | 224 | r = amdgpu_cs_destroy_ib(next); |
228 | if (r) | 225 | if (r) |
229 | break; | 226 | break; |
230 | } | 227 | } |
@@ -268,8 +265,7 @@ static int amdgpu_cs_init_pendings(amdgpu_context_handle context) | |||
268 | * | 265 | * |
269 | * \return 0 on success otherwise POSIX Error code | 266 | * \return 0 on success otherwise POSIX Error code |
270 | */ | 267 | */ |
271 | static int amdgpu_cs_destroy_pendings(amdgpu_device_handle dev, | 268 | static int amdgpu_cs_destroy_pendings(amdgpu_context_handle context) |
272 | amdgpu_context_handle context) | ||
273 | { | 269 | { |
274 | int ip, inst; | 270 | int ip, inst; |
275 | uint32_t ring; | 271 | uint32_t ring; |
@@ -285,7 +281,7 @@ static int amdgpu_cs_destroy_pendings(amdgpu_device_handle dev, | |||
285 | for (ring = 0; ring < AMDGPU_CS_MAX_RINGS; ring++) { | 281 | for (ring = 0; ring < AMDGPU_CS_MAX_RINGS; ring++) { |
286 | head = &context->pendings[ip][inst][ring]; | 282 | head = &context->pendings[ip][inst][ring]; |
287 | LIST_FOR_EACH_ENTRY_SAFE(next, s, head, list_node) { | 283 | LIST_FOR_EACH_ENTRY_SAFE(next, s, head, list_node) { |
288 | r = amdgpu_cs_destroy_ib(dev, next); | 284 | r = amdgpu_cs_destroy_ib(next); |
289 | if (r) | 285 | if (r) |
290 | break; | 286 | break; |
291 | } | 287 | } |
@@ -293,7 +289,7 @@ static int amdgpu_cs_destroy_pendings(amdgpu_device_handle dev, | |||
293 | 289 | ||
294 | head = &context->freed; | 290 | head = &context->freed; |
295 | LIST_FOR_EACH_ENTRY_SAFE(next, s, head, list_node) { | 291 | LIST_FOR_EACH_ENTRY_SAFE(next, s, head, list_node) { |
296 | r = amdgpu_cs_destroy_ib(dev, next); | 292 | r = amdgpu_cs_destroy_ib(next); |
297 | if (r) | 293 | if (r) |
298 | break; | 294 | break; |
299 | } | 295 | } |
@@ -441,39 +437,35 @@ static void amdgpu_cs_all_pending_gc(amdgpu_context_handle context) | |||
441 | * | 437 | * |
442 | * \return 0 on success otherwise POSIX Error code | 438 | * \return 0 on success otherwise POSIX Error code |
443 | */ | 439 | */ |
444 | static int amdgpu_cs_alloc_ib_local(amdgpu_device_handle dev, | 440 | static int amdgpu_cs_alloc_ib_local(amdgpu_context_handle context, |
445 | amdgpu_context_handle context, | ||
446 | enum amdgpu_cs_ib_size ib_size, | 441 | enum amdgpu_cs_ib_size ib_size, |
447 | amdgpu_ib_handle *ib) | 442 | amdgpu_ib_handle *ib) |
448 | { | 443 | { |
449 | int r; | 444 | int r; |
450 | 445 | ||
451 | r = amdgpu_cs_alloc_from_ib_pool(dev, context, ib_size, ib); | 446 | r = amdgpu_cs_alloc_from_ib_pool(context, ib_size, ib); |
452 | if (!r) | 447 | if (!r) |
453 | return r; | 448 | return r; |
454 | 449 | ||
455 | amdgpu_cs_all_pending_gc(context); | 450 | amdgpu_cs_all_pending_gc(context); |
456 | 451 | ||
457 | /* Retry to allocate from free IB pools after garbage collector. */ | 452 | /* Retry to allocate from free IB pools after garbage collector. */ |
458 | r = amdgpu_cs_alloc_from_ib_pool(dev, context, ib_size, ib); | 453 | r = amdgpu_cs_alloc_from_ib_pool(context, ib_size, ib); |
459 | if (!r) | 454 | if (!r) |
460 | return r; | 455 | return r; |
461 | 456 | ||
462 | /* There is no suitable IB in free pools. Create one. */ | 457 | /* There is no suitable IB in free pools. Create one. */ |
463 | r = amdgpu_cs_create_ib(dev, context, ib_size, ib); | 458 | r = amdgpu_cs_create_ib(context, ib_size, ib); |
464 | return r; | 459 | return r; |
465 | } | 460 | } |
466 | 461 | ||
467 | int amdgpu_cs_alloc_ib(amdgpu_device_handle dev, | 462 | int amdgpu_cs_alloc_ib(amdgpu_context_handle context, |
468 | amdgpu_context_handle context, | ||
469 | enum amdgpu_cs_ib_size ib_size, | 463 | enum amdgpu_cs_ib_size ib_size, |
470 | struct amdgpu_cs_ib_alloc_result *output) | 464 | struct amdgpu_cs_ib_alloc_result *output) |
471 | { | 465 | { |
472 | int r; | 466 | int r; |
473 | amdgpu_ib_handle ib; | 467 | amdgpu_ib_handle ib; |
474 | 468 | ||
475 | if (NULL == dev) | ||
476 | return -EINVAL; | ||
477 | if (NULL == context) | 469 | if (NULL == context) |
478 | return -EINVAL; | 470 | return -EINVAL; |
479 | if (NULL == output) | 471 | if (NULL == output) |
@@ -481,7 +473,7 @@ int amdgpu_cs_alloc_ib(amdgpu_device_handle dev, | |||
481 | if (ib_size >= AMDGPU_CS_IB_SIZE_NUM) | 473 | if (ib_size >= AMDGPU_CS_IB_SIZE_NUM) |
482 | return -EINVAL; | 474 | return -EINVAL; |
483 | 475 | ||
484 | r = amdgpu_cs_alloc_ib_local(dev, context, ib_size, &ib); | 476 | r = amdgpu_cs_alloc_ib_local(context, ib_size, &ib); |
485 | if (!r) { | 477 | if (!r) { |
486 | output->handle = ib; | 478 | output->handle = ib; |
487 | output->cpu = ib->cpu; | 479 | output->cpu = ib->cpu; |
@@ -491,17 +483,14 @@ int amdgpu_cs_alloc_ib(amdgpu_device_handle dev, | |||
491 | return r; | 483 | return r; |
492 | } | 484 | } |
493 | 485 | ||
494 | int amdgpu_cs_free_ib(amdgpu_device_handle dev, | 486 | int amdgpu_cs_free_ib(amdgpu_ib_handle handle) |
495 | amdgpu_context_handle context, | ||
496 | amdgpu_ib_handle handle) | ||
497 | { | 487 | { |
498 | if (NULL == dev) | 488 | amdgpu_context_handle context; |
499 | return -EINVAL; | 489 | |
500 | if (NULL == context) | ||
501 | return -EINVAL; | ||
502 | if (NULL == handle) | 490 | if (NULL == handle) |
503 | return -EINVAL; | 491 | return -EINVAL; |
504 | 492 | ||
493 | context = handle->context; | ||
505 | pthread_mutex_lock(&context->pendings_mutex); | 494 | pthread_mutex_lock(&context->pendings_mutex); |
506 | LIST_ADD(&handle->list_node, &context->freed); | 495 | LIST_ADD(&handle->list_node, &context->freed); |
507 | pthread_mutex_unlock(&context->pendings_mutex); | 496 | pthread_mutex_unlock(&context->pendings_mutex); |
@@ -532,6 +521,8 @@ int amdgpu_cs_ctx_create(amdgpu_device_handle dev, | |||
532 | if (NULL == gpu_context) | 521 | if (NULL == gpu_context) |
533 | return -ENOMEM; | 522 | return -ENOMEM; |
534 | 523 | ||
524 | gpu_context->dev = dev; | ||
525 | |||
535 | r = pthread_mutex_init(&gpu_context->sequence_mutex, NULL); | 526 | r = pthread_mutex_init(&gpu_context->sequence_mutex, NULL); |
536 | if (r) | 527 | if (r) |
537 | goto error_mutex; | 528 | goto error_mutex; |
@@ -544,7 +535,7 @@ int amdgpu_cs_ctx_create(amdgpu_device_handle dev, | |||
544 | if (r) | 535 | if (r) |
545 | goto error_pendings; | 536 | goto error_pendings; |
546 | 537 | ||
547 | r = amdgpu_cs_alloc_ib_local(dev, gpu_context, amdgpu_cs_ib_size_4K, | 538 | r = amdgpu_cs_alloc_ib_local(gpu_context, amdgpu_cs_ib_size_4K, |
548 | &gpu_context->fence_ib); | 539 | &gpu_context->fence_ib); |
549 | if (r) | 540 | if (r) |
550 | goto error_fence_ib; | 541 | goto error_fence_ib; |
@@ -562,13 +553,13 @@ int amdgpu_cs_ctx_create(amdgpu_device_handle dev, | |||
562 | return 0; | 553 | return 0; |
563 | 554 | ||
564 | error_kernel: | 555 | error_kernel: |
565 | amdgpu_cs_free_ib(dev, gpu_context, gpu_context->fence_ib); | 556 | amdgpu_cs_free_ib(gpu_context->fence_ib); |
566 | 557 | ||
567 | error_fence_ib: | 558 | error_fence_ib: |
568 | amdgpu_cs_destroy_pendings(dev, gpu_context); | 559 | amdgpu_cs_destroy_pendings(gpu_context); |
569 | 560 | ||
570 | error_pendings: | 561 | error_pendings: |
571 | amdgpu_cs_destroy_ib_pool(dev, gpu_context); | 562 | amdgpu_cs_destroy_ib_pool(gpu_context); |
572 | 563 | ||
573 | error_pool: | 564 | error_pool: |
574 | pthread_mutex_destroy(&gpu_context->sequence_mutex); | 565 | pthread_mutex_destroy(&gpu_context->sequence_mutex); |
@@ -586,26 +577,23 @@ error_mutex: | |||
586 | * | 577 | * |
587 | * \return 0 on success otherwise POSIX Error code | 578 | * \return 0 on success otherwise POSIX Error code |
588 | */ | 579 | */ |
589 | int amdgpu_cs_ctx_free(amdgpu_device_handle dev, | 580 | int amdgpu_cs_ctx_free(amdgpu_context_handle context) |
590 | amdgpu_context_handle context) | ||
591 | { | 581 | { |
592 | int r; | ||
593 | union drm_amdgpu_ctx args; | 582 | union drm_amdgpu_ctx args; |
583 | int r; | ||
594 | 584 | ||
595 | if (NULL == dev) | ||
596 | return -EINVAL; | ||
597 | if (NULL == context) | 585 | if (NULL == context) |
598 | return -EINVAL; | 586 | return -EINVAL; |
599 | 587 | ||
600 | r = amdgpu_cs_free_ib(dev, context, context->fence_ib); | 588 | r = amdgpu_cs_free_ib(context->fence_ib); |
601 | if (r) | 589 | if (r) |
602 | return r; | 590 | return r; |
603 | 591 | ||
604 | r = amdgpu_cs_destroy_pendings(dev, context); | 592 | r = amdgpu_cs_destroy_pendings(context); |
605 | if (r) | 593 | if (r) |
606 | return r; | 594 | return r; |
607 | 595 | ||
608 | r = amdgpu_cs_destroy_ib_pool(dev, context); | 596 | r = amdgpu_cs_destroy_ib_pool(context); |
609 | if (r) | 597 | if (r) |
610 | return r; | 598 | return r; |
611 | 599 | ||
@@ -615,15 +603,15 @@ int amdgpu_cs_ctx_free(amdgpu_device_handle dev, | |||
615 | memset(&args, 0, sizeof(args)); | 603 | memset(&args, 0, sizeof(args)); |
616 | args.in.op = AMDGPU_CTX_OP_FREE_CTX; | 604 | args.in.op = AMDGPU_CTX_OP_FREE_CTX; |
617 | args.in.ctx_id = context->id; | 605 | args.in.ctx_id = context->id; |
618 | r = drmCommandWriteRead(dev->fd, DRM_AMDGPU_CTX, &args, sizeof(args)); | 606 | r = drmCommandWriteRead(context->dev->fd, DRM_AMDGPU_CTX, |
607 | &args, sizeof(args)); | ||
619 | 608 | ||
620 | free(context); | 609 | free(context); |
621 | 610 | ||
622 | return r; | 611 | return r; |
623 | } | 612 | } |
624 | 613 | ||
625 | static int amdgpu_cs_create_bo_list(amdgpu_device_handle dev, | 614 | static int amdgpu_cs_create_bo_list(amdgpu_context_handle context, |
626 | amdgpu_context_handle context, | ||
627 | struct amdgpu_cs_request *request, | 615 | struct amdgpu_cs_request *request, |
628 | amdgpu_ib_handle fence_ib, | 616 | amdgpu_ib_handle fence_ib, |
629 | uint32_t *handle) | 617 | uint32_t *handle) |
@@ -663,7 +651,7 @@ static int amdgpu_cs_create_bo_list(amdgpu_device_handle dev, | |||
663 | if (fence_ib) | 651 | if (fence_ib) |
664 | list[i].bo_handle = fence_ib->buf_handle->handle; | 652 | list[i].bo_handle = fence_ib->buf_handle->handle; |
665 | 653 | ||
666 | r = drmCommandWriteRead(dev->fd, DRM_AMDGPU_BO_LIST, | 654 | r = drmCommandWriteRead(context->dev->fd, DRM_AMDGPU_BO_LIST, |
667 | &args, sizeof(args)); | 655 | &args, sizeof(args)); |
668 | if (r) | 656 | if (r) |
669 | return r; | 657 | return r; |
@@ -672,7 +660,7 @@ static int amdgpu_cs_create_bo_list(amdgpu_device_handle dev, | |||
672 | return 0; | 660 | return 0; |
673 | } | 661 | } |
674 | 662 | ||
675 | static int amdgpu_cs_free_bo_list(amdgpu_device_handle dev, uint32_t handle) | 663 | static int amdgpu_cs_free_bo_list(amdgpu_context_handle context, uint32_t handle) |
676 | { | 664 | { |
677 | union drm_amdgpu_bo_list args; | 665 | union drm_amdgpu_bo_list args; |
678 | int r; | 666 | int r; |
@@ -684,7 +672,7 @@ static int amdgpu_cs_free_bo_list(amdgpu_device_handle dev, uint32_t handle) | |||
684 | args.in.operation = AMDGPU_BO_LIST_OP_DESTROY; | 672 | args.in.operation = AMDGPU_BO_LIST_OP_DESTROY; |
685 | args.in.list_handle = handle; | 673 | args.in.list_handle = handle; |
686 | 674 | ||
687 | r = drmCommandWriteRead(dev->fd, DRM_AMDGPU_BO_LIST, | 675 | r = drmCommandWriteRead(context->dev->fd, DRM_AMDGPU_BO_LIST, |
688 | &args, sizeof(args)); | 676 | &args, sizeof(args)); |
689 | 677 | ||
690 | return r; | 678 | return r; |
@@ -705,8 +693,7 @@ static uint32_t amdgpu_cs_fence_index(unsigned ip, unsigned ring) | |||
705 | * \return 0 on success otherwise POSIX Error code | 693 | * \return 0 on success otherwise POSIX Error code |
706 | * \sa amdgpu_cs_submit() | 694 | * \sa amdgpu_cs_submit() |
707 | */ | 695 | */ |
708 | static int amdgpu_cs_submit_one(amdgpu_device_handle dev, | 696 | static int amdgpu_cs_submit_one(amdgpu_context_handle context, |
709 | amdgpu_context_handle context, | ||
710 | struct amdgpu_cs_request *ibs_request, | 697 | struct amdgpu_cs_request *ibs_request, |
711 | uint64_t *fence) | 698 | uint64_t *fence) |
712 | { | 699 | { |
@@ -763,7 +750,7 @@ static int amdgpu_cs_submit_one(amdgpu_device_handle dev, | |||
763 | chunk_data[i].ib_data.flags = AMDGPU_IB_FLAG_CE; | 750 | chunk_data[i].ib_data.flags = AMDGPU_IB_FLAG_CE; |
764 | } | 751 | } |
765 | 752 | ||
766 | r = amdgpu_cs_create_bo_list(dev, context, ibs_request, NULL, | 753 | r = amdgpu_cs_create_bo_list(context, ibs_request, NULL, |
767 | &bo_list_handle); | 754 | &bo_list_handle); |
768 | if (r) | 755 | if (r) |
769 | goto error_unlock; | 756 | goto error_unlock; |
@@ -789,7 +776,7 @@ static int amdgpu_cs_submit_one(amdgpu_device_handle dev, | |||
789 | chunk_data[i].fence_data.offset *= sizeof(uint64_t); | 776 | chunk_data[i].fence_data.offset *= sizeof(uint64_t); |
790 | } | 777 | } |
791 | 778 | ||
792 | r = drmCommandWriteRead(dev->fd, DRM_AMDGPU_CS, | 779 | r = drmCommandWriteRead(context->dev->fd, DRM_AMDGPU_CS, |
793 | &cs, sizeof(cs)); | 780 | &cs, sizeof(cs)); |
794 | if (r) | 781 | if (r) |
795 | goto error_unlock; | 782 | goto error_unlock; |
@@ -816,7 +803,7 @@ static int amdgpu_cs_submit_one(amdgpu_device_handle dev, | |||
816 | 803 | ||
817 | pthread_mutex_unlock(&context->sequence_mutex); | 804 | pthread_mutex_unlock(&context->sequence_mutex); |
818 | 805 | ||
819 | r = amdgpu_cs_free_bo_list(dev, bo_list_handle); | 806 | r = amdgpu_cs_free_bo_list(context, bo_list_handle); |
820 | if (r) | 807 | if (r) |
821 | goto error_free; | 808 | goto error_free; |
822 | 809 | ||
@@ -831,18 +818,15 @@ error_free: | |||
831 | return r; | 818 | return r; |
832 | } | 819 | } |
833 | 820 | ||
834 | int amdgpu_cs_submit(amdgpu_device_handle dev, | 821 | int amdgpu_cs_submit(amdgpu_context_handle context, |
835 | amdgpu_context_handle context, | ||
836 | uint64_t flags, | 822 | uint64_t flags, |
837 | struct amdgpu_cs_request *ibs_request, | 823 | struct amdgpu_cs_request *ibs_request, |
838 | uint32_t number_of_requests, | 824 | uint32_t number_of_requests, |
839 | uint64_t *fences) | 825 | uint64_t *fences) |
840 | { | 826 | { |
841 | int r; | ||
842 | uint32_t i; | 827 | uint32_t i; |
828 | int r; | ||
843 | 829 | ||
844 | if (NULL == dev) | ||
845 | return -EINVAL; | ||
846 | if (NULL == context) | 830 | if (NULL == context) |
847 | return -EINVAL; | 831 | return -EINVAL; |
848 | if (NULL == ibs_request) | 832 | if (NULL == ibs_request) |
@@ -852,7 +836,7 @@ int amdgpu_cs_submit(amdgpu_device_handle dev, | |||
852 | 836 | ||
853 | r = 0; | 837 | r = 0; |
854 | for (i = 0; i < number_of_requests; i++) { | 838 | for (i = 0; i < number_of_requests; i++) { |
855 | r = amdgpu_cs_submit_one(dev, context, ibs_request, fences); | 839 | r = amdgpu_cs_submit_one(context, ibs_request, fences); |
856 | if (r) | 840 | if (r) |
857 | break; | 841 | break; |
858 | fences++; | 842 | fences++; |
@@ -915,8 +899,7 @@ static int amdgpu_ioctl_wait_cs(amdgpu_device_handle dev, | |||
915 | return 0; | 899 | return 0; |
916 | } | 900 | } |
917 | 901 | ||
918 | int amdgpu_cs_query_fence_status(amdgpu_device_handle dev, | 902 | int amdgpu_cs_query_fence_status(struct amdgpu_cs_query_fence *fence, |
919 | struct amdgpu_cs_query_fence *fence, | ||
920 | uint32_t *expired) | 903 | uint32_t *expired) |
921 | { | 904 | { |
922 | amdgpu_context_handle context; | 905 | amdgpu_context_handle context; |
@@ -927,8 +910,6 @@ int amdgpu_cs_query_fence_status(amdgpu_device_handle dev, | |||
927 | bool busy = true; | 910 | bool busy = true; |
928 | int r; | 911 | int r; |
929 | 912 | ||
930 | if (NULL == dev) | ||
931 | return -EINVAL; | ||
932 | if (NULL == fence) | 913 | if (NULL == fence) |
933 | return -EINVAL; | 914 | return -EINVAL; |
934 | if (NULL == expired) | 915 | if (NULL == expired) |
@@ -969,7 +950,7 @@ int amdgpu_cs_query_fence_status(amdgpu_device_handle dev, | |||
969 | 950 | ||
970 | pthread_mutex_unlock(&context->sequence_mutex); | 951 | pthread_mutex_unlock(&context->sequence_mutex); |
971 | 952 | ||
972 | r = amdgpu_ioctl_wait_cs(dev, ip_type, ip_instance, ring, | 953 | r = amdgpu_ioctl_wait_cs(context->dev, ip_type, ip_instance, ring, |
973 | fence->fence, fence->timeout_ns, &busy); | 954 | fence->fence, fence->timeout_ns, &busy); |
974 | if (!r && !busy) { | 955 | if (!r && !busy) { |
975 | *expired = true; | 956 | *expired = true; |
diff --git a/amdgpu/amdgpu_internal.h b/amdgpu/amdgpu_internal.h index 19bc7e18..c91452ef 100644 --- a/amdgpu/amdgpu_internal.h +++ b/amdgpu/amdgpu_internal.h | |||
@@ -94,6 +94,7 @@ struct amdgpu_bo { | |||
94 | * sequence_mutex -> pendings_mutex -> pool_mutex. | 94 | * sequence_mutex -> pendings_mutex -> pool_mutex. |
95 | */ | 95 | */ |
96 | struct amdgpu_context { | 96 | struct amdgpu_context { |
97 | struct amdgpu_device *dev; | ||
97 | /** Mutex for accessing fences and to maintain command submissions | 98 | /** Mutex for accessing fences and to maintain command submissions |
98 | and pending lists in good sequence. */ | 99 | and pending lists in good sequence. */ |
99 | pthread_mutex_t sequence_mutex; | 100 | pthread_mutex_t sequence_mutex; |
@@ -116,6 +117,7 @@ struct amdgpu_context { | |||
116 | }; | 117 | }; |
117 | 118 | ||
118 | struct amdgpu_ib { | 119 | struct amdgpu_ib { |
120 | amdgpu_context_handle context; | ||
119 | struct list_head list_node; | 121 | struct list_head list_node; |
120 | amdgpu_bo_handle buf_handle; | 122 | amdgpu_bo_handle buf_handle; |
121 | void *cpu; | 123 | void *cpu; |