diff options
Diffstat (limited to 'freedreno/freedreno-symbol-check')
-rwxr-xr-x | freedreno/freedreno-symbol-check | 5 |
1 files changed, 4 insertions, 1 deletions
diff --git a/freedreno/freedreno-symbol-check b/freedreno/freedreno-symbol-check index 42f2c439..3b119528 100755 --- a/freedreno/freedreno-symbol-check +++ b/freedreno/freedreno-symbol-check | |||
@@ -3,7 +3,7 @@ | |||
3 | # The following symbols (past the first five) are taken from the public headers. | 3 | # The following symbols (past the first five) are taken from the public headers. |
4 | # A list of the latter should be available Makefile.sources/LIBDRM_FREEDRENO_H_FILES | 4 | # A list of the latter should be available Makefile.sources/LIBDRM_FREEDRENO_H_FILES |
5 | 5 | ||
6 | FUNCS=$(nm -D --format=bsd --defined-only ${1-.libs/libdrm_freedreno.so} | awk '{print $3}'| while read func; do | 6 | FUNCS=$($NM -D --format=bsd --defined-only ${1-.libs/libdrm_freedreno.so} | awk '{print $3}'| while read func; do |
7 | ( grep -q "^$func$" || echo $func ) <<EOF | 7 | ( grep -q "^$func$" || echo $func ) <<EOF |
8 | __bss_start | 8 | __bss_start |
9 | _edata | 9 | _edata |
@@ -18,10 +18,12 @@ fd_bo_from_dmabuf | |||
18 | fd_bo_from_fbdev | 18 | fd_bo_from_fbdev |
19 | fd_bo_from_handle | 19 | fd_bo_from_handle |
20 | fd_bo_from_name | 20 | fd_bo_from_name |
21 | fd_bo_get_iova | ||
21 | fd_bo_get_name | 22 | fd_bo_get_name |
22 | fd_bo_handle | 23 | fd_bo_handle |
23 | fd_bo_map | 24 | fd_bo_map |
24 | fd_bo_new | 25 | fd_bo_new |
26 | fd_bo_put_iova | ||
25 | fd_bo_ref | 27 | fd_bo_ref |
26 | fd_bo_size | 28 | fd_bo_size |
27 | fd_device_del | 29 | fd_device_del |
@@ -33,6 +35,7 @@ fd_device_version | |||
33 | fd_pipe_del | 35 | fd_pipe_del |
34 | fd_pipe_get_param | 36 | fd_pipe_get_param |
35 | fd_pipe_new | 37 | fd_pipe_new |
38 | fd_pipe_new2 | ||
36 | fd_pipe_wait | 39 | fd_pipe_wait |
37 | fd_pipe_wait_timeout | 40 | fd_pipe_wait_timeout |
38 | fd_ringbuffer_cmd_count | 41 | fd_ringbuffer_cmd_count |