diff options
Diffstat (limited to 'include/drm/i915_drm.h')
-rw-r--r-- | include/drm/i915_drm.h | 315 |
1 files changed, 300 insertions, 15 deletions
diff --git a/include/drm/i915_drm.h b/include/drm/i915_drm.h index 0e51d421..5ebe0462 100644 --- a/include/drm/i915_drm.h +++ b/include/drm/i915_drm.h | |||
@@ -29,6 +29,10 @@ | |||
29 | 29 | ||
30 | #include "drm.h" | 30 | #include "drm.h" |
31 | 31 | ||
32 | #if defined(__cplusplus) | ||
33 | extern "C" { | ||
34 | #endif | ||
35 | |||
32 | /* Please note that modifications to all structs defined here are | 36 | /* Please note that modifications to all structs defined here are |
33 | * subject to backwards-compatibility constraints. | 37 | * subject to backwards-compatibility constraints. |
34 | */ | 38 | */ |
@@ -58,6 +62,30 @@ | |||
58 | #define I915_ERROR_UEVENT "ERROR" | 62 | #define I915_ERROR_UEVENT "ERROR" |
59 | #define I915_RESET_UEVENT "RESET" | 63 | #define I915_RESET_UEVENT "RESET" |
60 | 64 | ||
65 | /* | ||
66 | * MOCS indexes used for GPU surfaces, defining the cacheability of the | ||
67 | * surface data and the coherency for this data wrt. CPU vs. GPU accesses. | ||
68 | */ | ||
69 | enum i915_mocs_table_index { | ||
70 | /* | ||
71 | * Not cached anywhere, coherency between CPU and GPU accesses is | ||
72 | * guaranteed. | ||
73 | */ | ||
74 | I915_MOCS_UNCACHED, | ||
75 | /* | ||
76 | * Cacheability and coherency controlled by the kernel automatically | ||
77 | * based on the DRM_I915_GEM_SET_CACHING IOCTL setting and the current | ||
78 | * usage of the surface (used for display scanout or not). | ||
79 | */ | ||
80 | I915_MOCS_PTE, | ||
81 | /* | ||
82 | * Cached in all GPU caches available on the platform. | ||
83 | * Coherency between CPU and GPU accesses to the surface is not | ||
84 | * guaranteed without extra synchronization. | ||
85 | */ | ||
86 | I915_MOCS_CACHED, | ||
87 | }; | ||
88 | |||
61 | /* Each region is a minimum of 16k, and there are at most 255 of them. | 89 | /* Each region is a minimum of 16k, and there are at most 255 of them. |
62 | */ | 90 | */ |
63 | #define I915_NR_TEX_REGIONS 255 /* table size 2k - maximum due to use | 91 | #define I915_NR_TEX_REGIONS 255 /* table size 2k - maximum due to use |
@@ -218,6 +246,7 @@ typedef struct _drm_i915_sarea { | |||
218 | #define DRM_I915_OVERLAY_PUT_IMAGE 0x27 | 246 | #define DRM_I915_OVERLAY_PUT_IMAGE 0x27 |
219 | #define DRM_I915_OVERLAY_ATTRS 0x28 | 247 | #define DRM_I915_OVERLAY_ATTRS 0x28 |
220 | #define DRM_I915_GEM_EXECBUFFER2 0x29 | 248 | #define DRM_I915_GEM_EXECBUFFER2 0x29 |
249 | #define DRM_I915_GEM_EXECBUFFER2_WR DRM_I915_GEM_EXECBUFFER2 | ||
221 | #define DRM_I915_GET_SPRITE_COLORKEY 0x2a | 250 | #define DRM_I915_GET_SPRITE_COLORKEY 0x2a |
222 | #define DRM_I915_SET_SPRITE_COLORKEY 0x2b | 251 | #define DRM_I915_SET_SPRITE_COLORKEY 0x2b |
223 | #define DRM_I915_GEM_WAIT 0x2c | 252 | #define DRM_I915_GEM_WAIT 0x2c |
@@ -230,6 +259,7 @@ typedef struct _drm_i915_sarea { | |||
230 | #define DRM_I915_GEM_USERPTR 0x33 | 259 | #define DRM_I915_GEM_USERPTR 0x33 |
231 | #define DRM_I915_GEM_CONTEXT_GETPARAM 0x34 | 260 | #define DRM_I915_GEM_CONTEXT_GETPARAM 0x34 |
232 | #define DRM_I915_GEM_CONTEXT_SETPARAM 0x35 | 261 | #define DRM_I915_GEM_CONTEXT_SETPARAM 0x35 |
262 | #define DRM_I915_PERF_OPEN 0x36 | ||
233 | 263 | ||
234 | #define DRM_IOCTL_I915_INIT DRM_IOW( DRM_COMMAND_BASE + DRM_I915_INIT, drm_i915_init_t) | 264 | #define DRM_IOCTL_I915_INIT DRM_IOW( DRM_COMMAND_BASE + DRM_I915_INIT, drm_i915_init_t) |
235 | #define DRM_IOCTL_I915_FLUSH DRM_IO ( DRM_COMMAND_BASE + DRM_I915_FLUSH) | 265 | #define DRM_IOCTL_I915_FLUSH DRM_IO ( DRM_COMMAND_BASE + DRM_I915_FLUSH) |
@@ -251,6 +281,7 @@ typedef struct _drm_i915_sarea { | |||
251 | #define DRM_IOCTL_I915_GEM_INIT DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_INIT, struct drm_i915_gem_init) | 281 | #define DRM_IOCTL_I915_GEM_INIT DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_INIT, struct drm_i915_gem_init) |
252 | #define DRM_IOCTL_I915_GEM_EXECBUFFER DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_EXECBUFFER, struct drm_i915_gem_execbuffer) | 282 | #define DRM_IOCTL_I915_GEM_EXECBUFFER DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_EXECBUFFER, struct drm_i915_gem_execbuffer) |
253 | #define DRM_IOCTL_I915_GEM_EXECBUFFER2 DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_EXECBUFFER2, struct drm_i915_gem_execbuffer2) | 283 | #define DRM_IOCTL_I915_GEM_EXECBUFFER2 DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_EXECBUFFER2, struct drm_i915_gem_execbuffer2) |
284 | #define DRM_IOCTL_I915_GEM_EXECBUFFER2_WR DRM_IOWR(DRM_COMMAND_BASE + DRM_I915_GEM_EXECBUFFER2_WR, struct drm_i915_gem_execbuffer2) | ||
254 | #define DRM_IOCTL_I915_GEM_PIN DRM_IOWR(DRM_COMMAND_BASE + DRM_I915_GEM_PIN, struct drm_i915_gem_pin) | 285 | #define DRM_IOCTL_I915_GEM_PIN DRM_IOWR(DRM_COMMAND_BASE + DRM_I915_GEM_PIN, struct drm_i915_gem_pin) |
255 | #define DRM_IOCTL_I915_GEM_UNPIN DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_UNPIN, struct drm_i915_gem_unpin) | 286 | #define DRM_IOCTL_I915_GEM_UNPIN DRM_IOW(DRM_COMMAND_BASE + DRM_I915_GEM_UNPIN, struct drm_i915_gem_unpin) |
256 | #define DRM_IOCTL_I915_GEM_BUSY DRM_IOWR(DRM_COMMAND_BASE + DRM_I915_GEM_BUSY, struct drm_i915_gem_busy) | 287 | #define DRM_IOCTL_I915_GEM_BUSY DRM_IOWR(DRM_COMMAND_BASE + DRM_I915_GEM_BUSY, struct drm_i915_gem_busy) |
@@ -283,6 +314,7 @@ typedef struct _drm_i915_sarea { | |||
283 | #define DRM_IOCTL_I915_GEM_USERPTR DRM_IOWR (DRM_COMMAND_BASE + DRM_I915_GEM_USERPTR, struct drm_i915_gem_userptr) | 314 | #define DRM_IOCTL_I915_GEM_USERPTR DRM_IOWR (DRM_COMMAND_BASE + DRM_I915_GEM_USERPTR, struct drm_i915_gem_userptr) |
284 | #define DRM_IOCTL_I915_GEM_CONTEXT_GETPARAM DRM_IOWR (DRM_COMMAND_BASE + DRM_I915_GEM_CONTEXT_GETPARAM, struct drm_i915_gem_context_param) | 315 | #define DRM_IOCTL_I915_GEM_CONTEXT_GETPARAM DRM_IOWR (DRM_COMMAND_BASE + DRM_I915_GEM_CONTEXT_GETPARAM, struct drm_i915_gem_context_param) |
285 | #define DRM_IOCTL_I915_GEM_CONTEXT_SETPARAM DRM_IOWR (DRM_COMMAND_BASE + DRM_I915_GEM_CONTEXT_SETPARAM, struct drm_i915_gem_context_param) | 316 | #define DRM_IOCTL_I915_GEM_CONTEXT_SETPARAM DRM_IOWR (DRM_COMMAND_BASE + DRM_I915_GEM_CONTEXT_SETPARAM, struct drm_i915_gem_context_param) |
317 | #define DRM_IOCTL_I915_PERF_OPEN DRM_IOW(DRM_COMMAND_BASE + DRM_I915_PERF_OPEN, struct drm_i915_perf_open_param) | ||
286 | 318 | ||
287 | /* Allow drivers to submit batchbuffers directly to hardware, relying | 319 | /* Allow drivers to submit batchbuffers directly to hardware, relying |
288 | * on the security mechanisms provided by hardware. | 320 | * on the security mechanisms provided by hardware. |
@@ -357,6 +389,28 @@ typedef struct drm_i915_irq_wait { | |||
357 | #define I915_PARAM_HAS_GPU_RESET 35 | 389 | #define I915_PARAM_HAS_GPU_RESET 35 |
358 | #define I915_PARAM_HAS_RESOURCE_STREAMER 36 | 390 | #define I915_PARAM_HAS_RESOURCE_STREAMER 36 |
359 | #define I915_PARAM_HAS_EXEC_SOFTPIN 37 | 391 | #define I915_PARAM_HAS_EXEC_SOFTPIN 37 |
392 | #define I915_PARAM_HAS_POOLED_EU 38 | ||
393 | #define I915_PARAM_MIN_EU_IN_POOL 39 | ||
394 | #define I915_PARAM_MMAP_GTT_VERSION 40 | ||
395 | |||
396 | /* Query whether DRM_I915_GEM_EXECBUFFER2 supports user defined execution | ||
397 | * priorities and the driver will attempt to execute batches in priority order. | ||
398 | */ | ||
399 | #define I915_PARAM_HAS_SCHEDULER 41 | ||
400 | #define I915_PARAM_HUC_STATUS 42 | ||
401 | |||
402 | /* Query whether DRM_I915_GEM_EXECBUFFER2 supports the ability to opt-out of | ||
403 | * synchronisation with implicit fencing on individual objects. | ||
404 | * See EXEC_OBJECT_ASYNC. | ||
405 | */ | ||
406 | #define I915_PARAM_HAS_EXEC_ASYNC 43 | ||
407 | |||
408 | /* Query whether DRM_I915_GEM_EXECBUFFER2 supports explicit fence support - | ||
409 | * both being able to pass in a sync_file fd to wait upon before executing, | ||
410 | * and being able to return a new sync_file fd that is signaled when the | ||
411 | * current request is complete. See I915_EXEC_FENCE_IN and I915_EXEC_FENCE_OUT. | ||
412 | */ | ||
413 | #define I915_PARAM_HAS_EXEC_FENCE 44 | ||
360 | 414 | ||
361 | typedef struct drm_i915_getparam { | 415 | typedef struct drm_i915_getparam { |
362 | __s32 param; | 416 | __s32 param; |
@@ -692,15 +746,41 @@ struct drm_i915_gem_exec_object2 { | |||
692 | */ | 746 | */ |
693 | __u64 offset; | 747 | __u64 offset; |
694 | 748 | ||
695 | #define EXEC_OBJECT_NEEDS_FENCE (1<<0) | 749 | #define EXEC_OBJECT_NEEDS_FENCE (1<<0) |
696 | #define EXEC_OBJECT_NEEDS_GTT (1<<1) | 750 | #define EXEC_OBJECT_NEEDS_GTT (1<<1) |
697 | #define EXEC_OBJECT_WRITE (1<<2) | 751 | #define EXEC_OBJECT_WRITE (1<<2) |
698 | #define EXEC_OBJECT_SUPPORTS_48B_ADDRESS (1<<3) | 752 | #define EXEC_OBJECT_SUPPORTS_48B_ADDRESS (1<<3) |
699 | #define EXEC_OBJECT_PINNED (1<<4) | 753 | #define EXEC_OBJECT_PINNED (1<<4) |
700 | #define __EXEC_OBJECT_UNKNOWN_FLAGS -(EXEC_OBJECT_PINNED<<1) | 754 | #define EXEC_OBJECT_PAD_TO_SIZE (1<<5) |
755 | /* The kernel implicitly tracks GPU activity on all GEM objects, and | ||
756 | * synchronises operations with outstanding rendering. This includes | ||
757 | * rendering on other devices if exported via dma-buf. However, sometimes | ||
758 | * this tracking is too coarse and the user knows better. For example, | ||
759 | * if the object is split into non-overlapping ranges shared between different | ||
760 | * clients or engines (i.e. suballocating objects), the implicit tracking | ||
761 | * by kernel assumes that each operation affects the whole object rather | ||
762 | * than an individual range, causing needless synchronisation between clients. | ||
763 | * The kernel will also forgo any CPU cache flushes prior to rendering from | ||
764 | * the object as the client is expected to be also handling such domain | ||
765 | * tracking. | ||
766 | * | ||
767 | * The kernel maintains the implicit tracking in order to manage resources | ||
768 | * used by the GPU - this flag only disables the synchronisation prior to | ||
769 | * rendering with this object in this execbuf. | ||
770 | * | ||
771 | * Opting out of implicit synhronisation requires the user to do its own | ||
772 | * explicit tracking to avoid rendering corruption. See, for example, | ||
773 | * I915_PARAM_HAS_EXEC_FENCE to order execbufs and execute them asynchronously. | ||
774 | */ | ||
775 | #define EXEC_OBJECT_ASYNC (1<<6) | ||
776 | /* All remaining bits are MBZ and RESERVED FOR FUTURE USE */ | ||
777 | #define __EXEC_OBJECT_UNKNOWN_FLAGS -(EXEC_OBJECT_ASYNC<<1) | ||
701 | __u64 flags; | 778 | __u64 flags; |
702 | 779 | ||
703 | __u64 rsvd1; | 780 | union { |
781 | __u64 rsvd1; | ||
782 | __u64 pad_to_size; | ||
783 | }; | ||
704 | __u64 rsvd2; | 784 | __u64 rsvd2; |
705 | }; | 785 | }; |
706 | 786 | ||
@@ -772,17 +852,44 @@ struct drm_i915_gem_execbuffer2 { | |||
772 | #define I915_EXEC_HANDLE_LUT (1<<12) | 852 | #define I915_EXEC_HANDLE_LUT (1<<12) |
773 | 853 | ||
774 | /** Used for switching BSD rings on the platforms with two BSD rings */ | 854 | /** Used for switching BSD rings on the platforms with two BSD rings */ |
775 | #define I915_EXEC_BSD_MASK (3<<13) | 855 | #define I915_EXEC_BSD_SHIFT (13) |
776 | #define I915_EXEC_BSD_DEFAULT (0<<13) /* default ping-pong mode */ | 856 | #define I915_EXEC_BSD_MASK (3 << I915_EXEC_BSD_SHIFT) |
777 | #define I915_EXEC_BSD_RING1 (1<<13) | 857 | /* default ping-pong mode */ |
778 | #define I915_EXEC_BSD_RING2 (2<<13) | 858 | #define I915_EXEC_BSD_DEFAULT (0 << I915_EXEC_BSD_SHIFT) |
859 | #define I915_EXEC_BSD_RING1 (1 << I915_EXEC_BSD_SHIFT) | ||
860 | #define I915_EXEC_BSD_RING2 (2 << I915_EXEC_BSD_SHIFT) | ||
779 | 861 | ||
780 | /** Tell the kernel that the batchbuffer is processed by | 862 | /** Tell the kernel that the batchbuffer is processed by |
781 | * the resource streamer. | 863 | * the resource streamer. |
782 | */ | 864 | */ |
783 | #define I915_EXEC_RESOURCE_STREAMER (1<<15) | 865 | #define I915_EXEC_RESOURCE_STREAMER (1<<15) |
784 | 866 | ||
785 | #define __I915_EXEC_UNKNOWN_FLAGS -(I915_EXEC_RESOURCE_STREAMER<<1) | 867 | /* Setting I915_EXEC_FENCE_IN implies that lower_32_bits(rsvd2) represent |
868 | * a sync_file fd to wait upon (in a nonblocking manner) prior to executing | ||
869 | * the batch. | ||
870 | * | ||
871 | * Returns -EINVAL if the sync_file fd cannot be found. | ||
872 | */ | ||
873 | #define I915_EXEC_FENCE_IN (1<<16) | ||
874 | |||
875 | /* Setting I915_EXEC_FENCE_OUT causes the ioctl to return a sync_file fd | ||
876 | * in the upper_32_bits(rsvd2) upon success. Ownership of the fd is given | ||
877 | * to the caller, and it should be close() after use. (The fd is a regular | ||
878 | * file descriptor and will be cleaned up on process termination. It holds | ||
879 | * a reference to the request, but nothing else.) | ||
880 | * | ||
881 | * The sync_file fd can be combined with other sync_file and passed either | ||
882 | * to execbuf using I915_EXEC_FENCE_IN, to atomic KMS ioctls (so that a flip | ||
883 | * will only occur after this request completes), or to other devices. | ||
884 | * | ||
885 | * Using I915_EXEC_FENCE_OUT requires use of | ||
886 | * DRM_IOCTL_I915_GEM_EXECBUFFER2_WR ioctl so that the result is written | ||
887 | * back to userspace. Failure to do so will cause the out-fence to always | ||
888 | * be reported as zero, and the real fence fd to be leaked. | ||
889 | */ | ||
890 | #define I915_EXEC_FENCE_OUT (1<<17) | ||
891 | |||
892 | #define __I915_EXEC_UNKNOWN_FLAGS (-(I915_EXEC_FENCE_OUT<<1)) | ||
786 | 893 | ||
787 | #define I915_EXEC_CONTEXT_ID_MASK (0xffffffff) | 894 | #define I915_EXEC_CONTEXT_ID_MASK (0xffffffff) |
788 | #define i915_execbuffer2_set_context_id(eb2, context) \ | 895 | #define i915_execbuffer2_set_context_id(eb2, context) \ |
@@ -812,10 +919,49 @@ struct drm_i915_gem_busy { | |||
812 | /** Handle of the buffer to check for busy */ | 919 | /** Handle of the buffer to check for busy */ |
813 | __u32 handle; | 920 | __u32 handle; |
814 | 921 | ||
815 | /** Return busy status (1 if busy, 0 if idle). | 922 | /** Return busy status |
816 | * The high word is used to indicate on which rings the object | 923 | * |
817 | * currently resides: | 924 | * A return of 0 implies that the object is idle (after |
818 | * 16:31 - busy (r or r/w) rings (16 render, 17 bsd, 18 blt, etc) | 925 | * having flushed any pending activity), and a non-zero return that |
926 | * the object is still in-flight on the GPU. (The GPU has not yet | ||
927 | * signaled completion for all pending requests that reference the | ||
928 | * object.) An object is guaranteed to become idle eventually (so | ||
929 | * long as no new GPU commands are executed upon it). Due to the | ||
930 | * asynchronous nature of the hardware, an object reported | ||
931 | * as busy may become idle before the ioctl is completed. | ||
932 | * | ||
933 | * Furthermore, if the object is busy, which engine is busy is only | ||
934 | * provided as a guide. There are race conditions which prevent the | ||
935 | * report of which engines are busy from being always accurate. | ||
936 | * However, the converse is not true. If the object is idle, the | ||
937 | * result of the ioctl, that all engines are idle, is accurate. | ||
938 | * | ||
939 | * The returned dword is split into two fields to indicate both | ||
940 | * the engines on which the object is being read, and the | ||
941 | * engine on which it is currently being written (if any). | ||
942 | * | ||
943 | * The low word (bits 0:15) indicate if the object is being written | ||
944 | * to by any engine (there can only be one, as the GEM implicit | ||
945 | * synchronisation rules force writes to be serialised). Only the | ||
946 | * engine for the last write is reported. | ||
947 | * | ||
948 | * The high word (bits 16:31) are a bitmask of which engines are | ||
949 | * currently reading from the object. Multiple engines may be | ||
950 | * reading from the object simultaneously. | ||
951 | * | ||
952 | * The value of each engine is the same as specified in the | ||
953 | * EXECBUFFER2 ioctl, i.e. I915_EXEC_RENDER, I915_EXEC_BSD etc. | ||
954 | * Note I915_EXEC_DEFAULT is a symbolic value and is mapped to | ||
955 | * the I915_EXEC_RENDER engine for execution, and so it is never | ||
956 | * reported as active itself. Some hardware may have parallel | ||
957 | * execution engines, e.g. multiple media engines, which are | ||
958 | * mapped to the same identifier in the EXECBUFFER2 ioctl and | ||
959 | * so are not separately reported for busyness. | ||
960 | * | ||
961 | * Caveat emptor: | ||
962 | * Only the boolean result of this query is reliable; that is whether | ||
963 | * the object is idle or busy. The report of which engines are busy | ||
964 | * should be only used as a heuristic. | ||
819 | */ | 965 | */ |
820 | __u32 busy; | 966 | __u32 busy; |
821 | }; | 967 | }; |
@@ -864,6 +1010,7 @@ struct drm_i915_gem_caching { | |||
864 | #define I915_TILING_NONE 0 | 1010 | #define I915_TILING_NONE 0 |
865 | #define I915_TILING_X 1 | 1011 | #define I915_TILING_X 1 |
866 | #define I915_TILING_Y 2 | 1012 | #define I915_TILING_Y 2 |
1013 | #define I915_TILING_LAST I915_TILING_Y | ||
867 | 1014 | ||
868 | #define I915_BIT_6_SWIZZLE_NONE 0 | 1015 | #define I915_BIT_6_SWIZZLE_NONE 0 |
869 | #define I915_BIT_6_SWIZZLE_9 1 | 1016 | #define I915_BIT_6_SWIZZLE_9 1 |
@@ -1140,7 +1287,145 @@ struct drm_i915_gem_context_param { | |||
1140 | #define I915_CONTEXT_PARAM_BAN_PERIOD 0x1 | 1287 | #define I915_CONTEXT_PARAM_BAN_PERIOD 0x1 |
1141 | #define I915_CONTEXT_PARAM_NO_ZEROMAP 0x2 | 1288 | #define I915_CONTEXT_PARAM_NO_ZEROMAP 0x2 |
1142 | #define I915_CONTEXT_PARAM_GTT_SIZE 0x3 | 1289 | #define I915_CONTEXT_PARAM_GTT_SIZE 0x3 |
1290 | #define I915_CONTEXT_PARAM_NO_ERROR_CAPTURE 0x4 | ||
1291 | #define I915_CONTEXT_PARAM_BANNABLE 0x5 | ||
1143 | __u64 value; | 1292 | __u64 value; |
1144 | }; | 1293 | }; |
1145 | 1294 | ||
1295 | enum drm_i915_oa_format { | ||
1296 | I915_OA_FORMAT_A13 = 1, | ||
1297 | I915_OA_FORMAT_A29, | ||
1298 | I915_OA_FORMAT_A13_B8_C8, | ||
1299 | I915_OA_FORMAT_B4_C8, | ||
1300 | I915_OA_FORMAT_A45_B8_C8, | ||
1301 | I915_OA_FORMAT_B4_C8_A16, | ||
1302 | I915_OA_FORMAT_C4_B8, | ||
1303 | |||
1304 | I915_OA_FORMAT_MAX /* non-ABI */ | ||
1305 | }; | ||
1306 | |||
1307 | enum drm_i915_perf_property_id { | ||
1308 | /** | ||
1309 | * Open the stream for a specific context handle (as used with | ||
1310 | * execbuffer2). A stream opened for a specific context this way | ||
1311 | * won't typically require root privileges. | ||
1312 | */ | ||
1313 | DRM_I915_PERF_PROP_CTX_HANDLE = 1, | ||
1314 | |||
1315 | /** | ||
1316 | * A value of 1 requests the inclusion of raw OA unit reports as | ||
1317 | * part of stream samples. | ||
1318 | */ | ||
1319 | DRM_I915_PERF_PROP_SAMPLE_OA, | ||
1320 | |||
1321 | /** | ||
1322 | * The value specifies which set of OA unit metrics should be | ||
1323 | * be configured, defining the contents of any OA unit reports. | ||
1324 | */ | ||
1325 | DRM_I915_PERF_PROP_OA_METRICS_SET, | ||
1326 | |||
1327 | /** | ||
1328 | * The value specifies the size and layout of OA unit reports. | ||
1329 | */ | ||
1330 | DRM_I915_PERF_PROP_OA_FORMAT, | ||
1331 | |||
1332 | /** | ||
1333 | * Specifying this property implicitly requests periodic OA unit | ||
1334 | * sampling and (at least on Haswell) the sampling frequency is derived | ||
1335 | * from this exponent as follows: | ||
1336 | * | ||
1337 | * 80ns * 2^(period_exponent + 1) | ||
1338 | */ | ||
1339 | DRM_I915_PERF_PROP_OA_EXPONENT, | ||
1340 | |||
1341 | DRM_I915_PERF_PROP_MAX /* non-ABI */ | ||
1342 | }; | ||
1343 | |||
1344 | struct drm_i915_perf_open_param { | ||
1345 | __u32 flags; | ||
1346 | #define I915_PERF_FLAG_FD_CLOEXEC (1<<0) | ||
1347 | #define I915_PERF_FLAG_FD_NONBLOCK (1<<1) | ||
1348 | #define I915_PERF_FLAG_DISABLED (1<<2) | ||
1349 | |||
1350 | /** The number of u64 (id, value) pairs */ | ||
1351 | __u32 num_properties; | ||
1352 | |||
1353 | /** | ||
1354 | * Pointer to array of u64 (id, value) pairs configuring the stream | ||
1355 | * to open. | ||
1356 | */ | ||
1357 | __u64 properties_ptr; | ||
1358 | }; | ||
1359 | |||
1360 | /** | ||
1361 | * Enable data capture for a stream that was either opened in a disabled state | ||
1362 | * via I915_PERF_FLAG_DISABLED or was later disabled via | ||
1363 | * I915_PERF_IOCTL_DISABLE. | ||
1364 | * | ||
1365 | * It is intended to be cheaper to disable and enable a stream than it may be | ||
1366 | * to close and re-open a stream with the same configuration. | ||
1367 | * | ||
1368 | * It's undefined whether any pending data for the stream will be lost. | ||
1369 | */ | ||
1370 | #define I915_PERF_IOCTL_ENABLE _IO('i', 0x0) | ||
1371 | |||
1372 | /** | ||
1373 | * Disable data capture for a stream. | ||
1374 | * | ||
1375 | * It is an error to try and read a stream that is disabled. | ||
1376 | */ | ||
1377 | #define I915_PERF_IOCTL_DISABLE _IO('i', 0x1) | ||
1378 | |||
1379 | /** | ||
1380 | * Common to all i915 perf records | ||
1381 | */ | ||
1382 | struct drm_i915_perf_record_header { | ||
1383 | __u32 type; | ||
1384 | __u16 pad; | ||
1385 | __u16 size; | ||
1386 | }; | ||
1387 | |||
1388 | enum drm_i915_perf_record_type { | ||
1389 | |||
1390 | /** | ||
1391 | * Samples are the work horse record type whose contents are extensible | ||
1392 | * and defined when opening an i915 perf stream based on the given | ||
1393 | * properties. | ||
1394 | * | ||
1395 | * Boolean properties following the naming convention | ||
1396 | * DRM_I915_PERF_SAMPLE_xyz_PROP request the inclusion of 'xyz' data in | ||
1397 | * every sample. | ||
1398 | * | ||
1399 | * The order of these sample properties given by userspace has no | ||
1400 | * affect on the ordering of data within a sample. The order is | ||
1401 | * documented here. | ||
1402 | * | ||
1403 | * struct { | ||
1404 | * struct drm_i915_perf_record_header header; | ||
1405 | * | ||
1406 | * { u32 oa_report[]; } && DRM_I915_PERF_PROP_SAMPLE_OA | ||
1407 | * }; | ||
1408 | */ | ||
1409 | DRM_I915_PERF_RECORD_SAMPLE = 1, | ||
1410 | |||
1411 | /* | ||
1412 | * Indicates that one or more OA reports were not written by the | ||
1413 | * hardware. This can happen for example if an MI_REPORT_PERF_COUNT | ||
1414 | * command collides with periodic sampling - which would be more likely | ||
1415 | * at higher sampling frequencies. | ||
1416 | */ | ||
1417 | DRM_I915_PERF_RECORD_OA_REPORT_LOST = 2, | ||
1418 | |||
1419 | /** | ||
1420 | * An error occurred that resulted in all pending OA reports being lost. | ||
1421 | */ | ||
1422 | DRM_I915_PERF_RECORD_OA_BUFFER_LOST = 3, | ||
1423 | |||
1424 | DRM_I915_PERF_RECORD_MAX /* non-ABI */ | ||
1425 | }; | ||
1426 | |||
1427 | #if defined(__cplusplus) | ||
1428 | } | ||
1429 | #endif | ||
1430 | |||
1146 | #endif /* _I915_DRM_H_ */ | 1431 | #endif /* _I915_DRM_H_ */ |