diff options
Diffstat (limited to 'intel/intel-symbol-check')
-rwxr-xr-x | intel/intel-symbol-check | 2 |
1 files changed, 1 insertions, 1 deletions
diff --git a/intel/intel-symbol-check b/intel/intel-symbol-check index 2aa2d819..4d30a4b1 100755 --- a/intel/intel-symbol-check +++ b/intel/intel-symbol-check | |||
@@ -3,7 +3,7 @@ | |||
3 | # The following symbols (past the first five) are taken from the public headers. | 3 | # The following symbols (past the first five) are taken from the public headers. |
4 | # A list of the latter should be available Makefile.sources/LIBDRM_INTEL_H_FILES | 4 | # A list of the latter should be available Makefile.sources/LIBDRM_INTEL_H_FILES |
5 | 5 | ||
6 | FUNCS=$(nm -D --format=bsd --defined-only ${1-.libs/libdrm_intel.so} | awk '{print $3}' | while read func; do | 6 | FUNCS=$($NM -D --format=bsd --defined-only ${1-.libs/libdrm_intel.so} | awk '{print $3}' | while read func; do |
7 | ( grep -q "^$func$" || echo $func ) <<EOF | 7 | ( grep -q "^$func$" || echo $func ) <<EOF |
8 | __bss_start | 8 | __bss_start |
9 | _edata | 9 | _edata |