aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Move libdrm.so to vendor partitionJiyong Park2017-04-251-0/+4
| | | | | | | | | | | Gralloc from QCOM is using this lib. However, instead of making this lib as VNDK-SP, it is moved to /vendor partition because no framework component is using this. Bug: 37567747 Bug: 37483222 Test: libdrm.so is in /vendor partion Change-Id: Ib1e9bf6d70e3616e599880d11e8a575d77e4d550
* tests: Split helpers into libraryThierry Reding2015-12-181-0/+1
| | | | | | | | | | Some of the helpers, such as the pattern drawing helpers or the format lookup helpers, have potential to be reused. Move them into a separate library to make it easier to share them. Acked-by: Laurent Pinchart <laurent.pinchart@ideasonboard.com> Signed-off-by: Thierry Reding <treding@nvidia.com> Reviewed-by: Emil Velikov <emil.l.velikov@gmail.com>
* android: add CleanSpec.mkEmil Velikov2014-09-011-0/+3
The file contains rules that are executed on incremental builds. This way one can avoid doing a full clean and ensure that the new object (library) is correctly build. Let's also cleanup the headers. Inspired by the work of Chih-Wei Huang, from the Android-x86 project. Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com>