aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* exynos: Introduce exynos_handle_event()Tobias Jakobi2015-12-181-0/+12
| | | | | | | | Used to handle kernel events specific to the Exynos platform. Currently only G2D events are handled. Signed-off-by: Tobias Jakobi <tjakobi@math.uni-bielefeld.de> Signed-off-by: Hyungwon Hwang <human.hwang@samsung.com>
* exynos: remove DRM_EXYNOS_GEM_{MAP_OFFSET/MMAP} ioctlsHyungwon Hwang2015-02-021-40/+0
| | | | | | | | | This patch removes the ioctls which are removed from the linux kernel. Signed-off-by: Hyungwon Hwang <human.hwang@samsung.com> Signed-off-by: Inki Dae <inki.dae@samsung.com> Signed-off-by: Tobias Jakobi <tjakobi@math.uni-bielefeld.de> Signed-off-by: Rob Clark <robclark@freedesktop.org>
* libdrm/exynos: add test application for 2d gpu.Inki Dae2013-03-081-0/+52
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This patch adds library and test application for g2d gpu(fimg2d). The fimg2d hardware is a 2D graphics accelerator(G2D) that supports Bit Block Transfer(BitBLT). The library includes the following primitive drawing operations: .solid fill - This operation fills the given buffer with the given color data. .copy - This operation copies contents in source buffer to destination buffer. .copy_with_scale - This operation copies contents in source buffer to destination buffer scaling up or down properly. .blend - This operation blends contents in source buffer with the ones in destination buffer. And the above operations uses gem handle or user space address allocated by malloc() as source or destination buffer. And the test application includes just simple primitive drawing tests with the above library. And the guide to test is as the following, "#exynos_fimg2d_test -s connector_id@crtc_id:mode" With this above simple command, four primitive drawing operations would be called step by step and also rendered on the output device to the given connector and crtc id. Signed-off-by: Inki Dae <inki.dae@samsung.com> Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com> Signed-off-by: Rob Clark <robdclark@gmail.com>
* libdrm/exynos: padding gem_mmap structure to 64-bit alignedCooper Yuan2012-07-061-1/+3
|
* libdrm: add exynos drm supportInki Dae2012-05-121-0/+146
this patch adds libdrm_exynos helper layer that inclues some intefaces for exynos specific gem and virtual display driver and also adds exynos module name to modtest and vbltest. Changelog v2: - fixed exynos broken ioctl. the pointer of uint64_t *edid should be removed. - removed unnecessary definitions. - added drm prime interfaces. this feature is used to share a buffer between drivers or memory managers and for this, please, refer to below links: http://www.mjmwired.net/kernel/Documentation/dma-buf-sharing.txt http://lwn.net/Articles/488664/ this patch is based on a link below: git://anongit.freedesktop.org/mesa/drm commit id: d72a44c7c4f5eea9c1e5bb0c36cb9e0224b9ca22 Reviewed-by: Rob Clark <rob@ti.com> Reviewed-by: Alex Deucher <alexander.deucher@amd.com> Signed-off-by: Inki Dae <inki.dae@samsung.com> Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com> Signed-off-by: Rob Clark <rob@ti.com>