From 8d34bba212342ec0e187cd3602d01edba2d7ec26 Mon Sep 17 00:00:00 2001 From: Eric Anholt Date: Wed, 8 Nov 2017 11:06:55 -0800 Subject: headers: Sync up some header guard changes from drm-next. This pulls in pieces of drm-next d65d31388a23 ("Merge tag 'drm-misc-next-fixes-2017-11-07' of git://anongit.freedesktop.org/drm/drm-misc into drm-next") Signed-off-by: Eric Anholt Reviewed-by: Emil Velikov --- include/drm/README | 4 ---- include/drm/mga_drm.h | 8 ++++++++ include/drm/nouveau_drm.h | 10 ++++++++++ include/drm/qxl_drm.h | 8 ++++++++ include/drm/r128_drm.h | 10 ++++++++++ include/drm/savage_drm.h | 10 ++++++++++ include/drm/sis_drm.h | 10 ++++++++++ include/drm/tegra_drm.h | 14 +++++++++++--- include/drm/via_drm.h | 8 ++++++++ include/drm/vmwgfx_drm.h | 9 +++++++++ 10 files changed, 84 insertions(+), 7 deletions(-) (limited to 'include') diff --git a/include/drm/README b/include/drm/README index 870b0b5b..47d80929 100644 --- a/include/drm/README +++ b/include/drm/README @@ -86,10 +86,6 @@ Outdated or Broken Headers This section contains a list of headers and the respective "issues" they might have relative to their kernel equivalent. -Nearly all headers: - - Missing extern C notation. -Status: Trivial. - Most UMS headers: - Not using fixed size integers - compat ioctls are broken. Status: ? diff --git a/include/drm/mga_drm.h b/include/drm/mga_drm.h index b630e8fa..f54e7a2e 100644 --- a/include/drm/mga_drm.h +++ b/include/drm/mga_drm.h @@ -37,6 +37,10 @@ #include "drm.h" +#if defined(__cplusplus) +extern "C" { +#endif + /* WARNING: If you change any of these defines, make sure to change the * defines in the Xserver file (mga_sarea.h) */ @@ -416,4 +420,8 @@ typedef struct drm_mga_getparam { void *value; } drm_mga_getparam_t; +#if defined(__cplusplus) +} +#endif + #endif diff --git a/include/drm/nouveau_drm.h b/include/drm/nouveau_drm.h index e418f9f3..542a732b 100644 --- a/include/drm/nouveau_drm.h +++ b/include/drm/nouveau_drm.h @@ -27,6 +27,12 @@ #define NOUVEAU_DRM_HEADER_PATCHLEVEL 16 +#include "drm.h" + +#if defined(__cplusplus) +extern "C" { +#endif + struct drm_nouveau_channel_alloc { uint32_t fb_ctxdma_handle; uint32_t tt_ctxdma_handle; @@ -207,4 +213,8 @@ struct drm_nouveau_sarea { #define DRM_NOUVEAU_GEM_CPU_FINI 0x43 #define DRM_NOUVEAU_GEM_INFO 0x44 +#if defined(__cplusplus) +} +#endif + #endif /* __NOUVEAU_DRM_H__ */ diff --git a/include/drm/qxl_drm.h b/include/drm/qxl_drm.h index 1e331a86..ccd841b1 100644 --- a/include/drm/qxl_drm.h +++ b/include/drm/qxl_drm.h @@ -27,6 +27,10 @@ #include #include "drm.h" +#if defined(__cplusplus) +extern "C" { +#endif + /* Please note that modifications to all structs defined here are * subject to backwards-compatibility constraints. * @@ -149,4 +153,8 @@ struct drm_qxl_alloc_surf { DRM_IOWR(DRM_COMMAND_BASE + DRM_QXL_ALLOC_SURF,\ struct drm_qxl_alloc_surf) +#if defined(__cplusplus) +} +#endif + #endif diff --git a/include/drm/r128_drm.h b/include/drm/r128_drm.h index ede78ff9..bf431a02 100644 --- a/include/drm/r128_drm.h +++ b/include/drm/r128_drm.h @@ -33,6 +33,12 @@ #ifndef __R128_DRM_H__ #define __R128_DRM_H__ +#include "drm.h" + +#if defined(__cplusplus) +extern "C" { +#endif + /* WARNING: If you change any of these defines, make sure to change the * defines in the X server file (r128_sarea.h) */ @@ -323,4 +329,8 @@ typedef struct drm_r128_getparam { void *value; } drm_r128_getparam_t; +#if defined(__cplusplus) +} +#endif + #endif diff --git a/include/drm/savage_drm.h b/include/drm/savage_drm.h index f7a75eff..26f387b7 100644 --- a/include/drm/savage_drm.h +++ b/include/drm/savage_drm.h @@ -26,6 +26,12 @@ #ifndef __SAVAGE_DRM_H__ #define __SAVAGE_DRM_H__ +#include "drm.h" + +#if defined(__cplusplus) +extern "C" { +#endif + #ifndef __SAVAGE_SAREA_DEFINES__ #define __SAVAGE_SAREA_DEFINES__ @@ -207,4 +213,8 @@ union drm_savage_cmd_header { } clear1; /* SAVAGE_CMD_CLEAR data */ }; +#if defined(__cplusplus) +} +#endif + #endif diff --git a/include/drm/sis_drm.h b/include/drm/sis_drm.h index 30f7b382..8e51bb9a 100644 --- a/include/drm/sis_drm.h +++ b/include/drm/sis_drm.h @@ -27,6 +27,12 @@ #ifndef __SIS_DRM_H__ #define __SIS_DRM_H__ +#include "drm.h" + +#if defined(__cplusplus) +extern "C" { +#endif + /* SiS specific ioctls */ #define NOT_USED_0_3 #define DRM_SIS_FB_ALLOC 0x04 @@ -64,4 +70,8 @@ typedef struct { unsigned int offset, size; } drm_sis_fb_t; +#if defined(__cplusplus) +} +#endif + #endif /* __SIS_DRM_H__ */ diff --git a/include/drm/tegra_drm.h b/include/drm/tegra_drm.h index 7c0fe0ed..12f9bf84 100644 --- a/include/drm/tegra_drm.h +++ b/include/drm/tegra_drm.h @@ -20,10 +20,14 @@ * OTHER DEALINGS IN THE SOFTWARE. */ -#ifndef _UAPI_TEGRA_DRM_H_ -#define _UAPI_TEGRA_DRM_H_ +#ifndef _TEGRA_DRM_H_ +#define _TEGRA_DRM_H_ -#include +#include "drm.h" + +#if defined(__cplusplus) +extern "C" { +#endif #define DRM_TEGRA_GEM_CREATE_TILED (1 << 0) #define DRM_TEGRA_GEM_CREATE_BOTTOM_UP (1 << 1) @@ -198,4 +202,8 @@ struct drm_tegra_gem_get_flags { #define DRM_IOCTL_TEGRA_GEM_SET_FLAGS DRM_IOWR(DRM_COMMAND_BASE + DRM_TEGRA_GEM_SET_FLAGS, struct drm_tegra_gem_set_flags) #define DRM_IOCTL_TEGRA_GEM_GET_FLAGS DRM_IOWR(DRM_COMMAND_BASE + DRM_TEGRA_GEM_GET_FLAGS, struct drm_tegra_gem_get_flags) +#if defined(__cplusplus) +} +#endif + #endif diff --git a/include/drm/via_drm.h b/include/drm/via_drm.h index 182f8792..8b69e819 100644 --- a/include/drm/via_drm.h +++ b/include/drm/via_drm.h @@ -26,6 +26,10 @@ #include "drm.h" +#if defined(__cplusplus) +extern "C" { +#endif + /* WARNING: These defines must be the same as what the Xserver uses. * if you change them, you must change the defines in the Xserver. */ @@ -272,4 +276,8 @@ typedef struct drm_via_dmablit { drm_via_blitsync_t sync; } drm_via_dmablit_t; +#if defined(__cplusplus) +} +#endif + #endif /* _VIA_DRM_H_ */ diff --git a/include/drm/vmwgfx_drm.h b/include/drm/vmwgfx_drm.h index 5b68b4d1..d325a410 100644 --- a/include/drm/vmwgfx_drm.h +++ b/include/drm/vmwgfx_drm.h @@ -30,6 +30,10 @@ #include "drm.h" +#if defined(__cplusplus) +extern "C" { +#endif + #define DRM_VMW_MAX_SURFACE_FACES 6 #define DRM_VMW_MAX_MIP_LEVELS 24 @@ -1087,4 +1091,9 @@ union drm_vmw_extended_context_arg { enum drm_vmw_extended_context req; struct drm_vmw_context_arg rep; }; + +#if defined(__cplusplus) +} +#endif + #endif -- cgit v1.2.3-54-g00ecf