/************************************************************************** * * Copyright © 2009 VMware, Inc., Palo Alto, CA., USA * All Rights Reserved. * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the * "Software"), to deal in the Software without restriction, including * without limitation the rights to use, copy, modify, merge, publish, * distribute, sub license, and/or sell copies of the Software, and to * permit persons to whom the Software is furnished to do so, subject to * the following conditions: * * The above copyright notice and this permission notice (including the * next paragraph) shall be included in all copies or substantial portions * of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. IN NO EVENT SHALL * THE COPYRIGHT HOLDERS, AUTHORS AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, * DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR * OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE * USE OR OTHER DEALINGS IN THE SOFTWARE. * **************************************************************************/ /* * Thanks to krh and jcristau for the tips on * going from fd to pci id via fstat and udev. */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include #include #include #include #include #include #include #include #ifdef MAJOR_IN_MKDEV #include #endif #ifdef MAJOR_IN_SYSMACROS #include #endif #include "libdrm_macros.h" #include "internal.h" #define PATH_SIZE 512 static int linux_name_from_sysfs(int fd, char **out) { char path[PATH_SIZE+1] = ""; /* initialize to please valgrind */ char link[PATH_SIZE+1] = ""; struct stat buffer; unsigned maj, min; char* slash_name; int ret; /* * Inside the sysfs directory for the device there is a symlink * to the directory representing the driver module, that path * happens to hold the name of the driver. * * So lets get the symlink for the drm device. Then read the link * and filter out the last directory which happens to be the name * of the driver, which we can use to load the correct interface. * * Thanks to Ray Strode of Plymouth for the code. */ ret = fstat(fd, &buffer); if (ret) return -EINVAL; if (!S_ISCHR(buffer.st_mode)) return -EINVAL; maj = major(buffer.st_rdev); min = minor(buffer.st_rdev); snprintf(path, PATH_SIZE, "/sys/dev/char/%d:%d/device/driver", maj, min); if (readlink(path, link, PATH_SIZE) < 0) return -EINVAL; /* link looks something like this: ../../../bus/pci/drivers/intel */ slash_name = strrchr(link, '/'); if (!slash_name) return -EINVAL; /* copy name and at the same time remove the slash */ *out = strdup(slash_name + 1); return 0; } static int linux_from_sysfs(int fd, struct kms_driver **out) { char *name; int ret; ret = linux_name_from_sysfs(fd, &name); if (ret) return ret; #if HAVE_INTEL if (!strcmp(name, "intel")) ret = intel_create(fd, out); else #endif #if HAVE_VMWGFX if (!strcmp(name, "vmwgfx")) ret = vmwgfx_create(fd, out); else #endif #if HAVE_NOUVEAU if (!strcmp(name, "nouveau")) ret = nouveau_create(fd, out); else #endif #if HAVE_RADEON if (!strcmp(name, "radeon")) ret = radeon_create(fd, out); else #endif #if HAVE_EXYNOS if (!strcmp(name, "exynos")) ret = exynos_create(fd, out); else #endif ret = -ENOSYS; free(name); return ret; } drm_private int linux_create(int fd, struct kms_driver **out) { if (!dumb_create(fd, out)) return 0; return linux_from_sysfs(fd, out); }