blob: 346abad2d02b0b90133884d2b8f7e60bed35d7de (
plain) (
tree)
|
|
<?xml version="1.0" encoding="utf-8"?>
<!-- Copyright (C) 2014 The Android Open Source Project
Licensed under the Apache License, Version 2.0 (the "License");
you may not use this file except in compliance with the License.
You may obtain a copy of the License at
http://www.apache.org/licenses/LICENSE-2.0
Unless required by applicable law or agreed to in writing, software
distributed under the License is distributed on an "AS IS" BASIS,
WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
See the License for the specific language governing permissions and
limitations under the License.
-->
<!-- These are the hardware and software components that all wearable devices
must include. Devices with optional hardware/software must also include
extra hardware/software files, per the comments below.
Wearable devices include watches, glasses, backpacks, and sweaters.
-->
<permissions>
<feature name="android.hardware.location" />
<feature name="android.hardware.sensor.compass" />
<feature name="android.hardware.sensor.accelerometer" />
<feature name="android.hardware.bluetooth" />
<feature name="android.hardware.touchscreen" />
<feature name="android.hardware.microphone" />
<!-- basic system services -->
<feature name="android.software.home_screen" />
<!-- devices that support a device administrator policy must include
android.software.device_admin.xml -->
<!-- devices with GPS must include device/google/clockwork/gps.xml -->
<!-- devices with an autofocus camera and/or flash must include either
android.hardware.camera.autofocus.xml or
android.hardware.camera.autofocus-flash.xml -->
<!-- devices with a front facing camera must include
android.hardware.camera.front.xml -->
<!-- devices with WiFi must also include android.hardware.wifi.xml -->
<!-- devices that support multitouch must include the most appropriate one
of these files:
If only partial (non-independent) pointers are supported:
android.hardware.touchscreen.multitouch.xml
If up to 4 independently tracked pointers are supported:
include android.hardware.touchscreen.multitouch.distinct.xml
If 5 or more independently tracked pointers are supported:
include android.hardware.touchscreen.multitouch.jazzhand.xml
ONLY ONE of the above should be included. -->
<!-- devices with an ambient light sensor must also include
android.hardware.sensor.light.xml -->
<!-- devices with a proximity sensor must also include
android.hardware.sensor.proximity.xml -->
<!-- Devices that have low-latency audio stacks suitable for apps like
VoIP may include android.hardware.audio.low_latency.xml. ONLY apps
that meet the requirements specified in the CDD may include this. -->
<!-- devices that have audio output capability as specified in the CDD must
also include android.hardware.audio.output.xml -->
</permissions>
|