summaryrefslogblamecommitdiffstats
blob: 880a24d6ada4199e0f1f018c4b9ec4c0ddabe575 (plain) (tree)
























                                                                           



                         


                   
                
























                                                                              
                                        

                

                                                                        
                                                       










                                                                              
                                                                      















                                                                              
                                                                             



                                                                             


                                                             




                                                                           
 



                                                                            

                                                              





                                                                              





                                                                              


                                                                   






                                     
                                               
                                     
                                                    
                                                    
 

                            







                                                                         



                                                                              

                                                                         
                            

                   




                                                                             


                                                                           









                                                                             

                                                                      

                                

                          




                                                                     



                                                                                



                                                                                




                            
/*
 * Copyright (C) 2012 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef ANDROID_DISPSYNC_H
#define ANDROID_DISPSYNC_H

#include <stddef.h>

#include <utils/Mutex.h>
#include <utils/Timers.h>
#include <utils/RefBase.h>

#include <ui/FenceTime.h>

#include <memory>

namespace android {

class String8;
class FenceTime;
class DispSyncThread;

// DispSync maintains a model of the periodic hardware-based vsync events of a
// display and uses that model to execute period callbacks at specific phase
// offsets from the hardware vsync events.  The model is constructed by
// feeding consecutive hardware event timestamps to the DispSync object via
// the addResyncSample method.
//
// The model is validated using timestamps from Fence objects that are passed
// to the DispSync object via the addPresentFence method.  These fence
// timestamps should correspond to a hardware vsync event, but they need not
// be consecutive hardware vsync times.  If this method determines that the
// current model accurately represents the hardware event times it will return
// false to indicate that a resynchronization (via addResyncSample) is not
// needed.
class DispSync {

public:

    class Callback: public virtual RefBase {
    public:
        virtual ~Callback() {};
        virtual void onDispSyncEvent(nsecs_t when) = 0;
    };

    explicit DispSync(const char* name);
    ~DispSync();

    void init(bool hasSyncFramework, int64_t dispSyncPresentTimeOffset);

    // reset clears the resync samples and error value.
    void reset();

    // addPresentFence adds a fence for use in validating the current vsync
    // event model.  The fence need not be signaled at the time
    // addPresentFence is called.  When the fence does signal, its timestamp
    // should correspond to a hardware vsync event.  Unlike the
    // addResyncSample method, the timestamps of consecutive fences need not
    // correspond to consecutive hardware vsync events.
    //
    // This method should be called with the retire fence from each HWComposer
    // set call that affects the display.
    bool addPresentFence(const std::shared_ptr<FenceTime>& fenceTime);

    // The beginResync, addResyncSample, and endResync methods are used to re-
    // synchronize the DispSync's model to the hardware vsync events.  The re-
    // synchronization process involves first calling beginResync, then
    // calling addResyncSample with a sequence of consecutive hardware vsync
    // event timestamps, and finally calling endResync when addResyncSample
    // indicates that no more samples are needed by returning false.
    //
    // This resynchronization process should be performed whenever the display
    // is turned on (i.e. once immediately after it's turned on) and whenever
    // addPresentFence returns true indicating that the model has drifted away
    // from the hardware vsync events.
    void beginResync();
    bool addResyncSample(nsecs_t timestamp);
    void endResync();

    // The setPeriod method sets the vsync event model's period to a specific
    // value.  This should be used to prime the model when a display is first
    // turned on.  It should NOT be used after that.
    void setPeriod(nsecs_t period);

    // The getPeriod method returns the current vsync period.
    nsecs_t getPeriod();

    // setRefreshSkipCount specifies an additional number of refresh
    // cycles to skip.  For example, on a 60Hz display, a skip count of 1
    // will result in events happening at 30Hz.  Default is zero.  The idea
    // is to sacrifice smoothness for battery life.
    void setRefreshSkipCount(int count);

    // addEventListener registers a callback to be called repeatedly at the
    // given phase offset from the hardware vsync events.  The callback is
    // called from a separate thread and it should return reasonably quickly
    // (i.e. within a few hundred microseconds).
    status_t addEventListener(const char* name, nsecs_t phase,
            const sp<Callback>& callback);

    // removeEventListener removes an already-registered event callback.  Once
    // this method returns that callback will no longer be called by the
    // DispSync object.
    status_t removeEventListener(const sp<Callback>& callback);

    // computeNextRefresh computes when the next refresh is expected to begin.
    // The periodOffset value can be used to move forward or backward; an
    // offset of zero is the next refresh, -1 is the previous refresh, 1 is
    // the refresh after next. etc.
    nsecs_t computeNextRefresh(int periodOffset) const;

    // dump appends human-readable debug info to the result string.
    void dump(String8& result) const;

private:

    void updateModelLocked();
    void updateErrorLocked();
    void resetErrorLocked();

    enum { MAX_RESYNC_SAMPLES = 32 };
    enum { MIN_RESYNC_SAMPLES_FOR_UPDATE = 6 };
    enum { NUM_PRESENT_SAMPLES = 8 };
    enum { MAX_RESYNC_SAMPLES_WITHOUT_PRESENT = 4 };
    enum { ACCEPTABLE_ZERO_ERR_SAMPLES_COUNT = 64 };

    const char* const mName;

    // mPeriod is the computed period of the modeled vsync events in
    // nanoseconds.
    nsecs_t mPeriod;

    // mPhase is the phase offset of the modeled vsync events.  It is the
    // number of nanoseconds from time 0 to the first vsync event.
    nsecs_t mPhase;

    // mReferenceTime is the reference time of the modeled vsync events.
    // It is the nanosecond timestamp of the first vsync event after a resync.
    nsecs_t mReferenceTime;

    // mError is the computed model error.  It is based on the difference
    // between the estimated vsync event times and those observed in the
    // mPresentFences array.
    nsecs_t mError;

    // mZeroErrSamplesCount keeps track of how many times in a row there were
    // zero timestamps available in the mPresentFences array.
    // Used to sanity check that we are able to calculate the model error.
    size_t mZeroErrSamplesCount;

    // Whether we have updated the vsync event model since the last resync.
    bool mModelUpdated;

    // These member variables are the state used during the resynchronization
    // process to store information about the hardware vsync event times used
    // to compute the model.
    nsecs_t mResyncSamples[MAX_RESYNC_SAMPLES];
    size_t mFirstResyncSample;
    size_t mNumResyncSamples;
    int mNumResyncSamplesSincePresent;

    // These member variables store information about the present fences used
    // to validate the currently computed model.
    std::shared_ptr<FenceTime>
            mPresentFences[NUM_PRESENT_SAMPLES] {FenceTime::NO_FENCE};
    size_t mPresentSampleOffset;

    int mRefreshSkipCount;

    // mThread is the thread from which all the callbacks are called.
    sp<DispSyncThread> mThread;

    // mMutex is used to protect access to all member variables.
    mutable Mutex mMutex;

    // This is the offset from the present fence timestamps to the corresponding
    // vsync event.
    int64_t mPresentTimeOffset;

    // Ignore present (retire) fences if the device doesn't have support for the
    // sync framework
    bool mIgnorePresentFences;
};

}

#endif // ANDROID_DISPSYNC_H