summaryrefslogtreecommitdiffstats
path: root/cmds
Commit message (Expand)AuthorAgeFilesLines
...
| * | Don't use su to when calling am or dumpsys.Felipe Leme2016-03-173-55/+104
* | | Capture systrace buffers.Felipe Leme2016-03-214-2/+68
* | | Added -q flag to showmap.Felipe Leme2016-03-171-1/+1
|/ /
* | Merge "Improve logging of child commands." into nyc-devFelipe Leme2016-03-173-16/+63
|\ \
| * | Improve logging of child commands.Felipe Leme2016-03-173-16/+63
* | | Merge "Otapreopt: Load properties from files" into nyc-devAndreas Gampe2016-03-173-54/+112
|\ \ \ | |_|/ |/| |
| * | Otapreopt: Load properties from filesAndreas Gampe2016-03-163-54/+112
* | | Merge "Otapreopt: Remove b_mount_path" into nyc-devAndreas Gampe2016-03-161-14/+7
|\| |
| * | Otapreopt: Remove b_mount_pathAndreas Gampe2016-03-161-14/+7
* | | Merge "atrace: Adding dumping message to logcat." into nyc-devPhilip Cuadra2016-03-161-0/+3
|\ \ \
| * | | atrace: Adding dumping message to logcat.Philip Cuadra2016-03-151-0/+3
* | | | Installd: Make extract-only = interpret-onlyAndreas Gampe2016-03-161-1/+3
| |/ / |/| |
* | | Merge "Otapreopt: Adapt for actual A/B" into nyc-devAndreas Gampe2016-03-154-20/+210
|\ \ \
| * | | Otapreopt: Adapt for actual A/BAndreas Gampe2016-03-154-20/+210
* | | | Added zip location on log message.Felipe Leme2016-03-151-1/+1
|/ / /
* | | Merge "installd: Avoid potential use of null 'src'." into nyc-devGreg Kaiser2016-03-151-4/+4
|\ \ \ | |/ / |/| |
| * | installd: Avoid potential use of null 'src'.Greg Kaiser2016-03-141-4/+4
* | | Pass -n to netstat.Lorenzo Colitti2016-03-131-1/+1
* | | Merge "svcmgr: don't send reply to one-way txn." into nyc-devDaniel Cashman2016-03-111-6/+15
|\ \ \ | |/ / |/| |
| * | svcmgr: don't send reply to one-way txn.dcashman2016-03-111-6/+15
* | | Merge "Installd: Do not log on missing B artifact" into nyc-devAndreas Gampe2016-03-111-1/+2
|\ \ \ | |_|/ |/| |
| * | Installd: Do not log on missing B artifactAndreas Gampe2016-03-111-1/+2
| |/
* | Merge "Remove the route command from dumpstate." into nyc-devLorenzo Colitti2016-03-111-1/+0
|\ \ | |/ |/|
| * Remove the route command from dumpstate.Lorenzo Colitti2016-03-101-1/+0
* | Improved usage of stderr for logging.Felipe Leme2016-03-082-25/+33
|/
* Fix name of argumentDavid Brazdil2016-03-081-1/+1
* Add 'rmprofiles' command to installdDavid Brazdil2016-03-083-5/+25
* dumpsys: switch to using a pipe to work around selinux denial.Josh Gao2016-03-041-3/+2
* Merge "Removed temporary 'v1-dev1-dumpsys-split' version and bumped version t...Felipe Leme2016-03-041-18/+9
|\
| * Removed temporary 'v1-dev1-dumpsys-split' version and bumped version toFelipe Leme2016-02-291-18/+9
* | Merge "Installd: Add move_ab command" into nyc-devAndreas Gampe2016-03-033-0/+87
|\ \
| * | Installd: Add move_ab commandAndreas Gampe2016-03-033-0/+87
* | | dumpsys: use a socket for dumping, add timeout support.Josh Gao2016-03-022-14/+112
|/ /
* | Merge "Clean up error logs for profiles which don't exists." into nyc-devCalin Juravle2016-03-021-2/+6
|\ \
| * | Clean up error logs for profiles which don't exists.Calin Juravle2016-02-291-2/+6
* | | Merge "Return an error if try to profile guide compile to a public oat file" ...Calin Juravle2016-03-011-1/+9
|\ \ \
| * | | Return an error if try to profile guide compile to a public oat fileCalin Juravle2016-03-011-1/+9
| |/ /
* | / Otapreopt: Fix patchoat delta parameterAndreas Gampe2016-02-291-1/+1
| |/ |/|
* | Merge "Rename .zip file if necessary." into nyc-devFelipe Leme2016-02-261-0/+11
|\ \
| * | Rename .zip file if necessary.Felipe Leme2016-02-261-0/+11
* | | Moved final vibration to the end of the process.Felipe Leme2016-02-251-8/+8
|/ /
* | Merge "Improved dumpstate logging." into nyc-devFelipe Leme2016-02-243-4/+21
|\ \ | |/ |/|
| * Improved dumpstate logging.Felipe Leme2016-02-223-4/+21
* | Merge "Send max duration when bugreport is finished so Shell can update metri...Felipe Leme2016-02-231-0/+1
|\ \
| * | Send max duration when bugreport is finished so Shell can updateFelipe Leme2016-02-221-0/+1
| |/
* | Merge "dumpstate: Remove deprecated /proc/wakelocks" into nyc-devRuchi Kandoi2016-02-221-1/+0
|\ \ | |/ |/|
| * dumpstate: Remove deprecated /proc/wakelocksRuchi Kandoi2016-02-221-1/+0
* | Extract profile files in their dedicated folderCalin Juravle2016-02-196-167/+364
* | Merge "Revert "Revert "Fix warnings in servicemanager and KeyCharacterMap""" ...Ian Pedowitz2016-02-193-6/+6
|\ \
| * | Revert "Revert "Fix warnings in servicemanager and KeyCharacterMap""Ian Pedowitz2016-02-193-6/+6