/* * Copyright (C) 2011 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef ANDROID_SURFACE_FLINGER_EVENT_THREAD_H #define ANDROID_SURFACE_FLINGER_EVENT_THREAD_H #include #include #include #include #include #include #include #include "DisplayDevice.h" #include "DisplayHardware/PowerHAL.h" // --------------------------------------------------------------------------- namespace android { // --------------------------------------------------------------------------- class SurfaceFlinger; class String8; // --------------------------------------------------------------------------- class VSyncSource : public virtual RefBase { public: class Callback: public virtual RefBase { public: virtual ~Callback() {} virtual void onVSyncEvent(nsecs_t when) = 0; }; virtual ~VSyncSource() {} virtual void setVSyncEnabled(bool enable) = 0; virtual void setCallback(const sp& callback) = 0; virtual void setPhaseOffset(nsecs_t phaseOffset) = 0; }; class EventThread : public Thread, private VSyncSource::Callback { class Connection : public BnDisplayEventConnection { public: Connection(const sp& eventThread); status_t postEvent(const DisplayEventReceiver::Event& event); // count >= 1 : continuous event. count is the vsync rate // count == 0 : one-shot event that has not fired // count ==-1 : one-shot event that fired this round / disabled int32_t count; private: virtual ~Connection(); virtual void onFirstRef(); virtual sp getDataChannel() const; virtual void setVsyncRate(uint32_t count); virtual void requestNextVsync(); // asynchronous sp const mEventThread; sp const mChannel; }; public: EventThread(const sp& src); sp createEventConnection() const; status_t registerDisplayEventConnection(const sp& connection); void setVsyncRate(uint32_t count, const sp& connection); void requestNextVsync(const sp& connection); // called before the screen is turned off from main thread void onScreenReleased(); // called after the screen is turned on from main thread void onScreenAcquired(); // called when receiving a hotplug event void onHotplugReceived(int type, bool connected); Vector< sp > waitForEvent( DisplayEventReceiver::Event* event); void dump(String8& result) const; void sendVsyncHintOff(); void setPhaseOffset(nsecs_t phaseOffset); private: virtual bool threadLoop(); virtual void onFirstRef(); virtual void onVSyncEvent(nsecs_t timestamp); void removeDisplayEventConnection(const wp& connection); void enableVSyncLocked(); void disableVSyncLocked(); void sendVsyncHintOnLocked(); // constants sp mVSyncSource; PowerHAL mPowerHAL; mutable Mutex mLock; mutable Condition mCondition; // protected by mLock SortedVector< wp > mDisplayEventConnections; Vector< DisplayEventReceiver::Event > mPendingEvents; DisplayEventReceiver::Event mVSyncEvent[DisplayDevice::NUM_BUILTIN_DISPLAY_TYPES]; bool mUseSoftwareVSync; bool mVsyncEnabled; // for debugging bool mDebugVsyncEnabled; bool mVsyncHintSent; timer_t mTimerId; }; // --------------------------------------------------------------------------- }; // namespace android // --------------------------------------------------------------------------- #endif /* ANDROID_SURFACE_FLINGER_EVENT_THREAD_H */