1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
|
/*
* Copyright (C) 2007 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef ANDROID_LAYER_H
#define ANDROID_LAYER_H
#include <stdint.h>
#include <sys/types.h>
#include <EGL/egl.h>
#include <EGL/eglext.h>
#include <utils/RefBase.h>
#include <utils/String8.h>
#include <utils/Timers.h>
#include <ui/FrameStats.h>
#include <ui/GraphicBuffer.h>
#include <ui/PixelFormat.h>
#include <ui/Region.h>
#include <gui/ISurfaceComposerClient.h>
#include <private/gui/LayerState.h>
#include "FrameTracker.h"
#include "Client.h"
#include "MonitoredProducer.h"
#include "SurfaceFlinger.h"
#include "SurfaceFlingerConsumer.h"
#include "Transform.h"
#include "DisplayHardware/HWComposer.h"
#include "DisplayHardware/FloatRect.h"
#include "RenderEngine/Mesh.h"
#include "RenderEngine/Texture.h"
namespace android {
// ---------------------------------------------------------------------------
class Client;
class Colorizer;
class DisplayDevice;
class GraphicBuffer;
class SurfaceFlinger;
// ---------------------------------------------------------------------------
/*
* A new BufferQueue and a new SurfaceFlingerConsumer are created when the
* Layer is first referenced.
*
* This also implements onFrameAvailable(), which notifies SurfaceFlinger
* that new data has arrived.
*/
class Layer : public SurfaceFlingerConsumer::ContentsChangedListener {
static int32_t sSequence;
public:
mutable bool contentDirty;
// regions below are in window-manager space
Region visibleRegion;
Region coveredRegion;
Region visibleNonTransparentRegion;
Region surfaceDamageRegion;
// Layer serial number. This gives layers an explicit ordering, so we
// have a stable sort order when their layer stack and Z-order are
// the same.
int32_t sequence;
enum { // flags for doTransaction()
eDontUpdateGeometryState = 0x00000001,
eVisibleRegion = 0x00000002,
};
struct Geometry {
uint32_t w;
uint32_t h;
Rect crop;
inline bool operator ==(const Geometry& rhs) const {
return (w == rhs.w && h == rhs.h && crop == rhs.crop);
}
inline bool operator !=(const Geometry& rhs) const {
return !operator ==(rhs);
}
};
struct State {
Geometry active;
Geometry requested;
uint32_t z;
uint32_t layerStack;
uint8_t alpha;
uint8_t flags;
uint8_t reserved[2];
int32_t sequence; // changes when visible regions can change
Transform transform;
// the transparentRegion hint is a bit special, it's latched only
// when we receive a buffer -- this is because it's "content"
// dependent.
Region activeTransparentRegion;
Region requestedTransparentRegion;
};
// -----------------------------------------------------------------------
Layer(SurfaceFlinger* flinger, const sp<Client>& client,
const String8& name, uint32_t w, uint32_t h, uint32_t flags);
virtual ~Layer();
// the this layer's size and format
status_t setBuffers(uint32_t w, uint32_t h, PixelFormat format, uint32_t flags);
// modify current state
bool setPosition(float x, float y);
bool setLayer(uint32_t z);
bool setSize(uint32_t w, uint32_t h);
bool setAlpha(uint8_t alpha);
bool setMatrix(const layer_state_t::matrix22_t& matrix);
bool setTransparentRegionHint(const Region& transparent);
bool setFlags(uint8_t flags, uint8_t mask);
bool setCrop(const Rect& crop);
bool setLayerStack(uint32_t layerStack);
// If we have received a new buffer this frame, we will pass its surface
// damage down to hardware composer. Otherwise, we must send a region with
// one empty rect.
void useSurfaceDamage();
void useEmptyDamage();
uint32_t getTransactionFlags(uint32_t flags);
uint32_t setTransactionFlags(uint32_t flags);
void computeGeometry(const sp<const DisplayDevice>& hw, Mesh& mesh,
bool useIdentityTransform) const;
Rect computeBounds(const Region& activeTransparentRegion) const;
Rect computeBounds() const;
sp<IBinder> getHandle();
sp<IGraphicBufferProducer> getProducer() const;
const String8& getName() const;
// -----------------------------------------------------------------------
// Virtuals
virtual const char* getTypeId() const { return "Layer"; }
/*
* isOpaque - true if this surface is opaque
*
* This takes into account the buffer format (i.e. whether or not the
* pixel format includes an alpha channel) and the "opaque" flag set
* on the layer. It does not examine the current plane alpha value.
*/
virtual bool isOpaque(const Layer::State& s) const;
/*
* isSecure - true if this surface is secure, that is if it prevents
* screenshots or VNC servers.
*/
virtual bool isSecure() const;
/*
* isProtected - true if the layer may contain protected content in the
* GRALLOC_USAGE_PROTECTED sense.
*/
virtual bool isProtected() const;
/*
* isVisible - true if this layer is visible, false otherwise
*/
virtual bool isVisible() const;
/*
* isFixedSize - true if content has a fixed size
*/
virtual bool isFixedSize() const;
protected:
/*
* onDraw - draws the surface.
*/
virtual void onDraw(const sp<const DisplayDevice>& hw, const Region& clip,
bool useIdentityTransform) const;
public:
// -----------------------------------------------------------------------
void setGeometry(const sp<const DisplayDevice>& hw,
HWComposer::HWCLayerInterface& layer);
void setPerFrameData(const sp<const DisplayDevice>& hw,
HWComposer::HWCLayerInterface& layer);
void setAcquireFence(const sp<const DisplayDevice>& hw,
HWComposer::HWCLayerInterface& layer);
Rect getPosition(const sp<const DisplayDevice>& hw);
/*
* called after page-flip
*/
void onLayerDisplayed(const sp<const DisplayDevice>& hw,
HWComposer::HWCLayerInterface* layer);
bool shouldPresentNow(const DispSync& dispSync) const;
/*
* called before composition.
* returns true if the layer has pending updates.
*/
bool onPreComposition();
/*
* called after composition.
*/
void onPostComposition();
/*
* draw - performs some global clipping optimizations
* and calls onDraw().
*/
void draw(const sp<const DisplayDevice>& hw, const Region& clip) const;
void draw(const sp<const DisplayDevice>& hw, bool useIdentityTransform) const;
void draw(const sp<const DisplayDevice>& hw) const;
/*
* doTransaction - process the transaction. This is a good place to figure
* out which attributes of the surface have changed.
*/
uint32_t doTransaction(uint32_t transactionFlags);
/*
* setVisibleRegion - called to set the new visible region. This gives
* a chance to update the new visible region or record the fact it changed.
*/
void setVisibleRegion(const Region& visibleRegion);
/*
* setCoveredRegion - called when the covered region changes. The covered
* region corresponds to any area of the surface that is covered
* (transparently or not) by another surface.
*/
void setCoveredRegion(const Region& coveredRegion);
/*
* setVisibleNonTransparentRegion - called when the visible and
* non-transparent region changes.
*/
void setVisibleNonTransparentRegion(const Region&
visibleNonTransparentRegion);
/*
* latchBuffer - called each time the screen is redrawn and returns whether
* the visible regions need to be recomputed (this is a fairly heavy
* operation, so this should be set only if needed). Typically this is used
* to figure out if the content or size of a surface has changed.
*/
Region latchBuffer(bool& recomputeVisibleRegions);
bool isPotentialCursor() const { return mPotentialCursor;}
/*
* called with the state lock when the surface is removed from the
* current list
*/
void onRemoved();
// Updates the transform hint in our SurfaceFlingerConsumer to match
// the current orientation of the display device.
void updateTransformHint(const sp<const DisplayDevice>& hw) const;
/*
* returns the rectangle that crops the content of the layer and scales it
* to the layer's size.
*/
Rect getContentCrop() const;
/*
* Returns if a frame is queued.
*/
bool hasQueuedFrame() const { return mQueuedFrames > 0 || mSidebandStreamChanged; }
// -----------------------------------------------------------------------
void clearWithOpenGL(const sp<const DisplayDevice>& hw, const Region& clip) const;
void setFiltering(bool filtering);
bool getFiltering() const;
// only for debugging
inline const sp<GraphicBuffer>& getActiveBuffer() const { return mActiveBuffer; }
inline const State& getDrawingState() const { return mDrawingState; }
inline const State& getCurrentState() const { return mCurrentState; }
inline State& getCurrentState() { return mCurrentState; }
/* always call base class first */
void dump(String8& result, Colorizer& colorizer) const;
void dumpFrameStats(String8& result) const;
void clearFrameStats();
void logFrameStats();
void getFrameStats(FrameStats* outStats) const;
protected:
// constant
sp<SurfaceFlinger> mFlinger;
virtual void onFirstRef();
/*
* Trivial class, used to ensure that mFlinger->onLayerDestroyed(mLayer)
* is called.
*/
class LayerCleaner {
sp<SurfaceFlinger> mFlinger;
wp<Layer> mLayer;
protected:
~LayerCleaner();
public:
LayerCleaner(const sp<SurfaceFlinger>& flinger, const sp<Layer>& layer);
};
private:
// Interface implementation for SurfaceFlingerConsumer::ContentsChangedListener
virtual void onFrameAvailable(const BufferItem& item) override;
virtual void onFrameReplaced(const BufferItem& item) override;
virtual void onSidebandStreamChanged() override;
void commitTransaction();
// needsLinearFiltering - true if this surface's state requires filtering
bool needsFiltering(const sp<const DisplayDevice>& hw) const;
uint32_t getEffectiveUsage(uint32_t usage) const;
FloatRect computeCrop(const sp<const DisplayDevice>& hw) const;
bool isCropped() const;
static bool getOpacityForFormat(uint32_t format);
// drawing
void clearWithOpenGL(const sp<const DisplayDevice>& hw, const Region& clip,
float r, float g, float b, float alpha) const;
void drawWithOpenGL(const sp<const DisplayDevice>& hw, const Region& clip,
bool useIdentityTransform) const;
// Temporary - Used only for LEGACY camera mode.
uint32_t getProducerStickyTransform() const;
// -----------------------------------------------------------------------
// constants
sp<SurfaceFlingerConsumer> mSurfaceFlingerConsumer;
sp<IGraphicBufferProducer> mProducer;
uint32_t mTextureName; // from GLES
bool mPremultipliedAlpha;
String8 mName;
PixelFormat mFormat;
// these are protected by an external lock
State mCurrentState;
State mDrawingState;
volatile int32_t mTransactionFlags;
// thread-safe
volatile int32_t mQueuedFrames;
volatile int32_t mSidebandStreamChanged; // used like an atomic boolean
FrameTracker mFrameTracker;
// main thread
sp<GraphicBuffer> mActiveBuffer;
sp<NativeHandle> mSidebandStream;
Rect mCurrentCrop;
uint32_t mCurrentTransform;
uint32_t mCurrentScalingMode;
bool mCurrentOpacity;
bool mRefreshPending;
bool mFrameLatencyNeeded;
// Whether filtering is forced on or not
bool mFiltering;
// Whether filtering is needed b/c of the drawingstate
bool mNeedsFiltering;
// The mesh used to draw the layer in GLES composition mode
mutable Mesh mMesh;
// The texture used to draw the layer in GLES composition mode
mutable Texture mTexture;
// page-flip thread (currently main thread)
bool mProtectedByApp; // application requires protected path to external sink
// protected by mLock
mutable Mutex mLock;
// Set to true once we've returned this surface's handle
mutable bool mHasSurface;
const wp<Client> mClientRef;
// This layer can be a cursor on some displays.
bool mPotentialCursor;
// Local copy of the queued contents of the incoming BufferQueue
mutable Mutex mQueueItemLock;
Condition mQueueItemCondition;
Vector<BufferItem> mQueueItems;
uint64_t mLastFrameNumberReceived;
bool mUpdateTexImageFailed; // This is only modified from the main thread
};
// ---------------------------------------------------------------------------
}; // namespace android
#endif // ANDROID_LAYER_H
|