1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
|
/*
* Copyright (C) 2011 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "LayerRejecter.h"
#include <gui/BufferItem.h>
#include <system/window.h>
#include "clz.h"
#define DEBUG_RESIZE 0
namespace android {
LayerRejecter::LayerRejecter(Layer::State& front,
Layer::State& current,
bool& recomputeVisibleRegions,
bool stickySet,
const char* name,
int32_t overrideScalingMode,
bool& freezePositionUpdates)
: mFront(front),
mCurrent(current),
mRecomputeVisibleRegions(recomputeVisibleRegions),
mStickyTransformSet(stickySet),
mName(name),
mOverrideScalingMode(overrideScalingMode),
mFreezeGeometryUpdates(freezePositionUpdates) {}
bool LayerRejecter::reject(const sp<GraphicBuffer>& buf, const BufferItem& item) {
if (buf == NULL) {
return false;
}
uint32_t bufWidth = buf->getWidth();
uint32_t bufHeight = buf->getHeight();
// check that we received a buffer of the right size
// (Take the buffer's orientation into account)
if (item.mTransform & Transform::ROT_90) {
swap(bufWidth, bufHeight);
}
int actualScalingMode = mOverrideScalingMode >= 0 ? mOverrideScalingMode : item.mScalingMode;
bool isFixedSize = actualScalingMode != NATIVE_WINDOW_SCALING_MODE_FREEZE;
if (mFront.active != mFront.requested) {
if (isFixedSize || (bufWidth == mFront.requested.w && bufHeight == mFront.requested.h)) {
// Here we pretend the transaction happened by updating the
// current and drawing states. Drawing state is only accessed
// in this thread, no need to have it locked
mFront.active = mFront.requested;
// We also need to update the current state so that
// we don't end-up overwriting the drawing state with
// this stale current state during the next transaction
//
// NOTE: We don't need to hold the transaction lock here
// because State::active is only accessed from this thread.
mCurrent.active = mFront.active;
mCurrent.modified = true;
// recompute visible region
mRecomputeVisibleRegions = true;
mFreezeGeometryUpdates = false;
if (mFront.crop != mFront.requestedCrop) {
mFront.crop = mFront.requestedCrop;
mCurrent.crop = mFront.requestedCrop;
mRecomputeVisibleRegions = true;
}
if (mFront.finalCrop != mFront.requestedFinalCrop) {
mFront.finalCrop = mFront.requestedFinalCrop;
mCurrent.finalCrop = mFront.requestedFinalCrop;
mRecomputeVisibleRegions = true;
}
}
ALOGD_IF(DEBUG_RESIZE,
"[%s] latchBuffer/reject: buffer (%ux%u, tr=%02x), scalingMode=%d\n"
" drawing={ active ={ wh={%4u,%4u} crop={%4d,%4d,%4d,%4d} (%4d,%4d) "
"}\n"
" requested={ wh={%4u,%4u} }}\n",
mName, bufWidth, bufHeight, item.mTransform, item.mScalingMode, mFront.active.w,
mFront.active.h, mFront.crop.left, mFront.crop.top, mFront.crop.right,
mFront.crop.bottom, mFront.crop.getWidth(), mFront.crop.getHeight(),
mFront.requested.w, mFront.requested.h);
}
if (!isFixedSize && !mStickyTransformSet) {
if (mFront.active.w != bufWidth || mFront.active.h != bufHeight) {
// reject this buffer
ALOGE("[%s] rejecting buffer: "
"bufWidth=%d, bufHeight=%d, front.active.{w=%d, h=%d}",
mName, bufWidth, bufHeight, mFront.active.w, mFront.active.h);
return true;
}
}
// if the transparent region has changed (this test is
// conservative, but that's fine, worst case we're doing
// a bit of extra work), we latch the new one and we
// trigger a visible-region recompute.
//
// We latch the transparent region here, instead of above where we latch
// the rest of the geometry because it is only content but not necessarily
// resize dependent.
if (!mFront.activeTransparentRegion.isTriviallyEqual(mFront.requestedTransparentRegion)) {
mFront.activeTransparentRegion = mFront.requestedTransparentRegion;
// We also need to update the current state so that
// we don't end-up overwriting the drawing state with
// this stale current state during the next transaction
//
// NOTE: We don't need to hold the transaction lock here
// because State::active is only accessed from this thread.
mCurrent.activeTransparentRegion = mFront.activeTransparentRegion;
// recompute visible region
mRecomputeVisibleRegions = true;
}
return false;
}
} // namespace android
|