1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
|
/*
* Copyright (C) 2012 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#define ATRACE_TAG ATRACE_TAG_GRAPHICS
//#define LOG_NDEBUG 0
#include "SurfaceFlingerConsumer.h"
#include "Layer.h"
#include <private/gui/SyncFeatures.h>
#include <gui/BufferItem.h>
#include <gui/BufferQueue.h>
#include <utils/Errors.h>
#include <utils/NativeHandle.h>
#include <utils/Trace.h>
namespace android {
// ---------------------------------------------------------------------------
status_t SurfaceFlingerConsumer::updateTexImage(BufferRejecter* rejecter,
const DispSync& dispSync, bool* autoRefresh, bool* queuedBuffer,
uint64_t maxFrameNumber)
{
ATRACE_CALL();
ALOGV("updateTexImage");
Mutex::Autolock lock(mMutex);
if (mAbandoned) {
ALOGE("updateTexImage: GLConsumer is abandoned!");
return NO_INIT;
}
// Make sure the EGL state is the same as in previous calls.
status_t err = checkAndUpdateEglStateLocked();
if (err != NO_ERROR) {
return err;
}
BufferItem item;
// Acquire the next buffer.
// In asynchronous mode the list is guaranteed to be one buffer
// deep, while in synchronous mode we use the oldest buffer.
err = acquireBufferLocked(&item, computeExpectedPresent(dispSync),
maxFrameNumber);
if (err != NO_ERROR) {
if (err == BufferQueue::NO_BUFFER_AVAILABLE) {
err = NO_ERROR;
} else if (err == BufferQueue::PRESENT_LATER) {
// return the error, without logging
} else {
ALOGE("updateTexImage: acquire failed: %s (%d)",
strerror(-err), err);
}
return err;
}
if (autoRefresh) {
*autoRefresh = item.mAutoRefresh;
}
if (queuedBuffer) {
*queuedBuffer = item.mQueuedBuffer;
}
// We call the rejecter here, in case the caller has a reason to
// not accept this buffer. This is used by SurfaceFlinger to
// reject buffers which have the wrong size
int slot = item.mSlot;
if (rejecter && rejecter->reject(mSlots[slot].mGraphicBuffer, item)) {
releaseBufferLocked(slot, mSlots[slot].mGraphicBuffer, EGL_NO_SYNC_KHR);
return BUFFER_REJECTED;
}
// Release the previous buffer.
#ifdef USE_HWC2
err = updateAndReleaseLocked(item, &mPendingRelease);
#else
err = updateAndReleaseLocked(item);
#endif
if (err != NO_ERROR) {
return err;
}
if (!SyncFeatures::getInstance().useNativeFenceSync()) {
// Bind the new buffer to the GL texture.
//
// Older devices require the "implicit" synchronization provided
// by glEGLImageTargetTexture2DOES, which this method calls. Newer
// devices will either call this in Layer::onDraw, or (if it's not
// a GL-composited layer) not at all.
err = bindTextureImageLocked();
}
return err;
}
status_t SurfaceFlingerConsumer::bindTextureImage()
{
Mutex::Autolock lock(mMutex);
return bindTextureImageLocked();
}
status_t SurfaceFlingerConsumer::acquireBufferLocked(BufferItem* item,
nsecs_t presentWhen, uint64_t maxFrameNumber) {
status_t result = GLConsumer::acquireBufferLocked(item, presentWhen,
maxFrameNumber);
if (result == NO_ERROR) {
mTransformToDisplayInverse = item->mTransformToDisplayInverse;
mSurfaceDamage = item->mSurfaceDamage;
}
return result;
}
bool SurfaceFlingerConsumer::getTransformToDisplayInverse() const {
Mutex::Autolock lock(mMutex);
return mTransformToDisplayInverse;
}
const Region& SurfaceFlingerConsumer::getSurfaceDamage() const {
return mSurfaceDamage;
}
sp<NativeHandle> SurfaceFlingerConsumer::getSidebandStream() const {
return mConsumer->getSidebandStream();
}
// We need to determine the time when a buffer acquired now will be
// displayed. This can be calculated:
// time when previous buffer's actual-present fence was signaled
// + current display refresh rate * HWC latency
// + a little extra padding
//
// Buffer producers are expected to set their desired presentation time
// based on choreographer time stamps, which (coming from vsync events)
// will be slightly later then the actual-present timing. If we get a
// desired-present time that is unintentionally a hair after the next
// vsync, we'll hold the frame when we really want to display it. We
// need to take the offset between actual-present and reported-vsync
// into account.
//
// If the system is configured without a DispSync phase offset for the app,
// we also want to throw in a bit of padding to avoid edge cases where we
// just barely miss. We want to do it here, not in every app. A major
// source of trouble is the app's use of the display's ideal refresh time
// (via Display.getRefreshRate()), which could be off of the actual refresh
// by a few percent, with the error multiplied by the number of frames
// between now and when the buffer should be displayed.
//
// If the refresh reported to the app has a phase offset, we shouldn't need
// to tweak anything here.
nsecs_t SurfaceFlingerConsumer::computeExpectedPresent(const DispSync& dispSync)
{
// The HWC doesn't currently have a way to report additional latency.
// Assume that whatever we submit now will appear right after the flip.
// For a smart panel this might be 1. This is expressed in frames,
// rather than time, because we expect to have a constant frame delay
// regardless of the refresh rate.
const uint32_t hwcLatency = 0;
// Ask DispSync when the next refresh will be (CLOCK_MONOTONIC).
const nsecs_t nextRefresh = dispSync.computeNextRefresh(hwcLatency);
// The DispSync time is already adjusted for the difference between
// vsync and reported-vsync (SurfaceFlinger::dispSyncPresentTimeOffset), so
// we don't need to factor that in here. Pad a little to avoid
// weird effects if apps might be requesting times right on the edge.
nsecs_t extraPadding = 0;
if (SurfaceFlinger::vsyncPhaseOffsetNs == 0) {
extraPadding = 1000000; // 1ms (6% of 60Hz)
}
return nextRefresh + extraPadding;
}
sp<Fence> SurfaceFlingerConsumer::getPrevFinalReleaseFence() const {
Mutex::Autolock lock(mMutex);
return ConsumerBase::mPrevFinalReleaseFence;
}
#ifdef USE_HWC2
void SurfaceFlingerConsumer::setReleaseFence(const sp<Fence>& fence)
{
if (!mPendingRelease.isPending) {
GLConsumer::setReleaseFence(fence);
return;
}
auto currentTexture = mPendingRelease.currentTexture;
if (fence->isValid() &&
currentTexture != BufferQueue::INVALID_BUFFER_SLOT) {
status_t result = addReleaseFence(currentTexture,
mPendingRelease.graphicBuffer, fence);
ALOGE_IF(result != NO_ERROR, "setReleaseFence: failed to add the"
" fence: %s (%d)", strerror(-result), result);
}
}
bool SurfaceFlingerConsumer::releasePendingBuffer()
{
if (!mPendingRelease.isPending) {
ALOGV("Pending buffer already released");
return false;
}
ALOGV("Releasing pending buffer");
Mutex::Autolock lock(mMutex);
status_t result = releaseBufferLocked(mPendingRelease.currentTexture,
mPendingRelease.graphicBuffer, mPendingRelease.display,
mPendingRelease.fence);
ALOGE_IF(result < NO_ERROR, "releasePendingBuffer failed: %s (%d)",
strerror(-result), result);
mPendingRelease = PendingRelease();
return true;
}
#endif
void SurfaceFlingerConsumer::setContentsChangedListener(
const wp<ContentsChangedListener>& listener) {
setFrameAvailableListener(listener);
Mutex::Autolock lock(mMutex);
mContentsChangedListener = listener;
}
void SurfaceFlingerConsumer::onSidebandStreamChanged() {
sp<ContentsChangedListener> listener;
{ // scope for the lock
Mutex::Autolock lock(mMutex);
ALOG_ASSERT(mFrameAvailableListener.unsafe_get() == mContentsChangedListener.unsafe_get());
listener = mContentsChangedListener.promote();
}
if (listener != NULL) {
listener->onSidebandStreamChanged();
}
}
void SurfaceFlingerConsumer::onDisconnect() {
sp<Layer> l = mLayer.promote();
if (l.get()) {
l->onDisconnect();
}
}
void SurfaceFlingerConsumer::addAndGetFrameTimestamps(
const NewFrameEventsEntry* newTimestamps,
FrameEventHistoryDelta *outDelta) {
sp<Layer> l = mLayer.promote();
if (l.get()) {
l->addAndGetFrameTimestamps(newTimestamps, outDelta);
}
}
// ---------------------------------------------------------------------------
}; // namespace android
|