/* Copyright (c) Imagination Technologies Ltd. * * The contents of this file are subject to the MIT license as set out below. * * Permission is hereby granted, free of charge, to any person obtaining a copy * of this software and associated documentation files (the "Software"), to deal * in the Software without restriction, including without limitation the rights * to use, copy, modify, merge, publish, distribute, sublicense, and/or sell * copies of the Software, and to permit persons to whom the Software is * furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice shall be included in * all copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE * AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN * THE SOFTWARE. */ #ifndef HAL_PUBLIC_H #define HAL_PUBLIC_H /* Authors of third party hardware composer (HWC) modules will need to include * this header to access functionality in the gralloc and framebuffer HALs. */ #include #include #define ALIGN(x,a) (((x) + (a) - 1L) & ~((a) - 1L)) #define HW_ALIGN 16 /* This can be tuned down as appropriate for the SOC. * * IMG formats are usually a single sub-alloc. * Some OEM video formats are two sub-allocs (Y, UV planes). * Future OEM video formats might be three sub-allocs (Y, U, V planes). */ #define MAX_SUB_ALLOCS 3 /* Format is not YCbCr (e.g. a RGB format) - bIsYUVFormat should be false */ #define YUV_CHROMA_ORDER_NONE 0 /* Cb follows Y */ #define YUV_CHROMA_ORDER_CBCR_UV 1 /* Cr follows Y */ #define YUV_CHROMA_ORDER_CRCB_VU 2 typedef struct { native_handle_t base; /* These fields can be sent cross process. They are also valid * to duplicate within the same process. * * A table is stored within psPrivateData on gralloc_module_t (this * is obviously per-process) which maps stamps to a mapped * PVRSRV_CLIENT_MEM_INFO in that process. Each map entry has a lock * count associated with it, satisfying the requirements of the * Android API. This also prevents us from leaking maps/allocations. * * This table has entries inserted either by alloc() * (alloc_device_t) or map() (gralloc_module_t). Entries are removed * by free() (alloc_device_t) and unmap() (gralloc_module_t). * * As a special case for framebuffer_device_t, framebuffer_open() * will add and framebuffer_close() will remove from this table. */ #define IMG_NATIVE_HANDLE_NUMFDS MAX_SUB_ALLOCS /* The `fd' field is used to "export" a meminfo to another process. * Therefore, it is allocated by alloc_device_t, and consumed by * gralloc_module_t. The framebuffer_device_t does not need a handle, * and the special value IMG_FRAMEBUFFER_FD is used instead. */ int fd[MAX_SUB_ALLOCS]; #define IMG_NATIVE_HANDLE_NUMINTS \ ((sizeof(unsigned long long) / sizeof(int)) + 5 + MAX_SUB_ALLOCS + 1 + MAX_SUB_ALLOCS + MAX_SUB_ALLOCS) /* A KERNEL unique identifier for any exported kernel meminfo. Each * exported kernel meminfo will have a unique stamp, but note that in * userspace, several meminfos across multiple processes could have * the same stamp. As the native_handle can be dup(2)'d, there could be * multiple handles with the same stamp but different file descriptors. */ unsigned long long ui64Stamp; /* This is used for buffer usage validation when locking a buffer, * and also in WSEGL (for the composition bypass feature). */ int usage; /* In order to do efficient cache flushes we need the buffer dimensions * and format. These are available on the ANativeWindowBuffer, * but the platform doesn't pass them down to the graphics HAL. */ int iWidth; int iHeight; int iFormat; unsigned int uiBpp; /* The ion allocation path doesn't allow for the allocation size and * mapping flags to be communicated cross-process automatically. * Cache these here so we can map buffers in client processes. */ unsigned int uiAllocSize[MAX_SUB_ALLOCS]; unsigned int uiFlags; /* For multi-planar allocations, there will be multiple hstrides */ int aiStride[MAX_SUB_ALLOCS]; /* For multi-planar allocations, there will be multiple vstrides */ int aiVStride[MAX_SUB_ALLOCS]; } __attribute__((aligned(sizeof(int)),packed)) IMG_native_handle_t; typedef struct { int l, t, w, h; } IMG_write_lock_rect_t; typedef int (*IMG_buffer_format_compute_params_pfn)( unsigned int uiPlane, int *piWidth, int *piHeight, int *piStride, int *piVStride, unsigned long *pulPlaneOffset); typedef struct IMG_buffer_format_public_t { /* Buffer formats are returned as a linked list */ struct IMG_buffer_format_public_t *psNext; /* HAL_PIXEL_FORMAT_... enumerant */ int iHalPixelFormat; /* WSEGL_PIXELFORMAT_... enumerant */ int iWSEGLPixelFormat; /* Friendly name for format */ const char *const szName; /* Bits (not bytes) per pixel */ unsigned int uiBpp; /* Supported HW usage bits. If this is GRALLOC_USAGE_HW_MASK, all usages * are supported. Used for HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED. */ int iSupportedUsage; /* YUV output format */ int bIsYUVFormat; /* YCBCR_ORDERING_* defined the order of the Cb/Cr values */ int eYUVChromaOrder; /* Utility function for adjusting YUV per-plane parameters */ IMG_buffer_format_compute_params_pfn pfnComputeParams; } IMG_buffer_format_public_t; typedef struct { /* Base memtrack record, copied to caller */ struct memtrack_record base; /* Record type, for filtering cached records */ enum memtrack_type eType; /* Process ID, for filtering cached records */ pid_t pid; } IMG_memtrack_record_public_t; typedef struct IMG_gralloc_module_public_t { gralloc_module_t base; /* This function is deprecated and might be NULL. Do not use it. */ int (*GetPhyAddrs)(gralloc_module_t const* module, buffer_handle_t handle, void **ppvPhyAddr); /* Obtain HAL's registered format list */ const IMG_buffer_format_public_t *(*GetBufferFormats)(void); int (*GetImplementationFormat) (struct IMG_gralloc_module_public_t const *psGrallocModule, int usage); int (*GetMemTrackRecords)(struct IMG_gralloc_module_public_t const *module, IMG_memtrack_record_public_t **ppsRecords, size_t *puNumRecords); /* Custom-blit components in lieu of overlay hardware */ int (*Blit)(struct IMG_gralloc_module_public_t const *module, buffer_handle_t src, void *dest[MAX_SUB_ALLOCS], int format); int (*Blit2)(struct IMG_gralloc_module_public_t const *module, buffer_handle_t src, buffer_handle_t dest, int w, int h, int x, int y); int (*Blit3)(struct IMG_gralloc_module_public_t const *module, unsigned long long ui64SrcStamp, int iSrcWidth, int iSrcHeight, int iSrcFormat, int eSrcRotation, buffer_handle_t dest, int eDestRotation); } IMG_gralloc_module_public_t; /** * pixel format definitions */ enum { /* * 0x100 = 0x1FF * * This range is reserved for pixel formats that are specific to the HAL * implementation. Implementations can use any value in this range to * communicate video pixel formats between their HAL modules. These * formats must not have an alpha channel. Additionally, an EGLimage * created from a gralloc buffer of one of these formats must be * supported for use with the GL_OES_EGL_image_external OpenGL ES * extension. */ /* * These are vendor specific pixel format, by (informal) convention * IMGTec formats start from the top of the range, TI formats start from * the bottom */ HAL_PIXEL_FORMAT_TI_NV12 = 0x100, HAL_PIXEL_FORMAT_TI_UNUSED = 0x101, HAL_PIXEL_FORMAT_TI_NV12_1D = 0x102, HAL_PIXEL_FORMAT_TI_Y8 = 0x103, HAL_PIXEL_FORMAT_TI_Y16 = 0x104, HAL_PIXEL_FORMAT_TI_UYVY = 0x105, HAL_PIXEL_FORMAT_BGRX_8888 = 0x1FF, /* generic format missing from Android list, not specific to vendor * implementation */ HAL_PIXEL_FORMAT_NV12 = 0x3231564E, // FourCC for NV12 }; #endif /* HAL_PUBLIC_H */