summaryrefslogtreecommitdiffstats
blob: 9ac2d64a57520a3f86c07c1b1d01ea0c1e90b8fe (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
/* Copyright (c) Imagination Technologies Ltd.
 *
 * The contents of this file are subject to the MIT license as set out below.
 *
 * Permission is hereby granted, free of charge, to any person obtaining a copy
 * of this software and associated documentation files (the "Software"), to deal
 * in the Software without restriction, including without limitation the rights
 * to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
 * copies of the Software, and to permit persons to whom the Software is
 * furnished to do so, subject to the following conditions:
 *
 * The above copyright notice and this permission notice shall be included in
 * all copies or substantial portions of the Software.
 *
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
 * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
 * AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
 * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
 * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN
 * THE SOFTWARE.
 */

#ifndef HAL_PUBLIC_H
#define HAL_PUBLIC_H

/* Authors of third party hardware composer (HWC) modules will need to include
 * this header to access functionality in the gralloc and framebuffer HALs.
 */

#include <hardware/gralloc.h>
#include <hardware/memtrack.h>

#define ALIGN(x,a)	(((x) + (a) - 1L) & ~((a) - 1L))
#define HW_ALIGN	8

/* This can be tuned down as appropriate for the SOC.
 *
 * IMG formats are usually a single sub-alloc.
 * Some OEM video formats are two sub-allocs (Y, UV planes).
 * Future OEM video formats might be three sub-allocs (Y, U, V planes).
 */
#define MAX_SUB_ALLOCS 3

/* Format is not YCbCr (e.g. a RGB format) - bIsYUVFormat should be false */
#define YUV_CHROMA_ORDER_NONE 0
/* Cb follows Y */
#define YUV_CHROMA_ORDER_CBCR_UV 1
/* Cr follows Y */
#define YUV_CHROMA_ORDER_CRCB_VU 2

typedef struct
{
	native_handle_t base;

	/* These fields can be sent cross process. They are also valid
	 * to duplicate within the same process.
	 *
	 * A table is stored within psPrivateData on gralloc_module_t (this
	 * is obviously per-process) which maps stamps to a mapped
	 * PVRSRV_CLIENT_MEM_INFO in that process. Each map entry has a lock
	 * count associated with it, satisfying the requirements of the
	 * Android API. This also prevents us from leaking maps/allocations.
	 *
	 * This table has entries inserted either by alloc()
	 * (alloc_device_t) or map() (gralloc_module_t). Entries are removed
	 * by free() (alloc_device_t) and unmap() (gralloc_module_t).
	 *
	 * As a special case for framebuffer_device_t, framebuffer_open()
	 * will add and framebuffer_close() will remove from this table.
	 */

#define IMG_NATIVE_HANDLE_NUMFDS MAX_SUB_ALLOCS
	/* The `fd' field is used to "export" a meminfo to another process.
	 * Therefore, it is allocated by alloc_device_t, and consumed by
	 * gralloc_module_t. The framebuffer_device_t does not need a handle,
	 * and the special value IMG_FRAMEBUFFER_FD is used instead.
	 */
	int fd[MAX_SUB_ALLOCS];

#define IMG_NATIVE_HANDLE_NUMINTS \
	((sizeof(unsigned long long) / sizeof(int)) + 5 + MAX_SUB_ALLOCS + 1 + MAX_SUB_ALLOCS + MAX_SUB_ALLOCS)
	/* A KERNEL unique identifier for any exported kernel meminfo. Each
	 * exported kernel meminfo will have a unique stamp, but note that in
	 * userspace, several meminfos across multiple processes could have
	 * the same stamp. As the native_handle can be dup(2)'d, there could be
	 * multiple handles with the same stamp but different file descriptors.
	 */
	unsigned long long ui64Stamp;

	/* This is used for buffer usage validation when locking a buffer,
	 * and also in WSEGL (for the composition bypass feature).
	 */
	int usage;

	/* In order to do efficient cache flushes we need the buffer dimensions
	 * and format. These are available on the ANativeWindowBuffer,
	 * but the platform doesn't pass them down to the graphics HAL.
	 */
	int iWidth;
	int iHeight;
	int iFormat;
	unsigned int uiBpp;

	/* The ion allocation path doesn't allow for the allocation size and
	 * mapping flags to be communicated cross-process automatically.
	 * Cache these here so we can map buffers in client processes.
	 */
	unsigned int uiAllocSize[MAX_SUB_ALLOCS];
	unsigned int uiFlags;
	/* For multi-planar allocations, there will be multiple hstrides */
	int aiStride[MAX_SUB_ALLOCS];

	/* For multi-planar allocations, there will be multiple vstrides */
	int aiVStride[MAX_SUB_ALLOCS];

}
__attribute__((aligned(sizeof(int)),packed)) IMG_native_handle_t;

typedef struct
{
	int l, t, w, h;
}
IMG_write_lock_rect_t;

typedef int (*IMG_buffer_format_compute_params_pfn)(
	unsigned int uiPlane, int *piWidth, int *piHeight,
	int *piStride, int *piVStride, unsigned long *pulPlaneOffset);

typedef struct IMG_buffer_format_public_t
{
	/* Buffer formats are returned as a linked list */
	struct IMG_buffer_format_public_t *psNext;

	/* HAL_PIXEL_FORMAT_... enumerant */
	int iHalPixelFormat;

	/* WSEGL_PIXELFORMAT_... enumerant */
	int iWSEGLPixelFormat;

	/* Friendly name for format */
	const char *const szName;

	/* Bits (not bytes) per pixel */
	unsigned int uiBpp;

	/* Supported HW usage bits. If this is GRALLOC_USAGE_HW_MASK, all usages
	 * are supported. Used for HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED.
	 */
	int iSupportedUsage;

	/* YUV output format */
	int bIsYUVFormat;

	/* YCBCR_ORDERING_* defined the order of the Cb/Cr values */
	int eYUVChromaOrder;

	/* Utility function for adjusting YUV per-plane parameters */
	IMG_buffer_format_compute_params_pfn pfnComputeParams;
}
IMG_buffer_format_public_t;

typedef struct
{
	/* Base memtrack record, copied to caller */
	struct memtrack_record	base;

	/* Record type, for filtering cached records */
	enum memtrack_type		eType;

	/* Process ID, for filtering cached records */
	pid_t					pid;
}
IMG_memtrack_record_public_t;

typedef struct IMG_gralloc_module_public_t
{
	gralloc_module_t base;

	/* This function is deprecated and might be NULL. Do not use it. */
	int (*GetPhyAddrs)(gralloc_module_t const* module,
					   buffer_handle_t handle, void **ppvPhyAddr);

	/* Obtain HAL's registered format list */
	const IMG_buffer_format_public_t *(*GetBufferFormats)(void);

	int (*GetImplementationFormat) (struct IMG_gralloc_module_public_t const *psGrallocModule, int usage);

	int (*GetMemTrackRecords)(struct IMG_gralloc_module_public_t const *module,
							  IMG_memtrack_record_public_t **ppsRecords,
							  size_t *puNumRecords);

	/* Custom-blit components in lieu of overlay hardware */
	int (*Blit)(struct IMG_gralloc_module_public_t const *module,
				buffer_handle_t src,
				void *dest[MAX_SUB_ALLOCS], int format);

	int (*Blit2)(struct IMG_gralloc_module_public_t const *module,
				 buffer_handle_t src, buffer_handle_t dest,
				 int w, int h, int x, int y);

	int (*Blit3)(struct IMG_gralloc_module_public_t const *module,
				 unsigned long long ui64SrcStamp, int iSrcWidth,
				 int iSrcHeight, int iSrcFormat, int eSrcRotation,
				 buffer_handle_t dest, int eDestRotation);
}
IMG_gralloc_module_public_t;

/**
 * pixel format definitions
 */

enum {
	/*
	 * 0x100 = 0x1FF
	 *
	 * This range is reserved for pixel formats that are specific to the HAL
	 * implementation. Implementations can use any value in this range to
	 * communicate video pixel formats between their HAL modules. These
	 * formats must not have an alpha channel. Additionally, an EGLimage
	 * created from a gralloc buffer of one of these formats must be
	 * supported for use with the GL_OES_EGL_image_external OpenGL ES
	 * extension.
	 */

	/*
	 * These are vendor specific pixel format, by (informal) convention
	 * IMGTec formats start from the top of the range, TI formats start from
	 * the bottom
	 */
	HAL_PIXEL_FORMAT_TI_NV12 = 0x100,
	HAL_PIXEL_FORMAT_TI_UNUSED = 0x101,
	HAL_PIXEL_FORMAT_TI_NV12_1D = 0x102,
	HAL_PIXEL_FORMAT_TI_Y8 = 0x103,
	HAL_PIXEL_FORMAT_TI_Y16 = 0x104,
	HAL_PIXEL_FORMAT_TI_UYVY = 0x105,
	HAL_PIXEL_FORMAT_BGRX_8888 = 0x1FF,

	/* generic format missing from Android list, not specific to vendor
	 * implementation
	 */
	HAL_PIXEL_FORMAT_NV12 = 0x3231564E, // FourCC for NV12
};

#endif /* HAL_PUBLIC_H */