blob: 731c53a2e1d4ea2933a41195c9fb701e5dd053ae (
plain) (
tree)
|
|
/*
* Copyright (C) Texas Instruments Incorporated - http://www.ti.com/
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#pragma once
#include <string>
#include <cstdint>
#include <drm/drm_fourcc.h>
#include <linux/types.h>
#include "hal_public.h"
static inline std::string HAL_FMT(uint32_t format)
{
switch (format) {
case HAL_PIXEL_FORMAT_TI_NV12: return "NV12";
case HAL_PIXEL_FORMAT_TI_NV12_1D: return "NV12";
case HAL_PIXEL_FORMAT_YV12: return "YV12";
case HAL_PIXEL_FORMAT_BGRX_8888: return "xRGB32";
case HAL_PIXEL_FORMAT_RGBX_8888: return "xBGR32";
case HAL_PIXEL_FORMAT_BGRA_8888: return "ARGB32";
case HAL_PIXEL_FORMAT_RGBA_8888: return "ABGR32";
case HAL_PIXEL_FORMAT_RGB_565: return "RGB565";
default: return "??";
}
}
static inline std::string DRM_FMT(uint32_t format)
{
switch (format) {
case DRM_FORMAT_NV12: return "NV12";
case DRM_FORMAT_XRGB8888: return "xRGB32";
case DRM_FORMAT_ARGB8888: return "ARGB32";
case DRM_FORMAT_RGB565: return "RGB565";
default: return "??";
}
}
bool is_valid_format(uint32_t format);
bool is_rgb_format(uint32_t format);
bool is_bgr_format(uint32_t format);
bool is_nv12_format(uint32_t format);
bool is_opaque_format(uint32_t format);
uint32_t get_format_bpp(uint32_t format);
uint32_t convert_hal_to_dss_format(uint32_t format, bool blended);
uint32_t convert_hal_to_drm_format(uint32_t hal_format, bool blended);
uint32_t convert_hal_to_ocd_format(uint32_t hal_format);
uint32_t get_stride_from_format(uint32_t format, uint32_t width);
|