diff options
Diffstat (limited to 'README')
-rw-r--r-- | README | 11 |
1 files changed, 7 insertions, 4 deletions
@@ -190,8 +190,8 @@ XDAS_Int32 VIDDEC3_control(VIDDEC3_Handle codec, VIDDEC3_Cmd id, | |||
190 | * inBufs->descs[0].buf should have a virtual pointer | 190 | * inBufs->descs[0].buf should have a virtual pointer |
191 | * to the Input Buffer in QNX. In Linux, it | 191 | * to the Input Buffer in QNX. In Linux, it |
192 | * should have a DMA Buf FD to the Input Buffer. | 192 | * should have a DMA Buf FD to the Input Buffer. |
193 | * In Android, it should have the ptr returned from | 193 | * In Android, it should have the memheader pointer |
194 | * memplugin, and the memheader->offset should have | 194 | * and the memheader->offset should have |
195 | * the offset for the actual data within the input buffer; | 195 | * the offset for the actual data within the input buffer; |
196 | * memheader->offset = pInBufHeader->nOffset; | 196 | * memheader->offset = pInBufHeader->nOffset; |
197 | * @ param outBufs [in] : Pointer to Output Buffer Descriptor structure | 197 | * @ param outBufs [in] : Pointer to Output Buffer Descriptor structure |
@@ -199,8 +199,11 @@ XDAS_Int32 VIDDEC3_control(VIDDEC3_Handle codec, VIDDEC3_Cmd id, | |||
199 | * outBufs->descs[0].buf and outBufs->descs[1].buf | 199 | * outBufs->descs[0].buf and outBufs->descs[1].buf |
200 | * should have virtual pointers to the Output | 200 | * should have virtual pointers to the Output |
201 | * Luma and Chroma Buffers respectively in QNX. | 201 | * Luma and Chroma Buffers respectively in QNX. |
202 | * In Linux/Android, these fields should have | 202 | * In Linux these fields should have |
203 | * DMA Buf FDs to the Output Buffers. | 203 | * DMA Buf FDs to the Output Buffers. In Android |
204 | * these fields should have the memheader pointer, | ||
205 | * and the memheader->offset should have the offset | ||
206 | * for the actual data with in the outbuffer. | ||
204 | * @ param inArgs [in] : Pointer to Input Arguments structure | 207 | * @ param inArgs [in] : Pointer to Input Arguments structure |
205 | * of codec allocated using dce_alloc() API. | 208 | * of codec allocated using dce_alloc() API. |
206 | * @ param outArgs [out] : Pointer to Output Arguments structure | 209 | * @ param outArgs [out] : Pointer to Output Arguments structure |