diff options
Diffstat (limited to 'libdce.c')
-rw-r--r-- | libdce.c | 2 |
1 files changed, 1 insertions, 1 deletions
@@ -153,7 +153,7 @@ void *dce_alloc(int sz) | |||
153 | Beware: The last argument is a bit field. As of now only core ID | 153 | Beware: The last argument is a bit field. As of now only core ID |
154 | is considered to be there in the last 4 bits of the word | 154 | is considered to be there in the last 4 bits of the word |
155 | */ | 155 | */ |
156 | return (memplugin_alloc(sz, 1, MEM_TILER_1D, 0, IPU)); | 156 | return (memplugin_alloc(sz, 1, DEFAULT_REGION, 0, IPU)); |
157 | } | 157 | } |
158 | 158 | ||
159 | void dce_free(void *ptr) | 159 | void dce_free(void *ptr) |