summaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* libdce[Android]: Fix NULL pointer dereference in dce_buf_unlockAngela Stegmaier2017-07-171-1/+5
| | | | | | | | | | | | | | | | | In the case where dce_buf_lock fails due to dce_ipc_init failure, then MmRpcHandle is not guaranteed to be initialized and could result in a NULL pointer de-reference. In some use-cases where the IPUMM takes a longer time to come up, this was resulting in a crash, causing the Android media service to stop and restart several times. This patch fixes the NULL pointer de-reference by first checking if the IPC is initialized in dce_buf_unlock before calling the IPC API. This patch also has a minor cleanup of an un-used static global variable. Change-Id: Idb74fb60c0b9696a0be87e4808b537ebfc84cd7e Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
* libdce[Android]: Add dce_ipc_recover APIAngela Stegmaier2017-01-171-1/+8
| | | | | | | | | | | | | | | | | In case of remote core recovery due to remote core crash, the rpmsg-dce handle needs to be closed and re-opened since any handles that were open when the crash happened are marked as stale in the driver. This patch adds a new API that the user can call to close the rpmsg-dce handle so that recovery can happen. In case the user receives notification of a remote core crash, it can call the dce_ipc_recover() API to make sure that the rpmsg-dce handle that is opened during dce_buf_lock is closed so that a new one can be opened the next time. Change-Id: I8ebc19e308ffe7431b57c31cfecd469e171777f6 Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
* libdce[Android]: Defer rpmsg_dce device open till buffer lock phaseSunita Nadampalli2016-08-291-0/+9
| | | | | | | | | | | | In the current architecture, rpmsg_dce device is opened during memplugin_open(), which can be called from any process context. With Android system configured in SE Linux Enforcement mode, it is not allowed to open rpmsg_dce in any process other than mediaserver. Hence the device open logic is deferred till dce buffer lock API where the actual device ioctls are needed. Change-Id: Iedacfd3327e0ee975a8a492b057aac576d7f7c10 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
* libdce: Add mutex protection for dce_buf_lock/dce_buf_unlockSunita Nadampalli2015-01-301-0/+11
| | | | | | | | | | | | The dce_buf_lock and dce_buf_unlock are meant for any video buffer locking and unlocking with the GEM allocator. Currently, these methods are being called from libdce apis with ipc mutex held. In order to enable other media components to make use of these buffer lock/unlock apis, explicit ipc mutex protection is added. Change-Id: I6d63a4cdcffec62a346341ff515a7ebb03dea8c0 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
* libdce[Android]: Added support for DRM based Android mempluginSunita Nadampalli2014-11-171-0/+96
This patch adds memplugin implementation for GEM allocator and dce buffer locking via MmRPC for Android builds. Android memplugin implement memplugin interface for buffers with and without memheaders. This implementation is for DRM/GEM buffer allocations. And libdce_android implements GEM buffer registration and unregistration with MmRPC. Change-Id: Ie72c988a37f987446f7d7c1d97225295de73d305 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>