summaryrefslogtreecommitdiffstats
blob: 5d4ffa85dc538a97ff926bb406f41004afb1eb71 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
/*
 * Copyright (c) 2013, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

#ifndef __LIBDCE_H__
#define __LIBDCE_H__


#include <ti/sdo/ce/Engine.h>
#include <ti/sdo/ce/video3/viddec3.h>
#include <ti/sdo/ce/video2/videnc2.h>

#if defined(BUILDOS_LINUX)
/* avoid some messy stuff in xdc/std.h which leads to gcc issues */
#define xdc__ARGTOPTR
#define xdc__ARGTOFXN
#endif /* BUILDOS_LINUX */


/* DCE Error Types */
typedef enum dce_error_status {
    DCE_EOK = 0,
    DCE_EXDM_FAIL = -1,
    DCE_EOUT_OF_MEMORY = -2,
    DCE_EXDM_UNSUPPORTED = -3,
    DCE_EIPC_CREATE_FAIL = -4,
    DCE_EIPC_CALL_FAIL = -5,
    DCE_EINVALID_INPUT = -6,
    DCE_EOMAPDRM_FAIL = -7
} dce_error_status;


/* other than the codec-engine API, you must use the following two functions
 * to allocate the data structures passed to codec-engine APIs (other than the
 * raw input/output buffers which should be passed as virtual addresses in
 * TILER space
 */
void *dce_alloc(int sz);
void dce_free(void *ptr);


/*********************************** APIs for Linux ***********************************/
/************************ Initialization/Deinitialization APIs ************************/
/*=====================================================================================*/
/** dce_init                : Initialize DCE. Only Linux applications are expected to call.
 *
 * @ return                 : Pointer to omap_device structure.
 */
void *dce_init(void);

/*===============================================================*/
/** dce_deinit              : Deinitialize DCE. Only Linux applications are expected to call.
 *
 * @ param dev    [in]      : Pointer to omap_device structure.
 */
void dce_deinit(void *dev);

/************************ Input/Output Buffer Lock/Unlock APIs ************************/
/*=====================================================================================*/
/** dce_buf_lock            : Pin or lock Tiler Buffers which would be used by the codec
 *                            as reference buffers. API is specific to GLP.
 *
 * @ param num    [in]      : Number of buffers to be locked.
 * @ param handle [in]      : Pointer to array of DMA Buf FDs of the buffers to be locked.
 * @ return                 : DCE error status is returned.
 */
int dce_buf_lock(int num, size_t *handle);

/*=====================================================================================*/
/** dce_buf_unlock          : Unpin or unlock Tiler Buffers which were locked to be used
 *                            by the codec as reference buffers. API is specific to GLP.
 *
 * @ param num    [in]      : Number of buffers to be locked.
 * @ param handle [in]      : Pointer to array of DMA Buf FDs of the buffers to be locked.
 * @ return                 : DCE error status is returned.
 */
int dce_buf_unlock(int num, size_t *handle);

/******************************* OMAPDRM Get/Set FD APIs *******************************/
int dce_get_fd();

void dce_set_fd(int fd);


#endif /* __LIBDCE_H__ */