# SPDX-License-Identifier: GPL-2.0
VERSION = 5
PATCHLEVEL = 10
SUBLEVEL = 3
EXTRAVERSION =
NAME = Kleptomaniac Octopus
# *DOCUMENTATION*
# To see a list of typical targets execute "make help"
# More info can be located in ./README
# Comments in this file are targeted only to the developer, do not
# expect to learn how to build the kernel reading this file.
$(if $(filter __%, $(MAKECMDGOALS)), \
$(error targets prefixed with '__' are only for internal use))
# That's our default target when none is given on the command line
PHONY := __all
__all:
# We are using a recursive build, so we need to do a little thinking
# to get the ordering right.
#
# Most importantly: sub-Makefiles should only ever modify files in
# their own directory. If in some directory we have a dependency on
# a file in another dir (which doesn't happen often, but it's often
# unavoidable when linking the built-in.a targets which finally
# turn into vmlinux), we will call a sub make in that other dir, and
# after that we are sure that everything which is in that other dir
# is now up to date.
#
# The only cases where we need to modify files which have global
# effects are thus separated out and done before the recursive
# descending is started. They are now explicitly listed as the
# prepare rule.
ifneq ($(sub_make_done),1)
# Do not use make's built-in rules and variables
# (this increases performance and avoids hard-to-debug behaviour)
MAKEFLAGS += -rR
# Avoid funny character set dependencies
unexport LC_ALL
LC_COLLATE=C
LC_NUMERIC=C
export LC_COLLATE LC_NUMERIC
# Avoid interference with shell env settings
unexport GREP_OPTIONS
# Beautify output
# ---------------------------------------------------------------------------
#
# Normally, we echo the whole command before executing it. By making
# that echo $($(quiet)$(cmd)), we now have the possibility to set
# $(quiet) to choose other forms of output instead, e.g.
#
# quiet_cmd_cc_o_c = Compiling $(RELDIR)/$@
# cmd_cc_o_c = $(CC) $(c_flags) -c -o $@ $<
#
# If $(quiet) is empty, the whole command will be printed.
# If it is set to "quiet_", only the short version will be printed.
# If it is set to "silent_", nothing will be printed at all, since
# the variable $(silent_cmd_cc_o_c) doesn't exist.
#
# A simple variant is to prefix commands with $(Q) - that's useful
# for commands that shall be hidden in non-verbose mode.
#
# $(Q)ln $@ :<
#
# If KBUILD_VERBOSE equals 0 then the above command will be hidden.
# If KBUILD_VERBOSE equals 1 then the above command is displayed.
# If KBUILD_VERBOSE equals 2 then give the reason why each target is rebuilt.
#
# To put more focus on warnings, be less verbose as default
# Use 'make V=1' to see the full commands
ifeq ("$(origin V)", "command line")
KBUILD_VERBOSE = $(V)
endif
ifndef KBUILD_VERBOSE
KBUILD_VERBOSE = 0
endif
ifeq ($(KBUILD_VERBOSE),1)
quiet =
Q =
else
quiet=quiet_
Q = @
endif
# If the user is running make -s (silent mode), suppress echoing of
# commands
ifneq ($(findstring s,$(filter-out --%,$(MAKEFLAGS))),)
quiet=silent_
endif
export quiet Q KBUILD_VERBOSE
# Kbuild will save output files in the current working directory.
# This does not need to match to the root of the kernel source tree.
#
# For example, you can do this:
#
# cd /dir/to/store/output/files; make -f /dir/to/kernel/source/Makefile
#
# If you want to save output files in a different location, there are
# two syntaxes to specify it.
#
# 1) O=
# Use "make O=dir/to/store/output/files/"
#
# 2) Set KBUILD_OUTPUT
# Set the environment variable KBUILD_OUTPUT to point to the output directory.
# export KBUILD_OUTPUT=dir/to/store/output/files/; make
#
# The O= assignment takes precedence over the KBUILD_OUTPUT environment
# variable.
# Do we want to change the working directory?
ifeq ("$(origin O)", "command line")
KBUILD_OUTPUT := $(O)
endif
ifneq ($(KBUILD_OUTPUT),)
# Make's built-in functions such as $(abspath ...), $(realpath ...) cannot
# expand a shell special character '~'. We use a somewhat tedious way here.
abs_objtree := $(shell mkdir -p $(KBUILD_OUTPUT) && cd $(KBUILD_OUTPUT) && pwd)
$(if $(abs_objtree),, \
$(error failed to create output directory "$(KBUILD_OUTPUT)"))
# $(realpath ...) resolves symlinks
abs_objtree := $(realpath $(abs_objtree))
else
abs_objtree := $(CURDIR)
endif # ifneq ($(KBUILD_OUTPUT),)
ifeq ($(abs_objtree),$(CURDIR))
# Suppress "Entering directory ..." unless we are changing the work directory.
MAKEFLAGS += --no-print-directory
else
need-sub-make := 1
endif
abs_srctree := $(realpath $(dir $(lastword $(MAKEFILE_LIST))))
ifneq ($(words $(subst :, ,$(abs_srctree))), 1)
$(error source directory cannot contain spaces or colons)
endif
ifneq ($(abs_srctree),$(abs_objtree))
# Look for make include files relative to root of kernel src
#
# This does not become effective immediately because MAKEFLAGS is re-parsed
# once after the Makefile is read. We need to invoke sub-make.
MAKEFLAGS += --include-dir=$(abs_srctree)
need-sub-make := 1
endif
this-makefile := $(lastword $(MAKEFILE_LIST))
ifneq ($(filter 3.%,$(MAKE_VERSION)),)
# 'MAKEFLAGS += -rR' does not immediately become effective for GNU Make 3.x
# We need to invoke sub-make to avoid implicit rules in the top Makefile.
need-sub-make := 1
# Cancel implicit rules for this Makefile.
$(this-makefile): ;
endif
export abs_srctree abs_objtree
export sub_make_done := 1
ifeq ($(need-sub-make),1)
PHONY += $(MAKECMDGOALS) __sub-make
$(filter-out $(this-makefile), $(MAKECMDGOALS)) __all: __sub-make
@:
# Invoke a second make in the output directory, passing relevant variables
__sub-make:
$(Q)$(MAKE) -C $(abs_objtree) -f $(abs_srctree)/Makefile $(MAKECMDGOALS)
endif # need-sub-make
endif # sub_make_done
# We process the rest of the Makefile if this is the final invocation of make
ifeq ($(need-sub-make),)
# Do not print "Entering directory ...",
# but we want to display it when entering to the output directory
# so that IDEs/editors are able to understand relative filenames.
MAKEFLAGS += --no-print-directory
# Call a source code checker (by default, "sparse") as part of the
# C compilation.
#
# Use 'make C=1' to enable checking of only re-compiled files.
# Use 'make C=2' to enable checking of *all* source files, regardless
# of whether they are re-compiled or not.
#
# See the file "Documentation/dev-tools/sparse.rst" for more details,
# including where to get the "sparse" utility.
ifeq ("$(origin C)", "command line")
KBUILD_CHECKSRC = $(C)
endif
ifndef KBUILD_CHECKSRC
KBUILD_CHECKSRC = 0
endif
# Use make M=dir or set the environment variable KBUILD_EXTMOD to specify the
# directory of external module to build. Setting M= takes precedence.
ifeq ("$(origin M)", "command line")
KBUILD_EXTMOD := $(M)
endif
$(if $(word 2, $(KBUILD_EXTMOD)), \
$(error building multiple external modules is not supported))
export KBUILD_CHECKSRC KBUILD_EXTMOD
extmod-prefix = $(if $(KBUILD_EXTMOD),$(KBUILD_EXTMOD)/)
ifeq ($(abs_srctree),$(abs_objtree))
# building in the source tree
srctree := .
building_out_of_srctree :=
else
ifeq ($(abs_srctree)/,$(dir $(abs_objtree)))
# building in a subdirectory of the source tree
srctree := ..
else
srctree := $(abs_srctree)
endif
building_out_of_srctree := 1
endif
ifneq ($(KBUILD_ABS_SRCTREE),)
srctree := $(abs_srctree)
endif
objtree := .
VPATH := $(srctree)
export building_out_of_srctree srctree objtree VPATH
# To make sure we do not include .config for any of the *config targets
# catch them early, and hand them over to scripts/kconfig/Makefile
# It is allowed to specify more targets when calling make, including
# mixing *config targets and build targets.
# For example 'make oldconfig all'.
# Detect when mixed targets is specified, and make a second invocation
# of make so .config is not included in this case either (for *config).
version_h := include/generated/uapi/linux/version.h
old_version_h := include/linux/version.h
clean-targets := %clean mrproper cleandocs
no-dot-config-targets := $(clean-targets) \
cscope gtags TAGS tags help% %docs check% coccicheck \
$(version_h) headers headers_% archheaders archscripts \
%asm-generic kernelversion %src-pkg dt_binding_check \
outputmakefile
no-sync-config-targets := $(no-dot-config-targets) %install kernelrelease
single-targets := %.a %.i %.ko %.lds %.ll %.lst %.mod %.o %.s %.symtypes %/
config-build :=
mixed-build :=
need-config := 1
may-sync-config := 1
single-build :=
ifneq ($(filter $(no-dot-config-targets), $(MAKECMDGOALS)),)
ifeq ($(filter-out $(no-dot-config-targets), $(MAKECMDGOALS)),)
need-config :=
endif
endif
ifneq ($(filter $(no-sync-config-targets), $(MAKECMDGOALS)),)
ifeq ($(filter-out $(no-sync-config-targets), $(MAKECMDGOALS)),)
may-sync-config :=
endif
endif
ifneq ($(KBUILD_EXTMOD),)
may-sync-config :=
endif
ifeq ($(KBUILD_EXTMOD),)
ifneq ($(filter %config,$(MAKECMDGOALS)),)
config-build := 1
ifneq ($(words $(MAKECMDGOALS)),1)
mixed-build := 1
endif
endif
endif
# We cannot build single targets and the others at the same time
ifneq ($(filter $(single-targets), $(MAKECMDGOALS)),)
single-build := 1
ifneq ($(filter-out $(single-targets), $(MAKECMDGOALS)),)
mixed-build := 1
endif
endif
# For "make -j clean all", "make -j mrproper defconfig all", etc.
ifneq ($(filter $(clean-targets),$(MAKECMDGOALS)),)
ifneq ($(filter-out $(clean-targets),$(MAKECMDGOALS)),)
mixed-build := 1
endif
endif
# install and modules_install need also be processed one by one
ifneq ($(filter install,$(MAKECMDGOALS)),)
ifneq ($(filter modules_install,$(MAKECMDGOALS)),)
mixed-build := 1
endif
endif
ifdef mixed-build
# ===========================================================================
# We're called with mixed targets (*config and build targets).
# Handle them one by one.
PHONY += $(MAKECMDGOALS) __build_one_by_one
$(MAKECMDGOALS): __build_one_by_one
@:
__build_one_by_one:
$(Q)set -e; \
for i in $(MAKECMDGOALS); do \
$(MAKE) -f $(srctree)/Makefile $$i; \
done
else # !mixed-build
include scripts/Kbuild.include
# Read KERNELRELEASE from include/config/kernel.release (if it exists)
KERNELRELEASE = $(shell cat include/config/kernel.release 2> /dev/null)
KERNELVERSION = $(VERSION)$(if $(PATCHLEVEL),.$(PATCHLEVEL)$(if $(SUBLEVEL),.$(SUBLEVEL)))$(EXTRAVERSION)
export VERSION PATCHLEVEL SUBLEVEL KERNELRELEASE KERNELVERSION
include scripts/subarch.include
# Cross compiling and selecting different set of gcc/bin-utils
# ---------------------------------------------------------------------------
#
# When performing cross compilation for other architectures ARCH shall be set
# to the target architecture. (See arch/* for the possibilities).
# ARCH can be set during invocation of make:
# make ARCH=ia64
# Another way is to have ARCH set in the environment.
# The default ARCH is the host where make is executed.
# CROSS_COMPILE specify the prefix used for all executables used
# during compilation. Only gcc and related bin-utils executables
# are prefixed with $(CROSS_COMPILE).
# CROSS_COMPILE can be set on the command line
# make CROSS_COMPILE=ia64-linux-
# Alternatively CROSS_COMPILE can be set in the environment.
# Default value for CROSS_COMPILE is not to prefix executables
# Note: Some architectures assign CROSS_COMPILE in their arch/*/Makefile
ARCH ?= $(SUBARCH)
# Architecture as present in compile.h
UTS_MACHINE := $(ARCH)
SRCARCH := $(ARCH)
# Additional ARCH settings for x86
ifeq ($(ARCH),i386)
SRCARCH := x86
endif
ifeq ($(ARCH),x86_64)
SRCARCH := x86
endif
# Additional ARCH settings for sparc
ifeq ($(ARCH),sparc32)
SRCARCH := sparc
endif
ifeq ($(ARCH),sparc64)
SRCARCH := sparc
endif
# Additional ARCH settings for sh
ifeq ($(ARCH),sh64)
SRCARCH := sh
endif
KCONFIG_CONFIG ?= .config
export KCONFIG_CONFIG
# Default file for 'make defconfig'. This may be overridden by arch-Makefile.
export KBUILD_DEFCONFIG := defconfig
# SHELL used by kbuild
CONFIG_SHELL := sh
HOST_LFS_CFLAGS := $(shell getconf LFS_CFLAGS 2>/dev/null)
HOST_LFS_LDFLAGS := $(shell getconf LFS_LDFLAGS 2>/dev/null)
HOST_LFS_LIBS := $(shell getconf LFS_LIBS 2>/dev/null)
ifneq ($(LLVM),)
HOSTCC = clang
HOSTCXX = clang++
else
HOSTCC = gcc
HOSTCXX = g++
endif
export KBUILD_USERCFLAGS := -Wall -Wmissing-prototypes -Wstrict-prototypes \
-O2 -fomit-frame-pointer -std=gnu89
export KBUILD_USERLDFLAGS :=
KBUILD_HOSTCFLAGS := $(KBUILD_USERCFLAGS) $(HOST_LFS_CFLAGS) $(HOSTCFLAGS)
KBUILD_HOSTCXXFLAGS := -Wall -O2 $(HOST_LFS_CFLAGS) $(HOSTCXXFLAGS)
KBUILD_HOSTLDFLAGS := $(HOST_LFS_LDFLAGS) $(HOSTLDFLAGS)
KBUILD_HOSTLDLIBS := $(HOST_LFS_LIBS) $(HOSTLDLIBS)
# Make variables (CC, etc...)
CPP = $(CC) -E
ifneq ($(LLVM),)
CC = clang
LD = ld.lld
AR = llvm-ar
NM = llvm-nm
OBJCOPY = llvm-objcopy
OBJDUMP = llvm-objdump
READELF = llvm-readelf
STRIP = llvm-strip
KBUILD_HOSTLDFLAGS += -fuse-ld=lld --rtlib=compiler-rt
else
CC = $(CROSS_COMPILE)gcc
LD = $(CROSS_COMPILE)ld
AR = $(CROSS_COMPILE)ar
NM = $(CROSS_COMPILE)nm
OBJCOPY = $(CROSS_COMPILE)objcopy
OBJDUMP = $(CROSS_COMPILE)objdump
READELF = $(CROSS_COMPILE)readelf
STRIP = $(CROSS_COMPILE)strip
endif
PAHOLE = pahole
RESOLVE_BTFIDS = $(objtree)/tools/bpf/resolve_btfids/resolve_btfids
LEX = flex
YACC = bison
AWK = awk
INSTALLKERNEL := installkernel
DEPMOD = /sbin/depmod
PERL = perl
PYTHON = python
PYTHON3 = python3
CHECK = sparse
BASH = bash
KGZIP = gzip
KBZIP2 = bzip2
KLZOP = lzop
LZMA = lzma
LZ4 = lz4
XZ = xz
ZSTD = zstd
CHECKFLAGS := -D__linux__ -Dlinux -D__STDC__ -Dunix -D__unix__ \
-Wbitwise -Wno-return-void -Wno-unknown-attribute $(CF)
NOSTDINC_FLAGS :=
CFLAGS_MODULE =
AFLAGS_MODULE =
LDFLAGS_MODULE =
CFLAGS_KERNEL =
AFLAGS_KERNEL =
LDFLAGS_vmlinux =
# Use USERINCLUDE when you must reference the UAPI directories only.
USERINCLUDE := \
-I$(srctree)/arch/$(SRCARCH)/include/uapi \
-I$(objtree)/arch/$(SRCARCH)/include/generated/uapi \
-I$(srctree)/include/uapi \
-I$(objtree)/include/generated/uapi \
-include $(srctree)/include/linux/kconfig.h
# Use LINUXINCLUDE when you must reference the include/ directory.
# Needed to be compatible with the O= option
LINUXINCLUDE := \
-I$(srctree)/arch/$(SRCARCH)/include \
-I$(objtree)/arch/$(SRCARCH)/include/generated \
$(if $(building_out_of_srctree),-I$(srctree)/include) \
-I$(objtree)/include \
$(USERINCLUDE)
KBUILD_AFLAGS := -D__ASSEMBLY__ -fno-PIE
KBUILD_CFLAGS := -Wall -Wundef -Werror=strict-prototypes -Wno-trigraphs \
-fno-strict-aliasing -fno-common -fshort-wchar -fno-PIE \
-Werror=implicit-function-declaration -Werror=implicit-int \
-Werror=return-type -Wno-format-security \
-std=gnu89
KBUILD_CPPFLAGS := -D__KERNEL__
KBUILD_AFLAGS_KERNEL :=
KBUILD_CFLAGS_KERNEL :=
KBUILD_AFLAGS_MODULE := -DMODULE
KBUILD_CFLAGS_MODULE := -DMODULE
KBUILD_LDFLAGS_MODULE :=
KBUILD_LDFLAGS :=
CLANG_FLAGS :=
export ARCH SRCARCH CONFIG_SHELL BASH HOSTCC KBUILD_HOSTCFLAGS CROSS_COMPILE LD CC
export CPP AR NM STRIP OBJCOPY OBJDUMP READELF PAHOLE RESOLVE_BTFIDS LEX YACC AWK INSTALLKERNEL
export PERL PYTHON PYTHON3 CHECK CHECKFLAGS MAKE UTS_MACHINE HOSTCXX
export KGZIP KBZIP2 KLZOP LZMA LZ4 XZ ZSTD
export KBUILD_HOSTCXXFLAGS KBUILD_HOSTLDFLAGS KBUILD_HOSTLDLIBS LDFLAGS_MODULE
export KBUILD_CPPFLAGS NOSTDINC_FLAGS LINUXINCLUDE OBJCOPYFLAGS KBUILD_LDFLAGS
export KBUILD_CFLAGS CFLAGS_KERNEL CFLAGS_MODULE
export KBUILD_AFLAGS AFLAGS_KERNEL AFLAGS_MODULE
export KBUILD_AFLAGS_MODULE KBUILD_CFLAGS_MODULE KBUILD_LDFLAGS_MODULE
export KBUILD_AFLAGS_KERNEL KBUILD_CFLAGS_KERNEL
# Files to ignore in find ... statements
export RCS_FIND_IGNORE := \( -name SCCS -o -name BitKeeper -o -name .svn -o \
-name CVS -o -name .pc -o -name .hg -o -name .git \) \
-prune -o
export RCS_TAR_IGNORE := --exclude SCCS --exclude BitKeeper --exclude .svn \
--exclude CVS --exclude .pc --exclude .hg --exclude .git
# ===========================================================================
# Rules shared between *config targets and build targets
# Basic helpers built in scripts/basic/
PHONY += scripts_basic
scripts_basic:
$(Q)$(MAKE) $(build)=scripts/basic
$(Q)rm -f .tmp_quiet_recordmcount
PHONY += outputmakefile
# Before starting out-of-tree build, make sure the source tree is clean.
# outputmakefile generates a Makefile in the output directory, if using a
# separate output directory. This allows convenient use of make in the
# output directory.
# At the same time when output Makefile generated, generate .gitignore to
# ignore whole output directory
outputmakefile:
ifdef building_out_of_srctree
$(Q)if [ -f $(srctree)/.config -o \
-d $(srctree)/include/config -o \
-d $(srctree)/arch/$(SRCARCH)/include/generated ]; then \
echo >&2 "***"; \
echo >&2 "*** The source tree is not clean, please run 'make$(if $(findstring command line, $(origin ARCH)), ARCH=$(ARCH)) mrproper'"; \
echo >&2 "*** in $(abs_srctree)";\
echo >&2 "***"; \
false; \
fi
$(Q)ln -fsn $(srctree) source
$(Q)$(CONFIG_SHELL) $(srctree)/scripts/mkmakefile $(srctree)
$(Q)test -e .gitignore || \
{ echo "# this is build directory, ignore it"; echo "*"; } > .gitignore
endif
ifneq ($(shell $(CC) --version 2>&1 | head -n 1 | grep clang),)
ifneq ($(CROSS_COMPILE),)
CLANG_FLAGS += --target=$(notdir $(CROSS_COMPILE:%-=%))
GCC_TOOLCHAIN_DIR := $(dir $(shell which $(CROSS_COMPILE)elfedit))
CLANG_FLAGS += --prefix=$(GCC_TOOLCHAIN_DIR)$(notdir $(CROSS_COMPILE))
GCC_TOOLCHAIN := $(realpath $(GCC_TOOLCHAIN_DIR)/..)
endif
ifneq ($(GCC_TOOLCHAIN),)
CLANG_FLAGS += --gcc-toolchain=$(GCC_TOOLCHAIN)
endif
ifneq ($(LLVM_IAS),1)
CLANG_FLAGS += -no-integrated-as
endif
CLANG_FLAGS += -Werror=unknown-warning-option
KBUILD_CFLAGS += $(CLANG_FLAGS)
KBUILD_AFLAGS += $(CLANG_FLAGS)
export CLANG_FLAGS
endif
# The expansion should be delayed until arch/$(SRCARCH)/Makefile is included.
# Some architectures define CROSS_COMPILE in arch/$(SRCARCH)/Makefile.
# CC_VERSION_TEXT is referenced from Kconfig (so it needs export),
# and from include/config/auto.conf.cmd to detect the compiler upgrade.
CC_VERSION_TEXT = $(shell $(CC) --version 2>/dev/null | head -n 1)
ifdef config-build
# ===========================================================================
# *config targets only - make sure prerequisites are updated, and descend
# in scripts/kconfig to make the *config target
# Read arch specific Makefile to set KBUILD_DEFCONFIG as needed.
# KBUILD_DEFCONFIG may point out an alternative default configuration
# used for 'make defconfig'
include arch/$(SRCARCH)/Makefile
export KBUILD_DEFCONFIG KBUILD_KCONFIG CC_VERSION_TEXT
config: outputmakefile scripts_basic FORCE
$(Q)$(MAKE) $(build)=scripts/kconfig $@
%config: outputmakefile scripts_basic FORCE
$(Q)$(MAKE) $(build)=scripts/kconfig $@
else #!config-build
# ===========================================================================
# Build targets only - this includes vmlinux, arch specific targets, clean
# targets and others. In general all targets except *config targets.
# If building an external module we do not care about the all: rule
# but instead __all depend on modules
PHONY += all
ifeq ($(KBUILD_EXTMOD),)
__all: all
else
__all: modules
endif
# Decide whether to build built-in, modular, or both.
# Normally, just do built-in.
KBUILD_MODULES :=
KBUILD_BUILTIN := 1
# If we have only "make modules", don't compile built-in objects.
ifeq ($(MAKECMDGOALS),modules)
KBUILD_BUILTIN :=
endif
# If we have "make <whatever> modules", compile modules
# in addition to whatever we do anyway.
# Just "make" or "make all" shall build modules as well
ifneq ($(filter all modules nsdeps %compile_commands.json clang-%,$(MAKECMDGOALS)),)
KBUILD_MODULES := 1
endif
ifeq ($(MAKECMDGOALS),)
KBUILD_MODULES := 1
endif
export KBUILD_MODULES KBUILD_BUILTIN
ifdef need-config
include include/config/auto.conf
endif
ifeq ($(KBUILD_EXTMOD),)
# Objects we will link into vmlinux / subdirs we need to visit
core-y := init/ usr/
drivers-y := drivers/ sound/
drivers-$(CONFIG_SAMPLES) += samples/
drivers-y += net/ virt/
libs-y := lib/
endif # KBUILD_EXTMOD
# The all: target is the default when no target is given on the
# command line.
# This allow a user to issue only 'make' to build a kernel including modules
# Defaults to vmlinux, but the arch makefile usually adds further targets
all: vmlinux
CFLAGS_GCOV := -fprofile-arcs -ftest-coverage \
$(call cc-option,-fno-tree-loop-im) \
$(call cc-disable-warning,maybe-uninitialized,)
export CFLAGS_GCOV
# The arch Makefiles can override CC_FLAGS_FTRACE. We may also append it later.
ifdef CONFIG_FUNCTION_TRACER
CC_FLAGS_FTRACE := -pg
endif
RETPOLINE_CFLAGS_GCC := -mindirect-branch=thunk-extern -mindirect-branch-register
RETPOLINE_VDSO_CFLAGS_GCC := -mindirect-branch=thunk-inline -mindirect-branch-register
RETPOLINE_CFLAGS_CLANG := -mretpoline-external-thunk
RETPOLINE_VDSO_CFLAGS_CLANG := -mretpoline
RETPOLINE_CFLAGS := $(call cc-option,$(RETPOLINE_CFLAGS_GCC),$(call cc-option,$(RETPOLINE_CFLAGS_CLANG)))
RETPOLINE_VDSO_CFLAGS := $(call cc-option,$(RETPOLINE_VDSO_CFLAGS_GCC),$(call cc-option,$(RETPOLINE_VDSO_CFLAGS_CLANG)))
export RETPOLINE_CFLAGS
export RETPOLINE_VDSO_CFLAGS
include arch/$(SRCARCH)/Makefile
ifdef need-config
ifdef may-sync-config
# Read in dependencies to all Kconfig* files, make sure to run syncconfig if
# changes are detected. This should be included after arch/$(SRCARCH)/Makefile
# because some architectures define CROSS_COMPILE there.
include include/config/auto.conf.cmd
$(KCONFIG_CONFIG):
@echo >&2 '***'
@echo >&2 '*** Configuration file "$@" not found!'
@echo >&2 '***'
@echo >&2 '*** Please run some configurator (e.g. "make oldconfig" or'
@echo >&2 '*** "make menuconfig" or "make xconfig").'
@echo >&2 '***'
@/bin/false
# The actual configuration files used during the build are stored in
# include/generated/ and include/config/. Update them if .config is newer than
# include/config/auto.conf (which mirrors .config).
#
# This exploits the 'multi-target pattern rule' trick.
# The syncconfig should be executed only once to make all the targets.
# (Note: use the grouped target '&:' when we bump to GNU Make 4.3)
quiet_cmd_syncconfig = SYNC $@
cmd_syncconfig = $(MAKE) -f $(srctree)/Makefile syncconfig
%/config/auto.conf %/config/auto.conf.cmd %/generated/autoconf.h: $(KCONFIG_CONFIG)
+$(call cmd,syncconfig)
else # !may-sync-config
# External modules and some install targets need include/generated/autoconf.h
# and include/config/auto.conf but do not care if they are up-to-date.
# Use auto.conf to trigger the test
PHONY += include/config/auto.conf
include/config/auto.conf:
$(Q)test -e include/generated/autoconf.h -a -e $@ || ( \
echo >&2; \
echo >&2 " ERROR: Kernel configuration is invalid."; \
echo >&2 " include/generated/autoconf.h or $@ are missing.";\
echo >&2 " Run 'make oldconfig && make prepare' on kernel src to fix it."; \
echo >&2 ; \
/bin/false)
endif # may-sync-config
endif # need-config
KBUILD_CFLAGS += $(call cc-option,-fno-delete-null-pointer-checks,)
KBUILD_CFLAGS += $(call cc-disable-warning,frame-address,)
KBUILD_CFLAGS += $(call cc-disable-warning, format-truncation)
KBUILD_CFLAGS += $(call cc-disable-warning, format-overflow)
KBUILD_CFLAGS += $(call cc-disable-warning, address-of-packed-member)
ifdef CONFIG_CC_OPTIMIZE_FOR_PERFORMANCE
KBUILD_CFLAGS += -O2
else ifdef CONFIG_CC_OPTIMIZE_FOR_PERFORMANCE_O3
KBUILD_CFLAGS += -O3
else ifdef CONFIG_CC_OPTIMIZE_FOR_SIZE
KBUILD_CFLAGS += -Os
endif
# Tell gcc to never replace conditional load with a non-conditional one
KBUILD_CFLAGS += $(call cc-option,--param=allow-store-data-races=0)
KBUILD_CFLAGS += $(call cc-option,-fno-allow-store-data-races)
ifdef CONFIG_READABLE_ASM
# Disable optimizations that make assembler listings hard to read.
# reorder blocks reorders the control in the function
# ipa clone creates specialized cloned functions
# partial inlining inlines only parts of functions
KBUILD_CFLAGS += $(call cc-option,-fno-reorder-blocks,) \
$(call cc-option,-fno-ipa-cp-clone,) \
$(call cc-option,-fno-partial-inlining)
endif
ifneq ($(CONFIG_FRAME_WARN),0)
KBUILD_CFLAGS += -Wframe-larger-than=$(CONFIG_FRAME_WARN)
endif
stackp-flags-y := -fno-stack-protector
stackp-flags-$(CONFIG_STACKPROTECTOR) := -fstack-protector
stackp-flags-$(CONFIG_STACKPROTECTOR_STRONG) := -fstack-protector-strong
KBUILD_CFLAGS += $(stackp-flags-y)
ifdef CONFIG_CC_IS_CLANG
KBUILD_CPPFLAGS += -Qunused-arguments
KBUILD_CFLAGS += -Wno-format-invalid-specifier
KBUILD_CFLAGS += -Wno-gnu
# CLANG uses a _MergedGlobals as optimization, but this breaks modpost, as the
# source of a reference will be _MergedGlobals and not on of the whitelisted names.
# See modpost pattern 2
KBUILD_CFLAGS += -mno-global-merge
else
# These warnings generated too much noise in a regular build.
# Use make W=1 to enable them (see scripts/Makefile.extrawarn)
KBUILD_CFLAGS += -Wno-unused-but-set-variable
# Warn about unmarked fall-throughs in switch statement.
# Disabled for clang while comment to attribute conversion happens and
# https://github.com/ClangBuiltLinux/linux/issues/636 is discussed.
KBUILD_CFLAGS += $(call cc-option,-Wimplicit-fallthrough,)
endif
KBUILD_CFLAGS += $(call cc-disable-warning, unused-const-variable)
ifdef CONFIG_FRAME_POINTER
KBUILD_CFLAGS += -fno-omit-frame-pointer -fno-optimize-sibling-calls
else
# Some targets (ARM with Thumb2, for example), can't be built with frame
# pointers. For those, we don't have FUNCTION_TRACER automatically
# select FRAME_POINTER. However, FUNCTION_TRACER adds -pg, and this is
# incompatible with -fomit-frame-pointer with current GCC, so we don't use
# -fomit-frame-pointer with FUNCTION_TRACER.
ifndef CONFIG_FUNCTION_TRACER
KBUILD_CFLAGS += -fomit-frame-pointer
endif
endif
# Initialize all stack variables with a 0xAA pattern.
ifdef CONFIG_INIT_STACK_ALL_PATTERN
KBUILD_CFLAGS += -ftrivial-auto-var-init=pattern
endif
# Initialize all stack variables with a zero value.
ifdef CONFIG_INIT_STACK_ALL_ZERO
# Future support for zero initialization is still being debated, see
# https://bugs.llvm.org/show_bug.cgi?id=45497. These flags are subject to being
# renamed or dropped.
KBUILD_CFLAGS += -ftrivial-auto-var-init=zero
KBUILD_CFLAGS += -enable-trivial-auto-var-init-zero-knowing-it-will-be-removed-from-clang
endif
# Workaround for GCC versions < 5.0
# https://gcc.gnu.org/bugzilla/show_bug.cgi?id=61801
ifdef CONFIG_CC_IS_GCC
DEBUG_CFLAGS := $(call cc-ifversion, -lt, 0500, $(call cc-option, -fno-var-tracking-assignments))
endif
ifdef CONFIG_DEBUG_INFO
ifdef CONFIG_DEBUG_INFO_SPLIT
DEBUG_CFLAGS += -gsplit-dwarf
else
DEBUG_CFLAGS += -g
endif
ifneq ($(LLVM_IAS),1)
KBUILD_AFLAGS += -Wa,-gdwarf-2
endif
ifdef CONFIG_DEBUG_INFO_DWARF4
DEBUG_CFLAGS += -gdwarf-4
endif
ifdef CONFIG_DEBUG_INFO_REDUCED
DEBUG_CFLAGS += $(call cc-option, -femit-struct-debug-baseonly) \
$(call cc-option,-fno-var-tracking)
endif
ifdef CONFIG_DEBUG_INFO_COMPRESSED
DEBUG_CFLAGS += -gz=zlib
KBUILD_AFLAGS += -gz=zlib
KBUILD_LDFLAGS += --compress-debug-sections=zlib
endif
endif # CONFIG_DEBUG_INFO
KBUILD_CFLAGS += $(DEBUG_CFLAGS)
export DEBUG_CFLAGS
ifdef CONFIG_FUNCTION_TRACER
ifdef CONFIG_FTRACE_MCOUNT_USE_CC
CC_FLAGS_FTRACE += -mrecord-mcount
ifdef CONFIG_HAVE_NOP_MCOUNT
ifeq ($(call cc-option-yn, -mnop-mcount),y)
CC_FLAGS_FTRACE += -mnop-mcount
CC_FLAGS_USING += -DCC_USING_NOP_MCOUNT
endif
endif
endif
ifdef CONFIG_FTRACE_MCOUNT_USE_OBJTOOL
CC_FLAGS_USING += -DCC_USING_NOP_MCOUNT
endif
ifdef CONFIG_FTRACE_MCOUNT_USE_RECORDMCOUNT
ifdef CONFIG_HAVE_C_RECORDMCOUNT
BUILD_C_RECORDMCOUNT := y
export BUILD_C_RECORDMCOUNT
endif
endif
ifdef CONFIG_HAVE_FENTRY
ifeq ($(call cc-option-yn, -mfentry),y)
CC_FLAGS_FTRACE += -mfentry
CC_FLAGS_USING += -DCC_USING_FENTRY
endif
endif
export CC_FLAGS_FTRACE
KBUILD_CFLAGS += $(CC_FLAGS_FTRACE) $(CC_FLAGS_USING)
KBUILD_AFLAGS += $(CC_FLAGS_USING)
endif
# We trigger additional mismatches with less inlining
ifdef CONFIG_DEBUG_SECTION_MISMATCH
KBUILD_CFLAGS += $(call cc-option, -fno-inline-functions-called-once)
endif
ifdef CONFIG_LD_DEAD_CODE_DATA_ELIMINATION
KBUILD_CFLAGS_KERNEL += -ffunction-sections -fdata-sections
LDFLAGS_vmlinux += --gc-sections
endif
ifdef CONFIG_SHADOW_CALL_STACK
CC_FLAGS_SCS := -fsanitize=shadow-call-stack
KBUILD_CFLAGS += $(CC_FLAGS_SCS)
export CC_FLAGS_SCS
endif
ifdef CONFIG_LTO_CLANG
ifdef CONFIG_LTO_CLANG_THIN
CC_FLAGS_LTO += -flto=thin -fsplit-lto-unit
KBUILD_LDFLAGS += --thinlto-cache-dir=$(extmod-prefix).thinlto-cache
else
CC_FLAGS_LTO += -flto
endif
CC_FLAGS_LTO += -fvisibility=hidden
# Limit inlining across translation units to reduce binary size
KBUILD_LDFLAGS += -mllvm -import-instr-limit=5
endif
ifdef CONFIG_LTO
KBUILD_CFLAGS += $(CC_FLAGS_LTO)
export CC_FLAGS_LTO
endif
ifdef CONFIG_DEBUG_FORCE_FUNCTION_ALIGN_32B
KBUILD_CFLAGS += -falign-functions=32
endif
# arch Makefile may override CC so keep this after arch Makefile is included
NOSTDINC_FLAGS += -nostdinc -isystem $(shell $(CC) -print-file-name=include)
# warn about C99 declaration after statement
KBUILD_CFLAGS += -Wdeclaration-after-statement
# Variable Length Arrays (VLAs) should not be used anywhere in the kernel
KBUILD_CFLAGS += -Wvla
# disable pointer signed / unsigned warnings in gcc 4.0
KBUILD_CFLAGS += -Wno-pointer-sign
# disable stringop warnings in gcc 8+
KBUILD_CFLAGS += $(call cc-disable-warning, stringop-truncation)
# We'll want to enable this eventually, but it's not going away for 5.7 at least
KBUILD_CFLAGS += $(call cc-disable-warning, zero-length-bounds)
KBUILD_CFLAGS += $(call cc-disable-warning, array-bounds)
KBUILD_CFLAGS += $(call cc-disable-warning, stringop-overflow)
# Another good warning that we'll want to enable eventually
KBUILD_CFLAGS += $(call cc-disable-warning, restrict)
# Enabled with W=2, disabled by default as noisy
KBUILD_CFLAGS += $(call cc-disable-warning, maybe-uninitialized)
# disable invalid "can't wrap" optimizations for signed / pointers
KBUILD_CFLAGS += -fno-strict-overflow
# Make sure -fstack-check isn't enabled (like gentoo apparently did)
KBUILD_CFLAGS += -fno-stack-check
# conserve stack if available
KBUILD_CFLAGS += $(call cc-option,-fconserve-stack)
# Prohibit date/time macros, which would make the build non-deterministic
KBUILD_CFLAGS += -Werror=date-time
# enforce correct pointer usage
KBUILD_CFLAGS += $(call cc-option,-Werror=incompatible-pointer-types)
# Require designated initializers for all marked structures
KBUILD_CFLAGS += $(call cc-option,-Werror=designated-init)
# change __FILE__ to the relative path from the srctree
KBUILD_CPPFLAGS += $(call cc-option,-fmacro-prefix-map=$(srctree)/=)
# ensure -fcf-protection is disabled when using retpoline as it is
# incompatible with -mindirect-branch=thunk-extern
ifdef CONFIG_RETPOLINE
KBUILD_CFLAGS += $(call cc-option,-fcf-protection=none)
endif
# include additional Makefiles when needed
include-y := scripts/Makefile.extrawarn
include-$(CONFIG_KASAN) += scripts/Makefile.kasan
include-$(CONFIG_KCSAN) += scripts/Makefile.kcsan
include-$(CONFIG_UBSAN) += scripts/Makefile.ubsan
include-$(CONFIG_KCOV) += scripts/Makefile.kcov
include-$(CONFIG_GCC_PLUGINS) += scripts/Makefile.gcc-plugins
include $(addprefix $(srctree)/, $(include-y))
# scripts/Makefile.gcc-plugins is intentionally included last.
# Do not add $(call cc-option,...) below this line. When you build the kernel
# from the clean source tree, the GCC plugins do not exist at this point.
# Add user supplied CPPFLAGS, AFLAGS and CFLAGS as the last assignments
KBUILD_CPPFLAGS += $(KCPPFLAGS)
KBUILD_AFLAGS += $(KAFLAGS)
KBUILD_CFLAGS += $(KCFLAGS)
KBUILD_LDFLAGS_MODULE += --build-id=sha1
LDFLAGS_vmlinux += --build-id=sha1
ifeq ($(CONFIG_STRIP_ASM_SYMS),y)
LDFLAGS_vmlinux += $(call ld-option, -X,)
endif
ifeq ($(CONFIG_RELR),y)
LDFLAGS_vmlinux += --pack-dyn-relocs=relr
endif
# We never want expected sections to be placed heuristically by the
# linker. All sections should be explicitly named in the linker script.
ifdef CONFIG_LD_ORPHAN_WARN
LDFLAGS_vmlinux += --orphan-handling=warn
endif
# Align the bit size of userspace programs with the kernel
KBUILD_USERCFLAGS += $(filter -m32 -m64 --target=%, $(KBUILD_CFLAGS))
KBUILD_USERLDFLAGS += $(filter -m32 -m64 --target=%, $(KBUILD_CFLAGS))
# make the checker run with the right architecture
CHECKFLAGS += --arch=$(ARCH)
# insure the checker run with the right endianness
CHECKFLAGS += $(if $(CONFIG_CPU_BIG_ENDIAN),-mbig-endian,-mlittle-endian)
# the checker needs the correct machine size
CHECKFLAGS += $(if $(CONFIG_64BIT),-m64,-m32)
# Default kernel image to build when no specific target is given.
# KBUILD_IMAGE may be overruled on the command line or
# set in the environment
# Also any assignments in arch/$(ARCH)/Makefile take precedence over
# this default value
export KBUILD_IMAGE ?= vmlinux
#
# INSTALL_PATH specifies where to place the updated kernel and system map
# images. Default is /boot, but you can set it to other values
export INSTALL_PATH ?= /boot
#
# INSTALL_DTBS_PATH specifies a prefix for relocations required by build roots.
# Like INSTALL_MOD_PATH, it isn't defined in the Makefile, but can be passed as
# an argument if needed. Otherwise it defaults to the kernel install path
#
export INSTALL_DTBS_PATH ?= $(INSTALL_PATH)/dtbs/$(KERNELRELEASE)
#
# INSTALL_MOD_PATH specifies a prefix to MODLIB for module directory
# relocations required by build roots. This is not defined in the
# makefile but the argument can be passed to make if needed.
#
MODLIB = $(INSTALL_MOD_PATH)/lib/modules/$(KERNELRELEASE)
export MODLIB
#
# INSTALL_MOD_STRIP, if defined, will cause modules to be
# stripped after they are installed. If INSTALL_MOD_STRIP is '1', then
# the default option --strip-debug will be used. Otherwise,
# INSTALL_MOD_STRIP value will be used as the options to the strip command.
ifdef INSTALL_MOD_STRIP
ifeq ($(INSTALL_MOD_STRIP),1)
mod_strip_cmd = $(STRIP) --strip-debug
else
mod_strip_cmd = $(STRIP) $(INSTALL_MOD_STRIP)
endif # INSTALL_MOD_STRIP=1
else
mod_strip_cmd = true
endif # INSTALL_MOD_STRIP
export mod_strip_cmd
# CONFIG_MODULE_COMPRESS, if defined, will cause module to be compressed
# after they are installed in agreement with CONFIG_MODULE_COMPRESS_GZIP
# or CONFIG_MODULE_COMPRESS_XZ.
mod_compress_cmd = true
ifdef CONFIG_MODULE_COMPRESS
ifdef CONFIG_MODULE_COMPRESS_GZIP
mod_compress_cmd = $(KGZIP) -n -f
endif # CONFIG_MODULE_COMPRESS_GZIP
ifdef CONFIG_MODULE_COMPRESS_XZ
mod_compress_cmd = $(XZ) -f
endif # CONFIG_MODULE_COMPRESS_XZ
endif # CONFIG_MODULE_COMPRESS
export mod_compress_cmd
ifdef CONFIG_MODULE_SIG_ALL
$(eval $(call config_filename,MODULE_SIG_KEY))
mod_sign_cmd = scripts/sign-file $(CONFIG_MODULE_SIG_HASH) $(MODULE_SIG_KEY_SRCPREFIX)$(CONFIG_MODULE_SIG_KEY) certs/signing_key.x509
else
mod_sign_cmd = true
endif
export mod_sign_cmd
HOST_LIBELF_LIBS = $(shell pkg-config libelf --libs 2>/dev/null || echo -lelf)
has_libelf = $(call try-run,\
echo "int main() {}" | $(HOSTCC) -xc -o /dev/null $(HOST_LIBELF_LIBS) -,1,0)
ifdef CONFIG_STACK_VALIDATION
ifeq ($(has_libelf),1)
objtool_target := tools/objtool FORCE
else
SKIP_STACK_VALIDATION := 1
export SKIP_STACK_VALIDATION
endif
endif
ifdef CONFIG_BPF
ifdef CONFIG_DEBUG_INFO_BTF
ifeq ($(has_libelf),1)
resolve_btfids_target := tools/bpf/resolve_btfids FORCE
else
ERROR_RESOLVE_BTFIDS := 1
endif
endif # CONFIG_DEBUG_INFO_BTF
endif # CONFIG_BPF
PHONY += prepare0
export MODORDER := $(extmod-prefix)modules.order
export MODULES_NSDEPS := $(extmod-prefix)modules.nsdeps
# ---------------------------------------------------------------------------
# Kernel headers
PHONY += headers
#Default location for installed headers
ifeq ($(KBUILD_EXTMOD),)
PHONY += archheaders archscripts
hdr-inst := -f $(srctree)/scripts/Makefile.headersinst obj
headers: $(version_h) scripts_unifdef uapi-asm-generic archheaders archscripts
else
hdr-prefix = $(KBUILD_EXTMOD)/
hdr-inst := -f $(srctree)/scripts/Makefile.headersinst dst=$(KBUILD_EXTMOD)/usr/include objtree=$(objtree)/$(KBUILD_EXTMOD) obj
endif
export INSTALL_HDR_PATH = $(objtree)/$(hdr-prefix)usr
quiet_cmd_headers_install = INSTALL $(INSTALL_HDR_PATH)/include
cmd_headers_install = \
mkdir -p $(INSTALL_HDR_PATH); \
rsync -mrl --include='*/' --include='*\.h' --exclude='*' \
usr/include $(INSTALL_HDR_PATH)
PHONY += headers_install
headers_install: headers
$(call cmd,headers_install)
headers:
ifeq ($(KBUILD_EXTMOD),)
$(if $(wildcard $(srctree)/arch/$(SRCARCH)/include/uapi/asm/Kbuild),, \
$(error Headers not exportable for the $(SRCARCH) architecture))
endif
$(Q)$(MAKE) $(hdr-inst)=$(hdr-prefix)include/uapi
$(Q)$(MAKE) $(hdr-inst)=$(hdr-prefix)arch/$(SRCARCH)/include/uapi
ifeq ($(KBUILD_EXTMOD),)
core-y += kernel/ certs/ mm/ fs/ ipc/ security/ crypto/ block/
vmlinux-dirs := $(patsubst %/,%,$(filter %/, \
$(core-y) $(core-m) $(drivers-y) $(drivers-m) \
$(libs-y) $(libs-m)))
vmlinux-alldirs := $(sort $(vmlinux-dirs) Documentation \
$(patsubst %/,%,$(filter %/, $(core-) \
$(drivers-) $(libs-))))
subdir-modorder := $(addsuffix modules.order,$(filter %/, \
$(core-y) $(core-m) $(libs-y) $(libs-m) \
$(drivers-y) $(drivers-m)))
build-dirs := $(vmlinux-dirs)
clean-dirs := $(vmlinux-alldirs)
# Externally visible symbols (used by link-vmlinux.sh)
KBUILD_VMLINUX_OBJS := $(head-y) $(patsubst %/,%/built-in.a, $(core-y))
KBUILD_VMLINUX_OBJS += $(addsuffix built-in.a, $(filter %/, $(libs-y)))
ifdef CONFIG_MODULES
KBUILD_VMLINUX_OBJS += $(patsubst %/, %/lib.a, $(filter %/, $(libs-y)))
KBUILD_VMLINUX_LIBS := $(filter-out %/, $(libs-y))
else
KBUILD_VMLINUX_LIBS := $(patsubst %/,%/lib.a, $(libs-y))
endif
KBUILD_VMLINUX_OBJS += $(patsubst %/,%/built-in.a, $(drivers-y))
export KBUILD_VMLINUX_OBJS KBUILD_VMLINUX_LIBS
export KBUILD_LDS := arch/$(SRCARCH)/kernel/vmlinux.lds
# used by scripts/Makefile.package
export KBUILD_ALLDIRS := $(sort $(filter-out arch/%,$(vmlinux-alldirs)) LICENSES arch include scripts tools)
vmlinux-deps := $(KBUILD_LDS) $(KBUILD_VMLINUX_OBJS) $(KBUILD_VMLINUX_LIBS)
# Recurse until adjust_autoksyms.sh is satisfied
PHONY += autoksyms_recursive
ifdef CONFIG_TRIM_UNUSED_KSYMS
# For the kernel to actually contain only the needed exported symbols,
# we have to build modules as well to determine what those symbols are.
# (this can be evaluated only once include/config/auto.conf has been included)
KBUILD_MODULES := 1
autoksyms_recursive: descend modules.order
$(Q)$(CONFIG_SHELL) $(srctree)/scripts/adjust_autoksyms.sh \
"$(MAKE) -f $(srctree)/Makefile vmlinux"
endif
autoksyms_h := $(if $(CONFIG_TRIM_UNUSED_KSYMS), include/generated/autoksyms.h)
quiet_cmd_autoksyms_h = GEN $@
cmd_autoksyms_h = mkdir -p $(dir $@); \
$(CONFIG_SHELL) $(srctree)/scripts/gen_autoksyms.sh $@
$(autoksyms_h):
$(call cmd,autoksyms_h)
ARCH_POSTLINK := $(wildcard $(srctree)/arch/$(SRCARCH)/Makefile.postlink)
# Final link of vmlinux with optional arch pass after final link
cmd_link-vmlinux = \
$(CONFIG_SHELL) $< "$(LD)" "$(KBUILD_LDFLAGS)" "$(LDFLAGS_vmlinux)"; \
$(if $(ARCH_POSTLINK), $(MAKE) -f $(ARCH_POSTLINK) $@, true)
vmlinux: scripts/link-vmlinux.sh autoksyms_recursive $(vmlinux-deps) FORCE
+$(call if_changed,link-vmlinux)
targets := vmlinux
# The actual objects are generated when descending,
# make sure no implicit rule kicks in
$(sort $(vmlinux-deps) $(subdir-modorder)): descend ;
filechk_kernel.release = \
echo "$(KERNELVERSION)$$($(CONFIG_SHELL) $(srctree)/scripts/setlocalversion \
$(srctree) $(BRANCH) $(KMI_GENERATION))"
# Store (new) KERNELRELEASE string in include/config/kernel.release
include/config/kernel.release: FORCE
$(call filechk,kernel.release)
# Additional helpers built in scripts/
# Carefully list dependencies so we do not try to build scripts twice
# in parallel
PHONY += scripts
scripts: scripts_basic scripts_dtc
$(Q)$(MAKE) $(build)=$(@)
# Things we need to do before we recursively start building the kernel
# or the modules are listed in "prepare".
# A multi level approach is used. prepareN is processed before prepareN-1.
# archprepare is used in arch Makefiles and when processed asm symlink,
# version.h and scripts_basic is processed / created.
PHONY += prepare archprepare
archprepare: outputmakefile archheaders archscripts scripts include/config/kernel.release \
asm-generic $(version_h) $(autoksyms_h) include/generated/utsrelease.h \
include/generated/autoconf.h
prepare0: archprepare
$(Q)$(MAKE) $(build)=scripts/mod
$(Q)$(MAKE) $(build)=.
# All the preparing..
prepare: prepare0 prepare-objtool prepare-resolve_btfids
# Support for using generic headers in asm-generic
asm-generic := -f $(srctree)/scripts/Makefile.asm-generic obj
PHONY += asm-generic uapi-asm-generic
asm-generic: uapi-asm-generic
$(Q)$(MAKE) $(asm-generic)=arch/$(SRCARCH)/include/generated/asm \
generic=include/asm-generic
uapi-asm-generic:
$(Q)$(MAKE) $(asm-generic)=arch/$(SRCARCH)/include/generated/uapi/asm \
generic=include/uapi/asm-generic
PHONY += prepare-objtool prepare-resolve_btfids
prepare-objtool: $(objtool_target)
ifeq ($(SKIP_STACK_VALIDATION),1)
ifdef CONFIG_FTRACE_MCOUNT_USE_OBJTOOL
@echo "error: Cannot generate __mcount_loc for CONFIG_DYNAMIC_FTRACE=y, please install libelf-dev, libelf-devel or elfutils-libelf-devel" >&2
@false
endif
ifdef CONFIG_UNWINDER_ORC
@echo "error: Cannot generate ORC metadata for CONFIG_UNWINDER_ORC=y, please install libelf-dev, libelf-devel or elfutils-libelf-devel" >&2
@false
else
@echo "warning: Cannot use CONFIG_STACK_VALIDATION=y, please install libelf-dev, libelf-devel or elfutils-libelf-devel" >&2
endif
endif
prepare-resolve_btfids: $(resolve_btfids_target)
ifeq ($(ERROR_RESOLVE_BTFIDS),1)
@echo "error: Cannot resolve BTF IDs for CONFIG_DEBUG_INFO_BTF, please install libelf-dev, libelf-devel or elfutils-libelf-devel" >&2
@false
endif
# Generate some files
# ---------------------------------------------------------------------------
# KERNELRELEASE can change from a few different places, meaning version.h
# needs to be updated, so this check is forced on all builds
uts_len := 64
ifneq (,$(BUILD_NUMBER))
UTS_RELEASE=$(KERNELRELEASE)-ab$(BUILD_NUMBER)
else
UTS_RELEASE=$(KERNELRELEASE)
endif
define filechk_utsrelease.h
if [ `echo -n "$(UTS_RELEASE)" | wc -c ` -gt $(uts_len) ]; then \
echo '"$(UTS_RELEASE)" exceeds $(uts_len) characters' >&2; \
exit 1; \
fi; \
echo \#define UTS_RELEASE \"$(UTS_RELEASE)\"
endef
define filechk_version.h
echo \#define LINUX_VERSION_CODE $(shell \
expr $(VERSION) \* 65536 + 0$(PATCHLEVEL) \* 256 + 0$(SUBLEVEL)); \
echo '#define KERNEL_VERSION(a,b,c) (((a) << 16) + ((b) << 8) + (c))'
endef
$(version_h): FORCE
$(call filechk,version.h)
$(Q)rm -f $(old_version_h)
include/generated/utsrelease.h: include/config/kernel.release FORCE
$(call filechk,utsrelease.h)
PHONY += headerdep
headerdep:
$(Q)find $(srctree)/include/ -name '*.h' | xargs --max-args 1 \
$(srctree)/scripts/headerdep.pl -I$(srctree)/include
# Deprecated. It is no-op now.
PHONY += headers_check
headers_check:
@:
ifdef CONFIG_HEADERS_INSTALL
prepare: headers
endif
PHONY += scripts_unifdef
scripts_unifdef: scripts_basic
$(Q)$(MAKE) $(build)=scripts scripts/unifdef
# ---------------------------------------------------------------------------
# Kernel selftest
PHONY += kselftest
kselftest:
$(Q)$(MAKE) -C $(srctree)/tools/testing/selftests run_tests
kselftest-%: FORCE
$(Q)$(MAKE) -C $(srctree)/tools/testing/selftests $*
PHONY += kselftest-merge
kselftest-merge:
$(if $(wildcard $(objtree)/.config),, $(error No .config exists, config your kernel first!))
$(Q)find $(srctree)/tools/testing/selftests -name config | \
xargs $(srctree)/scripts/kconfig/merge_config.sh -m $(objtree)/.config
$(Q)$(MAKE) -f $(srctree)/Makefile olddefconfig
# ---------------------------------------------------------------------------
# Devicetree files
ifneq ($(wildcard $(srctree)/arch/$(SRCARCH)/boot/dts/),)
dtstree := arch/$(SRCARCH)/boot/dts
endif
ifneq ($(dtstree),)
%.dtb: include/config/kernel.release scripts_dtc
$(Q)$(MAKE) $(build)=$(dtstree) $(dtstree)/$@
PHONY += dtbs dtbs_install dtbs_check
dtbs: include/config/kernel.release scripts_dtc
$(Q)$(MAKE) $(build)=$(dtstree)
ifneq ($(filter dtbs_check, $(MAKECMDGOALS)),)
export CHECK_DTBS=y
dtbs: dt_binding_check
endif
dtbs_check: dtbs
dtbs_install:
$(Q)$(MAKE) $(dtbinst)=$(dtstree) dst=$(INSTALL_DTBS_PATH)
ifdef CONFIG_OF_EARLY_FLATTREE
all: dtbs
endif
endif
PHONY += scripts_dtc
scripts_dtc: scripts_basic
$(Q)$(MAKE) $(build)=scripts/dtc
ifneq ($(filter dt_binding_check, $(MAKECMDGOALS)),)
export CHECK_DT_BINDING=y
endif
PHONY += dt_binding_check
dt_binding_check: scripts_dtc
$(Q)$(MAKE) $(build)=Documentation/devicetree/bindings
# ---------------------------------------------------------------------------
# Modules
ifdef CONFIG_MODULES
# By default, build modules as well
all: modules
# When we're building modules with modversions, we need to consider
# the built-in objects during the descend as well, in order to
# make sure the checksums are up to date before we record them.
ifdef CONFIG_MODVERSIONS
KBUILD_BUILTIN := 1
endif
# Build modules
#
# A module can be listed more than once in obj-m resulting in
# duplicate lines in modules.order files. Those are removed
# using awk while concatenating to the final file.
PHONY += modules
modules: $(if $(KBUILD_BUILTIN),vmlinux) modules_check modules_prepare
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
PHONY += modules_check
modules_check: modules.order
$(Q)$(CONFIG_SHELL) $(srctree)/scripts/modules-check.sh $<
cmd_modules_order = $(AWK) '!x[$$0]++' $(real-prereqs) > $@
modules.order: $(subdir-modorder) FORCE
$(call if_changed,modules_order)
targets += modules.order
# Target to prepare building external modules
PHONY += modules_prepare
modules_prepare: prepare
$(Q)$(MAKE) $(build)=scripts scripts/module.lds
# Target to install modules
PHONY += modules_install
modules_install: _modinst_ _modinst_post
PHONY += _modinst_
_modinst_:
@rm -rf $(MODLIB)/kernel
@rm -f $(MODLIB)/source
@mkdir -p $(MODLIB)/kernel
@ln -s $(abspath $(srctree)) $(MODLIB)/source
@if [ ! $(objtree) -ef $(MODLIB)/build ]; then \
rm -f $(MODLIB)/build ; \
ln -s $(CURDIR) $(MODLIB)/build ; \
fi
@sed 's:^:kernel/:' modules.order > $(MODLIB)/modules.order
@cp -f modules.builtin $(MODLIB)/
@cp -f $(objtree)/modules.builtin.modinfo $(MODLIB)/
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modinst
# This depmod is only for convenience to give the initial
# boot a modules.dep even before / is mounted read-write. However the
# boot script depmod is the master version.
PHONY += _modinst_post
_modinst_post: _modinst_
$(call cmd,depmod)
ifeq ($(CONFIG_MODULE_SIG), y)
PHONY += modules_sign
modules_sign:
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modsign
endif
else # CONFIG_MODULES
# Modules not configured
# ---------------------------------------------------------------------------
PHONY += modules modules_install
modules modules_install:
@echo >&2
@echo >&2 "The present kernel configuration has modules disabled."
@echo >&2 "Type 'make config' and enable loadable module support."
@echo >&2 "Then build a kernel with module support enabled."
@echo >&2
@exit 1
endif # CONFIG_MODULES
###
# Cleaning is done on three levels.
# make clean Delete most generated files
# Leave enough to build external modules
# make mrproper Delete the current configuration, and all generated files
# make distclean Remove editor backup files, patch leftover files and the like
# Directories & files removed with 'make clean'
CLEAN_FILES += include/ksym vmlinux.symvers \
modules.builtin modules.builtin.modinfo modules.nsdeps \
compile_commands.json
# Directories & files removed with 'make mrproper'
MRPROPER_FILES += include/config include/generated \
arch/$(SRCARCH)/include/generated .tmp_objdiff \
debian snap tar-install \
.config .config.old .version \
Module.symvers \
signing_key.pem signing_key.priv signing_key.x509 \
x509.genkey extra_certificates signing_key.x509.keyid \
signing_key.x509.signer vmlinux-gdb.py \
*.spec
# Directories & files removed with 'make distclean'
DISTCLEAN_FILES += tags TAGS cscope* GPATH GTAGS GRTAGS GSYMS .thinlto-cache
# clean - Delete most, but leave enough to build external modules
#
clean: rm-files := $(CLEAN_FILES)
PHONY += archclean vmlinuxclean
vmlinuxclean:
$(Q)$(CONFIG_SHELL) $(srctree)/scripts/link-vmlinux.sh clean
$(Q)$(if $(ARCH_POSTLINK), $(MAKE) -f $(ARCH_POSTLINK) clean)
clean: archclean vmlinuxclean
# mrproper - Delete all generated files, including .config
#
mrproper: rm-files := $(wildcard $(MRPROPER_FILES))
mrproper-dirs := $(addprefix _mrproper_,scripts)
PHONY += $(mrproper-dirs) mrproper
$(mrproper-dirs):
$(Q)$(MAKE) $(clean)=$(patsubst _mrproper_%,%,$@)
mrproper: clean $(mrproper-dirs)
$(call cmd,rmfiles)
# distclean
#
distclean: rm-files := $(wildcard $(DISTCLEAN_FILES))
PHONY += distclean
distclean: mrproper
$(call cmd,rmfiles)
@find $(srctree) $(RCS_FIND_IGNORE) \
\( -name '*.orig' -o -name '*.rej' -o -name '*~' \
-o -name '*.bak' -o -name '#*#' -o -name '*%' \
-o -name 'core' \) \
-type f -print | xargs rm -f
# Packaging of the kernel to various formats
# ---------------------------------------------------------------------------
%src-pkg: FORCE
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.package $@
%pkg: include/config/kernel.release FORCE
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.package $@
# Brief documentation of the typical targets used
# ---------------------------------------------------------------------------
boards := $(wildcard $(srctree)/arch/$(SRCARCH)/configs/*_defconfig)
boards := $(sort $(notdir $(boards)))
board-dirs := $(dir $(wildcard $(srctree)/arch/$(SRCARCH)/configs/*/*_defconfig))
board-dirs := $(sort $(notdir $(board-dirs:/=)))
PHONY += help
help:
@echo 'Cleaning targets:'
@echo ' clean - Remove most generated files but keep the config and'
@echo ' enough build support to build external modules'
@echo ' mrproper - Remove all generated files + config + various backup files'
@echo ' distclean - mrproper + remove editor backup and patch files'
@echo ''
@echo 'Configuration targets:'
@$(MAKE) -f $(srctree)/scripts/kconfig/Makefile help
@echo ''
@echo 'Other generic targets:'
@echo ' all - Build all targets marked with [*]'
@echo '* vmlinux - Build the bare kernel'
@echo '* modules - Build all modules'
@echo ' modules_install - Install all modules to INSTALL_MOD_PATH (default: /)'
@echo ' dir/ - Build all files in dir and below'
@echo ' dir/file.[ois] - Build specified target only'
@echo ' dir/file.ll - Build the LLVM assembly file'
@echo ' (requires compiler support for LLVM assembly generation)'
@echo ' dir/file.lst - Build specified mixed source/assembly target only'
@echo ' (requires a recent binutils and recent build (System.map))'
@echo ' dir/file.ko - Build module including final link'
@echo ' modules_prepare - Set up for building external modules'
@echo ' tags/TAGS - Generate tags file for editors'
@echo ' cscope - Generate cscope index'
@echo ' gtags - Generate GNU GLOBAL index'
@echo ' kernelrelease - Output the release version string (use with make -s)'
@echo ' kernelversion - Output the version stored in Makefile (use with make -s)'
@echo ' image_name - Output the image name (use with make -s)'
@echo ' headers_install - Install sanitised kernel headers to INSTALL_HDR_PATH'; \
echo ' (default: $(INSTALL_HDR_PATH))'; \
echo ''
@echo 'Static analysers:'
@echo ' checkstack - Generate a list of stack hogs'
@echo ' versioncheck - Sanity check on version.h usage'
@echo ' includecheck - Check for duplicate included header files'
@echo ' export_report - List the usages of all exported symbols'
@echo ' headerdep - Detect inclusion cycles in headers'
@echo ' coccicheck - Check with Coccinelle'
@echo ' clang-analyzer - Check with clang static analyzer'
@echo ' clang-tidy - Check with clang-tidy'
@echo ''
@echo 'Tools:'
@echo ' nsdeps - Generate missing symbol namespace dependencies'
@echo ''
@echo 'Kernel selftest:'
@echo ' kselftest - Build and run kernel selftest'
@echo ' Build, install, and boot kernel before'
@echo ' running kselftest on it'
@echo ' Run as root for full coverage'
@echo ' kselftest-all - Build kernel selftest'
@echo ' kselftest-install - Build and install kernel selftest'
@echo ' kselftest-clean - Remove all generated kselftest files'
@echo ' kselftest-merge - Merge all the config dependencies of'
@echo ' kselftest to existing .config.'
@echo ''
@$(if $(dtstree), \
echo 'Devicetree:'; \
echo '* dtbs - Build device tree blobs for enabled boards'; \
echo ' dtbs_install - Install dtbs to $(INSTALL_DTBS_PATH)'; \
echo ' dt_binding_check - Validate device tree binding documents'; \
echo ' dtbs_check - Validate device tree source files';\
echo '')
@echo 'Userspace tools targets:'
@echo ' use "make tools/help"'
@echo ' or "cd tools; make help"'
@echo ''
@echo 'Kernel packaging:'
@$(MAKE) -f $(srctree)/scripts/Makefile.package help
@echo ''
@echo 'Documentation targets:'
@$(MAKE) -f $(srctree)/Documentation/Makefile dochelp
@echo ''
@echo 'Architecture specific targets ($(SRCARCH)):'
@$(if $(archhelp),$(archhelp),\
echo ' No architecture specific help defined for $(SRCARCH)')
@echo ''
@$(if $(boards), \
$(foreach b, $(boards), \
printf " %-27s - Build for %s\\n" $(b) $(subst _defconfig,,$(b));) \
echo '')
@$(if $(board-dirs), \
$(foreach b, $(board-dirs), \
printf " %-16s - Show %s-specific targets\\n" help-$(b) $(b);) \
printf " %-16s - Show all of the above\\n" help-boards; \
echo '')
@echo ' make V=0|1 [targets] 0 => quiet build (default), 1 => verbose build'
@echo ' make V=2 [targets] 2 => give reason for rebuild of target'
@echo ' make O=dir [targets] Locate all output files in "dir", including .config'
@echo ' make C=1 [targets] Check re-compiled c source with $$CHECK'
@echo ' (sparse by default)'
@echo ' make C=2 [targets] Force check of all c source with $$CHECK'
@echo ' make RECORDMCOUNT_WARN=1 [targets] Warn about ignored mcount sections'
@echo ' make W=n [targets] Enable extra build checks, n=1,2,3 where'
@echo ' 1: warnings which may be relevant and do not occur too often'
@echo ' 2: warnings which occur quite often but may still be relevant'
@echo ' 3: more obscure warnings, can most likely be ignored'
@echo ' Multiple levels can be combined with W=12 or W=123'
@echo ''
@echo 'Execute "make" or "make all" to build all targets marked with [*] '
@echo 'For further info see the ./README file'
help-board-dirs := $(addprefix help-,$(board-dirs))
help-boards: $(help-board-dirs)
boards-per-dir = $(sort $(notdir $(wildcard $(srctree)/arch/$(SRCARCH)/configs/$*/*_defconfig)))
$(help-board-dirs): help-%:
@echo 'Architecture specific targets ($(SRCARCH) $*):'
@$(if $(boards-per-dir), \
$(foreach b, $(boards-per-dir), \
printf " %-24s - Build for %s\\n" $*/$(b) $(subst _defconfig,,$(b));) \
echo '')
# Documentation targets
# ---------------------------------------------------------------------------
DOC_TARGETS := xmldocs latexdocs pdfdocs htmldocs epubdocs cleandocs \
linkcheckdocs dochelp refcheckdocs
PHONY += $(DOC_TARGETS)
$(DOC_TARGETS):
$(Q)$(MAKE) $(build)=Documentation $@
# Misc
# ---------------------------------------------------------------------------
PHONY += scripts_gdb
scripts_gdb: prepare0
$(Q)$(MAKE) $(build)=scripts/gdb
$(Q)ln -fsn $(abspath $(srctree)/scripts/gdb/vmlinux-gdb.py)
ifdef CONFIG_GDB_SCRIPTS
all: scripts_gdb
endif
else # KBUILD_EXTMOD
###
# External module support.
# When building external modules the kernel used as basis is considered
# read-only, and no consistency checks are made and the make
# system is not used on the basis kernel. If updates are required
# in the basis kernel ordinary make commands (without M=...) must
# be used.
#
# The following are the only valid targets when building external
# modules.
# make M=dir clean Delete all automatically generated files
# make M=dir modules Make all modules in specified dir
# make M=dir Same as 'make M=dir modules'
# make M=dir modules_install
# Install the modules built in the module directory
# Assumes install directory is already created
# We are always building only modules.
KBUILD_BUILTIN :=
KBUILD_MODULES := 1
build-dirs := $(KBUILD_EXTMOD)
PHONY += modules
modules: $(MODORDER)
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
$(MODORDER): descend
@:
PHONY += modules_install
modules_install: _emodinst_ _emodinst_post
install-dir := $(if $(INSTALL_MOD_DIR),$(INSTALL_MOD_DIR),extra)
PHONY += _emodinst_
_emodinst_:
$(Q)mkdir -p $(MODLIB)/$(install-dir)
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modinst
PHONY += _emodinst_post
_emodinst_post: _emodinst_
$(call cmd,depmod)
compile_commands.json: $(extmod-prefix)compile_commands.json
PHONY += compile_commands.json
clean-dirs := $(KBUILD_EXTMOD)
clean: rm-files := $(KBUILD_EXTMOD)/Module.symvers $(KBUILD_EXTMOD)/modules.nsdeps \
$(KBUILD_EXTMOD)/compile_commands.json $(KBUILD_EXTMOD)/.thinlto-cache
PHONY += help
help:
@echo ' Building external modules.'
@echo ' Syntax: make -C path/to/kernel/src M=$$PWD target'
@echo ''
@echo ' modules - default target, build the module(s)'
@echo ' modules_install - install the module'
@echo ' headers_install - Install sanitised kernel headers to INSTALL_HDR_PATH'
@echo ' (default: $(abspath $(INSTALL_HDR_PATH)))'
@echo ' clean - remove generated files in module directory only'
@echo ''
# no-op for external module builds
PHONY += prepare modules_prepare
endif # KBUILD_EXTMOD
# Single targets
# ---------------------------------------------------------------------------
# To build individual files in subdirectories, you can do like this:
#
# make foo/bar/baz.s
#
# The supported suffixes for single-target are listed in 'single-targets'
#
# To build only under specific subdirectories, you can do like this:
#
# make foo/bar/baz/
ifdef single-build
# .ko is special because modpost is needed
single-ko := $(sort $(filter %.ko, $(MAKECMDGOALS)))
single-no-ko := $(sort $(patsubst %.ko,%.mod, $(MAKECMDGOALS)))
$(single-ko): single_modpost
@:
$(single-no-ko): descend
@:
ifeq ($(KBUILD_EXTMOD),)
# For the single build of in-tree modules, use a temporary file to avoid
# the situation of modules_install installing an invalid modules.order.
MODORDER := .modules.tmp
endif
PHONY += single_modpost
single_modpost: $(single-no-ko) modules_prepare
$(Q){ $(foreach m, $(single-ko), echo $(extmod-prefix)$m;) } > $(MODORDER)
$(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
KBUILD_MODULES := 1
export KBUILD_SINGLE_TARGETS := $(addprefix $(extmod-prefix), $(single-no-ko))
# trim unrelated directories
build-dirs := $(foreach d, $(build-dirs), \
$(if $(filter $(d)/%, $(KBUILD_SINGLE_TARGETS)), $(d)))
endif
ifndef CONFIG_MODULES
KBUILD_MODULES :=
endif
# Handle descending into subdirectories listed in $(build-dirs)
# Preset locale variables to speed up the build process. Limit locale
# tweaks to this spot to avoid wrong language settings when running
# make menuconfig etc.
# Error messages still appears in the original language
PHONY += descend $(build-dirs)
descend: $(build-dirs)
$(build-dirs): prepare
$(Q)$(MAKE) $(build)=$@ \
single-build=$(if $(filter-out $@/, $(filter $@/%, $(KBUILD_SINGLE_TARGETS))),1) \
need-builtin=1 need-modorder=1
clean-dirs := $(addprefix _clean_, $(clean-dirs))
PHONY += $(clean-dirs) clean
$(clean-dirs):
$(Q)$(MAKE) $(clean)=$(patsubst _clean_%,%,$@)
clean: $(clean-dirs)
$(call cmd,rmfiles)
@find $(if $(KBUILD_EXTMOD), $(KBUILD_EXTMOD), .) $(RCS_FIND_IGNORE) \
\( -name '*.[aios]' -o -name '*.ko' -o -name '.*.cmd' \
-o -name '*.ko.*' \
-o -name '*.dtb' -o -name '*.dtb.S' -o -name '*.dt.yaml' \
-o -name '*.dwo' -o -name '*.lst' \
-o -name '*.su' -o -name '*.mod' \
-o -name '.*.d' -o -name '.*.tmp' -o -name '*.mod.c' \
-o -name '*.lex.c' -o -name '*.tab.[ch]' \
-o -name '*.asn1.[ch]' \
-o -name '*.symtypes' -o -name 'modules.order' \
-o -name '.tmp_*.o.*' \
-o -name '*.c.[012]*.*' \
-o -name '*.ll' \
-o -name '*.gcno' \
-o -name '*.*.symversions' \) -type f -print | xargs rm -f
# Generate tags for editors
# ---------------------------------------------------------------------------
quiet_cmd_tags = GEN $@
cmd_tags = $(BASH) $(srctree)/scripts/tags.sh $@
tags TAGS cscope gtags: FORCE
$(call cmd,tags)
# Script to generate missing namespace dependencies
# ---------------------------------------------------------------------------
PHONY += nsdeps
nsdeps: export KBUILD_NSDEPS=1
nsdeps: modules
$(Q)$(CONFIG_SHELL) $(srctree)/scripts/nsdeps
# Clang Tooling
# ---------------------------------------------------------------------------
quiet_cmd_gen_compile_commands = GEN $@
cmd_gen_compile_commands = $(PYTHON3) $< -a $(AR) -o $@ $(filter-out $<, $(real-prereqs))
$(extmod-prefix)compile_commands.json: scripts/clang-tools/gen_compile_commands.py \
$(if $(KBUILD_EXTMOD),,$(KBUILD_VMLINUX_OBJS) $(KBUILD_VMLINUX_LIBS)) \
$(if $(CONFIG_MODULES), $(MODORDER)) FORCE
$(call if_changed,gen_compile_commands)
targets += $(extmod-prefix)compile_commands.json
PHONY += clang-tidy clang-analyzer
ifdef CONFIG_CC_IS_CLANG
quiet_cmd_clang_tools = CHECK $<
cmd_clang_tools = $(PYTHON3) $(srctree)/scripts/clang-tools/run-clang-tools.py $@ $<
clang-tidy clang-analyzer: $(extmod-prefix)compile_commands.json
$(call cmd,clang_tools)
else
clang-tidy clang-analyzer:
@echo "$@ requires CC=clang" >&2
@false
endif
# Scripts to check various things for consistency
# ---------------------------------------------------------------------------
PHONY += includecheck versioncheck coccicheck export_report
includecheck:
find $(srctree)/* $(RCS_FIND_IGNORE) \
-name '*.[hcS]' -type f -print | sort \
| xargs $(PERL) -w $(srctree)/scripts/checkincludes.pl
versioncheck:
find $(srctree)/* $(RCS_FIND_IGNORE) \
-name '*.[hcS]' -type f -print | sort \
| xargs $(PERL) -w $(srctree)/scripts/checkversion.pl
coccicheck:
$(Q)$(BASH) $(srctree)/scripts/$@
export_report:
$(PERL) $(srctree)/scripts/export_report.pl
PHONY += checkstack kernelrelease kernelversion image_name
# UML needs a little special treatment here. It wants to use the host
# toolchain, so needs $(SUBARCH) passed to checkstack.pl. Everyone
# else wants $(ARCH), including people doing cross-builds, which means
# that $(SUBARCH) doesn't work here.
ifeq ($(ARCH), um)
CHECKSTACK_ARCH := $(SUBARCH)
else
CHECKSTACK_ARCH := $(ARCH)
endif
checkstack:
$(OBJDUMP) -d vmlinux $$(find . -name '*.ko') | \
$(PERL) $(srctree)/scripts/checkstack.pl $(CHECKSTACK_ARCH)
kernelrelease:
@echo "$(KERNELVERSION)$$($(CONFIG_SHELL) $(srctree)/scripts/setlocalversion \
$(srctree) $(BRANCH) $(KMI_GENERATION))"
kernelversion:
@echo $(KERNELVERSION)
image_name:
@echo $(KBUILD_IMAGE)
# Clear a bunch of variables before executing the submake
ifeq ($(quiet),silent_)
tools_silent=s
endif
tools/: FORCE
$(Q)mkdir -p $(objtree)/tools
$(Q)$(MAKE) LDFLAGS= MAKEFLAGS="$(tools_silent) $(filter --j% -j,$(MAKEFLAGS))" O=$(abspath $(objtree)) subdir=tools -C $(srctree)/tools/
tools/%: FORCE
$(Q)mkdir -p $(objtree)/tools
$(Q)$(MAKE) LDFLAGS= MAKEFLAGS="$(tools_silent) $(filter --j% -j,$(MAKEFLAGS))" O=$(abspath $(objtree)) subdir=tools -C $(srctree)/tools/ $*
quiet_cmd_rmfiles = $(if $(wildcard $(rm-files)),CLEAN $(wildcard $(rm-files)))
cmd_rmfiles = rm -rf $(rm-files)
# Run depmod only if we have System.map and depmod is executable
quiet_cmd_depmod = DEPMOD $(KERNELRELEASE)
cmd_depmod = $(CONFIG_SHELL) $(srctree)/scripts/depmod.sh $(DEPMOD) \
$(KERNELRELEASE)
# read saved command lines for existing targets
existing-targets := $(wildcard $(sort $(targets)))
-include $(foreach f,$(existing-targets),$(dir $(f)).$(notdir $(f)).cmd)
endif # config-build
endif # mixed-build
endif # need-sub-make
PHONY += FORCE
FORCE:
# Declare the contents of the PHONY variable as phony. We keep that
# information in a variable so we can use it in if_changed and friends.
.PHONY: $(PHONY)