aboutsummaryrefslogblamecommitdiffstats
blob: 25d59a95bd6681465d9e57af06f77c3d641b0649 (plain) (tree)




















































































                                                                             
                                                                    



































































































































































                                                                              



                                                                  












































































                                                                              
                                                                               































































                                                                           










                                                                
/*
 * Wrapper for decompressing XZ-compressed kernel, initramfs, and initrd
 *
 * Author: Lasse Collin <lasse.collin@tukaani.org>
 *
 * This file has been put into the public domain.
 * You can do whatever you want with this file.
 */

/*
 * Important notes about in-place decompression
 *
 * At least on x86, the kernel is decompressed in place: the compressed data
 * is placed to the end of the output buffer, and the decompressor overwrites
 * most of the compressed data. There must be enough safety margin to
 * guarantee that the write position is always behind the read position.
 *
 * The safety margin for XZ with LZMA2 or BCJ+LZMA2 is calculated below.
 * Note that the margin with XZ is bigger than with Deflate (gzip)!
 *
 * The worst case for in-place decompression is that the beginning of
 * the file is compressed extremely well, and the rest of the file is
 * uncompressible. Thus, we must look for worst-case expansion when the
 * compressor is encoding uncompressible data.
 *
 * The structure of the .xz file in case of a compresed kernel is as follows.
 * Sizes (as bytes) of the fields are in parenthesis.
 *
 *    Stream Header (12)
 *    Block Header:
 *      Block Header (8-12)
 *      Compressed Data (N)
 *      Block Padding (0-3)
 *      CRC32 (4)
 *    Index (8-20)
 *    Stream Footer (12)
 *
 * Normally there is exactly one Block, but let's assume that there are
 * 2-4 Blocks just in case. Because Stream Header and also Block Header
 * of the first Block don't make the decompressor produce any uncompressed
 * data, we can ignore them from our calculations. Block Headers of possible
 * additional Blocks have to be taken into account still. With these
 * assumptions, it is safe to assume that the total header overhead is
 * less than 128 bytes.
 *
 * Compressed Data contains LZMA2 or BCJ+LZMA2 encoded data. Since BCJ
 * doesn't change the size of the data, it is enough to calculate the
 * safety margin for LZMA2.
 *
 * LZMA2 stores the data in chunks. Each chunk has a header whose size is
 * a maximum of 6 bytes, but to get round 2^n numbers, let's assume that
 * the maximum chunk header size is 8 bytes. After the chunk header, there
 * may be up to 64 KiB of actual payload in the chunk. Often the payload is
 * quite a bit smaller though; to be safe, let's assume that an average
 * chunk has only 32 KiB of payload.
 *
 * The maximum uncompressed size of the payload is 2 MiB. The minimum
 * uncompressed size of the payload is in practice never less than the
 * payload size itself. The LZMA2 format would allow uncompressed size
 * to be less than the payload size, but no sane compressor creates such
 * files. LZMA2 supports storing uncompressible data in uncompressed form,
 * so there's never a need to create payloads whose uncompressed size is
 * smaller than the compressed size.
 *
 * The assumption, that the uncompressed size of the payload is never
 * smaller than the payload itself, is valid only when talking about
 * the payload as a whole. It is possible that the payload has parts where
 * the decompressor consumes more input than it produces output. Calculating
 * the worst case for this would be tricky. Instead of trying to do that,
 * let's simply make sure that the decompressor never overwrites any bytes
 * of the payload which it is currently reading.
 *
 * Now we have enough information to calculate the safety margin. We need
 *   - 128 bytes for the .xz file format headers;
 *   - 8 bytes per every 32 KiB of uncompressed size (one LZMA2 chunk header
 *     per chunk, each chunk having average payload size of 32 KiB); and
 *   - 64 KiB (biggest possible LZMA2 chunk payload size) to make sure that
 *     the decompressor never overwrites anything from the LZMA2 chunk
 *     payload it is currently reading.
 *
 * We get the following formula:
 *
 *    safety_margin = 128 + uncompressed_size * 8 / 32768 + 65536
 *                  = 128 + (uncompressed_size >> 12) + 65536
 *
 * For comparison, according to arch/x86/boot/compressed/misc.c, the
 * equivalent formula for Deflate is this:
 *
 *    safety_margin = 18 + (uncompressed_size >> 12) + 32768
 *
 * Thus, when updating Deflate-only in-place kernel decompressor to
 * support XZ, the fixed overhead has to be increased from 18+32768 bytes
 * to 128+65536 bytes.
 */

/*
 * STATIC is defined to "static" if we are being built for kernel
 * decompression (pre-boot code). <linux/decompress/mm.h> will define
 * STATIC to empty if it wasn't already defined. Since we will need to
 * know later if we are being used for kernel decompression, we define
 * XZ_PREBOOT here.
 */
#ifdef STATIC
#	define XZ_PREBOOT
#endif
#ifdef __KERNEL__
#	include <linux/decompress/mm.h>
#endif
#define XZ_EXTERN STATIC

#ifndef XZ_PREBOOT
#	include <linux/slab.h>
#	include <linux/xz.h>
#else
/*
 * Use the internal CRC32 code instead of kernel's CRC32 module, which
 * is not available in early phase of booting.
 */
#define XZ_INTERNAL_CRC32 1

/*
 * For boot time use, we enable only the BCJ filter of the current
 * architecture or none if no BCJ filter is available for the architecture.
 */
#ifdef CONFIG_X86
#	define XZ_DEC_X86
#endif
#ifdef CONFIG_PPC
#	define XZ_DEC_POWERPC
#endif
#ifdef CONFIG_ARM
#	define XZ_DEC_ARM
#endif
#ifdef CONFIG_IA64
#	define XZ_DEC_IA64
#endif
#ifdef CONFIG_SPARC
#	define XZ_DEC_SPARC
#endif

/*
 * This will get the basic headers so that memeq() and others
 * can be defined.
 */
#include "xz/xz_private.h"

/*
 * Replace the normal allocation functions with the versions from
 * <linux/decompress/mm.h>. vfree() needs to support vfree(NULL)
 * when XZ_DYNALLOC is used, but the pre-boot free() doesn't support it.
 * Workaround it here because the other decompressors don't need it.
 */
#undef kmalloc
#undef kfree
#undef vmalloc
#undef vfree
#define kmalloc(size, flags) malloc(size)
#define kfree(ptr) free(ptr)
#define vmalloc(size) malloc(size)
#define vfree(ptr) do { if (ptr != NULL) free(ptr); } while (0)

/*
 * FIXME: Not all basic memory functions are provided in architecture-specific
 * files (yet). We define our own versions here for now, but this should be
 * only a temporary solution.
 *
 * memeq and memzero are not used much and any remotely sane implementation
 * is fast enough. memcpy/memmove speed matters in multi-call mode, but
 * the kernel image is decompressed in single-call mode, in which only
 * memcpy speed can matter and only if there is a lot of uncompressible data
 * (LZMA2 stores uncompressible chunks in uncompressed form). Thus, the
 * functions below should just be kept small; it's probably not worth
 * optimizing for speed.
 */

#ifndef memeq
static bool memeq(const void *a, const void *b, size_t size)
{
	const uint8_t *x = a;
	const uint8_t *y = b;
	size_t i;

	for (i = 0; i < size; ++i)
		if (x[i] != y[i])
			return false;

	return true;
}
#endif

#ifndef memzero
static void memzero(void *buf, size_t size)
{
	uint8_t *b = buf;
	uint8_t *e = b + size;

	while (b != e)
		*b++ = '\0';
}
#endif

#ifndef memmove
/* Not static to avoid a conflict with the prototype in the Linux headers. */
void *memmove(void *dest, const void *src, size_t size)
{
	uint8_t *d = dest;
	const uint8_t *s = src;
	size_t i;

	if (d < s) {
		for (i = 0; i < size; ++i)
			d[i] = s[i];
	} else if (d > s) {
		i = size;
		while (i-- > 0)
			d[i] = s[i];
	}

	return dest;
}
#endif

/*
 * Since we need memmove anyway, would use it as memcpy too.
 * Commented out for now to avoid breaking things.
 */
/*
#ifndef memcpy
#	define memcpy memmove
#endif
*/

#include "xz/xz_crc32.c"
#include "xz/xz_dec_stream.c"
#include "xz/xz_dec_lzma2.c"
#include "xz/xz_dec_bcj.c"

#endif /* XZ_PREBOOT */

/* Size of the input and output buffers in multi-call mode */
#define XZ_IOBUF_SIZE 4096

/*
 * This function implements the API defined in <linux/decompress/generic.h>.
 *
 * This wrapper will automatically choose single-call or multi-call mode
 * of the native XZ decoder API. The single-call mode can be used only when
 * both input and output buffers are available as a single chunk, i.e. when
 * fill() and flush() won't be used.
 */
STATIC int INIT unxz(unsigned char *in, long in_size,
		     long (*fill)(void *dest, unsigned long size),
		     long (*flush)(void *src, unsigned long size),
		     unsigned char *out, long *in_used,
		     void (*error)(char *x))
{
	struct xz_buf b;
	struct xz_dec *s;
	enum xz_ret ret;
	bool must_free_in = false;

#if XZ_INTERNAL_CRC32
	xz_crc32_init();
#endif

	if (in_used != NULL)
		*in_used = 0;

	if (fill == NULL && flush == NULL)
		s = xz_dec_init(XZ_SINGLE, 0);
	else
		s = xz_dec_init(XZ_DYNALLOC, (uint32_t)-1);

	if (s == NULL)
		goto error_alloc_state;

	if (flush == NULL) {
		b.out = out;
		b.out_size = (size_t)-1;
	} else {
		b.out_size = XZ_IOBUF_SIZE;
		b.out = malloc(XZ_IOBUF_SIZE);
		if (b.out == NULL)
			goto error_alloc_out;
	}

	if (in == NULL) {
		must_free_in = true;
		in = malloc(XZ_IOBUF_SIZE);
		if (in == NULL)
			goto error_alloc_in;
	}

	b.in = in;
	b.in_pos = 0;
	b.in_size = in_size;
	b.out_pos = 0;

	if (fill == NULL && flush == NULL) {
		ret = xz_dec_run(s, &b);
	} else {
		do {
			if (b.in_pos == b.in_size && fill != NULL) {
				if (in_used != NULL)
					*in_used += b.in_pos;

				b.in_pos = 0;

				in_size = fill(in, XZ_IOBUF_SIZE);
				if (in_size < 0) {
					/*
					 * This isn't an optimal error code
					 * but it probably isn't worth making
					 * a new one either.
					 */
					ret = XZ_BUF_ERROR;
					break;
				}

				b.in_size = in_size;
			}

			ret = xz_dec_run(s, &b);

			if (flush != NULL && (b.out_pos == b.out_size
					|| (ret != XZ_OK && b.out_pos > 0))) {
				/*
				 * Setting ret here may hide an error
				 * returned by xz_dec_run(), but probably
				 * it's not too bad.
				 */
				if (flush(b.out, b.out_pos) != (long)b.out_pos)
					ret = XZ_BUF_ERROR;

				b.out_pos = 0;
			}
		} while (ret == XZ_OK);

		if (must_free_in)
			free(in);

		if (flush != NULL)
			free(b.out);
	}

	if (in_used != NULL)
		*in_used += b.in_pos;

	xz_dec_end(s);

	switch (ret) {
	case XZ_STREAM_END:
		return 0;

	case XZ_MEM_ERROR:
		/* This can occur only in multi-call mode. */
		error("XZ decompressor ran out of memory");
		break;

	case XZ_FORMAT_ERROR:
		error("Input is not in the XZ format (wrong magic bytes)");
		break;

	case XZ_OPTIONS_ERROR:
		error("Input was encoded with settings that are not "
				"supported by this XZ decoder");
		break;

	case XZ_DATA_ERROR:
	case XZ_BUF_ERROR:
		error("XZ-compressed data is corrupt");
		break;

	default:
		error("Bug in the XZ decompressor");
		break;
	}

	return -1;

error_alloc_in:
	if (flush != NULL)
		free(b.out);

error_alloc_out:
	xz_dec_end(s);

error_alloc_state:
	error("XZ decompressor ran out of memory");
	return -1;
}

/*
 * This macro is used by architecture-specific files to decompress
 * the kernel image.
 */
#ifdef XZ_PREBOOT
STATIC int INIT __decompress(unsigned char *buf, long len,
			   long (*fill)(void*, unsigned long),
			   long (*flush)(void*, unsigned long),
			   unsigned char *out_buf, long olen,
			   long *pos,
			   void (*error)(char *x))
{
	return unxz(buf, len, fill, flush, out_buf, pos, error);
}
#endif