aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorAndi Kleen2014-07-30 13:50:18 -0500
committerMichal Marek2014-07-30 15:54:52 -0500
commit866ced950bcd54820c3e571229356adc2b2dd72e (patch)
tree13cd5b869ab355f7bd193aed1452d260b1165808 /.gitignore
parent011bf1254772b20083b1bab53f3aa58b1ec95eb1 (diff)
downloadkernel-866ced950bcd54820c3e571229356adc2b2dd72e.tar.gz
kernel-866ced950bcd54820c3e571229356adc2b2dd72e.tar.xz
kernel-866ced950bcd54820c3e571229356adc2b2dd72e.zip
kbuild: Support split debug info v4
This is an alternative approach to lower the overhead of debug info (as we discussed a few days ago) gcc 4.7+ and newer binutils have a new "split debug info" debug info model where the debug info is only written once into central ".dwo" files. This avoids having to copy it around multiple times, from the object files to the final executable. It lowers the disk space requirements. In addition it defaults to compressed debug data. More details here: http://gcc.gnu.org/wiki/DebugFission This patch adds a new option to enable it. It has to be an option, because it'll undoubtedly break everyone's debuginfo packaging scheme. gdb/objdump/etc. all still work, if you have new enough versions. I don't see big compile wins (maybe a second or two faster or so), but the object dirs with debuginfo get significantly smaller. My standard kernel config (slightly bigger than defconfig) shrinks from 2.9G disk space to 1.1G objdir (with non reduced debuginfo). I presume if you are IO limited the compile time difference will be larger. Only problem I've seen so far is that it doesn't play well with older versions of ccache (apparently fixed, see https://bugzilla.samba.org/show_bug.cgi?id=10005) v2: various fixes from Dirk Gouders. Improve commit message slightly. v3: Fix clean rules and improve Kconfig slightly v4: Fix merge error in last version (Sam Ravnborg) Clarify description that it mainly helps disk size. Cc: Dirk Gouders <dirk@gouders.net> Signed-off-by: Andi Kleen <ak@linux.intel.com> Acked-by: Sam Ravnborg <sam@ravnborg.org> Signed-off-by: Michal Marek <mmarek@suse.cz>
Diffstat (limited to '.gitignore')
-rw-r--r--.gitignore1
1 files changed, 1 insertions, 0 deletions
diff --git a/.gitignore b/.gitignore
index f4c0b091dcf4..e213b27f3921 100644
--- a/.gitignore
+++ b/.gitignore
@@ -34,6 +34,7 @@
34*.gcno 34*.gcno
35modules.builtin 35modules.builtin
36Module.symvers 36Module.symvers
37*.dwo
37 38
38# 39#
39# Top-level generic files 40# Top-level generic files