diff options
author | Daniel Rosenberg | 2020-11-19 00:09:02 -0600 |
---|---|---|
committer | Jaegeuk Kim | 2020-12-21 15:33:13 -0600 |
commit | c35a25795ed5cbcdf1ca93959ae8e5ec49822ace (patch) | |
tree | c2aeb1a6e10dde23794e5c76d59e7e8815b31c2b | |
parent | c60814e9fb8b99da3e31222966ea0a0934c79500 (diff) | |
download | kernel-c35a25795ed5cbcdf1ca93959ae8e5ec49822ace.tar.gz kernel-c35a25795ed5cbcdf1ca93959ae8e5ec49822ace.tar.xz kernel-c35a25795ed5cbcdf1ca93959ae8e5ec49822ace.zip |
libfs: Add generic function for setting dentry_ops
This adds a function to set dentry operations at lookup time that will
work for both encrypted filenames and casefolded filenames.
A filesystem that supports both features simultaneously can use this
function during lookup preparations to set up its dentry operations once
fscrypt no longer does that itself.
Currently the casefolding dentry operation are always set if the
filesystem defines an encoding because the features is toggleable on
empty directories. Unlike in the encryption case, the dentry operations
used come from the parent. Since we don't know what set of functions
we'll eventually need, and cannot change them later, we enable the
casefolding operations if the filesystem supports them at all.
By splitting out the various cases, we support as few dentry operations
as we can get away with, maximizing compatibility with overlayfs, which
will not function if a filesystem supports certain dentry_operations.
Signed-off-by: Daniel Rosenberg <drosen@google.com>
Reviewed-by: Theodore Ts'o <tytso@mit.edu>
Reviewed-by: Eric Biggers <ebiggers@google.com>
Reviewed-by: Gabriel Krisman Bertazi <krisman@collabora.com>
Signed-off-by: Jaegeuk Kim <jaegeuk@kernel.org>
-rw-r--r-- | fs/libfs.c | 70 | ||||
-rw-r--r-- | include/linux/fs.h | 1 |
2 files changed, 71 insertions, 0 deletions
diff --git a/fs/libfs.c b/fs/libfs.c index 7124c2e8df2f..d1c3bade9f30 100644 --- a/fs/libfs.c +++ b/fs/libfs.c | |||
@@ -1451,4 +1451,74 @@ int generic_ci_d_hash(const struct dentry *dentry, struct qstr *str) | |||
1451 | return 0; | 1451 | return 0; |
1452 | } | 1452 | } |
1453 | EXPORT_SYMBOL(generic_ci_d_hash); | 1453 | EXPORT_SYMBOL(generic_ci_d_hash); |
1454 | |||
1455 | static const struct dentry_operations generic_ci_dentry_ops = { | ||
1456 | .d_hash = generic_ci_d_hash, | ||
1457 | .d_compare = generic_ci_d_compare, | ||
1458 | }; | ||
1459 | #endif | ||
1460 | |||
1461 | #ifdef CONFIG_FS_ENCRYPTION | ||
1462 | static const struct dentry_operations generic_encrypted_dentry_ops = { | ||
1463 | .d_revalidate = fscrypt_d_revalidate, | ||
1464 | }; | ||
1465 | #endif | ||
1466 | |||
1467 | #if defined(CONFIG_FS_ENCRYPTION) && defined(CONFIG_UNICODE) | ||
1468 | static const struct dentry_operations generic_encrypted_ci_dentry_ops = { | ||
1469 | .d_hash = generic_ci_d_hash, | ||
1470 | .d_compare = generic_ci_d_compare, | ||
1471 | .d_revalidate = fscrypt_d_revalidate, | ||
1472 | }; | ||
1473 | #endif | ||
1474 | |||
1475 | /** | ||
1476 | * generic_set_encrypted_ci_d_ops - helper for setting d_ops for given dentry | ||
1477 | * @dentry: dentry to set ops on | ||
1478 | * | ||
1479 | * Casefolded directories need d_hash and d_compare set, so that the dentries | ||
1480 | * contained in them are handled case-insensitively. Note that these operations | ||
1481 | * are needed on the parent directory rather than on the dentries in it, and | ||
1482 | * while the casefolding flag can be toggled on and off on an empty directory, | ||
1483 | * dentry_operations can't be changed later. As a result, if the filesystem has | ||
1484 | * casefolding support enabled at all, we have to give all dentries the | ||
1485 | * casefolding operations even if their inode doesn't have the casefolding flag | ||
1486 | * currently (and thus the casefolding ops would be no-ops for now). | ||
1487 | * | ||
1488 | * Encryption works differently in that the only dentry operation it needs is | ||
1489 | * d_revalidate, which it only needs on dentries that have the no-key name flag. | ||
1490 | * The no-key flag can't be set "later", so we don't have to worry about that. | ||
1491 | * | ||
1492 | * Finally, to maximize compatibility with overlayfs (which isn't compatible | ||
1493 | * with certain dentry operations) and to avoid taking an unnecessary | ||
1494 | * performance hit, we use custom dentry_operations for each possible | ||
1495 | * combination rather than always installing all operations. | ||
1496 | */ | ||
1497 | void generic_set_encrypted_ci_d_ops(struct dentry *dentry) | ||
1498 | { | ||
1499 | #ifdef CONFIG_FS_ENCRYPTION | ||
1500 | bool needs_encrypt_ops = dentry->d_flags & DCACHE_NOKEY_NAME; | ||
1501 | #endif | ||
1502 | #ifdef CONFIG_UNICODE | ||
1503 | bool needs_ci_ops = dentry->d_sb->s_encoding; | ||
1504 | #endif | ||
1505 | #if defined(CONFIG_FS_ENCRYPTION) && defined(CONFIG_UNICODE) | ||
1506 | if (needs_encrypt_ops && needs_ci_ops) { | ||
1507 | d_set_d_op(dentry, &generic_encrypted_ci_dentry_ops); | ||
1508 | return; | ||
1509 | } | ||
1454 | #endif | 1510 | #endif |
1511 | #ifdef CONFIG_FS_ENCRYPTION | ||
1512 | if (needs_encrypt_ops) { | ||
1513 | d_set_d_op(dentry, &generic_encrypted_dentry_ops); | ||
1514 | return; | ||
1515 | } | ||
1516 | #endif | ||
1517 | #ifdef CONFIG_UNICODE | ||
1518 | if (needs_ci_ops) { | ||
1519 | d_set_d_op(dentry, &generic_ci_dentry_ops); | ||
1520 | return; | ||
1521 | } | ||
1522 | #endif | ||
1523 | } | ||
1524 | EXPORT_SYMBOL(generic_set_encrypted_ci_d_ops); | ||
diff --git a/include/linux/fs.h b/include/linux/fs.h index 8667d0cdc71e..11345e66353b 100644 --- a/include/linux/fs.h +++ b/include/linux/fs.h | |||
@@ -3202,6 +3202,7 @@ extern int generic_ci_d_hash(const struct dentry *dentry, struct qstr *str); | |||
3202 | extern int generic_ci_d_compare(const struct dentry *dentry, unsigned int len, | 3202 | extern int generic_ci_d_compare(const struct dentry *dentry, unsigned int len, |
3203 | const char *str, const struct qstr *name); | 3203 | const char *str, const struct qstr *name); |
3204 | #endif | 3204 | #endif |
3205 | extern void generic_set_encrypted_ci_d_ops(struct dentry *dentry); | ||
3205 | 3206 | ||
3206 | #ifdef CONFIG_MIGRATION | 3207 | #ifdef CONFIG_MIGRATION |
3207 | extern int buffer_migrate_page(struct address_space *, | 3208 | extern int buffer_migrate_page(struct address_space *, |