diff options
author | Andrey Ryabinin | 2016-01-20 17:00:55 -0600 |
---|---|---|
committer | Linus Torvalds | 2016-01-20 19:09:18 -0600 |
commit | c6d308534aef6c99904bf5862066360ae067abc4 (patch) | |
tree | 0c3b9cabd10101dea1c6433f76835c17c538d5fe /Makefile | |
parent | 68920c973254c5b71a684645c5f6f82d6732c5d6 (diff) | |
download | kernel-c6d308534aef6c99904bf5862066360ae067abc4.tar.gz kernel-c6d308534aef6c99904bf5862066360ae067abc4.tar.xz kernel-c6d308534aef6c99904bf5862066360ae067abc4.zip |
UBSAN: run-time undefined behavior sanity checker
UBSAN uses compile-time instrumentation to catch undefined behavior
(UB). Compiler inserts code that perform certain kinds of checks before
operations that could cause UB. If check fails (i.e. UB detected)
__ubsan_handle_* function called to print error message.
So the most of the work is done by compiler. This patch just implements
ubsan handlers printing errors.
GCC has this capability since 4.9.x [1] (see -fsanitize=undefined
option and its suboptions).
However GCC 5.x has more checkers implemented [2].
Article [3] has a bit more details about UBSAN in the GCC.
[1] - https://gcc.gnu.org/onlinedocs/gcc-4.9.0/gcc/Debugging-Options.html
[2] - https://gcc.gnu.org/onlinedocs/gcc/Debugging-Options.html
[3] - http://developerblog.redhat.com/2014/10/16/gcc-undefined-behavior-sanitizer-ubsan/
Issues which UBSAN has found thus far are:
Found bugs:
* out-of-bounds access - 97840cb67ff5 ("netfilter: nfnetlink: fix
insufficient validation in nfnetlink_bind")
undefined shifts:
* d48458d4a768 ("jbd2: use a better hash function for the revoke
table")
* 10632008b9e1 ("clockevents: Prevent shift out of bounds")
* 'x << -1' shift in ext4 -
http://lkml.kernel.org/r/<5444EF21.8020501@samsung.com>
* undefined rol32(0) -
http://lkml.kernel.org/r/<1449198241-20654-1-git-send-email-sasha.levin@oracle.com>
* undefined dirty_ratelimit calculation -
http://lkml.kernel.org/r/<566594E2.3050306@odin.com>
* undefined roundown_pow_of_two(0) -
http://lkml.kernel.org/r/<1449156616-11474-1-git-send-email-sasha.levin@oracle.com>
* [WONTFIX] undefined shift in __bpf_prog_run -
http://lkml.kernel.org/r/<CACT4Y+ZxoR3UjLgcNdUm4fECLMx2VdtfrENMtRRCdgHB2n0bJA@mail.gmail.com>
WONTFIX here because it should be fixed in bpf program, not in kernel.
signed overflows:
* 32a8df4e0b33f ("sched: Fix odd values in effective_load()
calculations")
* mul overflow in ntp -
http://lkml.kernel.org/r/<1449175608-1146-1-git-send-email-sasha.levin@oracle.com>
* incorrect conversion into rtc_time in rtc_time64_to_tm() -
http://lkml.kernel.org/r/<1449187944-11730-1-git-send-email-sasha.levin@oracle.com>
* unvalidated timespec in io_getevents() -
http://lkml.kernel.org/r/<CACT4Y+bBxVYLQ6LtOKrKtnLthqLHcw-BMp3aqP3mjdAvr9FULQ@mail.gmail.com>
* [NOTABUG] signed overflow in ktime_add_safe() -
http://lkml.kernel.org/r/<CACT4Y+aJ4muRnWxsUe1CMnA6P8nooO33kwG-c8YZg=0Xc8rJqw@mail.gmail.com>
[akpm@linux-foundation.org: fix unused local warning]
[akpm@linux-foundation.org: fix __int128 build woes]
Signed-off-by: Andrey Ryabinin <aryabinin@virtuozzo.com>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Sasha Levin <sasha.levin@oracle.com>
Cc: Randy Dunlap <rdunlap@infradead.org>
Cc: Rasmus Villemoes <linux@rasmusvillemoes.dk>
Cc: Jonathan Corbet <corbet@lwn.net>
Cc: Michal Marek <mmarek@suse.cz>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: "H. Peter Anvin" <hpa@zytor.com>
Cc: Yury Gribov <y.gribov@samsung.com>
Cc: Dmitry Vyukov <dvyukov@google.com>
Cc: Konstantin Khlebnikov <koct9i@gmail.com>
Cc: Kostya Serebryany <kcc@google.com>
Cc: Johannes Berg <johannes@sipsolutions.net>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'Makefile')
-rw-r--r-- | Makefile | 3 |
1 files changed, 2 insertions, 1 deletions
@@ -411,7 +411,7 @@ export MAKE AWK GENKSYMS INSTALLKERNEL PERL PYTHON UTS_MACHINE | |||
411 | export HOSTCXX HOSTCXXFLAGS LDFLAGS_MODULE CHECK CHECKFLAGS | 411 | export HOSTCXX HOSTCXXFLAGS LDFLAGS_MODULE CHECK CHECKFLAGS |
412 | 412 | ||
413 | export KBUILD_CPPFLAGS NOSTDINC_FLAGS LINUXINCLUDE OBJCOPYFLAGS LDFLAGS | 413 | export KBUILD_CPPFLAGS NOSTDINC_FLAGS LINUXINCLUDE OBJCOPYFLAGS LDFLAGS |
414 | export KBUILD_CFLAGS CFLAGS_KERNEL CFLAGS_MODULE CFLAGS_GCOV CFLAGS_KASAN | 414 | export KBUILD_CFLAGS CFLAGS_KERNEL CFLAGS_MODULE CFLAGS_GCOV CFLAGS_KASAN CFLAGS_UBSAN |
415 | export KBUILD_AFLAGS AFLAGS_KERNEL AFLAGS_MODULE | 415 | export KBUILD_AFLAGS AFLAGS_KERNEL AFLAGS_MODULE |
416 | export KBUILD_AFLAGS_MODULE KBUILD_CFLAGS_MODULE KBUILD_LDFLAGS_MODULE | 416 | export KBUILD_AFLAGS_MODULE KBUILD_CFLAGS_MODULE KBUILD_LDFLAGS_MODULE |
417 | export KBUILD_AFLAGS_KERNEL KBUILD_CFLAGS_KERNEL | 417 | export KBUILD_AFLAGS_KERNEL KBUILD_CFLAGS_KERNEL |
@@ -784,6 +784,7 @@ endif | |||
784 | 784 | ||
785 | include scripts/Makefile.kasan | 785 | include scripts/Makefile.kasan |
786 | include scripts/Makefile.extrawarn | 786 | include scripts/Makefile.extrawarn |
787 | include scripts/Makefile.ubsan | ||
787 | 788 | ||
788 | # Add any arch overrides and user supplied CPPFLAGS, AFLAGS and CFLAGS as the | 789 | # Add any arch overrides and user supplied CPPFLAGS, AFLAGS and CFLAGS as the |
789 | # last assignments | 790 | # last assignments |