diff options
author | Linus Torvalds | 2005-04-16 17:20:36 -0500 |
---|---|---|
committer | Linus Torvalds | 2005-04-16 17:20:36 -0500 |
commit | 1da177e4c3f41524e886b7f1b8a0c1fc7321cac2 (patch) | |
tree | 0bba044c4ce775e45a88a51686b5d9f90697ea9d /README | |
download | kernel-1da177e4c3f41524e886b7f1b8a0c1fc7321cac2.tar.gz kernel-1da177e4c3f41524e886b7f1b8a0c1fc7321cac2.tar.xz kernel-1da177e4c3f41524e886b7f1b8a0c1fc7321cac2.zip |
Linux-2.6.12-rc2v2.6.12-rc2
Initial git repository build. I'm not bothering with the full history,
even though we have it. We can create a separate "historical" git
archive of that later if we want to, and in the meantime it's about
3.2GB when imported into git - space that would just make the early
git days unnecessarily complicated, when we don't have a lot of good
infrastructure for it.
Let it rip!
Diffstat (limited to 'README')
-rw-r--r-- | README | 305 |
1 files changed, 305 insertions, 0 deletions
diff --git a/README b/README new file mode 100644 index 000000000000..0df20f07227b --- /dev/null +++ b/README | |||
@@ -0,0 +1,305 @@ | |||
1 | Linux kernel release 2.6.xx | ||
2 | |||
3 | These are the release notes for Linux version 2.6. Read them carefully, | ||
4 | as they tell you what this is all about, explain how to install the | ||
5 | kernel, and what to do if something goes wrong. | ||
6 | |||
7 | WHAT IS LINUX? | ||
8 | |||
9 | Linux is a Unix clone written from scratch by Linus Torvalds with | ||
10 | assistance from a loosely-knit team of hackers across the Net. | ||
11 | It aims towards POSIX compliance. | ||
12 | |||
13 | It has all the features you would expect in a modern fully-fledged | ||
14 | Unix, including true multitasking, virtual memory, shared libraries, | ||
15 | demand loading, shared copy-on-write executables, proper memory | ||
16 | management and TCP/IP networking. | ||
17 | |||
18 | It is distributed under the GNU General Public License - see the | ||
19 | accompanying COPYING file for more details. | ||
20 | |||
21 | ON WHAT HARDWARE DOES IT RUN? | ||
22 | |||
23 | Linux was first developed for 386/486-based PCs. These days it also | ||
24 | runs on ARMs, DEC Alphas, SUN Sparcs, M68000 machines (like Atari and | ||
25 | Amiga), MIPS and PowerPC, and others. | ||
26 | |||
27 | DOCUMENTATION: | ||
28 | |||
29 | - There is a lot of documentation available both in electronic form on | ||
30 | the Internet and in books, both Linux-specific and pertaining to | ||
31 | general UNIX questions. I'd recommend looking into the documentation | ||
32 | subdirectories on any Linux FTP site for the LDP (Linux Documentation | ||
33 | Project) books. This README is not meant to be documentation on the | ||
34 | system: there are much better sources available. | ||
35 | |||
36 | - There are various README files in the Documentation/ subdirectory: | ||
37 | these typically contain kernel-specific installation notes for some | ||
38 | drivers for example. See Documentation/00-INDEX for a list of what | ||
39 | is contained in each file. Please read the Changes file, as it | ||
40 | contains information about the problems, which may result by upgrading | ||
41 | your kernel. | ||
42 | |||
43 | - The Documentation/DocBook/ subdirectory contains several guides for | ||
44 | kernel developers and users. These guides can be rendered in a | ||
45 | number of formats: PostScript (.ps), PDF, and HTML, among others. | ||
46 | After installation, "make psdocs", "make pdfdocs", or "make htmldocs" | ||
47 | will render the documentation in the requested format. | ||
48 | |||
49 | INSTALLING the kernel: | ||
50 | |||
51 | - If you install the full sources, put the kernel tarball in a | ||
52 | directory where you have permissions (eg. your home directory) and | ||
53 | unpack it: | ||
54 | |||
55 | gzip -cd linux-2.6.XX.tar.gz | tar xvf - | ||
56 | |||
57 | Replace "XX" with the version number of the latest kernel. | ||
58 | |||
59 | Do NOT use the /usr/src/linux area! This area has a (usually | ||
60 | incomplete) set of kernel headers that are used by the library header | ||
61 | files. They should match the library, and not get messed up by | ||
62 | whatever the kernel-du-jour happens to be. | ||
63 | |||
64 | - You can also upgrade between 2.6.xx releases by patching. Patches are | ||
65 | distributed in the traditional gzip and the new bzip2 format. To | ||
66 | install by patching, get all the newer patch files, enter the | ||
67 | top level directory of the kernel source (linux-2.6.xx) and execute: | ||
68 | |||
69 | gzip -cd ../patch-2.6.xx.gz | patch -p1 | ||
70 | |||
71 | or | ||
72 | bzip2 -dc ../patch-2.6.xx.bz2 | patch -p1 | ||
73 | |||
74 | (repeat xx for all versions bigger than the version of your current | ||
75 | source tree, _in_order_) and you should be ok. You may want to remove | ||
76 | the backup files (xxx~ or xxx.orig), and make sure that there are no | ||
77 | failed patches (xxx# or xxx.rej). If there are, either you or me has | ||
78 | made a mistake. | ||
79 | |||
80 | Alternatively, the script patch-kernel can be used to automate this | ||
81 | process. It determines the current kernel version and applies any | ||
82 | patches found. | ||
83 | |||
84 | linux/scripts/patch-kernel linux | ||
85 | |||
86 | The first argument in the command above is the location of the | ||
87 | kernel source. Patches are applied from the current directory, but | ||
88 | an alternative directory can be specified as the second argument. | ||
89 | |||
90 | - Make sure you have no stale .o files and dependencies lying around: | ||
91 | |||
92 | cd linux | ||
93 | make mrproper | ||
94 | |||
95 | You should now have the sources correctly installed. | ||
96 | |||
97 | SOFTWARE REQUIREMENTS | ||
98 | |||
99 | Compiling and running the 2.6.xx kernels requires up-to-date | ||
100 | versions of various software packages. Consult | ||
101 | Documentation/Changes for the minimum version numbers required | ||
102 | and how to get updates for these packages. Beware that using | ||
103 | excessively old versions of these packages can cause indirect | ||
104 | errors that are very difficult to track down, so don't assume that | ||
105 | you can just update packages when obvious problems arise during | ||
106 | build or operation. | ||
107 | |||
108 | BUILD directory for the kernel: | ||
109 | |||
110 | When compiling the kernel all output files will per default be | ||
111 | stored together with the kernel source code. | ||
112 | Using the option "make O=output/dir" allow you to specify an alternate | ||
113 | place for the output files (including .config). | ||
114 | Example: | ||
115 | kernel source code: /usr/src/linux-2.6.N | ||
116 | build directory: /home/name/build/kernel | ||
117 | |||
118 | To configure and build the kernel use: | ||
119 | cd /usr/src/linux-2.6.N | ||
120 | make O=/home/name/build/kernel menuconfig | ||
121 | make O=/home/name/build/kernel | ||
122 | sudo make O=/home/name/build/kernel modules_install install | ||
123 | |||
124 | Please note: If the 'O=output/dir' option is used then it must be | ||
125 | used for all invocations of make. | ||
126 | |||
127 | CONFIGURING the kernel: | ||
128 | |||
129 | Do not skip this step even if you are only upgrading one minor | ||
130 | version. New configuration options are added in each release, and | ||
131 | odd problems will turn up if the configuration files are not set up | ||
132 | as expected. If you want to carry your existing configuration to a | ||
133 | new version with minimal work, use "make oldconfig", which will | ||
134 | only ask you for the answers to new questions. | ||
135 | |||
136 | - Alternate configuration commands are: | ||
137 | "make menuconfig" Text based color menus, radiolists & dialogs. | ||
138 | "make xconfig" X windows (Qt) based configuration tool. | ||
139 | "make gconfig" X windows (Gtk) based configuration tool. | ||
140 | "make oldconfig" Default all questions based on the contents of | ||
141 | your existing ./.config file. | ||
142 | |||
143 | NOTES on "make config": | ||
144 | - having unnecessary drivers will make the kernel bigger, and can | ||
145 | under some circumstances lead to problems: probing for a | ||
146 | nonexistent controller card may confuse your other controllers | ||
147 | - compiling the kernel with "Processor type" set higher than 386 | ||
148 | will result in a kernel that does NOT work on a 386. The | ||
149 | kernel will detect this on bootup, and give up. | ||
150 | - A kernel with math-emulation compiled in will still use the | ||
151 | coprocessor if one is present: the math emulation will just | ||
152 | never get used in that case. The kernel will be slightly larger, | ||
153 | but will work on different machines regardless of whether they | ||
154 | have a math coprocessor or not. | ||
155 | - the "kernel hacking" configuration details usually result in a | ||
156 | bigger or slower kernel (or both), and can even make the kernel | ||
157 | less stable by configuring some routines to actively try to | ||
158 | break bad code to find kernel problems (kmalloc()). Thus you | ||
159 | should probably answer 'n' to the questions for | ||
160 | "development", "experimental", or "debugging" features. | ||
161 | |||
162 | - Check the top Makefile for further site-dependent configuration | ||
163 | (default SVGA mode etc). | ||
164 | |||
165 | COMPILING the kernel: | ||
166 | |||
167 | - Make sure you have gcc 2.95.3 available. | ||
168 | gcc 2.91.66 (egcs-1.1.2), and gcc 2.7.2.3 are known to miscompile | ||
169 | some parts of the kernel, and are *no longer supported*. | ||
170 | Also remember to upgrade your binutils package (for as/ld/nm and company) | ||
171 | if necessary. For more information, refer to Documentation/Changes. | ||
172 | |||
173 | Please note that you can still run a.out user programs with this kernel. | ||
174 | |||
175 | - Do a "make" to create a compressed kernel image. It is also | ||
176 | possible to do "make install" if you have lilo installed to suit the | ||
177 | kernel makefiles, but you may want to check your particular lilo setup first. | ||
178 | |||
179 | To do the actual install you have to be root, but none of the normal | ||
180 | build should require that. Don't take the name of root in vain. | ||
181 | |||
182 | - If you configured any of the parts of the kernel as `modules', you | ||
183 | will also have to do "make modules_install". | ||
184 | |||
185 | - Keep a backup kernel handy in case something goes wrong. This is | ||
186 | especially true for the development releases, since each new release | ||
187 | contains new code which has not been debugged. Make sure you keep a | ||
188 | backup of the modules corresponding to that kernel, as well. If you | ||
189 | are installing a new kernel with the same version number as your | ||
190 | working kernel, make a backup of your modules directory before you | ||
191 | do a "make modules_install". | ||
192 | |||
193 | - In order to boot your new kernel, you'll need to copy the kernel | ||
194 | image (e.g. .../linux/arch/i386/boot/bzImage after compilation) | ||
195 | to the place where your regular bootable kernel is found. | ||
196 | |||
197 | - Booting a kernel directly from a floppy without the assistance of a | ||
198 | bootloader such as LILO, is no longer supported. | ||
199 | |||
200 | If you boot Linux from the hard drive, chances are you use LILO which | ||
201 | uses the kernel image as specified in the file /etc/lilo.conf. The | ||
202 | kernel image file is usually /vmlinuz, /boot/vmlinuz, /bzImage or | ||
203 | /boot/bzImage. To use the new kernel, save a copy of the old image | ||
204 | and copy the new image over the old one. Then, you MUST RERUN LILO | ||
205 | to update the loading map!! If you don't, you won't be able to boot | ||
206 | the new kernel image. | ||
207 | |||
208 | Reinstalling LILO is usually a matter of running /sbin/lilo. | ||
209 | You may wish to edit /etc/lilo.conf to specify an entry for your | ||
210 | old kernel image (say, /vmlinux.old) in case the new one does not | ||
211 | work. See the LILO docs for more information. | ||
212 | |||
213 | After reinstalling LILO, you should be all set. Shutdown the system, | ||
214 | reboot, and enjoy! | ||
215 | |||
216 | If you ever need to change the default root device, video mode, | ||
217 | ramdisk size, etc. in the kernel image, use the 'rdev' program (or | ||
218 | alternatively the LILO boot options when appropriate). No need to | ||
219 | recompile the kernel to change these parameters. | ||
220 | |||
221 | - Reboot with the new kernel and enjoy. | ||
222 | |||
223 | IF SOMETHING GOES WRONG: | ||
224 | |||
225 | - If you have problems that seem to be due to kernel bugs, please check | ||
226 | the file MAINTAINERS to see if there is a particular person associated | ||
227 | with the part of the kernel that you are having trouble with. If there | ||
228 | isn't anyone listed there, then the second best thing is to mail | ||
229 | them to me (torvalds@osdl.org), and possibly to any other relevant | ||
230 | mailing-list or to the newsgroup. | ||
231 | |||
232 | - In all bug-reports, *please* tell what kernel you are talking about, | ||
233 | how to duplicate the problem, and what your setup is (use your common | ||
234 | sense). If the problem is new, tell me so, and if the problem is | ||
235 | old, please try to tell me when you first noticed it. | ||
236 | |||
237 | - If the bug results in a message like | ||
238 | |||
239 | unable to handle kernel paging request at address C0000010 | ||
240 | Oops: 0002 | ||
241 | EIP: 0010:XXXXXXXX | ||
242 | eax: xxxxxxxx ebx: xxxxxxxx ecx: xxxxxxxx edx: xxxxxxxx | ||
243 | esi: xxxxxxxx edi: xxxxxxxx ebp: xxxxxxxx | ||
244 | ds: xxxx es: xxxx fs: xxxx gs: xxxx | ||
245 | Pid: xx, process nr: xx | ||
246 | xx xx xx xx xx xx xx xx xx xx | ||
247 | |||
248 | or similar kernel debugging information on your screen or in your | ||
249 | system log, please duplicate it *exactly*. The dump may look | ||
250 | incomprehensible to you, but it does contain information that may | ||
251 | help debugging the problem. The text above the dump is also | ||
252 | important: it tells something about why the kernel dumped code (in | ||
253 | the above example it's due to a bad kernel pointer). More information | ||
254 | on making sense of the dump is in Documentation/oops-tracing.txt | ||
255 | |||
256 | - If you compiled the kernel with CONFIG_KALLSYMS you can send the dump | ||
257 | as is, otherwise you will have to use the "ksymoops" program to make | ||
258 | sense of the dump. This utility can be downloaded from | ||
259 | ftp://ftp.<country>.kernel.org/pub/linux/utils/kernel/ksymoops. | ||
260 | Alternately you can do the dump lookup by hand: | ||
261 | |||
262 | - In debugging dumps like the above, it helps enormously if you can | ||
263 | look up what the EIP value means. The hex value as such doesn't help | ||
264 | me or anybody else very much: it will depend on your particular | ||
265 | kernel setup. What you should do is take the hex value from the EIP | ||
266 | line (ignore the "0010:"), and look it up in the kernel namelist to | ||
267 | see which kernel function contains the offending address. | ||
268 | |||
269 | To find out the kernel function name, you'll need to find the system | ||
270 | binary associated with the kernel that exhibited the symptom. This is | ||
271 | the file 'linux/vmlinux'. To extract the namelist and match it against | ||
272 | the EIP from the kernel crash, do: | ||
273 | |||
274 | nm vmlinux | sort | less | ||
275 | |||
276 | This will give you a list of kernel addresses sorted in ascending | ||
277 | order, from which it is simple to find the function that contains the | ||
278 | offending address. Note that the address given by the kernel | ||
279 | debugging messages will not necessarily match exactly with the | ||
280 | function addresses (in fact, that is very unlikely), so you can't | ||
281 | just 'grep' the list: the list will, however, give you the starting | ||
282 | point of each kernel function, so by looking for the function that | ||
283 | has a starting address lower than the one you are searching for but | ||
284 | is followed by a function with a higher address you will find the one | ||
285 | you want. In fact, it may be a good idea to include a bit of | ||
286 | "context" in your problem report, giving a few lines around the | ||
287 | interesting one. | ||
288 | |||
289 | If you for some reason cannot do the above (you have a pre-compiled | ||
290 | kernel image or similar), telling me as much about your setup as | ||
291 | possible will help. | ||
292 | |||
293 | - Alternately, you can use gdb on a running kernel. (read-only; i.e. you | ||
294 | cannot change values or set break points.) To do this, first compile the | ||
295 | kernel with -g; edit arch/i386/Makefile appropriately, then do a "make | ||
296 | clean". You'll also need to enable CONFIG_PROC_FS (via "make config"). | ||
297 | |||
298 | After you've rebooted with the new kernel, do "gdb vmlinux /proc/kcore". | ||
299 | You can now use all the usual gdb commands. The command to look up the | ||
300 | point where your system crashed is "l *0xXXXXXXXX". (Replace the XXXes | ||
301 | with the EIP value.) | ||
302 | |||
303 | gdb'ing a non-running kernel currently fails because gdb (wrongly) | ||
304 | disregards the starting offset for which the kernel is compiled. | ||
305 | |||