aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorMichal Hocko2013-08-22 18:35:46 -0500
committerLinus Torvalds2013-08-23 11:51:22 -0500
commit07555ac144bbf45b1751340c6ee75da1f4e5756d (patch)
treea2e1ef0f4ab35a078c1dfb604cccba30ddf7dfc0 /init/Kconfig
parent4bf93b50fd04118ac7f33a3c2b8a0a1f9fa80bc9 (diff)
downloadkernel-07555ac144bbf45b1751340c6ee75da1f4e5756d.tar.gz
kernel-07555ac144bbf45b1751340c6ee75da1f4e5756d.tar.xz
kernel-07555ac144bbf45b1751340c6ee75da1f4e5756d.zip
memcg: get rid of swapaccount leftovers
The swapaccount kernel parameter without any values has been removed by commit a2c8990aed5a ("memsw: remove noswapaccount kernel parameter") but it seems that we didn't get rid of all the left overs. Make sure that menuconfig help text and kernel-parameters.txt are clear about value for the paramter and remove the stalled comment which is not very much useful on its own. Signed-off-by: Michal Hocko <mhocko@suse.cz> Reported-by: Gergely Risko <gergely@risko.hu> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'init/Kconfig')
-rw-r--r--init/Kconfig2
1 files changed, 1 insertions, 1 deletions
diff --git a/init/Kconfig b/init/Kconfig
index 247084be0590..fed81b576f29 100644
--- a/init/Kconfig
+++ b/init/Kconfig
@@ -955,7 +955,7 @@ config MEMCG_SWAP_ENABLED
955 Memory Resource Controller Swap Extension comes with its price in 955 Memory Resource Controller Swap Extension comes with its price in
956 a bigger memory consumption. General purpose distribution kernels 956 a bigger memory consumption. General purpose distribution kernels
957 which want to enable the feature but keep it disabled by default 957 which want to enable the feature but keep it disabled by default
958 and let the user enable it by swapaccount boot command line 958 and let the user enable it by swapaccount=1 boot command line
959 parameter should have this option unselected. 959 parameter should have this option unselected.
960 For those who want to have the feature enabled by default should 960 For those who want to have the feature enabled by default should
961 select this option (if, for some reason, they need to disable it 961 select this option (if, for some reason, they need to disable it