diff options
author | Kees Cook | 2012-10-02 13:19:29 -0500 |
---|---|---|
committer | Kees Cook | 2013-01-11 13:39:33 -0600 |
commit | 19c92399817995382522c09ca21e8784a028c023 (patch) | |
tree | 3d7f81f6aa8248572154a47b1b2216f22aa18f45 /init/Kconfig | |
parent | d9777b8de415f2e699dcc4ce8825732ba8af732a (diff) | |
download | kernel-19c92399817995382522c09ca21e8784a028c023.tar.gz kernel-19c92399817995382522c09ca21e8784a028c023.tar.xz kernel-19c92399817995382522c09ca21e8784a028c023.zip |
init: remove depends on CONFIG_EXPERIMENTAL
The CONFIG_EXPERIMENTAL config item has not carried much meaning for a
while now and is almost always enabled by default. As agreed during the
Linux kernel summit, remove it from any "depends on" lines in Kconfigs.
CC: "Eric W. Biederman" <ebiederm@xmission.com>
CC: Serge Hallyn <serge.hallyn@canonical.com>
CC: "Paul E. McKenney" <paulmck@linux.vnet.ibm.com>
CC: Andrew Morton <akpm@linux-foundation.org>
CC: Frederic Weisbecker <fweisbec@gmail.com>
Signed-off-by: Kees Cook <keescook@chromium.org>
Acked-by: Serge Hallyn <serge.hallyn@ubuntu.com>
Diffstat (limited to 'init/Kconfig')
-rw-r--r-- | init/Kconfig | 23 |
1 files changed, 10 insertions, 13 deletions
diff --git a/init/Kconfig b/init/Kconfig index 66eefd9ba73c..3020d81c05bc 100644 --- a/init/Kconfig +++ b/init/Kconfig | |||
@@ -220,7 +220,7 @@ config SYSVIPC_SYSCTL | |||
220 | 220 | ||
221 | config POSIX_MQUEUE | 221 | config POSIX_MQUEUE |
222 | bool "POSIX Message Queues" | 222 | bool "POSIX Message Queues" |
223 | depends on NET && EXPERIMENTAL | 223 | depends on NET |
224 | ---help--- | 224 | ---help--- |
225 | POSIX variant of message queues is a part of IPC. In POSIX message | 225 | POSIX variant of message queues is a part of IPC. In POSIX message |
226 | queues every message has a priority which decides about succession | 226 | queues every message has a priority which decides about succession |
@@ -366,7 +366,7 @@ config BSD_PROCESS_ACCT_V3 | |||
366 | at <http://www.gnu.org/software/acct/>. | 366 | at <http://www.gnu.org/software/acct/>. |
367 | 367 | ||
368 | config TASKSTATS | 368 | config TASKSTATS |
369 | bool "Export task/process statistics through netlink (EXPERIMENTAL)" | 369 | bool "Export task/process statistics through netlink" |
370 | depends on NET | 370 | depends on NET |
371 | default n | 371 | default n |
372 | help | 372 | help |
@@ -379,7 +379,7 @@ config TASKSTATS | |||
379 | Say N if unsure. | 379 | Say N if unsure. |
380 | 380 | ||
381 | config TASK_DELAY_ACCT | 381 | config TASK_DELAY_ACCT |
382 | bool "Enable per-task delay accounting (EXPERIMENTAL)" | 382 | bool "Enable per-task delay accounting" |
383 | depends on TASKSTATS | 383 | depends on TASKSTATS |
384 | help | 384 | help |
385 | Collect information on time spent by a task waiting for system | 385 | Collect information on time spent by a task waiting for system |
@@ -390,7 +390,7 @@ config TASK_DELAY_ACCT | |||
390 | Say N if unsure. | 390 | Say N if unsure. |
391 | 391 | ||
392 | config TASK_XACCT | 392 | config TASK_XACCT |
393 | bool "Enable extended accounting over taskstats (EXPERIMENTAL)" | 393 | bool "Enable extended accounting over taskstats" |
394 | depends on TASKSTATS | 394 | depends on TASKSTATS |
395 | help | 395 | help |
396 | Collect extended task accounting data and send the data | 396 | Collect extended task accounting data and send the data |
@@ -399,7 +399,7 @@ config TASK_XACCT | |||
399 | Say N if unsure. | 399 | Say N if unsure. |
400 | 400 | ||
401 | config TASK_IO_ACCOUNTING | 401 | config TASK_IO_ACCOUNTING |
402 | bool "Enable per-task storage I/O accounting (EXPERIMENTAL)" | 402 | bool "Enable per-task storage I/O accounting" |
403 | depends on TASK_XACCT | 403 | depends on TASK_XACCT |
404 | help | 404 | help |
405 | Collect information on the number of bytes of storage I/O which this | 405 | Collect information on the number of bytes of storage I/O which this |
@@ -853,8 +853,8 @@ config MEMCG_SWAP_ENABLED | |||
853 | select this option (if, for some reason, they need to disable it | 853 | select this option (if, for some reason, they need to disable it |
854 | then swapaccount=0 does the trick). | 854 | then swapaccount=0 does the trick). |
855 | config MEMCG_KMEM | 855 | config MEMCG_KMEM |
856 | bool "Memory Resource Controller Kernel Memory accounting (EXPERIMENTAL)" | 856 | bool "Memory Resource Controller Kernel Memory accounting" |
857 | depends on MEMCG && EXPERIMENTAL | 857 | depends on MEMCG |
858 | depends on SLUB || SLAB | 858 | depends on SLUB || SLAB |
859 | help | 859 | help |
860 | The Kernel Memory extension for Memory Resource Controller can limit | 860 | The Kernel Memory extension for Memory Resource Controller can limit |
@@ -866,7 +866,7 @@ config MEMCG_KMEM | |||
866 | 866 | ||
867 | config CGROUP_HUGETLB | 867 | config CGROUP_HUGETLB |
868 | bool "HugeTLB Resource Controller for Control Groups" | 868 | bool "HugeTLB Resource Controller for Control Groups" |
869 | depends on RESOURCE_COUNTERS && HUGETLB_PAGE && EXPERIMENTAL | 869 | depends on RESOURCE_COUNTERS && HUGETLB_PAGE |
870 | default n | 870 | default n |
871 | help | 871 | help |
872 | Provides a cgroup Resource Controller for HugeTLB pages. | 872 | Provides a cgroup Resource Controller for HugeTLB pages. |
@@ -905,7 +905,6 @@ config FAIR_GROUP_SCHED | |||
905 | 905 | ||
906 | config CFS_BANDWIDTH | 906 | config CFS_BANDWIDTH |
907 | bool "CPU bandwidth provisioning for FAIR_GROUP_SCHED" | 907 | bool "CPU bandwidth provisioning for FAIR_GROUP_SCHED" |
908 | depends on EXPERIMENTAL | ||
909 | depends on FAIR_GROUP_SCHED | 908 | depends on FAIR_GROUP_SCHED |
910 | default n | 909 | default n |
911 | help | 910 | help |
@@ -917,7 +916,6 @@ config CFS_BANDWIDTH | |||
917 | 916 | ||
918 | config RT_GROUP_SCHED | 917 | config RT_GROUP_SCHED |
919 | bool "Group scheduling for SCHED_RR/FIFO" | 918 | bool "Group scheduling for SCHED_RR/FIFO" |
920 | depends on EXPERIMENTAL | ||
921 | depends on CGROUP_SCHED | 919 | depends on CGROUP_SCHED |
922 | default n | 920 | default n |
923 | help | 921 | help |
@@ -999,8 +997,7 @@ config IPC_NS | |||
999 | different IPC objects in different namespaces. | 997 | different IPC objects in different namespaces. |
1000 | 998 | ||
1001 | config USER_NS | 999 | config USER_NS |
1002 | bool "User namespace (EXPERIMENTAL)" | 1000 | bool "User namespace" |
1003 | depends on EXPERIMENTAL | ||
1004 | depends on UIDGID_CONVERTED | 1001 | depends on UIDGID_CONVERTED |
1005 | select UIDGID_STRICT_TYPE_CHECKS | 1002 | select UIDGID_STRICT_TYPE_CHECKS |
1006 | 1003 | ||
@@ -1581,7 +1578,7 @@ config MODULE_UNLOAD | |||
1581 | 1578 | ||
1582 | config MODULE_FORCE_UNLOAD | 1579 | config MODULE_FORCE_UNLOAD |
1583 | bool "Forced module unloading" | 1580 | bool "Forced module unloading" |
1584 | depends on MODULE_UNLOAD && EXPERIMENTAL | 1581 | depends on MODULE_UNLOAD |
1585 | help | 1582 | help |
1586 | This option allows you to force a module to unload, even if the | 1583 | This option allows you to force a module to unload, even if the |
1587 | kernel believes it is unsafe: the kernel will remove the module | 1584 | kernel believes it is unsafe: the kernel will remove the module |