diff options
author | Ard Biesheuvel | 2016-03-15 16:58:19 -0500 |
---|---|---|
committer | Linus Torvalds | 2016-03-15 18:55:16 -0500 |
commit | 2213e9a66bb87d8344a1256b4ef568220d9587fb (patch) | |
tree | 0729c7a1170f86b2f830024f12bf6a785f3b3e9e /init/Kconfig | |
parent | 8c996940b3be9c3ac40ce558c270817e1722a95b (diff) | |
download | kernel-2213e9a66bb87d8344a1256b4ef568220d9587fb.tar.gz kernel-2213e9a66bb87d8344a1256b4ef568220d9587fb.tar.xz kernel-2213e9a66bb87d8344a1256b4ef568220d9587fb.zip |
kallsyms: add support for relative offsets in kallsyms address table
Similar to how relative extables are implemented, it is possible to emit
the kallsyms table in such a way that it contains offsets relative to
some anchor point in the kernel image rather than absolute addresses.
On 64-bit architectures, it cuts the size of the kallsyms address table
in half, since offsets between kernel symbols can typically be expressed
in 32 bits. This saves several hundreds of kilobytes of permanent
.rodata on average. In addition, the kallsyms address table is no
longer subject to dynamic relocation when CONFIG_RELOCATABLE is in
effect, so the relocation work done after decompression now doesn't have
to do relocation updates for all these values. This saves up to 24
bytes (i.e., the size of a ELF64 RELA relocation table entry) per value,
which easily adds up to a couple of megabytes of uncompressed __init
data on ppc64 or arm64. Even if these relocation entries typically
compress well, the combined size reduction of 2.8 MB uncompressed for a
ppc64_defconfig build (of which 2.4 MB is __init data) results in a ~500
KB space saving in the compressed image.
Since it is useful for some architectures (like x86) to retain the
ability to emit absolute values as well, this patch also adds support
for capturing both absolute and relative values when
KALLSYMS_ABSOLUTE_PERCPU is in effect, by emitting absolute per-cpu
addresses as positive 32-bit values, and addresses relative to the
lowest encountered relative symbol as negative values, which are
subtracted from the runtime address of this base symbol to produce the
actual address.
Support for the above is enabled by default for all architectures except
IA-64 and Tile-GX, whose symbols are too far apart to capture in this
manner.
Signed-off-by: Ard Biesheuvel <ard.biesheuvel@linaro.org>
Tested-by: Guenter Roeck <linux@roeck-us.net>
Reviewed-by: Kees Cook <keescook@chromium.org>
Tested-by: Kees Cook <keescook@chromium.org>
Cc: Heiko Carstens <heiko.carstens@de.ibm.com>
Cc: Michael Ellerman <mpe@ellerman.id.au>
Cc: Ingo Molnar <mingo@kernel.org>
Cc: H. Peter Anvin <hpa@zytor.com>
Cc: Benjamin Herrenschmidt <benh@kernel.crashing.org>
Cc: Michal Marek <mmarek@suse.cz>
Cc: Rusty Russell <rusty@rustcorp.com.au>
Cc: Arnd Bergmann <arnd@arndb.de>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'init/Kconfig')
-rw-r--r-- | init/Kconfig | 18 |
1 files changed, 18 insertions, 0 deletions
diff --git a/init/Kconfig b/init/Kconfig index b17824a875fa..fd664b3ab99e 100644 --- a/init/Kconfig +++ b/init/Kconfig | |||
@@ -1424,6 +1424,24 @@ config KALLSYMS_ABSOLUTE_PERCPU | |||
1424 | bool | 1424 | bool |
1425 | default X86_64 && SMP | 1425 | default X86_64 && SMP |
1426 | 1426 | ||
1427 | config KALLSYMS_BASE_RELATIVE | ||
1428 | bool | ||
1429 | depends on KALLSYMS | ||
1430 | default !IA64 && !(TILE && 64BIT) | ||
1431 | help | ||
1432 | Instead of emitting them as absolute values in the native word size, | ||
1433 | emit the symbol references in the kallsyms table as 32-bit entries, | ||
1434 | each containing a relative value in the range [base, base + U32_MAX] | ||
1435 | or, when KALLSYMS_ABSOLUTE_PERCPU is in effect, each containing either | ||
1436 | an absolute value in the range [0, S32_MAX] or a relative value in the | ||
1437 | range [base, base + S32_MAX], where base is the lowest relative symbol | ||
1438 | address encountered in the image. | ||
1439 | |||
1440 | On 64-bit builds, this reduces the size of the address table by 50%, | ||
1441 | but more importantly, it results in entries whose values are build | ||
1442 | time constants, and no relocation pass is required at runtime to fix | ||
1443 | up the entries based on the runtime load address of the kernel. | ||
1444 | |||
1427 | config PRINTK | 1445 | config PRINTK |
1428 | default y | 1446 | default y |
1429 | bool "Enable support for printk" if EXPERT | 1447 | bool "Enable support for printk" if EXPERT |