diff options
author | Eric W. Biederman | 2006-09-27 03:51:04 -0500 |
---|---|---|
committer | Linus Torvalds | 2006-09-27 10:26:19 -0500 |
commit | b89a81712f486e4f7a606987413e387605fdeaf4 (patch) | |
tree | 98702b89a50e927c38f2e31cf824c10d2585722f /init/Kconfig | |
parent | 571817849c76aabf34d534c905b5e604f2e824c5 (diff) | |
download | kernel-b89a81712f486e4f7a606987413e387605fdeaf4.tar.gz kernel-b89a81712f486e4f7a606987413e387605fdeaf4.tar.xz kernel-b89a81712f486e4f7a606987413e387605fdeaf4.zip |
[PATCH] sysctl: Allow /proc/sys without sys_sysctl
Since sys_sysctl is deprecated start allow it to be compiled out. This
should catch any remaining user space code that cares, and paves the way
for further sysctl cleanups.
[akpm@osdl.org: If sys_sysctl() is not compiled-in, emit a warning]
Signed-off-by: Eric W. Biederman <ebiederm@xmission.com>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Diffstat (limited to 'init/Kconfig')
-rw-r--r-- | init/Kconfig | 31 |
1 files changed, 17 insertions, 14 deletions
diff --git a/init/Kconfig b/init/Kconfig index 9a7656f0b5ec..4381006dd666 100644 --- a/init/Kconfig +++ b/init/Kconfig | |||
@@ -273,21 +273,24 @@ config UID16 | |||
273 | This enables the legacy 16-bit UID syscall wrappers. | 273 | This enables the legacy 16-bit UID syscall wrappers. |
274 | 274 | ||
275 | config SYSCTL | 275 | config SYSCTL |
276 | bool "Sysctl support" if EMBEDDED | 276 | bool |
277 | default y | 277 | |
278 | config SYSCTL_SYSCALL | ||
279 | bool "Sysctl syscall support" | ||
280 | default n | ||
281 | select SYSCTL | ||
278 | ---help--- | 282 | ---help--- |
279 | The sysctl interface provides a means of dynamically changing | 283 | Enable the deprecated sysctl system call. sys_sysctl uses |
280 | certain kernel parameters and variables on the fly without requiring | 284 | binary paths that have been found to be a major pain to maintain |
281 | a recompile of the kernel or reboot of the system. The primary | 285 | and use. The interface in /proc/sys is now the primary and what |
282 | interface consists of a system call, but if you say Y to "/proc | 286 | everyone uses. |
283 | file system support", a tree of modifiable sysctl entries will be | 287 | |
284 | generated beneath the /proc/sys directory. They are explained in the | 288 | Nothing has been using the binary sysctl interface for some time |
285 | files in <file:Documentation/sysctl/>. Note that enabling this | 289 | time now so nothing should break if you disable sysctl syscall |
286 | option will enlarge the kernel by at least 8 KB. | 290 | support, and you kernel will get marginally smaller. |
287 | 291 | ||
288 | As it is generally a good thing, you should say Y here unless | 292 | Unless you have an application that uses the sys_syscall interface |
289 | building a kernel for install/rescue disks or your system is very | 293 | you should probably say N here. |
290 | limited in memory. | ||
291 | 294 | ||
292 | config KALLSYMS | 295 | config KALLSYMS |
293 | bool "Load all symbols for debugging/kksymoops" if EMBEDDED | 296 | bool "Load all symbols for debugging/kksymoops" if EMBEDDED |