diff options
author | Michal Hocko | 2017-05-08 17:57:15 -0500 |
---|---|---|
committer | Linus Torvalds | 2017-05-08 19:15:12 -0500 |
commit | 6c5ab6511f718c3fb19bcc3f78a90b0e0b601675 (patch) | |
tree | 6f3f4eb344c0e10e966b63192bda55f91b68f80c /mm | |
parent | 1f5307b1e094bfffa83c65c40ac6e3415c108780 (diff) | |
download | kernel-6c5ab6511f718c3fb19bcc3f78a90b0e0b601675.tar.gz kernel-6c5ab6511f718c3fb19bcc3f78a90b0e0b601675.tar.xz kernel-6c5ab6511f718c3fb19bcc3f78a90b0e0b601675.zip |
mm: support __GFP_REPEAT in kvmalloc_node for >32kB
vhost code uses __GFP_REPEAT when allocating vhost_virtqueue resp.
vhost_vsock because it would really like to prefer kmalloc to the
vmalloc fallback - see 23cc5a991c7a ("vhost-net: extend device
allocation to vmalloc") for more context. Michael Tsirkin has also
noted:
"__GFP_REPEAT overhead is during allocation time. Using vmalloc means
all accesses are slowed down. Allocation is not on data path, accesses
are."
The similar applies to other vhost_kvzalloc users.
Let's teach kvmalloc_node to handle __GFP_REPEAT properly. There are
two things to be careful about. First we should prevent from the OOM
killer and so have to involve __GFP_NORETRY by default and secondly
override __GFP_REPEAT for !costly order requests as the __GFP_REPEAT is
ignored for !costly orders.
Supporting __GFP_REPEAT like semantic for !costly request is possible it
would require changes in the page allocator. This is out of scope of
this patch.
This patch shouldn't introduce any functional change.
Link: http://lkml.kernel.org/r/20170306103032.2540-3-mhocko@kernel.org
Signed-off-by: Michal Hocko <mhocko@suse.com>
Acked-by: Vlastimil Babka <vbabka@suse.cz>
Acked-by: Michael S. Tsirkin <mst@redhat.com>
Cc: David Miller <davem@davemloft.net>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'mm')
-rw-r--r-- | mm/util.c | 18 |
1 files changed, 15 insertions, 3 deletions
@@ -339,7 +339,9 @@ EXPORT_SYMBOL(vm_mmap); | |||
339 | * Uses kmalloc to get the memory but if the allocation fails then falls back | 339 | * Uses kmalloc to get the memory but if the allocation fails then falls back |
340 | * to the vmalloc allocator. Use kvfree for freeing the memory. | 340 | * to the vmalloc allocator. Use kvfree for freeing the memory. |
341 | * | 341 | * |
342 | * Reclaim modifiers - __GFP_NORETRY, __GFP_REPEAT and __GFP_NOFAIL are not supported | 342 | * Reclaim modifiers - __GFP_NORETRY and __GFP_NOFAIL are not supported. __GFP_REPEAT |
343 | * is supported only for large (>32kB) allocations, and it should be used only if | ||
344 | * kmalloc is preferable to the vmalloc fallback, due to visible performance drawbacks. | ||
343 | * | 345 | * |
344 | * Any use of gfp flags outside of GFP_KERNEL should be consulted with mm people. | 346 | * Any use of gfp flags outside of GFP_KERNEL should be consulted with mm people. |
345 | */ | 347 | */ |
@@ -358,8 +360,18 @@ void *kvmalloc_node(size_t size, gfp_t flags, int node) | |||
358 | * Make sure that larger requests are not too disruptive - no OOM | 360 | * Make sure that larger requests are not too disruptive - no OOM |
359 | * killer and no allocation failure warnings as we have a fallback | 361 | * killer and no allocation failure warnings as we have a fallback |
360 | */ | 362 | */ |
361 | if (size > PAGE_SIZE) | 363 | if (size > PAGE_SIZE) { |
362 | kmalloc_flags |= __GFP_NORETRY | __GFP_NOWARN; | 364 | kmalloc_flags |= __GFP_NOWARN; |
365 | |||
366 | /* | ||
367 | * We have to override __GFP_REPEAT by __GFP_NORETRY for !costly | ||
368 | * requests because there is no other way to tell the allocator | ||
369 | * that we want to fail rather than retry endlessly. | ||
370 | */ | ||
371 | if (!(kmalloc_flags & __GFP_REPEAT) || | ||
372 | (size <= PAGE_SIZE << PAGE_ALLOC_COSTLY_ORDER)) | ||
373 | kmalloc_flags |= __GFP_NORETRY; | ||
374 | } | ||
363 | 375 | ||
364 | ret = kmalloc_node(size, kmalloc_flags, node); | 376 | ret = kmalloc_node(size, kmalloc_flags, node); |
365 | 377 | ||