aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* init/do_mounts: initrd_load() can be booleanYaowei Bai2016-01-201-3/+3
| | | | | | | | | | | Make initrd_load() return bool due to this particular function only using either one or zero as its return value. No functional change. Signed-off-by: Yaowei Bai <baiyaowei@cmss.chinamobile.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* usermodehelper: split remaining calls to call_usermodehelper_fns()Lucas De Marchi2013-04-301-2/+6
| | | | | | | | | | | | | | | | | | These are the only users of call_usermodehelper_fns(). This function suffers from not being able to determine if the cleanup is called. Even if in this places the cleanup pointer is NULL, convert them to use the separate call_usermodehelper_setup() + call_usermodehelper_exec() functions so we can remove the _fns variant. Signed-off-by: Lucas De Marchi <lucas.demarchi@profusion.mobi> Cc: Oleg Nesterov <oleg@redhat.com> Cc: David Howells <dhowells@redhat.com> Cc: James Morris <james.l.morris@oracle.com> Cc: Al Viro <viro@zeniv.linux.org.uk> Cc: Tejun Heo <tj@kernel.org> Cc: "Rafael J. Wysocki" <rjw@sisk.pl> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Merge branch 'master' into for-3.9-asyncTejun Heo2013-01-231-0/+4
|\ | | | | | | | | | | | | To receive f56c3196f251012de9b3ebaff55732a9074fdaae ("async: fix __lowest_in_progress()"). Signed-off-by: Tejun Heo <tj@kernel.org>
| * make sure that /linuxrc has std{in,out,err}Al Viro2013-01-191-0/+4
| | | | | | | | Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* | init, block: try to load default elevator module early during bootTejun Heo2013-01-181-0/+3
|/ | | | | | | | | | | | | | | | | | | | | | This patch adds default module loading and uses it to load the default block elevator. During boot, it's called right after initramfs or initrd is made available and right before control is passed to userland. This ensures that as long as the modules are available in the usual places in initramfs, initrd or the root filesystem, the default modules are loaded as soon as possible. This will replace the on-demand elevator module loading from elevator init path. v2: Fixed build breakage when !CONFIG_BLOCK. Reported by kbuild test robot. Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Jens Axboe <axboe@kernel.dk> Cc: Arjan van de Ven <arjan@linux.intel.com> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Alex Riesen <raa.lkml@gmail.com> Cc: Fengguang We <fengguang.wu@intel.com>
* don't bother with kernel_thread/kernel_execve for launching linuxrcAl Viro2012-10-111-25/+16
| | | | | | exec_usermodehelper_fns() will do just fine... Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* init: disable sparse checking of the mount.o source filesH Hartley Sweeten2012-05-311-0/+10
| | | | | | | | | | | | | | | | | | | | | | | | The init/mount.o source files produce a number of sparse warnings of the type: warning: incorrect type in argument 1 (different address spaces) expected char [noderef] <asn:1>*dev_name got char *name This is due to the syscalls expecting some of the arguments to be user pointers but they are being passed as kernel pointers. This is harmless but adds a lot of noise to a sparse build. To limit the noise just disable the sparse checking in the relevant source files, but still display a warning so that the user knows this has been done. Since the sparse checking has been disabled we can also remove the __user __force casts that are scattered thru the source. Signed-off-by: H Hartley Sweeten <hsweeten@visionengravers.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* get rid of pointless includes of ext2_fs.hAl Viro2012-03-311-1/+0
| | | | Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* Make do_execve() take a const filename pointerDavid Howells2010-08-171-3/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | Make do_execve() take a const filename pointer so that kernel_execve() compiles correctly on ARM: arch/arm/kernel/sys_arm.c:88: warning: passing argument 1 of 'do_execve' discards qualifiers from pointer target type This also requires the argv and envp arguments to be consted twice, once for the pointer array and once for the strings the array points to. This is because do_execve() passes a pointer to the filename (now const) to copy_strings_kernel(). A simpler alternative would be to cast the filename pointer in do_execve() when it's passed to copy_strings_kernel(). do_execve() may not change any of the strings it is passed as part of the argv or envp lists as they are some of them in .rodata, so marking these strings as const should be fine. Further kernel_execve() and sys_execve() need to be changed to match. This has been test built on x86_64, frv, arm and mips. Signed-off-by: David Howells <dhowells@redhat.com> Tested-by: Ralf Baechle <ralf@linux-mips.org> Acked-by: Russell King <rmk+kernel@arm.linux.org.uk> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* init: Open /dev/console from rootfsEric W. Biederman2010-03-031-4/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | To avoid potential problems with an empty /dev open /dev/console from rootfs instead of waiting to mount our root filesystem and mounting it there. This effectively guarantees that there will be a device node, and it won't be on a filesystem that we will ever unmount, so there are no issues with leaving /dev/console open and pinning the filesystem. This is actually more effective than automatically mounting devtmpfs on /dev because it removes removes the occasionally problematic assumption that /dev/console exists from the boot code. With this patch I was able to throw busybox on my /boot partition (which has no /dev directory) and boot into userspace without problems. The only possible negative consequence I can think of is that someone out there deliberately used did not use a character device that is major 5 minor 2 for /dev/console. Does anyone know of a situation in which that could make sense? Signed-off-by: Eric W. Biederman <ebiederm@xmission.com> Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* Freezer: Fix s2disk resume from initrdRafael J. Wysocki2007-11-201-3/+9
| | | | | | | | | | | | | | Add appropriate freezer annotations to handle_initrd(), so that it's possible to resume from disk from an initrd. http://bugzilla.kernel.org/show_bug.cgi?id=9345 Signed-off-by: Rafael J. Wysocki <rjw@sisk.pl> Cc: Pavel Machek <pavel@ucw.cz> Cc: Nigel Cunningham <nigel@nigel.suspend2.net> Cc: Ingo Molnar <mingo@elte.hu> Cc: Chris Friedhoff <chris@friedhoff.org> Signed-off-by: Len Brown <len.brown@intel.com>
* Fix failure to resume from initrdsNigel Cunningham2007-09-191-1/+3
| | | | | | | | | | | | | | | | | Commit 831441862956fffa17b9801db37e6ea1650b0f69 (Freezer: make kernel threads nonfreezable by default) breaks freezing when attempting to resume from an initrd, because the init (which is freezeable) spins while waiting for another thread to run /linuxrc, but doesn't check whether it has been told to enter the refrigerator. The original patch replaced a call to try_to_freeze() with a call to yield(). I believe a simple reversion is wrong because if !CONFIG_PM_SLEEP, try_to_freeze() is a noop. It should still yield. Signed-off-by: Nigel Cunningham <nigel@nigel.suspend2.net> Acked-by: Rafael J. Wysocki <rjw@sisk.pl> Acked-by: Pavel Machek <pavel@ucw.cz> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Freezer: make kernel threads nonfreezable by defaultRafael J. Wysocki2007-07-171-5/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Currently, the freezer treats all tasks as freezable, except for the kernel threads that explicitly set the PF_NOFREEZE flag for themselves. This approach is problematic, since it requires every kernel thread to either set PF_NOFREEZE explicitly, or call try_to_freeze(), even if it doesn't care for the freezing of tasks at all. It seems better to only require the kernel threads that want to or need to be frozen to use some freezer-related code and to remove any freezer-related code from the other (nonfreezable) kernel threads, which is done in this patch. The patch causes all kernel threads to be nonfreezable by default (ie. to have PF_NOFREEZE set by default) and introduces the set_freezable() function that should be called by the freezable kernel threads in order to unset PF_NOFREEZE. It also makes all of the currently freezable kernel threads call set_freezable(), so it shouldn't cause any (intentional) change of behaviour to appear. Additionally, it updates documentation to describe the freezing of tasks more accurately. [akpm@linux-foundation.org: build fixes] Signed-off-by: Rafael J. Wysocki <rjw@sisk.pl> Acked-by: Nigel Cunningham <nigel@nigel.suspend2.net> Cc: Pavel Machek <pavel@ucw.cz> Cc: Oleg Nesterov <oleg@tv-sign.ru> Cc: Gautham R Shenoy <ego@in.ibm.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* freezer: remove PF_NOFREEZE from handle_initrdRafael J. Wysocki2007-05-071-2/+3
| | | | | | | | | | | Make handle_initrd() call try_to_freeze() in a suitable place instead of setting PF_NOFREEZE for the current task. Signed-off-by: Rafael J. Wysocki <rjw@sisk.pl> Acked-by: Nigel Cunningham <nigel@nigel.suspend2.net> Acked-by: Pavel Machek <pavel@ucw.cz> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* [PATCH] Add include/linux/freezer.h and move definitions from sched.hNigel Cunningham2006-12-071-0/+1
| | | | | | | | | | | | | Move process freezing functions from include/linux/sched.h to freezer.h, so that modifications to the freezer or the kernel configuration don't require recompiling just about everything. [akpm@osdl.org: fix ueagle driver] Signed-off-by: Nigel Cunningham <nigel@suspend2.net> Cc: "Rafael J. Wysocki" <rjw@sisk.pl> Cc: Pavel Machek <pavel@ucw.cz> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] introduce kernel_execveArnd Bergmann2006-10-021-2/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The use of execve() in the kernel is dubious, since it relies on the __KERNEL_SYSCALLS__ mechanism that stores the result in a global errno variable. As a first step of getting rid of this, change all users to a global kernel_execve function that returns a proper error code. This function is a terrible hack, and a later patch removes it again after the kernel syscalls are gone. Signed-off-by: Arnd Bergmann <arnd@arndb.de> Cc: Andi Kleen <ak@muc.de> Cc: Paul Mackerras <paulus@samba.org> Cc: Benjamin Herrenschmidt <benh@kernel.crashing.org> Cc: Richard Henderson <rth@twiddle.net> Cc: Ivan Kokshaysky <ink@jurassic.park.msu.ru> Cc: Russell King <rmk@arm.linux.org.uk> Cc: Ian Molton <spyro@f2s.com> Cc: Mikael Starvik <starvik@axis.com> Cc: David Howells <dhowells@redhat.com> Cc: Yoshinori Sato <ysato@users.sourceforge.jp> Cc: Hirokazu Takata <takata.hirokazu@renesas.com> Cc: Ralf Baechle <ralf@linux-mips.org> Cc: Kyle McMartin <kyle@mcmartin.ca> Cc: Heiko Carstens <heiko.carstens@de.ibm.com> Cc: Martin Schwidefsky <schwidefsky@de.ibm.com> Cc: Paul Mundt <lethal@linux-sh.org> Cc: Kazumoto Kojima <kkojima@rr.iij4u.or.jp> Cc: Richard Curnow <rc@rc0.org.uk> Cc: William Lee Irwin III <wli@holomorphy.com> Cc: "David S. Miller" <davem@davemloft.net> Cc: Jeff Dike <jdike@addtoit.com> Cc: Paolo 'Blaisorblade' Giarrusso <blaisorblade@yahoo.it> Cc: Miles Bader <uclinux-v850@lsi.nec.co.jp> Cc: Chris Zankel <chris@zankel.net> Cc: "Luck, Tony" <tony.luck@intel.com> Cc: Geert Uytterhoeven <geert@linux-m68k.org> Cc: Roman Zippel <zippel@linux-m68k.org> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] devfs: Remove devfs from the init codeGreg Kroah-Hartman2006-06-261-4/+2
| | | | | | This patch removes the devfs code from the init/ directory. Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* [PATCH] swsusp: userland interfaceRafael J. Wysocki2006-03-231-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | This patch introduces a user space interface for swsusp. The interface is based on a special character device, called the snapshot device, that allows user space processes to perform suspend and resume-related operations with the help of some ioctls and the read()/write() functions.  Additionally it allows these processes to allocate free swap pages from a selected swap partition, called the resume partition, so that they know which sectors of the resume partition are available to them. The interface uses the same low-level system memory snapshot-handling functions that are used by the built-it swap-writing/reading code of swsusp. The interface documentation is included in the patch. The patch assumes that the major and minor numbers of the snapshot device will be 10 (ie. misc device) and 231, the registration of which has already been requested. Signed-off-by: Rafael J. Wysocki <rjw@sisk.pl> Acked-by: Pavel Machek <pavel@ucw.cz> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] Improper initrd failure message at boot timeJay Lan2005-06-301-1/+4
| | | | | | | | | | | | | | | | | | | | | | On system boot up, there was an failure reported to boot.msg: <5>Trying to move old root to /initrd ... failed According to initrd(4) man page, step #7 of BOOT-UP OPERATION is described as below: 7. If the normal root file has directory /initrd, device /dev/ram0 is moved from / to /initrd. Otherwise if directory /initrd does not exist device /dev/ram0 is unmounted. We got service calls from customers concerning about this failure message at boot time. Many systems do not have /initrd and thus the message can be changed in the case of non-existing /initrd so that it does not sound like a failure of the system. Signed-off-by: Jay Lan <jlan@sgi.com> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] init/do_mounts_initrd.c: fix sparse warningDomen Puncer2005-06-251-2/+2
| | | | | | | Signed-off-by: Alexey Dobriyan <adobriyan@mail.ru> Signed-off-by: Domen Puncer <domen@coderock.org> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* Linux-2.6.12-rc2v2.6.12-rc2Linus Torvalds2005-04-161-0/+121
Initial git repository build. I'm not bothering with the full history, even though we have it. We can create a separate "historical" git archive of that later if we want to, and in the meantime it's about 3.2GB when imported into git - space that would just make the early git days unnecessarily complicated, when we don't have a lot of good infrastructure for it. Let it rip!