/* * binfmt_misc.c * * Copyright (C) 1997 Richard Günther * * binfmt_misc detects binaries via a magic or filename extension and invokes * a specified wrapper. See Documentation/binfmt_misc.txt for more details. */ #define pr_fmt(fmt) KBUILD_MODNAME ": " fmt #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "internal.h" #ifdef DEBUG # define USE_DEBUG 1 #else # define USE_DEBUG 0 #endif enum { VERBOSE_STATUS = 1 /* make it zero to save 400 bytes kernel memory */ }; static LIST_HEAD(entries); static int enabled = 1; enum {Enabled, Magic}; #define MISC_FMT_PRESERVE_ARGV0 (1 << 31) #define MISC_FMT_OPEN_BINARY (1 << 30) #define MISC_FMT_CREDENTIALS (1 << 29) #define MISC_FMT_OPEN_FILE (1 << 28) typedef struct { struct list_head list; unsigned long flags; /* type, status, etc. */ int offset; /* offset of magic */ int size; /* size of magic/mask */ char *magic; /* magic or filename extension */ char *mask; /* mask, NULL for exact match */ char *interpreter; /* filename of interpreter */ char *name; struct dentry *dentry; struct file *interp_file; } Node; static DEFINE_RWLOCK(entries_lock); static struct file_system_type bm_fs_type; static struct vfsmount *bm_mnt; static int entry_count; /* * Max length of the register string. Determined by: * - 7 delimiters * - name: ~50 bytes * - type: 1 byte * - offset: 3 bytes (has to be smaller than BINPRM_BUF_SIZE) * - magic: 128 bytes (512 in escaped form) * - mask: 128 bytes (512 in escaped form) * - interp: ~50 bytes * - flags: 5 bytes * Round that up a bit, and then back off to hold the internal data * (like struct Node). */ #define MAX_REGISTER_LENGTH 1920 /* * Check if we support the binfmt * if we do, return the node, else NULL * locking is done in load_misc_binary */ static Node *check_file(struct linux_binprm *bprm) { char *p = strrchr(bprm->interp, '.'); struct list_head *l; /* Walk all the registered handlers. */ list_for_each(l, &entries) { Node *e = list_entry(l, Node, list); char *s; int j; /* Make sure this one is currently enabled. */ if (!test_bit(Enabled, &e->flags)) continue; /* Do matching based on extension if applicable. */ if (!test_bit(Magic, &e->flags)) { if (p && !strcmp(e->magic, p + 1)) return e; continue; } /* Do matching based on magic & mask. */ s = bprm->buf + e->offset; if (e->mask) { for (j = 0; j < e->size; j++) if ((*s++ ^ e->magic[j]) & e->mask[j]) break; } else { for (j = 0; j < e->size; j++) if ((*s++ ^ e->magic[j])) break; } if (j == e->size) return e; } return NULL; } /* * the loader itself */ static int load_misc_binary(struct linux_binprm *bprm) { Node *fmt; struct file *interp_file = NULL; char iname[BINPRM_BUF_SIZE]; const char *iname_addr = iname; int retval; int fd_binary = -1; retval = -ENOEXEC; if (!enabled) goto ret; /* to keep locking time low, we copy the interpreter string */ read_lock(&entries_lock); fmt = check_file(bprm); if (fmt) strlcpy(iname, fmt->interpreter, BINPRM_BUF_SIZE); read_unlock(&entries_lock); if (!fmt) goto ret; /* Need to be able to load the file after exec */ if (bprm->interp_flags & BINPRM_FLAGS_PATH_INACCESSIBLE) return -ENOENT; if (!(fmt->flags & MISC_FMT_PRESERVE_ARGV0)) { retval = remove_arg_zero(bprm); if (retval) goto ret; } if (fmt->flags & MISC_FMT_OPEN_BINARY) { /* if the binary should be opened on behalf of the * interpreter than keep it open and assign descriptor * to it */ fd_binary = get_unused_fd_flags(0); if (fd_binary < 0) { retval = fd_binary; goto ret; } fd_install(fd_binary, bprm->file); /* if the binary is not readable than enforce mm->dumpable=0 regardless of the interpreter's permissions */ would_dump(bprm, bprm->file); allow_write_access(bprm->file); bprm->file = NULL; /* mark the bprm that fd should be passed to interp */ bprm->interp_flags |= BINPRM_FLAGS_EXECFD; bprm->interp_data = fd_binary; } else { allow_write_access(bprm->file); fput(bprm->file); bprm->file = NULL; } /* make argv[1] be the path to the binary */ retval = copy_strings_kernel(1, &bprm->interp, bprm); if (retval < 0) goto error; bprm->argc++; /* add the interp as argv[0] */ retval = copy_strings_kernel(1, &iname_addr, bprm); if (retval < 0) goto error; bprm->argc++; /* Update interp in case binfmt_script needs it. */ retval = bprm_change_interp(iname, bprm); if (retval < 0) goto error; if (fmt->flags & MISC_FMT_OPEN_FILE && fmt->interp_file) { interp_file = filp_clone_open(fmt->interp_file); if (!IS_ERR(interp_file)) deny_write_access(interp_file); } else { interp_file = open_exec(iname); } retval = PTR_ERR(interp_file); if (IS_ERR(interp_file)) goto error; bprm->file = interp_file; if (fmt->flags & MISC_FMT_CREDENTIALS) { /* * No need to call prepare_binprm(), it's already been * done. bprm->buf is stale, update from interp_file. */ memset(bprm->buf, 0, BINPRM_BUF_SIZE); retval = kernel_read(bprm->file, 0, bprm->buf, BINPRM_BUF_SIZE); } else retval = prepare_binprm(bprm); if (retval < 0) goto error; retval = search_binary_handler(bprm); if (retval < 0) goto error; ret: return retval; error: if (fd_binary > 0) sys_close(fd_binary); bprm->interp_flags = 0; bprm->interp_data = 0; goto ret; } /* Command parsers */ /* * parses and copies one argument enclosed in del from *sp to *dp, * recognising the \x special. * returns pointer to the copied argument or NULL in case of an * error (and sets err) or null argument length. */ static char *scanarg(char *s, char del) { char c; while ((c = *s++) != del) { if (c == '\\' && *s == 'x') { s++; if (!isxdigit(*s++)) return NULL; if (!isxdigit(*s++)) return NULL; } } s[-1] ='\0'; return s; } static char *check_special_flags(char *sfs, Node *e) { char *p = sfs; int cont = 1; /* special flags */ while (cont) { switch (*p) { case 'P': pr_debug("register: flag: P (preserve argv0)\n"); p++; e->flags |= MISC_FMT_PRESERVE_ARGV0; break; case 'O': pr_debug("register: flag: O (open binary)\n"); p++; e->flags |= MISC_FMT_OPEN_BINARY; break; case 'C': pr_debug("register: flag: C (preserve creds)\n"); p++; /* this flags also implies the open-binary flag */ e->flags |= (MISC_FMT_CREDENTIALS | MISC_FMT_OPEN_BINARY); break; case 'F': pr_debug("register: flag: F: open interpreter file now\n"); p++; e->flags |= MISC_FMT_OPEN_FILE; break; default: cont = 0; } } return p; } /* * This registers a new binary format, it recognises the syntax * ':name:type:offset:magic:mask:interpreter:flags' * where the ':' is the IFS, that can be chosen with the first char */ static Node *create_entry(const char __user *buffer, size_t count) { Node *e; int memsize, err; char *buf, *p; char del; pr_debug("register: received %zu bytes\n", count); /* some sanity checks */ err = -EINVAL; if ((count < 11) || (count > MAX_REGISTER_LENGTH)) goto out; err = -ENOMEM; memsize = sizeof(Node) + count + 8; e = kmalloc(memsize, GFP_KERNEL); if (!e) goto out; p = buf = (char *)e + sizeof(Node); memset(e, 0, sizeof(Node)); if (copy_from_user(buf, buffer, count)) goto efault; del = *p++; /* delimeter */ pr_debug("register: delim: %#x {%c}\n", del, del); /* Pad the buffer with the delim to simplify parsing below. */ memset(buf + count, del, 8); /* Parse the 'name' field. */ e->name = p; p = strchr(p, del); if (!p) goto einval; *p++ = '\0'; if (!e->name[0] || !strcmp(e->name, ".") || !strcmp(e->name, "..") || strchr(e->name, '/')) goto einval; pr_debug("register: name: {%s}\n", e->name); /* Parse the 'type' field. */ switch (*p++) { case 'E': pr_debug("register: type: E (extension)\n"); e->flags = 1 << Enabled; break; case 'M': pr_debug("register: type: M (magic)\n"); e->flags = (1 << Enabled) | (1 << Magic); break; default: goto einval; } if (*p++ != del) goto einval; if (test_bit(Magic, &e->flags)) { /* Handle the 'M' (magic) format. */ char *s; /* Parse the 'offset' field. */ s = strchr(p, del); if (!s) goto einval; *s++ = '\0'; e->offset = simple_strtoul(p, &p, 10); if (*p++) goto einval; pr_debug("register: offset: %#x\n", e->offset); /* Parse the 'magic' field. */ e->magic = p; p = scanarg(p, del); if (!p) goto einval; if (!e->magic[0]) goto einval; if (USE_DEBUG) print_hex_dump_bytes( KBUILD_MODNAME ": register: magic[raw]: ", DUMP_PREFIX_NONE, e->magic, p - e->magic); /* Parse the 'mask' field. */ e->mask = p; p = scanarg(p, del); if (!p) goto einval; if (!e->mask[0]) { e->mask = NULL; pr_debug("register: mask[raw]: none\n"); } else if (USE_DEBUG) print_hex_dump_bytes( KBUILD_MODNAME ": register: mask[raw]: ", DUMP_PREFIX_NONE, e->mask, p - e->mask); /* * Decode the magic & mask fields. * Note: while we might have accepted embedded NUL bytes from * above, the unescape helpers here will stop at the first one * it encounters. */ e->size = string_unescape_inplace(e->magic, UNESCAPE_HEX); if (e->mask && string_unescape_inplace(e->mask, UNESCAPE_HEX) != e->size) goto einval; if (e->size + e->offset > BINPRM_BUF_SIZE) goto einval; pr_debug("register: magic/mask length: %i\n", e->size); if (USE_DEBUG) { print_hex_dump_bytes( KBUILD_MODNAME ": register: magic[decoded]: ", DUMP_PREFIX_NONE, e->magic, e->size); if (e->mask) { int i; char *masked = kmalloc(e->size, GFP_KERNEL); print_hex_dump_bytes( KBUILD_MODNAME ": register: mask[decoded]: ", DUMP_PREFIX_NONE, e->mask, e->size); if (masked) { for (i = 0; i < e->size; ++i) masked[i] = e->magic[i] & e->mask[i]; print_hex_dump_bytes( KBUILD_MODNAME ": register: magic[masked]: ", DUMP_PREFIX_NONE, masked, e->size); kfree(masked); } } } } else { /* Handle the 'E' (extension) format. */ /* Skip the 'offset' field. */ p = strchr(p, del); if (!p) goto einval; *p++ = '\0'; /* Parse the 'magic' field. */ e->magic = p; p = strchr(p, del); if (!p) goto einval; *p++ = '\0'; if (!e->magic[0] || strchr(e->magic, '/')) goto einval; pr_debug("register: extension: {%s}\n", e->magic); /* Skip the 'mask' field. */ p = strchr(p, del); if (!p) goto einval; *p++ = '\0'; } /* Parse the 'interpreter' field. */ e->interpreter = p; p = strchr(p, del); if (!p) goto einval; *p++ = '\0'; if (!e->interpreter[0]) goto einval; pr_debug("register: interpreter: {%s}\n", e->interpreter); /* Parse the 'flags' field. */ p = check_special_flags(p, e); if (*p == '\n') p++; if (p != buf + count) goto einval; return e; out: return ERR_PTR(err); efault: kfree(e); return ERR_PTR(-EFAULT); einval: kfree(e); return ERR_PTR(-EINVAL); } /* * Set status of entry/binfmt_misc: * '1' enables, '0' disables and '-1' clears entry/binfmt_misc */ static int parse_command(const char __user *buffer, size_t count) { char s[4]; if (count > 3) return -EINVAL; if (copy_from_user(s, buffer, count)) return -EFAULT; if (!count) return 0; if (s[count - 1] == '\n') count--; if (count == 1 && s[0] == '0') return 1; if (count == 1 && s[0] == '1') return 2; if (count == 2 && s[0] == '-' && s[1] == '1') return 3; return -EINVAL; } /* generic stuff */ static void entry_status(Node *e, char *page) { char *dp = page; const char *status = "disabled"; if (test_bit(Enabled, &e->flags)) status = "enabled"; if (!VERBOSE_STATUS) { sprintf(page, "%s\n", status); return; } dp += sprintf(dp, "%s\ninterpreter %s\n", status, e->interpreter); /* print the special flags */ dp += sprintf(dp, "flags: "); if (e->flags & MISC_FMT_PRESERVE_ARGV0) *dp++ = 'P'; if (e->flags & MISC_FMT_OPEN_BINARY) *dp++ = 'O'; if (e->flags & MISC_FMT_CREDENTIALS) *dp++ = 'C'; if (e->flags & MISC_FMT_OPEN_FILE) *dp++ = 'F'; *dp++ = '\n'; if (!test_bit(Magic, &e->flags)) { sprintf(dp, "extension .%s\n", e->magic); } else { dp += sprintf(dp, "offset %i\nmagic ", e->offset); dp = bin2hex(dp, e->magic, e->size); if (e->mask) { dp += sprintf(dp, "\nmask "); dp = bin2hex(dp, e->mask, e->size); } *dp++ = '\n'; *dp = '\0'; } } static struct inode *bm_get_inode(struct super_block *sb, int mode) { struct inode *inode = new_inode(sb); if (inode) { inode->i_ino = get_next_ino(); inode->i_mode = mode; inode->i_atime = inode->i_mtime = inode->i_ctime = current_time(inode); } return inode; } static void bm_evict_inode(struct inode *inode) { clear_inode(inode); kfree(inode->i_private); } static void kill_node(Node *e) { struct dentry *dentry; write_lock(&entries_lock); dentry = e->dentry; if (dentry) { list_del_init(&e->list); e->dentry = NULL; } write_unlock(&entries_lock); if ((e->flags & MISC_FMT_OPEN_FILE) && e->interp_file) { filp_close(e->interp_file, NULL); e->interp_file = NULL; } if (dentry) { drop_nlink(d_inode(dentry)); d_drop(dentry); dput(dentry); simple_release_fs(&bm_mnt, &entry_count); } } /* / */ static ssize_t bm_entry_read(struct file *file, char __user *buf, size_t nbytes, loff_t *ppos) { Node *e = file_inode(file)->i_private; ssize_t res; char *page; page = (char *) __get_free_page(GFP_KERNEL); if (!page) return -ENOMEM; entry_status(e, page); res = simple_read_from_buffer(buf, nbytes, ppos, page, strlen(page)); free_page((unsigned long) page); return res; } static ssize_t bm_entry_write(struct file *file, const char __user *buffer, size_t count, loff_t *ppos) { struct dentry *root; Node *e = file_inode(file)->i_private; int res = parse_command(buffer, count); switch (res) { case 1: /* Disable this handler. */ clear_bit(Enabled, &e->flags); break; case 2: /* Enable this handler. */ set_bit(Enabled, &e->flags); break; case 3: /* Delete this handler. */ root = file_inode(file)->i_sb->s_root; inode_lock(d_inode(root)); kill_node(e); inode_unlock(d_inode(root)); break; default: return res; } return count; } static const struct file_operations bm_entry_operations = { .read = bm_entry_read, .write = bm_entry_write, .llseek = default_llseek, }; /* /register */ static ssize_t bm_register_write(struct file *file, const char __user *buffer, size_t count, loff_t *ppos) { Node *e; struct inode *inode; struct super_block *sb = file_inode(file)->i_sb; struct dentry *root = sb->s_root, *dentry; int err = 0; e = create_entry(buffer, count); if (IS_ERR(e)) return PTR_ERR(e); inode_lock(d_inode(root)); dentry = lookup_one_len(e->name, root, strlen(e->name)); err = PTR_ERR(dentry); if (IS_ERR(dentry)) goto out; err = -EEXIST; if (d_really_is_positive(dentry)) goto out2; inode = bm_get_inode(sb, S_IFREG | 0644); err = -ENOMEM; if (!inode) goto out2; err = simple_pin_fs(&bm_fs_type, &bm_mnt, &entry_count); if (err) { iput(inode); inode = NULL; goto out2; } if (e->flags & MISC_FMT_OPEN_FILE) { struct file *f; f = open_exec(e->interpreter); if (IS_ERR(f)) { err = PTR_ERR(f); pr_notice("register: failed to install interpreter file %s\n", e->interpreter); simple_release_fs(&bm_mnt, &entry_count); iput(inode); inode = NULL; goto out2; } e->interp_file = f; } e->dentry = dget(dentry); inode->i_private = e; inode->i_fop = &bm_entry_operations; d_instantiate(dentry, inode); write_lock(&entries_lock); list_add(&e->list, &entries); write_unlock(&entries_lock); err = 0; out2: dput(dentry); out: inode_unlock(d_inode(root)); if (err) { kfree(e); return err; } return count; } static const struct file_operations bm_register_operations = { .write = bm_register_write, .llseek = noop_llseek, }; /* /status */ static ssize_t bm_status_read(struct file *file, char __user *buf, size_t nbytes, loff_t *ppos) { char *s = enabled ? "enabled\n" : "disabled\n"; return simple_read_from_buffer(buf, nbytes, ppos, s, strlen(s)); } static ssize_t bm_status_write(struct file *file, const char __user *buffer, size_t count, loff_t *ppos) { int res = parse_command(buffer, count); struct dentry *root; switch (res) { case 1: /* Disable all handlers. */ enabled = 0; break; case 2: /* Enable all handlers. */ enabled = 1; break; case 3: /* Delete all handlers. */ root = file_inode(file)->i_sb->s_root; inode_lock(d_inode(root)); while (!list_empty(&entries)) kill_node(list_entry(entries.next, Node, list)); inode_unlock(d_inode(root)); break; default: return res; } return count; } static const struct file_operations bm_status_operations = { .read = bm_status_read, .write = bm_status_write, .llseek = default_llseek, }; /* Superblock handling */ static const struct super_operations s_ops = { .statfs = simple_statfs, .evict_inode = bm_evict_inode, }; static int bm_fill_super(struct super_block *sb, void *data, int silent) { int err; static const struct tree_descr bm_files[] = { [2] = {"status", &bm_status_operations, S_IWUSR|S_IRUGO}, [3] = {"register", &bm_register_operations, S_IWUSR}, /* last one */ {""} }; err = simple_fill_super(sb, BINFMTFS_MAGIC, bm_files); if (!err) sb->s_op = &s_ops; return err; } static struct dentry *bm_mount(struct file_system_type *fs_type, int flags, const char *dev_name, void *data) { return mount_single(fs_type, flags, data, bm_fill_super); } static struct linux_binfmt misc_format = { .module = THIS_MODULE, .load_binary = load_misc_binary, }; static struct file_system_type bm_fs_type = { .owner = THIS_MODULE, .name = "binfmt_misc", .mount = bm_mount, .kill_sb = kill_litter_super, }; MODULE_ALIAS_FS("binfmt_misc"); static int __init init_misc_binfmt(void) { int err = register_filesystem(&bm_fs_type); if (!err) insert_binfmt(&misc_format); return err; } static void __exit exit_misc_binfmt(void) { unregister_binfmt(&misc_format); unregister_filesystem(&bm_fs_type); } core_initcall(init_misc_binfmt); module_exit(exit_misc_binfmt); MODULE_LICENSE("GPL");