/* * The "user cache". * * (C) Copyright 1991-2000 Linus Torvalds * * We have a per-user structure to keep track of how many * processes, files etc the user has claimed, in order to be * able to have per-user limits for system resources. */ #include #include #include #include #include #include #include #include #include #include /* * userns count is 1 for root user, 1 for init_uts_ns, * and 1 for... ? */ struct user_namespace init_user_ns = { .uid_map = { .nr_extents = 1, .extent[0] = { .first = 0, .lower_first = 0, .count = 4294967295U, }, }, .gid_map = { .nr_extents = 1, .extent[0] = { .first = 0, .lower_first = 0, .count = 4294967295U, }, }, .projid_map = { .nr_extents = 1, .extent[0] = { .first = 0, .lower_first = 0, .count = 4294967295U, }, }, .count = ATOMIC_INIT(3), .owner = GLOBAL_ROOT_UID, .group = GLOBAL_ROOT_GID, .ns.inum = PROC_USER_INIT_INO, #ifdef CONFIG_USER_NS .ns.ops = &userns_operations, #endif .flags = USERNS_INIT_FLAGS, #ifdef CONFIG_PERSISTENT_KEYRINGS .persistent_keyring_register_sem = __RWSEM_INITIALIZER(init_user_ns.persistent_keyring_register_sem), #endif }; EXPORT_SYMBOL_GPL(init_user_ns); /* * UID task count cache, to get fast user lookup in "alloc_uid" * when changing user ID's (ie setuid() and friends). */ #define UIDHASH_BITS (CONFIG_BASE_SMALL ? 3 : 7) #define UIDHASH_SZ (1 << UIDHASH_BITS) #define UIDHASH_MASK (UIDHASH_SZ - 1) #define __uidhashfn(uid) (((uid >> UIDHASH_BITS) + uid) & UIDHASH_MASK) #define uidhashentry(uid) (uidhash_table + __uidhashfn((__kuid_val(uid)))) static struct kmem_cache *uid_cachep; struct hlist_head uidhash_table[UIDHASH_SZ]; /* * The uidhash_lock is mostly taken from process context, but it is * occasionally also taken from softirq/tasklet context, when * task-structs get RCU-freed. Hence all locking must be softirq-safe. * But free_uid() is also called with local interrupts disabled, and running * local_bh_enable() with local interrupts disabled is an error - we'll run * softirq callbacks, and they can unconditionally enable interrupts, and * the caller of free_uid() didn't expect that.. */ static DEFINE_SPINLOCK(uidhash_lock); /* root_user.__count is 1, for init task cred */ struct user_struct root_user = { .__count = ATOMIC_INIT(1), .processes = ATOMIC_INIT(1), .sigpending = ATOMIC_INIT(0), .locked_shm = 0, .uid = GLOBAL_ROOT_UID, }; /* * These routines must be called with the uidhash spinlock held! */ static void uid_hash_insert(struct user_struct *up, struct hlist_head *hashent) { hlist_add_head(&up->uidhash_node, hashent); } static void uid_hash_remove(struct user_struct *up) { hlist_del_init(&up->uidhash_node); } static struct user_struct *uid_hash_find(kuid_t uid, struct hlist_head *hashent) { struct user_struct *user; hlist_for_each_entry(user, hashent, uidhash_node) { if (uid_eq(user->uid, uid)) { atomic_inc(&user->__count); return user; } } return NULL; } /* IRQs are disabled and uidhash_lock is held upon function entry. * IRQ state (as stored in flags) is restored and uidhash_lock released * upon function exit. */ static void free_user(struct user_struct *up, unsigned long flags) __releases(&uidhash_lock) { uid_hash_remove(up); spin_unlock_irqrestore(&uidhash_lock, flags); key_put(up->uid_keyring); key_put(up->session_keyring); kmem_cache_free(uid_cachep, up); } /* * Locate the user_struct for the passed UID. If found, take a ref on it. The * caller must undo that ref with free_uid(). * * If the user_struct could not be found, return NULL. */ struct user_struct *find_user(kuid_t uid) { struct user_struct *ret; unsigned long flags; spin_lock_irqsave(&uidhash_lock, flags); ret = uid_hash_find(uid, uidhashentry(uid)); spin_unlock_irqrestore(&uidhash_lock, flags); return ret; } void free_uid(struct user_struct *up) { unsigned long flags; if (!up) return; local_irq_save(flags); if (atomic_dec_and_lock(&up->__count, &uidhash_lock)) free_user(up, flags); else local_irq_restore(flags); } struct user_struct *alloc_uid(kuid_t uid) { struct hlist_head *hashent = uidhashentry(uid); struct user_struct *up, *new; spin_lock_irq(&uidhash_lock); up = uid_hash_find(uid, hashent); spin_unlock_irq(&uidhash_lock); if (!up) { new = kmem_cache_zalloc(uid_cachep, GFP_KERNEL); if (!new) goto out_unlock; new->uid = uid; atomic_set(&new->__count, 1); /* * Before adding this, check whether we raced * on adding the same user already.. */ spin_lock_irq(&uidhash_lock); up = uid_hash_find(uid, hashent); if (up) { key_put(new->uid_keyring); key_put(new->session_keyring); kmem_cache_free(uid_cachep, new); } else { uid_hash_insert(new, hashent); up = new; } spin_unlock_irq(&uidhash_lock); } return up; out_unlock: return NULL; } static int __init uid_cache_init(void) { int n; uid_cachep = kmem_cache_create("uid_cache", sizeof(struct user_struct), 0, SLAB_HWCACHE_ALIGN|SLAB_PANIC, NULL); for(n = 0; n < UIDHASH_SZ; ++n) INIT_HLIST_HEAD(uidhash_table + n); /* Insert the root user immediately (init already runs as root) */ spin_lock_irq(&uidhash_lock); uid_hash_insert(&root_user, uidhashentry(GLOBAL_ROOT_UID)); spin_unlock_irq(&uidhash_lock); return 0; } subsys_initcall(uid_cache_init);