aboutsummaryrefslogtreecommitdiffstats
blob: f8e946471a58d7bb6ac07d22cf6a876d8c509410 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
* Generic Exynos Bus frequency device

The Samsung Exynos SoC has many buses for data transfer between DRAM
and sub-blocks in SoC. Most Exynos SoCs share the common architecture
for buses. Generally, each bus of Exynos SoC includes a source clock
and a power line, which are able to change the clock frequency
of the bus in runtime. To monitor the usage of each bus in runtime,
the driver uses the PPMU (Platform Performance Monitoring Unit), which
is able to measure the current load of sub-blocks.

The Exynos SoC includes the various sub-blocks which have the each AXI bus.
The each AXI bus has the owned source clock but, has not the only owned
power line. The power line might be shared among one more sub-blocks.
So, we can divide into two type of device as the role of each sub-block.
There are two type of bus devices as following:
- parent bus device
- passive bus device

Basically, parent and passive bus device share the same power line.
The parent bus device can only change the voltage of shared power line
and the rest bus devices (passive bus device) depend on the decision of
the parent bus device. If there are three blocks which share the VDD_xxx
power line, Only one block should be parent device and then the rest blocks
should depend on the parent device as passive device.

	VDD_xxx |--- A block (parent)
		|--- B block (passive)
		|--- C block (passive)

There are a little different composition among Exynos SoC because each Exynos
SoC has different sub-blocks. Therefore, such difference should be specified
in devicetree file instead of each device driver. In result, this driver
is able to support the bus frequency for all Exynos SoCs.

Required properties for all bus devices:
- compatible: Should be "samsung,exynos-bus".
- clock-names : the name of clock used by the bus, "bus".
- clocks : phandles for clock specified in "clock-names" property.
- operating-points-v2: the OPP table including frequency/voltage information
  to support DVFS (Dynamic Voltage/Frequency Scaling) feature.

Required properties only for parent bus device:
- vdd-supply: the regulator to provide the buses with the voltage.
- devfreq-events: the devfreq-event device to monitor the current utilization
  of buses.

Required properties only for passive bus device:
- devfreq: the parent bus device.

Optional properties only for parent bus device:
- exynos,saturation-ratio: the percentage value which is used to calibrate
			the performance count against total cycle count.
- exynos,voltage-tolerance: the percentage value for bus voltage tolerance
			which is used to calculate the max voltage.

Detailed correlation between sub-blocks and power line according to Exynos SoC:
- In case of Exynos3250, there are two power line as following:
	VDD_MIF |--- DMC

	VDD_INT |--- LEFTBUS (parent device)
		|--- PERIL
		|--- MFC
		|--- G3D
		|--- RIGHTBUS
		|--- PERIR
		|--- FSYS
		|--- LCD0
		|--- PERIR
		|--- ISP
		|--- CAM

- In case of Exynos4210, there is one power line as following:
	VDD_INT |--- DMC (parent device)
		|--- LEFTBUS
		|--- PERIL
		|--- MFC(L)
		|--- G3D
		|--- TV
		|--- LCD0
		|--- RIGHTBUS
		|--- PERIR
		|--- MFC(R)
		|--- CAM
		|--- FSYS
		|--- GPS
		|--- LCD0
		|--- LCD1

- In case of Exynos4x12, there are two power line as following:
	VDD_MIF |--- DMC

	VDD_INT |--- LEFTBUS (parent device)
		|--- PERIL
		|--- MFC(L)
		|--- G3D
		|--- TV
		|--- IMAGE
		|--- RIGHTBUS
		|--- PERIR
		|--- MFC(R)
		|--- CAM
		|--- FSYS
		|--- GPS
		|--- LCD0
		|--- ISP

- In case of Exynos5422, there are two power line as following:
	VDD_MIF |--- DREX 0 (parent device, DRAM EXpress controller)
	        |--- DREX 1

	VDD_INT |--- NoC_Core (parent device)
		|--- G2D
		|--- G3D
		|--- DISP1
		|--- NoC_WCORE
		|--- GSCL
		|--- MSCL
		|--- ISP
		|--- MFC
		|--- GEN
		|--- PERIS
		|--- PERIC
		|--- FSYS
		|--- FSYS2

- In case of Exynos5433, there is VDD_INT power line as following:
	VDD_INT |--- G2D (parent device)
		|--- MSCL
		|--- GSCL
		|--- JPEG
		|--- MFC
		|--- HEVC
		|--- BUS0
		|--- BUS1
		|--- BUS2
		|--- PERIS (Fixed clock rate)
		|--- PERIC (Fixed clock rate)
		|--- FSYS  (Fixed clock rate)

Example1:
	Show the AXI buses of Exynos3250 SoC. Exynos3250 divides the buses to
	power line (regulator). The MIF (Memory Interface) AXI bus is used to
	transfer data between DRAM and CPU and uses the VDD_MIF regulator.

	- MIF (Memory Interface) block
	: VDD_MIF |--- DMC (Dynamic Memory Controller)

	- INT (Internal) block
	: VDD_INT |--- LEFTBUS (parent device)
		  |--- PERIL
		  |--- MFC
		  |--- G3D
		  |--- RIGHTBUS
		  |--- FSYS
		  |--- LCD0
		  |--- PERIR
		  |--- ISP
		  |--- CAM

	- MIF bus's frequency/voltage table
	-----------------------
	|Lv| Freq   | Voltage |
	-----------------------
	|L1| 50000  |800000   |
	|L2| 100000 |800000   |
	|L3| 134000 |800000   |
	|L4| 200000 |825000   |
	|L5| 400000 |875000   |
	-----------------------

	- INT bus's frequency/voltage table
	----------------------------------------------------------
	|Block|LEFTBUS|RIGHTBUS|MCUISP |ISP    |PERIL  ||VDD_INT |
	| name|       |LCD0    |       |       |       ||        |
	|     |       |FSYS    |       |       |       ||        |
	|     |       |MFC     |       |       |       ||        |
	----------------------------------------------------------
	|Mode |*parent|passive |passive|passive|passive||        |
	----------------------------------------------------------
	|Lv   |Frequency                               ||Voltage |
	----------------------------------------------------------
	|L1   |50000  |50000   |50000  |50000  |50000  ||900000  |
	|L2   |80000  |80000   |80000  |80000  |80000  ||900000  |
	|L3   |100000 |100000  |100000 |100000 |100000 ||1000000 |
	|L4   |134000 |134000  |200000 |200000 |       ||1000000 |
	|L5   |200000 |200000  |400000 |300000 |       ||1000000 |
	----------------------------------------------------------

Example2 :
	The bus of DMC (Dynamic Memory Controller) block in exynos3250.dtsi
	is listed below:

	bus_dmc: bus_dmc {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu_dmc CLK_DIV_DMC>;
		clock-names = "bus";
		operating-points-v2 = <&bus_dmc_opp_table>;
		status = "disabled";
	};

	bus_dmc_opp_table: opp_table1 {
		compatible = "operating-points-v2";
		opp-shared;

		opp-50000000 {
			opp-hz = /bits/ 64 <50000000>;
			opp-microvolt = <800000>;
		};
		opp-100000000 {
			opp-hz = /bits/ 64 <100000000>;
			opp-microvolt = <800000>;
		};
		opp-134000000 {
			opp-hz = /bits/ 64 <134000000>;
			opp-microvolt = <800000>;
		};
		opp-200000000 {
			opp-hz = /bits/ 64 <200000000>;
			opp-microvolt = <825000>;
		};
		opp-400000000 {
			opp-hz = /bits/ 64 <400000000>;
			opp-microvolt = <875000>;
		};
	};

	bus_leftbus: bus_leftbus {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_GDL>;
		clock-names = "bus";
		operating-points-v2 = <&bus_leftbus_opp_table>;
		status = "disabled";
	};

	bus_rightbus: bus_rightbus {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_GDR>;
		clock-names = "bus";
		operating-points-v2 = <&bus_leftbus_opp_table>;
		status = "disabled";
	};

	bus_lcd0: bus_lcd0 {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_ACLK_160>;
		clock-names = "bus";
		operating-points-v2 = <&bus_leftbus_opp_table>;
		status = "disabled";
	};

	bus_fsys: bus_fsys {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_ACLK_200>;
		clock-names = "bus";
		operating-points-v2 = <&bus_leftbus_opp_table>;
		status = "disabled";
	};

	bus_mcuisp: bus_mcuisp {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_ACLK_400_MCUISP>;
		clock-names = "bus";
		operating-points-v2 = <&bus_mcuisp_opp_table>;
		status = "disabled";
	};

	bus_isp: bus_isp {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_ACLK_266>;
		clock-names = "bus";
		operating-points-v2 = <&bus_isp_opp_table>;
		status = "disabled";
	};

	bus_peril: bus_peril {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_DIV_ACLK_100>;
		clock-names = "bus";
		operating-points-v2 = <&bus_peril_opp_table>;
		status = "disabled";
	};

	bus_mfc: bus_mfc {
		compatible = "samsung,exynos-bus";
		clocks = <&cmu CLK_SCLK_MFC>;
		clock-names = "bus";
		operating-points-v2 = <&bus_leftbus_opp_table>;
		status = "disabled";
	};

	bus_leftbus_opp_table: opp_table1 {
		compatible = "operating-points-v2";
		opp-shared;

		opp-50000000 {
			opp-hz = /bits/ 64 <50000000>;
			opp-microvolt = <900000>;
		};
		opp-80000000 {
			opp-hz = /bits/ 64 <80000000>;
			opp-microvolt = <900000>;
		};
		opp-100000000 {
			opp-hz = /bits/ 64 <100000000>;
			opp-microvolt = <1000000>;
		};
		opp-134000000 {
			opp-hz = /bits/ 64 <134000000>;
			opp-microvolt = <1000000>;
		};
		opp-200000000 {
			opp-hz = /bits/ 64 <200000000>;
			opp-microvolt = <1000000>;
		};
	};

	bus_mcuisp_opp_table: opp_table2 {
		compatible = "operating-points-v2";
		opp-shared;

		opp-50000000 {
			opp-hz = /bits/ 64 <50000000>;
		};
		opp-80000000 {
			opp-hz = /bits/ 64 <80000000>;
		};
		opp-100000000 {
			opp-hz = /bits/ 64 <100000000>;
		};
		opp-200000000 {
			opp-hz = /bits/ 64 <200000000>;
		};
		opp-400000000 {
			opp-hz = /bits/ 64 <400000000>;
		};
	};

	bus_isp_opp_table: opp_table3 {
		compatible = "operating-points-v2";
		opp-shared;

		opp-50000000 {
			opp-hz = /bits/ 64 <50000000>;
		};
		opp-80000000 {
			opp-hz = /bits/ 64 <80000000>;
		};
		opp-100000000 {
			opp-hz = /bits/ 64 <100000000>;
		};
		opp-200000000 {
			opp-hz = /bits/ 64 <200000000>;
		};
		opp-300000000 {
			opp-hz = /bits/ 64 <300000000>;
		};
	};

	bus_peril_opp_table: opp_table4 {
		compatible = "operating-points-v2";
		opp-shared;

		opp-50000000 {
			opp-hz = /bits/ 64 <50000000>;
		};
		opp-80000000 {
			opp-hz = /bits/ 64 <80000000>;
		};
		opp-100000000 {
			opp-hz = /bits/ 64 <100000000>;
		};
	};


	Usage case to handle the frequency and voltage of bus on runtime
	in exynos3250-rinato.dts is listed below:

	&bus_dmc {
		devfreq-events = <&ppmu_dmc0_3>, <&ppmu_dmc1_3>;
		vdd-supply = <&buck1_reg>;	/* VDD_MIF */
		status = "okay";
	};

	&bus_leftbus {
		devfreq-events = <&ppmu_leftbus_3>, <&ppmu_rightbus_3>;
		vdd-supply = <&buck3_reg>;
		status = "okay";
	};

	&bus_rightbus {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};

	&bus_lcd0 {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};

	&bus_fsys {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};

	&bus_mcuisp {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};

	&bus_isp {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};

	&bus_peril {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};

	&bus_mfc {
		devfreq = <&bus_leftbus>;
		status = "okay";
	};