aboutsummaryrefslogtreecommitdiffstats
blob: 57a8d061006276730b07ff1ebf9867f52841e673 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
Allwinner A10 Display Pipeline
==============================

The Allwinner A10 Display pipeline is composed of several components
that are going to be documented below:

TV Encoder
----------

The TV Encoder supports the composite and VGA output. It is one end of
the pipeline.

Required properties:
 - compatible: value should be "allwinner,sun4i-a10-tv-encoder".
 - reg: base address and size of memory-mapped region
 - clocks: the clocks driving the TV encoder
 - resets: phandle to the reset controller driving the encoder

- ports: A ports node with endpoint definitions as defined in
  Documentation/devicetree/bindings/media/video-interfaces.txt. The
  first port should be the input endpoint.

TCON
----

The TCON acts as a timing controller for RGB, LVDS and TV interfaces.

Required properties:
 - compatible: value must be either:
   * allwinner,sun5i-a13-tcon
   * allwinner,sun6i-a31-tcon
   * allwinner,sun6i-a31s-tcon
   * allwinner,sun8i-a33-tcon
 - reg: base address and size of memory-mapped region
 - interrupts: interrupt associated to this IP
 - clocks: phandles to the clocks feeding the TCON. Three are needed:
   - 'ahb': the interface clocks
   - 'tcon-ch0': The clock driving the TCON channel 0
 - resets: phandles to the reset controllers driving the encoder
   - "lcd": the reset line for the TCON channel 0

 - clock-names: the clock names mentioned above
 - reset-names: the reset names mentioned above
 - clock-output-names: Name of the pixel clock created

- ports: A ports node with endpoint definitions as defined in
  Documentation/devicetree/bindings/media/video-interfaces.txt. The
  first port should be the input endpoint, the second one the output

  The output should have two endpoints. The first is the block
  connected to the TCON channel 0 (usually a panel or a bridge), the
  second the block connected to the TCON channel 1 (usually the TV
  encoder)

On SoCs other than the A33, there is one more clock required:
   - 'tcon-ch1': The clock driving the TCON channel 1

DRC
---

The DRC (Dynamic Range Controller), found in the latest Allwinner SoCs
(A31, A23, A33), allows to dynamically adjust pixel
brightness/contrast based on histogram measurements for LCD content
adaptive backlight control.


Required properties:
  - compatible: value must be one of:
    * allwinner,sun6i-a31-drc
    * allwinner,sun6i-a31s-drc
    * allwinner,sun8i-a33-drc
  - reg: base address and size of the memory-mapped region.
  - interrupts: interrupt associated to this IP
  - clocks: phandles to the clocks feeding the DRC
    * ahb: the DRC interface clock
    * mod: the DRC module clock
    * ram: the DRC DRAM clock
  - clock-names: the clock names mentioned above
  - resets: phandles to the reset line driving the DRC

- ports: A ports node with endpoint definitions as defined in
  Documentation/devicetree/bindings/media/video-interfaces.txt. The
  first port should be the input endpoints, the second one the outputs

Display Engine Backend
----------------------

The display engine backend exposes layers and sprites to the
system.

Required properties:
  - compatible: value must be one of:
    * allwinner,sun5i-a13-display-backend
    * allwinner,sun6i-a31-display-backend
    * allwinner,sun8i-a33-display-backend
  - reg: base address and size of the memory-mapped region.
  - interrupts: interrupt associated to this IP
  - clocks: phandles to the clocks feeding the frontend and backend
    * ahb: the backend interface clock
    * mod: the backend module clock
    * ram: the backend DRAM clock
  - clock-names: the clock names mentioned above
  - resets: phandles to the reset controllers driving the backend

- ports: A ports node with endpoint definitions as defined in
  Documentation/devicetree/bindings/media/video-interfaces.txt. The
  first port should be the input endpoints, the second one the output

On the A33, some additional properties are required:
  - reg needs to have an additional region corresponding to the SAT
  - reg-names need to be set, with "be" and "sat"
  - clocks and clock-names need to have a phandle to the SAT bus
    clocks, whose name will be "sat"
  - resets and reset-names need to have a phandle to the SAT bus
    resets, whose name will be "sat"

Display Engine Frontend
-----------------------

The display engine frontend does formats conversion, scaling,
deinterlacing and color space conversion.

Required properties:
  - compatible: value must be one of:
    * allwinner,sun5i-a13-display-frontend
    * allwinner,sun6i-a31-display-frontend
    * allwinner,sun8i-a33-display-frontend
  - reg: base address and size of the memory-mapped region.
  - interrupts: interrupt associated to this IP
  - clocks: phandles to the clocks feeding the frontend and backend
    * ahb: the backend interface clock
    * mod: the backend module clock
    * ram: the backend DRAM clock
  - clock-names: the clock names mentioned above
  - resets: phandles to the reset controllers driving the backend

- ports: A ports node with endpoint definitions as defined in
  Documentation/devicetree/bindings/media/video-interfaces.txt. The
  first port should be the input endpoints, the second one the outputs


Display Engine Pipeline
-----------------------

The display engine pipeline (and its entry point, since it can be
either directly the backend or the frontend) is represented as an
extra node.

Required properties:
  - compatible: value must be one of:
    * allwinner,sun5i-a13-display-engine
    * allwinner,sun6i-a31-display-engine
    * allwinner,sun6i-a31s-display-engine
    * allwinner,sun8i-a33-display-engine

  - allwinner,pipelines: list of phandle to the display engine
    frontends available.

Example:

panel: panel {
	compatible = "olimex,lcd-olinuxino-43-ts";
	#address-cells = <1>;
	#size-cells = <0>;

	port {
		#address-cells = <1>;
		#size-cells = <0>;

		panel_input: endpoint {
			remote-endpoint = <&tcon0_out_panel>;
		};
	};
};

tve0: tv-encoder@01c0a000 {
	compatible = "allwinner,sun4i-a10-tv-encoder";
	reg = <0x01c0a000 0x1000>;
	clocks = <&ahb_gates 34>;
	resets = <&tcon_ch0_clk 0>;

	port {
		#address-cells = <1>;
		#size-cells = <0>;

		tve0_in_tcon0: endpoint@0 {
			reg = <0>;
			remote-endpoint = <&tcon0_out_tve0>;
		};
	};
};

tcon0: lcd-controller@1c0c000 {
	compatible = "allwinner,sun5i-a13-tcon";
	reg = <0x01c0c000 0x1000>;
	interrupts = <44>;
	resets = <&tcon_ch0_clk 1>;
	reset-names = "lcd";
	clocks = <&ahb_gates 36>,
		 <&tcon_ch0_clk>,
		 <&tcon_ch1_clk>;
	clock-names = "ahb",
		      "tcon-ch0",
		      "tcon-ch1";
	clock-output-names = "tcon-pixel-clock";

	ports {
		#address-cells = <1>;
		#size-cells = <0>;

		tcon0_in: port@0 {
			#address-cells = <1>;
			#size-cells = <0>;
			reg = <0>;

			tcon0_in_be0: endpoint@0 {
				reg = <0>;
				remote-endpoint = <&be0_out_tcon0>;
			};
		};

		tcon0_out: port@1 {
			#address-cells = <1>;
			#size-cells = <0>;
			reg = <1>;

			tcon0_out_panel: endpoint@0 {
				reg = <0>;
				remote-endpoint = <&panel_input>;
			};

			tcon0_out_tve0: endpoint@1 {
				reg = <1>;
				remote-endpoint = <&tve0_in_tcon0>;
			};
		};
	};
};

fe0: display-frontend@1e00000 {
	compatible = "allwinner,sun5i-a13-display-frontend";
	reg = <0x01e00000 0x20000>;
	interrupts = <47>;
	clocks = <&ahb_gates 46>, <&de_fe_clk>,
		 <&dram_gates 25>;
	clock-names = "ahb", "mod",
		      "ram";
	resets = <&de_fe_clk>;

	ports {
		#address-cells = <1>;
		#size-cells = <0>;

		fe0_out: port@1 {
			#address-cells = <1>;
			#size-cells = <0>;
			reg = <1>;

			fe0_out_be0: endpoint {
				remote-endpoint = <&be0_in_fe0>;
			};
		};
	};
};

be0: display-backend@1e60000 {
	compatible = "allwinner,sun5i-a13-display-backend";
	reg = <0x01e60000 0x10000>;
	interrupts = <47>;
	clocks = <&ahb_gates 44>, <&de_be_clk>,
		 <&dram_gates 26>;
	clock-names = "ahb", "mod",
		      "ram";
	resets = <&de_be_clk>;

	ports {
		#address-cells = <1>;
		#size-cells = <0>;

		be0_in: port@0 {
			#address-cells = <1>;
			#size-cells = <0>;
			reg = <0>;

			be0_in_fe0: endpoint@0 {
				reg = <0>;
				remote-endpoint = <&fe0_out_be0>;
			};
		};

		be0_out: port@1 {
			#address-cells = <1>;
			#size-cells = <0>;
			reg = <1>;

			be0_out_tcon0: endpoint@0 {
				reg = <0>;
				remote-endpoint = <&tcon0_in_be0>;
			};
		};
	};
};

display-engine {
	compatible = "allwinner,sun5i-a13-display-engine";
	allwinner,pipelines = <&fe0>;
};