aboutsummaryrefslogtreecommitdiffstats
blob: 503160a7b9a0956e4325587e5230aa40fc714bb0 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
# SPDX-License-Identifier: GPL-2.0-only
%YAML 1.2
---
$id: http://devicetree.org/schemas/iommu/arm,smmu.yaml#
$schema: http://devicetree.org/meta-schemas/core.yaml#

title: ARM System MMU Architecture Implementation

maintainers:
  - Will Deacon <will@kernel.org>
  - Robin Murphy <Robin.Murphy@arm.com>

description: |+
  ARM SoCs may contain an implementation of the ARM System Memory
  Management Unit Architecture, which can be used to provide 1 or 2 stages
  of address translation to bus masters external to the CPU.

  The SMMU may also raise interrupts in response to various fault
  conditions.

properties:
  $nodename:
    pattern: "^iommu@[0-9a-f]*"
  compatible:
    oneOf:
      - description: Qcom SoCs implementing "arm,smmu-v2"
        items:
          - enum:
              - qcom,msm8996-smmu-v2
              - qcom,msm8998-smmu-v2
              - qcom,sc7180-smmu-v2
              - qcom,sdm845-smmu-v2
          - const: qcom,smmu-v2

      - description: Qcom SoCs implementing "arm,mmu-500"
        items:
          - enum:
              - qcom,sc7180-smmu-500
              - qcom,sdm845-smmu-500
              - qcom,sm8150-smmu-500
              - qcom,sm8250-smmu-500
          - const: arm,mmu-500
      - description: Marvell SoCs implementing "arm,mmu-500"
        items:
          - const: marvell,ap806-smmu-500
          - const: arm,mmu-500
      - description: NVIDIA SoCs that program two ARM MMU-500s identically
        items:
          - enum:
              - nvidia,tegra194-smmu
          - const: nvidia,smmu-500
      - items:
          - const: arm,mmu-500
          - const: arm,smmu-v2
      - items:
          - enum:
              - arm,mmu-400
              - arm,mmu-401
          - const: arm,smmu-v1
      - enum:
          - arm,smmu-v1
          - arm,smmu-v2
          - arm,mmu-400
          - arm,mmu-401
          - arm,mmu-500
          - cavium,smmu-v2

  reg:
    minItems: 1
    maxItems: 2

  '#global-interrupts':
    description: The number of global interrupts exposed by the device.
    $ref: /schemas/types.yaml#/definitions/uint32
    minimum: 0
    maximum: 260   # 2 secure, 2 non-secure, and up to 256 perf counters

  '#iommu-cells':
    enum: [ 1, 2 ]
    description: |
      See Documentation/devicetree/bindings/iommu/iommu.txt for details. With a
      value of 1, each IOMMU specifier represents a distinct stream ID emitted
      by that device into the relevant SMMU.

      SMMUs with stream matching support and complex masters may use a value of
      2, where the second cell of the IOMMU specifier represents an SMR mask to
      combine with the ID in the first cell.  Care must be taken to ensure the
      set of matched IDs does not result in conflicts.

  interrupts:
    minItems: 1
    maxItems: 388   # 260 plus 128 contexts
    description: |
      Interrupt list, with the first #global-interrupts entries corresponding to
      the global interrupts and any following entries corresponding to context
      interrupts, specified in order of their indexing by the SMMU.

      For SMMUv2 implementations, there must be exactly one interrupt per
      context bank. In the case of a single, combined interrupt, it must be
      listed multiple times.

  dma-coherent:
    description: |
      Present if page table walks made by the SMMU are cache coherent with the
      CPU.

      NOTE: this only applies to the SMMU itself, not masters connected
      upstream of the SMMU.

  calxeda,smmu-secure-config-access:
    type: boolean
    description:
      Enable proper handling of buggy implementations that always use secure
      access to SMMU configuration registers. In this case non-secure aliases of
      secure registers have to be used during SMMU configuration.

  stream-match-mask:
    $ref: /schemas/types.yaml#/definitions/uint32
    description: |
      For SMMUs supporting stream matching and using #iommu-cells = <1>,
      specifies a mask of bits to ignore when matching stream IDs (e.g. this may
      be programmed into the SMRn.MASK field of every stream match register
      used). For cases where it is desirable to ignore some portion of every
      Stream ID (e.g. for certain MMU-500 configurations given globally unique
      input IDs). This property is not valid for SMMUs using stream indexing, or
      using stream matching with #iommu-cells = <2>, and may be ignored if
      present in such cases.

  clock-names:
    items:
      - const: bus
      - const: iface

  clocks:
    items:
      - description: bus clock required for downstream bus access and for the
          smmu ptw
      - description: interface clock required to access smmu's registers
          through the TCU's programming interface.

  power-domains:
    maxItems: 1

required:
  - compatible
  - reg
  - '#global-interrupts'
  - '#iommu-cells'
  - interrupts

additionalProperties: false

allOf:
  - if:
      properties:
        compatible:
          contains:
            enum:
              - nvidia,tegra194-smmu
    then:
      properties:
        reg:
          minItems: 2
          maxItems: 2
    else:
      properties:
        reg:
          maxItems: 1

examples:
  - |+
    /* SMMU with stream matching or stream indexing */
    smmu1: iommu@ba5e0000 {
            compatible = "arm,smmu-v1";
            reg = <0xba5e0000 0x10000>;
            #global-interrupts = <2>;
            interrupts = <0 32 4>,
                         <0 33 4>,
                         <0 34 4>, /* This is the first context interrupt */
                         <0 35 4>,
                         <0 36 4>,
                         <0 37 4>;
            #iommu-cells = <1>;
    };

    /* device with two stream IDs, 0 and 7 */
    master1 {
            iommus = <&smmu1 0>,
                     <&smmu1 7>;
    };


    /* SMMU with stream matching */
    smmu2: iommu@ba5f0000 {
            compatible = "arm,smmu-v1";
            reg = <0xba5f0000 0x10000>;
            #global-interrupts = <2>;
            interrupts = <0 38 4>,
                         <0 39 4>,
                         <0 40 4>, /* This is the first context interrupt */
                         <0 41 4>,
                         <0 42 4>,
                         <0 43 4>;
            #iommu-cells = <2>;
    };

    /* device with stream IDs 0 and 7 */
    master2 {
            iommus = <&smmu2 0 0>,
                     <&smmu2 7 0>;
    };

    /* device with stream IDs 1, 17, 33 and 49 */
    master3 {
            iommus = <&smmu2 1 0x30>;
    };


    /* ARM MMU-500 with 10-bit stream ID input configuration */
    smmu3: iommu@ba600000 {
            compatible = "arm,mmu-500", "arm,smmu-v2";
            reg = <0xba600000 0x10000>;
            #global-interrupts = <2>;
            interrupts = <0 44 4>,
                         <0 45 4>,
                         <0 46 4>, /* This is the first context interrupt */
                         <0 47 4>,
                         <0 48 4>,
                         <0 49 4>;
            #iommu-cells = <1>;
            /* always ignore appended 5-bit TBU number */
            stream-match-mask = <0x7c00>;
    };

    bus {
            /* bus whose child devices emit one unique 10-bit stream
               ID each, but may master through multiple SMMU TBUs */
            iommu-map = <0 &smmu3 0 0x400>;


    };

  - |+
    /* Qcom's arm,smmu-v2 implementation */
    #include <dt-bindings/interrupt-controller/arm-gic.h>
    #include <dt-bindings/interrupt-controller/irq.h>
    smmu4: iommu@d00000 {
      compatible = "qcom,msm8996-smmu-v2", "qcom,smmu-v2";
      reg = <0xd00000 0x10000>;

      #global-interrupts = <1>;
      interrupts = <GIC_SPI 73 IRQ_TYPE_LEVEL_HIGH>,
             <GIC_SPI 320 IRQ_TYPE_LEVEL_HIGH>,
             <GIC_SPI 321 IRQ_TYPE_LEVEL_HIGH>;
      #iommu-cells = <1>;
      power-domains = <&mmcc 0>;

      clocks = <&mmcc 123>,
        <&mmcc 124>;
      clock-names = "bus", "iface";
    };