aboutsummaryrefslogtreecommitdiffstats
blob: aa2d6da9d187be21b1f38ac116f40941bb5dc39d (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
/*
 * Copyright (C) 2004, 2007-2010, 2011-2012 Synopsys, Inc. (www.synopsys.com)
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 */

#ifndef __ASM_ARC_ELF_H
#define __ASM_ARC_ELF_H

#include <linux/types.h>
#include <uapi/asm/elf.h>

/* These ELF defines belong to uapi but libc elf.h already defines them */
#define EM_ARCOMPACT		93

#define EM_ARCV2		195	/* ARCv2 Cores */

#define EM_ARC_INUSE		(IS_ENABLED(CONFIG_ISA_ARCOMPACT) ? \
					EM_ARCOMPACT : EM_ARCV2)

/* ARC Relocations (kernel Modules only) */
#define  R_ARC_32		0x4
#define  R_ARC_32_ME		0x1B
#define  R_ARC_32_PCREL		0x31

/*to set parameters in the core dumps */
#define ELF_ARCH		EM_ARCOMPACT
#define ELF_CLASS		ELFCLASS32

#ifdef CONFIG_CPU_BIG_ENDIAN
#define ELF_DATA		ELFDATA2MSB
#else
#define ELF_DATA		ELFDATA2LSB
#endif

/*
 * To ensure that
 *  -we don't load something for the wrong architecture.
 *  -The userspace is using the correct syscall ABI
 */
struct elf32_hdr;
extern int elf_check_arch(const struct elf32_hdr *);
#define elf_check_arch	elf_check_arch

#define CORE_DUMP_USE_REGSET

#define ELF_EXEC_PAGESIZE	PAGE_SIZE

/*
 * This is the location that an ET_DYN program is loaded if exec'ed.  Typical
 * use of this is to invoke "./ld.so someprog" to test out a new version of
 * the loader.  We need to make sure that it is out of the way of the program
 * that it will "exec", and that there is sufficient room for the brk.
 */
#define ELF_ET_DYN_BASE		(2UL * TASK_SIZE / 3)

/*
 * When the program starts, a1 contains a pointer to a function to be
 * registered with atexit, as per the SVR4 ABI.  A value of 0 means we
 * have no such handler.
 */
#define ELF_PLAT_INIT(_r, load_addr)	((_r)->r0 = 0)

/*
 * This yields a mask that user programs can use to figure out what
 * instruction set this cpu supports.
 */
#define ELF_HWCAP	(0)

/*
 * This yields a string that ld.so will use to load implementation
 * specific libraries for optimization.  This is more specific in
 * intent than poking at uname or /proc/cpuinfo.
 */
#define ELF_PLATFORM	(NULL)

#endif