aboutsummaryrefslogtreecommitdiffstats
blob: 2cd27c830ab68b3e7e340adb9bfab9d0e42a38ee (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
/*
 * arch/arm/mach-at91/pm.c
 * AT91 Power Management
 *
 * Copyright (C) 2005 David Brownell
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 */

#include <linux/genalloc.h>
#include <linux/io.h>
#include <linux/of_address.h>
#include <linux/of.h>
#include <linux/of_platform.h>
#include <linux/suspend.h>

#include <linux/clk/at91_pmc.h>

#include <asm/cacheflush.h>
#include <asm/fncpy.h>
#include <asm/system_misc.h>

#include "generic.h"
#include "pm.h"

/*
 * FIXME: this is needed to communicate between the pinctrl driver and
 * the PM implementation in the machine. Possibly part of the PM
 * implementation should be moved down into the pinctrl driver and get
 * called as part of the generic suspend/resume path.
 */
#ifdef CONFIG_PINCTRL_AT91
extern void at91_pinctrl_gpio_suspend(void);
extern void at91_pinctrl_gpio_resume(void);
#endif

static struct at91_pm_data pm_data;

#define at91_ramc_read(id, field) \
	__raw_readl(pm_data.ramc[id] + field)

#define at91_ramc_write(id, field, value) \
	__raw_writel(value, pm_data.ramc[id] + field)

static int at91_pm_valid_state(suspend_state_t state)
{
	switch (state) {
		case PM_SUSPEND_ON:
		case PM_SUSPEND_STANDBY:
		case PM_SUSPEND_MEM:
			return 1;

		default:
			return 0;
	}
}


static suspend_state_t target_state;

/*
 * Called after processes are frozen, but before we shutdown devices.
 */
static int at91_pm_begin(suspend_state_t state)
{
	target_state = state;
	return 0;
}

/*
 * Verify that all the clocks are correct before entering
 * slow-clock mode.
 */
static int at91_pm_verify_clocks(void)
{
	unsigned long scsr;
	int i;

	scsr = readl(pm_data.pmc + AT91_PMC_SCSR);

	/* USB must not be using PLLB */
	if ((scsr & pm_data.uhp_udp_mask) != 0) {
		pr_err("AT91: PM - Suspend-to-RAM with USB still active\n");
		return 0;
	}

	/* PCK0..PCK3 must be disabled, or configured to use clk32k */
	for (i = 0; i < 4; i++) {
		u32 css;

		if ((scsr & (AT91_PMC_PCK0 << i)) == 0)
			continue;
		css = readl(pm_data.pmc + AT91_PMC_PCKR(i)) & AT91_PMC_CSS;
		if (css != AT91_PMC_CSS_SLOW) {
			pr_err("AT91: PM - Suspend-to-RAM with PCK%d src %d\n", i, css);
			return 0;
		}
	}

	return 1;
}

/*
 * Call this from platform driver suspend() to see how deeply to suspend.
 * For example, some controllers (like OHCI) need one of the PLL clocks
 * in order to act as a wakeup source, and those are not available when
 * going into slow clock mode.
 *
 * REVISIT: generalize as clk_will_be_available(clk)?  Other platforms have
 * the very same problem (but not using at91 main_clk), and it'd be better
 * to add one generic API rather than lots of platform-specific ones.
 */
int at91_suspend_entering_slow_clock(void)
{
	return (target_state == PM_SUSPEND_MEM);
}
EXPORT_SYMBOL(at91_suspend_entering_slow_clock);

static void (*at91_suspend_sram_fn)(struct at91_pm_data *);
extern void at91_pm_suspend_in_sram(struct at91_pm_data *pm_data);
extern u32 at91_pm_suspend_in_sram_sz;

static void at91_pm_suspend(suspend_state_t state)
{
	pm_data.mode = (state == PM_SUSPEND_MEM) ? AT91_PM_SLOW_CLOCK : 0;

	flush_cache_all();
	outer_disable();

	at91_suspend_sram_fn(&pm_data);

	outer_resume();
}

static int at91_pm_enter(suspend_state_t state)
{
#ifdef CONFIG_PINCTRL_AT91
	at91_pinctrl_gpio_suspend();
#endif
	switch (state) {
	/*
	 * Suspend-to-RAM is like STANDBY plus slow clock mode, so
	 * drivers must suspend more deeply, the master clock switches
	 * to the clk32k and turns off the main oscillator
	 */
	case PM_SUSPEND_MEM:
		/*
		 * Ensure that clocks are in a valid state.
		 */
		if (!at91_pm_verify_clocks())
			goto error;

		at91_pm_suspend(state);

		break;

	/*
	 * STANDBY mode has *all* drivers suspended; ignores irqs not
	 * marked as 'wakeup' event sources; and reduces DRAM power.
	 * But otherwise it's identical to PM_SUSPEND_ON: cpu idle, and
	 * nothing fancy done with main or cpu clocks.
	 */
	case PM_SUSPEND_STANDBY:
		at91_pm_suspend(state);
		break;

	case PM_SUSPEND_ON:
		cpu_do_idle();
		break;

	default:
		pr_debug("AT91: PM - bogus suspend state %d\n", state);
		goto error;
	}

error:
	target_state = PM_SUSPEND_ON;

#ifdef CONFIG_PINCTRL_AT91
	at91_pinctrl_gpio_resume();
#endif
	return 0;
}

/*
 * Called right prior to thawing processes.
 */
static void at91_pm_end(void)
{
	target_state = PM_SUSPEND_ON;
}


static const struct platform_suspend_ops at91_pm_ops = {
	.valid	= at91_pm_valid_state,
	.begin	= at91_pm_begin,
	.enter	= at91_pm_enter,
	.end	= at91_pm_end,
};

static struct platform_device at91_cpuidle_device = {
	.name = "cpuidle-at91",
};

/*
 * The AT91RM9200 goes into self-refresh mode with this command, and will
 * terminate self-refresh automatically on the next SDRAM access.
 *
 * Self-refresh mode is exited as soon as a memory access is made, but we don't
 * know for sure when that happens. However, we need to restore the low-power
 * mode if it was enabled before going idle. Restoring low-power mode while
 * still in self-refresh is "not recommended", but seems to work.
 */
static void at91rm9200_standby(void)
{
	asm volatile(
		"b    1f\n\t"
		".align    5\n\t"
		"1:  mcr    p15, 0, %0, c7, c10, 4\n\t"
		"    str    %2, [%1, %3]\n\t"
		"    mcr    p15, 0, %0, c7, c0, 4\n\t"
		:
		: "r" (0), "r" (pm_data.ramc[0]),
		  "r" (1), "r" (AT91_MC_SDRAMC_SRR));
}

/* We manage both DDRAM/SDRAM controllers, we need more than one value to
 * remember.
 */
static void at91_ddr_standby(void)
{
	/* Those two values allow us to delay self-refresh activation
	 * to the maximum. */
	u32 lpr0, lpr1 = 0;
	u32 mdr, saved_mdr0, saved_mdr1 = 0;
	u32 saved_lpr0, saved_lpr1 = 0;

	/* LPDDR1 --> force DDR2 mode during self-refresh */
	saved_mdr0 = at91_ramc_read(0, AT91_DDRSDRC_MDR);
	if ((saved_mdr0 & AT91_DDRSDRC_MD) == AT91_DDRSDRC_MD_LOW_POWER_DDR) {
		mdr = saved_mdr0 & ~AT91_DDRSDRC_MD;
		mdr |= AT91_DDRSDRC_MD_DDR2;
		at91_ramc_write(0, AT91_DDRSDRC_MDR, mdr);
	}

	if (pm_data.ramc[1]) {
		saved_lpr1 = at91_ramc_read(1, AT91_DDRSDRC_LPR);
		lpr1 = saved_lpr1 & ~AT91_DDRSDRC_LPCB;
		lpr1 |= AT91_DDRSDRC_LPCB_SELF_REFRESH;
		saved_mdr1 = at91_ramc_read(1, AT91_DDRSDRC_MDR);
		if ((saved_mdr1 & AT91_DDRSDRC_MD) == AT91_DDRSDRC_MD_LOW_POWER_DDR) {
			mdr = saved_mdr1 & ~AT91_DDRSDRC_MD;
			mdr |= AT91_DDRSDRC_MD_DDR2;
			at91_ramc_write(1, AT91_DDRSDRC_MDR, mdr);
		}
	}

	saved_lpr0 = at91_ramc_read(0, AT91_DDRSDRC_LPR);
	lpr0 = saved_lpr0 & ~AT91_DDRSDRC_LPCB;
	lpr0 |= AT91_DDRSDRC_LPCB_SELF_REFRESH;

	/* self-refresh mode now */
	at91_ramc_write(0, AT91_DDRSDRC_LPR, lpr0);
	if (pm_data.ramc[1])
		at91_ramc_write(1, AT91_DDRSDRC_LPR, lpr1);

	cpu_do_idle();

	at91_ramc_write(0, AT91_DDRSDRC_MDR, saved_mdr0);
	at91_ramc_write(0, AT91_DDRSDRC_LPR, saved_lpr0);
	if (pm_data.ramc[1]) {
		at91_ramc_write(0, AT91_DDRSDRC_MDR, saved_mdr1);
		at91_ramc_write(1, AT91_DDRSDRC_LPR, saved_lpr1);
	}
}

static void sama5d3_ddr_standby(void)
{
	u32 lpr0;
	u32 saved_lpr0;

	saved_lpr0 = at91_ramc_read(0, AT91_DDRSDRC_LPR);
	lpr0 = saved_lpr0 & ~AT91_DDRSDRC_LPCB;
	lpr0 |= AT91_DDRSDRC_LPCB_POWER_DOWN;

	at91_ramc_write(0, AT91_DDRSDRC_LPR, lpr0);

	cpu_do_idle();

	at91_ramc_write(0, AT91_DDRSDRC_LPR, saved_lpr0);
}

/* We manage both DDRAM/SDRAM controllers, we need more than one value to
 * remember.
 */
static void at91sam9_sdram_standby(void)
{
	u32 lpr0, lpr1 = 0;
	u32 saved_lpr0, saved_lpr1 = 0;

	if (pm_data.ramc[1]) {
		saved_lpr1 = at91_ramc_read(1, AT91_SDRAMC_LPR);
		lpr1 = saved_lpr1 & ~AT91_SDRAMC_LPCB;
		lpr1 |= AT91_SDRAMC_LPCB_SELF_REFRESH;
	}

	saved_lpr0 = at91_ramc_read(0, AT91_SDRAMC_LPR);
	lpr0 = saved_lpr0 & ~AT91_SDRAMC_LPCB;
	lpr0 |= AT91_SDRAMC_LPCB_SELF_REFRESH;

	/* self-refresh mode now */
	at91_ramc_write(0, AT91_SDRAMC_LPR, lpr0);
	if (pm_data.ramc[1])
		at91_ramc_write(1, AT91_SDRAMC_LPR, lpr1);

	cpu_do_idle();

	at91_ramc_write(0, AT91_SDRAMC_LPR, saved_lpr0);
	if (pm_data.ramc[1])
		at91_ramc_write(1, AT91_SDRAMC_LPR, saved_lpr1);
}

struct ramc_info {
	void (*idle)(void);
	unsigned int memctrl;
};

static const struct ramc_info ramc_infos[] __initconst = {
	{ .idle = at91rm9200_standby, .memctrl = AT91_MEMCTRL_MC},
	{ .idle = at91sam9_sdram_standby, .memctrl = AT91_MEMCTRL_SDRAMC},
	{ .idle = at91_ddr_standby, .memctrl = AT91_MEMCTRL_DDRSDR},
	{ .idle = sama5d3_ddr_standby, .memctrl = AT91_MEMCTRL_DDRSDR},
};

static const struct of_device_id const ramc_ids[] __initconst = {
	{ .compatible = "atmel,at91rm9200-sdramc", .data = &ramc_infos[0] },
	{ .compatible = "atmel,at91sam9260-sdramc", .data = &ramc_infos[1] },
	{ .compatible = "atmel,at91sam9g45-ddramc", .data = &ramc_infos[2] },
	{ .compatible = "atmel,sama5d3-ddramc", .data = &ramc_infos[3] },
	{ /*sentinel*/ }
};

static __init void at91_dt_ramc(void)
{
	struct device_node *np;
	const struct of_device_id *of_id;
	int idx = 0;
	void *standby = NULL;
	const struct ramc_info *ramc;

	for_each_matching_node_and_match(np, ramc_ids, &of_id) {
		pm_data.ramc[idx] = of_iomap(np, 0);
		if (!pm_data.ramc[idx])
			panic(pr_fmt("unable to map ramc[%d] cpu registers\n"), idx);

		ramc = of_id->data;
		if (!standby)
			standby = ramc->idle;
		pm_data.memctrl = ramc->memctrl;

		idx++;
	}

	if (!idx)
		panic(pr_fmt("unable to find compatible ram controller node in dtb\n"));

	if (!standby) {
		pr_warn("ramc no standby function available\n");
		return;
	}

	at91_cpuidle_device.dev.platform_data = standby;
}

static void at91rm9200_idle(void)
{
	/*
	 * Disable the processor clock.  The processor will be automatically
	 * re-enabled by an interrupt or by a reset.
	 */
	writel(AT91_PMC_PCK, pm_data.pmc + AT91_PMC_SCDR);
}

static void at91sam9_idle(void)
{
	writel(AT91_PMC_PCK, pm_data.pmc + AT91_PMC_SCDR);
	cpu_do_idle();
}

static void __init at91_pm_sram_init(void)
{
	struct gen_pool *sram_pool;
	phys_addr_t sram_pbase;
	unsigned long sram_base;
	struct device_node *node;
	struct platform_device *pdev = NULL;

	for_each_compatible_node(node, NULL, "mmio-sram") {
		pdev = of_find_device_by_node(node);
		if (pdev) {
			of_node_put(node);
			break;
		}
	}

	if (!pdev) {
		pr_warn("%s: failed to find sram device!\n", __func__);
		return;
	}

	sram_pool = gen_pool_get(&pdev->dev, NULL);
	if (!sram_pool) {
		pr_warn("%s: sram pool unavailable!\n", __func__);
		return;
	}

	sram_base = gen_pool_alloc(sram_pool, at91_pm_suspend_in_sram_sz);
	if (!sram_base) {
		pr_warn("%s: unable to alloc sram!\n", __func__);
		return;
	}

	sram_pbase = gen_pool_virt_to_phys(sram_pool, sram_base);
	at91_suspend_sram_fn = __arm_ioremap_exec(sram_pbase,
					at91_pm_suspend_in_sram_sz, false);
	if (!at91_suspend_sram_fn) {
		pr_warn("SRAM: Could not map\n");
		return;
	}

	/* Copy the pm suspend handler to SRAM */
	at91_suspend_sram_fn = fncpy(at91_suspend_sram_fn,
			&at91_pm_suspend_in_sram, at91_pm_suspend_in_sram_sz);
}

struct pmc_info {
	unsigned long uhp_udp_mask;
};

static const struct pmc_info pmc_infos[] __initconst = {
	{ .uhp_udp_mask = AT91RM9200_PMC_UHP | AT91RM9200_PMC_UDP },
	{ .uhp_udp_mask = AT91SAM926x_PMC_UHP | AT91SAM926x_PMC_UDP },
	{ .uhp_udp_mask = AT91SAM926x_PMC_UHP },
};

static const struct of_device_id atmel_pmc_ids[] __initconst = {
	{ .compatible = "atmel,at91rm9200-pmc", .data = &pmc_infos[0] },
	{ .compatible = "atmel,at91sam9260-pmc", .data = &pmc_infos[1] },
	{ .compatible = "atmel,at91sam9g45-pmc", .data = &pmc_infos[2] },
	{ .compatible = "atmel,at91sam9n12-pmc", .data = &pmc_infos[1] },
	{ .compatible = "atmel,at91sam9x5-pmc", .data = &pmc_infos[1] },
	{ .compatible = "atmel,sama5d3-pmc", .data = &pmc_infos[1] },
	{ .compatible = "atmel,sama5d2-pmc", .data = &pmc_infos[1] },
	{ /* sentinel */ },
};

static void __init at91_pm_init(void (*pm_idle)(void))
{
	struct device_node *pmc_np;
	const struct of_device_id *of_id;
	const struct pmc_info *pmc;

	if (at91_cpuidle_device.dev.platform_data)
		platform_device_register(&at91_cpuidle_device);

	pmc_np = of_find_matching_node_and_match(NULL, atmel_pmc_ids, &of_id);
	pm_data.pmc = of_iomap(pmc_np, 0);
	if (!pm_data.pmc) {
		pr_err("AT91: PM not supported, PMC not found\n");
		return;
	}

	pmc = of_id->data;
	pm_data.uhp_udp_mask = pmc->uhp_udp_mask;

	if (pm_idle)
		arm_pm_idle = pm_idle;

	at91_pm_sram_init();

	if (at91_suspend_sram_fn)
		suspend_set_ops(&at91_pm_ops);
	else
		pr_info("AT91: PM not supported, due to no SRAM allocated\n");
}

void __init at91rm9200_pm_init(void)
{
	at91_dt_ramc();

	/*
	 * AT91RM9200 SDRAM low-power mode cannot be used with self-refresh.
	 */
	at91_ramc_write(0, AT91_MC_SDRAMC_LPR, 0);

	at91_pm_init(at91rm9200_idle);
}

void __init at91sam9_pm_init(void)
{
	at91_dt_ramc();
	at91_pm_init(at91sam9_idle);
}

void __init sama5_pm_init(void)
{
	at91_dt_ramc();
	at91_pm_init(NULL);
}