aboutsummaryrefslogtreecommitdiffstats
blob: 6277e7596ae58fd4934a9a399ec95b52ebfc4dee (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
/* SPDX-License-Identifier: GPL-2.0 */
#ifndef _ASM_POWERPC_NOHASH_PGTABLE_H
#define _ASM_POWERPC_NOHASH_PGTABLE_H

#if defined(CONFIG_PPC64)
#include <asm/nohash/64/pgtable.h>
#else
#include <asm/nohash/32/pgtable.h>
#endif

/* Permission masks used for kernel mappings */
#define PAGE_KERNEL	__pgprot(_PAGE_BASE | _PAGE_KERNEL_RW)
#define PAGE_KERNEL_NC	__pgprot(_PAGE_BASE_NC | _PAGE_KERNEL_RW | _PAGE_NO_CACHE)
#define PAGE_KERNEL_NCG	__pgprot(_PAGE_BASE_NC | _PAGE_KERNEL_RW | \
				 _PAGE_NO_CACHE | _PAGE_GUARDED)
#define PAGE_KERNEL_X	__pgprot(_PAGE_BASE | _PAGE_KERNEL_RWX)
#define PAGE_KERNEL_RO	__pgprot(_PAGE_BASE | _PAGE_KERNEL_RO)
#define PAGE_KERNEL_ROX	__pgprot(_PAGE_BASE | _PAGE_KERNEL_ROX)

/*
 * Protection used for kernel text. We want the debuggers to be able to
 * set breakpoints anywhere, so don't write protect the kernel text
 * on platforms where such control is possible.
 */
#if defined(CONFIG_KGDB) || defined(CONFIG_XMON) || defined(CONFIG_BDI_SWITCH) ||\
	defined(CONFIG_KPROBES) || defined(CONFIG_DYNAMIC_FTRACE)
#define PAGE_KERNEL_TEXT	PAGE_KERNEL_X
#else
#define PAGE_KERNEL_TEXT	PAGE_KERNEL_ROX
#endif

/* Make modules code happy. We don't set RO yet */
#define PAGE_KERNEL_EXEC	PAGE_KERNEL_X

/* Advertise special mapping type for AGP */
#define PAGE_AGP		(PAGE_KERNEL_NC)
#define HAVE_PAGE_AGP

#ifndef __ASSEMBLY__

/* Generic accessors to PTE bits */
#ifndef pte_write
static inline int pte_write(pte_t pte)
{
	return pte_val(pte) & _PAGE_RW;
}
#endif
static inline int pte_read(pte_t pte)		{ return 1; }
static inline int pte_dirty(pte_t pte)		{ return pte_val(pte) & _PAGE_DIRTY; }
static inline int pte_special(pte_t pte)	{ return pte_val(pte) & _PAGE_SPECIAL; }
static inline int pte_none(pte_t pte)		{ return (pte_val(pte) & ~_PTE_NONE_MASK) == 0; }
static inline bool pte_hashpte(pte_t pte)	{ return false; }
static inline bool pte_ci(pte_t pte)		{ return pte_val(pte) & _PAGE_NO_CACHE; }
static inline bool pte_exec(pte_t pte)		{ return pte_val(pte) & _PAGE_EXEC; }

#ifdef CONFIG_NUMA_BALANCING
/*
 * These work without NUMA balancing but the kernel does not care. See the
 * comment in include/linux/pgtable.h . On powerpc, this will only
 * work for user pages and always return true for kernel pages.
 */
static inline int pte_protnone(pte_t pte)
{
	return pte_present(pte) && !pte_user(pte);
}

static inline int pmd_protnone(pmd_t pmd)
{
	return pte_protnone(pmd_pte(pmd));
}
#endif /* CONFIG_NUMA_BALANCING */

static inline int pte_present(pte_t pte)
{
	return pte_val(pte) & _PAGE_PRESENT;
}

static inline bool pte_hw_valid(pte_t pte)
{
	return pte_val(pte) & _PAGE_PRESENT;
}

/*
 * Don't just check for any non zero bits in __PAGE_USER, since for book3e
 * and PTE_64BIT, PAGE_KERNEL_X contains _PAGE_BAP_SR which is also in
 * _PAGE_USER.  Need to explicitly match _PAGE_BAP_UR bit in that case too.
 */
#ifndef pte_user
static inline bool pte_user(pte_t pte)
{
	return (pte_val(pte) & _PAGE_USER) == _PAGE_USER;
}
#endif

/*
 * We only find page table entry in the last level
 * Hence no need for other accessors
 */
#define pte_access_permitted pte_access_permitted
static inline bool pte_access_permitted(pte_t pte, bool write)
{
	/*
	 * A read-only access is controlled by _PAGE_USER bit.
	 * We have _PAGE_READ set for WRITE and EXECUTE
	 */
	if (!pte_present(pte) || !pte_user(pte) || !pte_read(pte))
		return false;

	if (write && !pte_write(pte))
		return false;

	return true;
}

/* Conversion functions: convert a page and protection to a page entry,
 * and a page entry and page directory to the page they refer to.
 *
 * Even if PTEs can be unsigned long long, a PFN is always an unsigned
 * long for now.
 */
static inline pte_t pfn_pte(unsigned long pfn, pgprot_t pgprot) {
	return __pte(((pte_basic_t)(pfn) << PTE_RPN_SHIFT) |
		     pgprot_val(pgprot)); }
static inline unsigned long pte_pfn(pte_t pte)	{
	return pte_val(pte) >> PTE_RPN_SHIFT; }

/* Generic modifiers for PTE bits */
static inline pte_t pte_exprotect(pte_t pte)
{
	return __pte(pte_val(pte) & ~_PAGE_EXEC);
}

static inline pte_t pte_mkclean(pte_t pte)
{
	return __pte(pte_val(pte) & ~_PAGE_DIRTY);
}

static inline pte_t pte_mkold(pte_t pte)
{
	return __pte(pte_val(pte) & ~_PAGE_ACCESSED);
}

static inline pte_t pte_mkspecial(pte_t pte)
{
	return __pte(pte_val(pte) | _PAGE_SPECIAL);
}

#ifndef pte_mkhuge
static inline pte_t pte_mkhuge(pte_t pte)
{
	return __pte(pte_val(pte));
}
#endif

#ifndef pte_mkprivileged
static inline pte_t pte_mkprivileged(pte_t pte)
{
	return __pte(pte_val(pte) & ~_PAGE_USER);
}
#endif

#ifndef pte_mkuser
static inline pte_t pte_mkuser(pte_t pte)
{
	return __pte(pte_val(pte) | _PAGE_USER);
}
#endif

static inline pte_t pte_modify(pte_t pte, pgprot_t newprot)
{
	return __pte((pte_val(pte) & _PAGE_CHG_MASK) | pgprot_val(newprot));
}

/* Insert a PTE, top-level function is out of line. It uses an inline
 * low level function in the respective pgtable-* files
 */
extern void set_pte_at(struct mm_struct *mm, unsigned long addr, pte_t *ptep,
		       pte_t pte);

/* This low level function performs the actual PTE insertion
 * Setting the PTE depends on the MMU type and other factors. It's
 * an horrible mess that I'm not going to try to clean up now but
 * I'm keeping it in one place rather than spread around
 */
static inline void __set_pte_at(struct mm_struct *mm, unsigned long addr,
				pte_t *ptep, pte_t pte, int percpu)
{
	/* Second case is 32-bit with 64-bit PTE.  In this case, we
	 * can just store as long as we do the two halves in the right order
	 * with a barrier in between.
	 * In the percpu case, we also fallback to the simple update
	 */
	if (IS_ENABLED(CONFIG_PPC32) && IS_ENABLED(CONFIG_PTE_64BIT) && !percpu) {
		__asm__ __volatile__("\
			stw%U0%X0 %2,%0\n\
			eieio\n\
			stw%U0%X0 %L2,%1"
		: "=m" (*ptep), "=m" (*((unsigned char *)ptep+4))
		: "r" (pte) : "memory");
		return;
	}
	/* Anything else just stores the PTE normally. That covers all 64-bit
	 * cases, and 32-bit non-hash with 32-bit PTEs.
	 */
#if defined(CONFIG_PPC_8xx) && defined(CONFIG_PPC_16K_PAGES)
	ptep->pte = ptep->pte1 = ptep->pte2 = ptep->pte3 = pte_val(pte);
#else
	*ptep = pte;
#endif

	/*
	 * With hardware tablewalk, a sync is needed to ensure that
	 * subsequent accesses see the PTE we just wrote.  Unlike userspace
	 * mappings, we can't tolerate spurious faults, so make sure
	 * the new PTE will be seen the first time.
	 */
	if (IS_ENABLED(CONFIG_PPC_BOOK3E_64) && is_kernel_addr(addr))
		mb();
}


#define __HAVE_ARCH_PTEP_SET_ACCESS_FLAGS
extern int ptep_set_access_flags(struct vm_area_struct *vma, unsigned long address,
				 pte_t *ptep, pte_t entry, int dirty);

/*
 * Macro to mark a page protection value as "uncacheable".
 */

#define _PAGE_CACHE_CTL	(_PAGE_COHERENT | _PAGE_GUARDED | _PAGE_NO_CACHE | \
			 _PAGE_WRITETHRU)

#define pgprot_noncached(prot)	  (__pgprot((pgprot_val(prot) & ~_PAGE_CACHE_CTL) | \
				            _PAGE_NO_CACHE | _PAGE_GUARDED))

#define pgprot_noncached_wc(prot) (__pgprot((pgprot_val(prot) & ~_PAGE_CACHE_CTL) | \
				            _PAGE_NO_CACHE))

#define pgprot_cached(prot)       (__pgprot((pgprot_val(prot) & ~_PAGE_CACHE_CTL) | \
				            _PAGE_COHERENT))

#if _PAGE_WRITETHRU != 0
#define pgprot_cached_wthru(prot) (__pgprot((pgprot_val(prot) & ~_PAGE_CACHE_CTL) | \
				            _PAGE_COHERENT | _PAGE_WRITETHRU))
#else
#define pgprot_cached_wthru(prot)	pgprot_noncached(prot)
#endif

#define pgprot_cached_noncoherent(prot) \
		(__pgprot(pgprot_val(prot) & ~_PAGE_CACHE_CTL))

#define pgprot_writecombine pgprot_noncached_wc

struct file;
extern pgprot_t phys_mem_access_prot(struct file *file, unsigned long pfn,
				     unsigned long size, pgprot_t vma_prot);
#define __HAVE_PHYS_MEM_ACCESS_PROT

#ifdef CONFIG_HUGETLB_PAGE
static inline int hugepd_ok(hugepd_t hpd)
{
#ifdef CONFIG_PPC_8xx
	return ((hpd_val(hpd) & _PMD_PAGE_MASK) == _PMD_PAGE_8M);
#else
	/* We clear the top bit to indicate hugepd */
	return (hpd_val(hpd) && (hpd_val(hpd) & PD_HUGE) == 0);
#endif
}

static inline int pmd_huge(pmd_t pmd)
{
	return 0;
}

static inline int pud_huge(pud_t pud)
{
	return 0;
}

static inline int pgd_huge(pgd_t pgd)
{
	return 0;
}
#define pgd_huge		pgd_huge

#define is_hugepd(hpd)		(hugepd_ok(hpd))
#endif

/*
 * This gets called at the end of handling a page fault, when
 * the kernel has put a new PTE into the page table for the process.
 * We use it to ensure coherency between the i-cache and d-cache
 * for the page which has just been mapped in.
 */
#if defined(CONFIG_PPC_FSL_BOOK3E) && defined(CONFIG_HUGETLB_PAGE)
void update_mmu_cache(struct vm_area_struct *vma, unsigned long address, pte_t *ptep);
#else
static inline
void update_mmu_cache(struct vm_area_struct *vma, unsigned long address, pte_t *ptep) {}
#endif

#endif /* __ASSEMBLY__ */
#endif