aboutsummaryrefslogtreecommitdiffstats
blob: 7f5aae3c387d29e4b6862b7fd0aa16c98732ff4f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
// SPDX-License-Identifier: GPL-2.0-or-later
/*
 * c 2001 PPC 64 Team, IBM Corp
 */

#include <linux/smp.h>
#include <linux/export.h>
#include <linux/memblock.h>
#include <linux/sched/task.h>
#include <linux/numa.h>
#include <linux/pgtable.h>

#include <asm/lppaca.h>
#include <asm/paca.h>
#include <asm/sections.h>
#include <asm/kexec.h>
#include <asm/svm.h>
#include <asm/ultravisor.h>
#include <asm/rtas.h>

#include "setup.h"

#ifndef CONFIG_SMP
#define boot_cpuid 0
#endif

static void *__init alloc_paca_data(unsigned long size, unsigned long align,
				unsigned long limit, int cpu)
{
	void *ptr;
	int nid;

	/*
	 * boot_cpuid paca is allocated very early before cpu_to_node is up.
	 * Set bottom-up mode, because the boot CPU should be on node-0,
	 * which will put its paca in the right place.
	 */
	if (cpu == boot_cpuid) {
		nid = NUMA_NO_NODE;
		memblock_set_bottom_up(true);
	} else {
		nid = early_cpu_to_node(cpu);
	}

	ptr = memblock_alloc_try_nid(size, align, MEMBLOCK_LOW_LIMIT,
				     limit, nid);
	if (!ptr)
		panic("cannot allocate paca data");

	if (cpu == boot_cpuid)
		memblock_set_bottom_up(false);

	return ptr;
}

#ifdef CONFIG_PPC_PSERIES

#define LPPACA_SIZE 0x400

static void *__init alloc_shared_lppaca(unsigned long size, unsigned long limit,
					int cpu)
{
	size_t shared_lppaca_total_size = PAGE_ALIGN(nr_cpu_ids * LPPACA_SIZE);
	static unsigned long shared_lppaca_size;
	static void *shared_lppaca;
	void *ptr;

	if (!shared_lppaca) {
		memblock_set_bottom_up(true);

		/*
		 * See Documentation/powerpc/ultravisor.rst for more details.
		 *
		 * UV/HV data sharing is in PAGE_SIZE granularity. In order to
		 * minimize the number of pages shared, align the allocation to
		 * PAGE_SIZE.
		 */
		shared_lppaca =
			memblock_alloc_try_nid(shared_lppaca_total_size,
					       PAGE_SIZE, MEMBLOCK_LOW_LIMIT,
					       limit, NUMA_NO_NODE);
		if (!shared_lppaca)
			panic("cannot allocate shared data");

		memblock_set_bottom_up(false);
		uv_share_page(PHYS_PFN(__pa(shared_lppaca)),
			      shared_lppaca_total_size >> PAGE_SHIFT);
	}

	ptr = shared_lppaca + shared_lppaca_size;
	shared_lppaca_size += size;

	/*
	 * This is very early in boot, so no harm done if the kernel crashes at
	 * this point.
	 */
	BUG_ON(shared_lppaca_size > shared_lppaca_total_size);

	return ptr;
}

/*
 * See asm/lppaca.h for more detail.
 *
 * lppaca structures must must be 1kB in size, L1 cache line aligned,
 * and not cross 4kB boundary. A 1kB size and 1kB alignment will satisfy
 * these requirements.
 */
static inline void init_lppaca(struct lppaca *lppaca)
{
	BUILD_BUG_ON(sizeof(struct lppaca) != 640);

	*lppaca = (struct lppaca) {
		.desc = cpu_to_be32(0xd397d781),	/* "LpPa" */
		.size = cpu_to_be16(LPPACA_SIZE),
		.fpregs_in_use = 1,
		.slb_count = cpu_to_be16(64),
		.vmxregs_in_use = 0,
		.page_ins = 0, };
};

static struct lppaca * __init new_lppaca(int cpu, unsigned long limit)
{
	struct lppaca *lp;

	BUILD_BUG_ON(sizeof(struct lppaca) > LPPACA_SIZE);

	if (early_cpu_has_feature(CPU_FTR_HVMODE))
		return NULL;

	if (is_secure_guest())
		lp = alloc_shared_lppaca(LPPACA_SIZE, limit, cpu);
	else
		lp = alloc_paca_data(LPPACA_SIZE, 0x400, limit, cpu);

	init_lppaca(lp);

	return lp;
}
#endif /* CONFIG_PPC_PSERIES */

#ifdef CONFIG_PPC_BOOK3S_64

/*
 * 3 persistent SLBs are allocated here.  The buffer will be zero
 * initially, hence will all be invaild until we actually write them.
 *
 * If you make the number of persistent SLB entries dynamic, please also
 * update PR KVM to flush and restore them accordingly.
 */
static struct slb_shadow * __init new_slb_shadow(int cpu, unsigned long limit)
{
	struct slb_shadow *s;

	if (cpu != boot_cpuid) {
		/*
		 * Boot CPU comes here before early_radix_enabled
		 * is parsed (e.g., for disable_radix). So allocate
		 * always and this will be fixed up in free_unused_pacas.
		 */
		if (early_radix_enabled())
			return NULL;
	}

	s = alloc_paca_data(sizeof(*s), L1_CACHE_BYTES, limit, cpu);

	s->persistent = cpu_to_be32(SLB_NUM_BOLTED);
	s->buffer_length = cpu_to_be32(sizeof(*s));

	return s;
}

#endif /* CONFIG_PPC_BOOK3S_64 */

#ifdef CONFIG_PPC_PSERIES
/**
 * new_rtas_args() - Allocates rtas args
 * @cpu:	CPU number
 * @limit:	Memory limit for this allocation
 *
 * Allocates a struct rtas_args and return it's pointer,
 * if not in Hypervisor mode
 *
 * Return:	Pointer to allocated rtas_args
 *		NULL if CPU in Hypervisor Mode
 */
static struct rtas_args * __init new_rtas_args(int cpu, unsigned long limit)
{
	limit = min_t(unsigned long, limit, RTAS_INSTANTIATE_MAX);

	if (early_cpu_has_feature(CPU_FTR_HVMODE))
		return NULL;

	return alloc_paca_data(sizeof(struct rtas_args), L1_CACHE_BYTES,
			       limit, cpu);
}
#endif /* CONFIG_PPC_PSERIES */

/* The Paca is an array with one entry per processor.  Each contains an
 * lppaca, which contains the information shared between the
 * hypervisor and Linux.
 * On systems with hardware multi-threading, there are two threads
 * per processor.  The Paca array must contain an entry for each thread.
 * The VPD Areas will give a max logical processors = 2 * max physical
 * processors.  The processor VPD array needs one entry per physical
 * processor (not thread).
 */
struct paca_struct **paca_ptrs __read_mostly;
EXPORT_SYMBOL(paca_ptrs);

void __init initialise_paca(struct paca_struct *new_paca, int cpu)
{
#ifdef CONFIG_PPC_PSERIES
	new_paca->lppaca_ptr = NULL;
#endif
#ifdef CONFIG_PPC_BOOK3E
	new_paca->kernel_pgd = swapper_pg_dir;
#endif
	new_paca->lock_token = 0x8000;
	new_paca->paca_index = cpu;
	new_paca->kernel_toc = kernel_toc_addr();
	new_paca->kernelbase = (unsigned long) _stext;
	/* Only set MSR:IR/DR when MMU is initialized */
	new_paca->kernel_msr = MSR_KERNEL & ~(MSR_IR | MSR_DR);
	new_paca->hw_cpu_id = 0xffff;
	new_paca->kexec_state = KEXEC_STATE_NONE;
	new_paca->__current = &init_task;
	new_paca->data_offset = 0xfeeeeeeeeeeeeeeeULL;
#ifdef CONFIG_PPC_BOOK3S_64
	new_paca->slb_shadow_ptr = NULL;
#endif

#ifdef CONFIG_PPC_BOOK3E
	/* For now -- if we have threads this will be adjusted later */
	new_paca->tcd_ptr = &new_paca->tcd;
#endif

#ifdef CONFIG_PPC_PSERIES
	new_paca->rtas_args_reentrant = NULL;
#endif
}

/* Put the paca pointer into r13 and SPRG_PACA */
void setup_paca(struct paca_struct *new_paca)
{
	/* Setup r13 */
	local_paca = new_paca;

#ifdef CONFIG_PPC_BOOK3E
	/* On Book3E, initialize the TLB miss exception frames */
	mtspr(SPRN_SPRG_TLB_EXFRAME, local_paca->extlb);
#else
	/*
	 * In HV mode, we setup both HPACA and PACA to avoid problems
	 * if we do a GET_PACA() before the feature fixups have been
	 * applied.
	 *
	 * Normally you should test against CPU_FTR_HVMODE, but CPU features
	 * are not yet set up when we first reach here.
	 */
	if (mfmsr() & MSR_HV)
		mtspr(SPRN_SPRG_HPACA, local_paca);
#endif
	mtspr(SPRN_SPRG_PACA, local_paca);

}

static int __initdata paca_nr_cpu_ids;
static int __initdata paca_ptrs_size;
static int __initdata paca_struct_size;

void __init allocate_paca_ptrs(void)
{
	paca_nr_cpu_ids = nr_cpu_ids;

	paca_ptrs_size = sizeof(struct paca_struct *) * nr_cpu_ids;
	paca_ptrs = memblock_alloc_raw(paca_ptrs_size, SMP_CACHE_BYTES);
	if (!paca_ptrs)
		panic("Failed to allocate %d bytes for paca pointers\n",
		      paca_ptrs_size);

	memset(paca_ptrs, 0x88, paca_ptrs_size);
}

void __init allocate_paca(int cpu)
{
	u64 limit;
	struct paca_struct *paca;

	BUG_ON(cpu >= paca_nr_cpu_ids);

#ifdef CONFIG_PPC_BOOK3S_64
	/*
	 * We access pacas in real mode, and cannot take SLB faults
	 * on them when in virtual mode, so allocate them accordingly.
	 */
	limit = min(ppc64_bolted_size(), ppc64_rma_size);
#else
	limit = ppc64_rma_size;
#endif

	paca = alloc_paca_data(sizeof(struct paca_struct), L1_CACHE_BYTES,
				limit, cpu);
	paca_ptrs[cpu] = paca;

	initialise_paca(paca, cpu);
#ifdef CONFIG_PPC_PSERIES
	paca->lppaca_ptr = new_lppaca(cpu, limit);
#endif
#ifdef CONFIG_PPC_BOOK3S_64
	paca->slb_shadow_ptr = new_slb_shadow(cpu, limit);
#endif
#ifdef CONFIG_PPC_PSERIES
	paca->rtas_args_reentrant = new_rtas_args(cpu, limit);
#endif
	paca_struct_size += sizeof(struct paca_struct);
}

void __init free_unused_pacas(void)
{
	int new_ptrs_size;

	new_ptrs_size = sizeof(struct paca_struct *) * nr_cpu_ids;
	if (new_ptrs_size < paca_ptrs_size)
		memblock_free(__pa(paca_ptrs) + new_ptrs_size,
					paca_ptrs_size - new_ptrs_size);

	paca_nr_cpu_ids = nr_cpu_ids;
	paca_ptrs_size = new_ptrs_size;

#ifdef CONFIG_PPC_BOOK3S_64
	if (early_radix_enabled()) {
		/* Ugly fixup, see new_slb_shadow() */
		memblock_free(__pa(paca_ptrs[boot_cpuid]->slb_shadow_ptr),
				sizeof(struct slb_shadow));
		paca_ptrs[boot_cpuid]->slb_shadow_ptr = NULL;
	}
#endif

	printk(KERN_DEBUG "Allocated %u bytes for %u pacas\n",
			paca_ptrs_size + paca_struct_size, nr_cpu_ids);
}

void copy_mm_to_paca(struct mm_struct *mm)
{
#ifdef CONFIG_PPC_BOOK3S
	mm_context_t *context = &mm->context;

	get_paca()->mm_ctx_id = context->id;
#ifdef CONFIG_PPC_MM_SLICES
	VM_BUG_ON(!mm_ctx_slb_addr_limit(context));
	get_paca()->mm_ctx_slb_addr_limit = mm_ctx_slb_addr_limit(context);
	memcpy(&get_paca()->mm_ctx_low_slices_psize, mm_ctx_low_slices(context),
	       LOW_SLICE_ARRAY_SZ);
	memcpy(&get_paca()->mm_ctx_high_slices_psize, mm_ctx_high_slices(context),
	       TASK_SLICE_ARRAY_SZ(context));
#else /* CONFIG_PPC_MM_SLICES */
	get_paca()->mm_ctx_user_psize = context->user_psize;
	get_paca()->mm_ctx_sllp = context->sllp;
#endif
#else /* !CONFIG_PPC_BOOK3S */
	return;
#endif
}