aboutsummaryrefslogtreecommitdiffstats
blob: ce635dccf3d96921249a2e20084d9f67b5361b33 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
/* calibrate.c: default delay calibration
 *
 * Excised from init/main.c
 *  Copyright (C) 1991, 1992  Linus Torvalds
 */

#include <linux/jiffies.h>
#include <linux/delay.h>
#include <linux/init.h>
#include <linux/timex.h>
#include <linux/smp.h>
#include <linux/percpu.h>

unsigned long lpj_fine;
unsigned long preset_lpj;
static int __init lpj_setup(char *str)
{
	preset_lpj = simple_strtoul(str,NULL,0);
	return 1;
}

__setup("lpj=", lpj_setup);

#ifdef ARCH_HAS_READ_CURRENT_TIMER

/* This routine uses the read_current_timer() routine and gets the
 * loops per jiffy directly, instead of guessing it using delay().
 * Also, this code tries to handle non-maskable asynchronous events
 * (like SMIs)
 */
#define DELAY_CALIBRATION_TICKS			((HZ < 100) ? 1 : (HZ/100))
#define MAX_DIRECT_CALIBRATION_RETRIES		5

static unsigned long calibrate_delay_direct(void)
{
	unsigned long pre_start, start, post_start;
	unsigned long pre_end, end, post_end;
	unsigned long start_jiffies;
	unsigned long timer_rate_min, timer_rate_max;
	unsigned long good_timer_sum = 0;
	unsigned long good_timer_count = 0;
	unsigned long measured_times[MAX_DIRECT_CALIBRATION_RETRIES];
	int max = -1; /* index of measured_times with max/min values or not set */
	int min = -1;
	int i;

	if (read_current_timer(&pre_start) < 0 )
		return 0;

	/*
	 * A simple loop like
	 *	while ( jiffies < start_jiffies+1)
	 *		start = read_current_timer();
	 * will not do. As we don't really know whether jiffy switch
	 * happened first or timer_value was read first. And some asynchronous
	 * event can happen between these two events introducing errors in lpj.
	 *
	 * So, we do
	 * 1. pre_start <- When we are sure that jiffy switch hasn't happened
	 * 2. check jiffy switch
	 * 3. start <- timer value before or after jiffy switch
	 * 4. post_start <- When we are sure that jiffy switch has happened
	 *
	 * Note, we don't know anything about order of 2 and 3.
	 * Now, by looking at post_start and pre_start difference, we can
	 * check whether any asynchronous event happened or not
	 */

	for (i = 0; i < MAX_DIRECT_CALIBRATION_RETRIES; i++) {
		pre_start = 0;
		read_current_timer(&start);
		start_jiffies = jiffies;
		while (time_before_eq(jiffies, start_jiffies + 1)) {
			pre_start = start;
			read_current_timer(&start);
		}
		read_current_timer(&post_start);

		pre_end = 0;
		end = post_start;
		while (time_before_eq(jiffies, start_jiffies + 1 +
					       DELAY_CALIBRATION_TICKS)) {
			pre_end = end;
			read_current_timer(&end);
		}
		read_current_timer(&post_end);

		timer_rate_max = (post_end - pre_start) /
					DELAY_CALIBRATION_TICKS;
		timer_rate_min = (pre_end - post_start) /
					DELAY_CALIBRATION_TICKS;

		/*
		 * If the upper limit and lower limit of the timer_rate is
		 * >= 12.5% apart, redo calibration.
		 */
		if (start >= post_end)
			printk(KERN_NOTICE "calibrate_delay_direct() ignoring "
					"timer_rate as we had a TSC wrap around"
					" start=%lu >=post_end=%lu\n",
				start, post_end);
		if (start < post_end && pre_start != 0 && pre_end != 0 &&
		    (timer_rate_max - timer_rate_min) < (timer_rate_max >> 3)) {
			good_timer_count++;
			good_timer_sum += timer_rate_max;
			measured_times[i] = timer_rate_max;
			if (max < 0 || timer_rate_max > measured_times[max])
				max = i;
			if (min < 0 || timer_rate_max < measured_times[min])
				min = i;
		} else
			measured_times[i] = 0;

	}

	/*
	 * Find the maximum & minimum - if they differ too much throw out the
	 * one with the largest difference from the mean and try again...
	 */
	while (good_timer_count > 1) {
		unsigned long estimate;
		unsigned long maxdiff;

		/* compute the estimate */
		estimate = (good_timer_sum/good_timer_count);
		maxdiff = estimate >> 3;

		/* if range is within 12% let's take it */
		if ((measured_times[max] - measured_times[min]) < maxdiff)
			return estimate;

		/* ok - drop the worse value and try again... */
		good_timer_sum = 0;
		good_timer_count = 0;
		if ((measured_times[max] - estimate) <
				(estimate - measured_times[min])) {
			printk(KERN_NOTICE "calibrate_delay_direct() dropping "
					"min bogoMips estimate %d = %lu\n",
				min, measured_times[min]);
			measured_times[min] = 0;
			min = max;
		} else {
			printk(KERN_NOTICE "calibrate_delay_direct() dropping "
					"max bogoMips estimate %d = %lu\n",
				max, measured_times[max]);
			measured_times[max] = 0;
			max = min;
		}

		for (i = 0; i < MAX_DIRECT_CALIBRATION_RETRIES; i++) {
			if (measured_times[i] == 0)
				continue;
			good_timer_count++;
			good_timer_sum += measured_times[i];
			if (measured_times[i] < measured_times[min])
				min = i;
			if (measured_times[i] > measured_times[max])
				max = i;
		}

	}

	printk(KERN_NOTICE "calibrate_delay_direct() failed to get a good "
	       "estimate for loops_per_jiffy.\nProbably due to long platform "
		"interrupts. Consider using \"lpj=\" boot option.\n");
	return 0;
}
#else
static unsigned long calibrate_delay_direct(void)
{
	return 0;
}
#endif

/*
 * This is the number of bits of precision for the loops_per_jiffy.  Each
 * time we refine our estimate after the first takes 1.5/HZ seconds, so try
 * to start with a good estimate.
 * For the boot cpu we can skip the delay calibration and assign it a value
 * calculated based on the timer frequency.
 * For the rest of the CPUs we cannot assume that the timer frequency is same as
 * the cpu frequency, hence do the calibration for those.
 */
#define LPS_PREC 8

static unsigned long calibrate_delay_converge(void)
{
	/* First stage - slowly accelerate to find initial bounds */
	unsigned long lpj, lpj_base, ticks, loopadd, loopadd_base, chop_limit;
	int trials = 0, band = 0, trial_in_band = 0;

	lpj = (1<<12);

	/* wait for "start of" clock tick */
	ticks = jiffies;
	while (ticks == jiffies)
		; /* nothing */
	/* Go .. */
	ticks = jiffies;
	do {
		if (++trial_in_band == (1<<band)) {
			++band;
			trial_in_band = 0;
		}
		__delay(lpj * band);
		trials += band;
	} while (ticks == jiffies);
	/*
	 * We overshot, so retreat to a clear underestimate. Then estimate
	 * the largest likely undershoot. This defines our chop bounds.
	 */
	trials -= band;
	loopadd_base = lpj * band;
	lpj_base = lpj * trials;

recalibrate:
	lpj = lpj_base;
	loopadd = loopadd_base;

	/*
	 * Do a binary approximation to get lpj set to
	 * equal one clock (up to LPS_PREC bits)
	 */
	chop_limit = lpj >> LPS_PREC;
	while (loopadd > chop_limit) {
		lpj += loopadd;
		ticks = jiffies;
		while (ticks == jiffies)
			; /* nothing */
		ticks = jiffies;
		__delay(lpj);
		if (jiffies != ticks)	/* longer than 1 tick */
			lpj -= loopadd;
		loopadd >>= 1;
	}
	/*
	 * If we incremented every single time possible, presume we've
	 * massively underestimated initially, and retry with a higher
	 * start, and larger range. (Only seen on x86_64, due to SMIs)
	 */
	if (lpj + loopadd * 2 == lpj_base + loopadd_base * 2) {
		lpj_base = lpj;
		loopadd_base <<= 2;
		goto recalibrate;
	}

	return lpj;
}

static DEFINE_PER_CPU(unsigned long, cpu_loops_per_jiffy) = { 0 };

/*
 * Check if cpu calibration delay is already known. For example,
 * some processors with multi-core sockets may have all cores
 * with the same calibration delay.
 *
 * Architectures should override this function if a faster calibration
 * method is available.
 */
unsigned long __attribute__((weak)) calibrate_delay_is_known(void)
{
	return 0;
}

/*
 * Indicate the cpu delay calibration is done. This can be used by
 * architectures to stop accepting delay timer registrations after this point.
 */

void __attribute__((weak)) calibration_delay_done(void)
{
}

void calibrate_delay(void)
{
	unsigned long lpj;
	static bool printed;
	int this_cpu = smp_processor_id();

	if (per_cpu(cpu_loops_per_jiffy, this_cpu)) {
		lpj = per_cpu(cpu_loops_per_jiffy, this_cpu);
		if (!printed)
			pr_info("Calibrating delay loop (skipped) "
				"already calibrated this CPU");
	} else if (preset_lpj) {
		lpj = preset_lpj;
		if (!printed)
			pr_info("Calibrating delay loop (skipped) "
				"preset value.. ");
	} else if ((!printed) && lpj_fine) {
		lpj = lpj_fine;
		pr_info("Calibrating delay loop (skipped), "
			"value calculated using timer frequency.. ");
	} else if ((lpj = calibrate_delay_is_known())) {
		;
	} else if ((lpj = calibrate_delay_direct()) != 0) {
		if (!printed)
			pr_info("Calibrating delay using timer "
				"specific routine.. ");
	} else {
		if (!printed)
			pr_info("Calibrating delay loop... ");
		lpj = calibrate_delay_converge();
	}
	per_cpu(cpu_loops_per_jiffy, this_cpu) = lpj;
	if (!printed)
		pr_cont("%lu.%02lu BogoMIPS (lpj=%lu)\n",
			lpj/(500000/HZ),
			(lpj/(5000/HZ)) % 100, lpj);

	loops_per_jiffy = lpj;
	printed = true;

	calibration_delay_done();
}