aboutsummaryrefslogtreecommitdiffstats
blob: 8cb6db54285ba64f81af9ba2b388a7c216ceec61 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
/*
 * Many of the syscalls used in this file expect some of the arguments
 * to be __user pointers not __kernel pointers.  To limit the sparse
 * noise, turn off sparse checking for this file.
 */
#ifdef __CHECKER__
#undef __CHECKER__
#warning "Sparse checking disabled for this file"
#endif

#include <linux/delay.h>
#include <linux/raid/md_u.h>
#include <linux/raid/md_p.h>

#include "do_mounts.h"

/*
 * When md (and any require personalities) are compiled into the kernel
 * (not a module), arrays can be assembles are boot time using with AUTODETECT
 * where specially marked partitions are registered with md_autodetect_dev(),
 * and with MD_BOOT where devices to be collected are given on the boot line
 * with md=.....
 * The code for that is here.
 */

#ifdef CONFIG_MD_AUTODETECT
static int __initdata raid_noautodetect;
#else
static int __initdata raid_noautodetect=1;
#endif
static int __initdata raid_autopart;

static struct {
	int minor;
	int partitioned;
	int level;
	int chunk;
	char *device_names;
} md_setup_args[256] __initdata;

static int md_setup_ents __initdata;

/*
 * Parse the command-line parameters given our kernel, but do not
 * actually try to invoke the MD device now; that is handled by
 * md_setup_drive after the low-level disk drivers have initialised.
 *
 * 27/11/1999: Fixed to work correctly with the 2.3 kernel (which
 *             assigns the task of parsing integer arguments to the
 *             invoked program now).  Added ability to initialise all
 *             the MD devices (by specifying multiple "md=" lines)
 *             instead of just one.  -- KTK
 * 18May2000: Added support for persistent-superblock arrays:
 *             md=n,0,factor,fault,device-list   uses RAID0 for device n
 *             md=n,-1,factor,fault,device-list  uses LINEAR for device n
 *             md=n,device-list      reads a RAID superblock from the devices
 *             elements in device-list are read by name_to_kdev_t so can be
 *             a hex number or something like /dev/hda1 /dev/sdb
 * 2001-06-03: Dave Cinege <dcinege@psychosis.com>
 *		Shifted name_to_kdev_t() and related operations to md_set_drive()
 *		for later execution. Rewrote section to make devfs compatible.
 */
static int __init md_setup(char *str)
{
	int minor, level, factor, fault, partitioned = 0;
	char *pername = "";
	char *str1;
	int ent;

	if (*str == 'd') {
		partitioned = 1;
		str++;
	}
	if (get_option(&str, &minor) != 2) {	/* MD Number */
		printk(KERN_WARNING "md: Too few arguments supplied to md=.\n");
		return 0;
	}
	str1 = str;
	for (ent=0 ; ent< md_setup_ents ; ent++)
		if (md_setup_args[ent].minor == minor &&
		    md_setup_args[ent].partitioned == partitioned) {
			printk(KERN_WARNING "md: md=%s%d, Specified more than once. "
			       "Replacing previous definition.\n", partitioned?"d":"", minor);
			break;
		}
	if (ent >= ARRAY_SIZE(md_setup_args)) {
		printk(KERN_WARNING "md: md=%s%d - too many md initialisations\n", partitioned?"d":"", minor);
		return 0;
	}
	if (ent >= md_setup_ents)
		md_setup_ents++;
	switch (get_option(&str, &level)) {	/* RAID level */
	case 2: /* could be 0 or -1.. */
		if (level == 0 || level == LEVEL_LINEAR) {
			if (get_option(&str, &factor) != 2 ||	/* Chunk Size */
					get_option(&str, &fault) != 2) {
				printk(KERN_WARNING "md: Too few arguments supplied to md=.\n");
				return 0;
			}
			md_setup_args[ent].level = level;
			md_setup_args[ent].chunk = 1 << (factor+12);
			if (level ==  LEVEL_LINEAR)
				pername = "linear";
			else
				pername = "raid0";
			break;
		}
		/* FALL THROUGH */
	case 1: /* the first device is numeric */
		str = str1;
		/* FALL THROUGH */
	case 0:
		md_setup_args[ent].level = LEVEL_NONE;
		pername="super-block";
	}

	printk(KERN_INFO "md: Will configure md%d (%s) from %s, below.\n",
		minor, pername, str);
	md_setup_args[ent].device_names = str;
	md_setup_args[ent].partitioned = partitioned;
	md_setup_args[ent].minor = minor;

	return 1;
}

static void __init md_setup_drive(void)
{
	int minor, i, ent, partitioned;
	dev_t dev;
	dev_t devices[MD_SB_DISKS+1];

	for (ent = 0; ent < md_setup_ents ; ent++) {
		int fd;
		int err = 0;
		char *devname;
		mdu_disk_info_t dinfo;
		char name[16];

		minor = md_setup_args[ent].minor;
		partitioned = md_setup_args[ent].partitioned;
		devname = md_setup_args[ent].device_names;

		sprintf(name, "/dev/md%s%d", partitioned?"_d":"", minor);
		if (partitioned)
			dev = MKDEV(mdp_major, minor << MdpMinorShift);
		else
			dev = MKDEV(MD_MAJOR, minor);
		create_dev(name, dev);
		for (i = 0; i < MD_SB_DISKS && devname != NULL; i++) {
			char *p;
			char comp_name[64];
			u32 rdev;

			p = strchr(devname, ',');
			if (p)
				*p++ = 0;

			dev = name_to_dev_t(devname);
			if (strncmp(devname, "/dev/", 5) == 0)
				devname += 5;
			snprintf(comp_name, 63, "/dev/%s", devname);
			rdev = bstat(comp_name);
			if (rdev)
				dev = new_decode_dev(rdev);
			if (!dev) {
				printk(KERN_WARNING "md: Unknown device name: %s\n", devname);
				break;
			}

			devices[i] = dev;

			devname = p;
		}
		devices[i] = 0;

		if (!i)
			continue;

		printk(KERN_INFO "md: Loading md%s%d: %s\n",
			partitioned ? "_d" : "", minor,
			md_setup_args[ent].device_names);

		fd = sys_open(name, 0, 0);
		if (fd < 0) {
			printk(KERN_ERR "md: open failed - cannot start "
					"array %s\n", name);
			continue;
		}
		if (sys_ioctl(fd, SET_ARRAY_INFO, 0) == -EBUSY) {
			printk(KERN_WARNING
			       "md: Ignoring md=%d, already autodetected. (Use raid=noautodetect)\n",
			       minor);
			sys_close(fd);
			continue;
		}

		if (md_setup_args[ent].level != LEVEL_NONE) {
			/* non-persistent */
			mdu_array_info_t ainfo;
			ainfo.level = md_setup_args[ent].level;
			ainfo.size = 0;
			ainfo.nr_disks =0;
			ainfo.raid_disks =0;
			while (devices[ainfo.raid_disks])
				ainfo.raid_disks++;
			ainfo.md_minor =minor;
			ainfo.not_persistent = 1;

			ainfo.state = (1 << MD_SB_CLEAN);
			ainfo.layout = 0;
			ainfo.chunk_size = md_setup_args[ent].chunk;
			err = sys_ioctl(fd, SET_ARRAY_INFO, (long)&ainfo);
			for (i = 0; !err && i <= MD_SB_DISKS; i++) {
				dev = devices[i];
				if (!dev)
					break;
				dinfo.number = i;
				dinfo.raid_disk = i;
				dinfo.state = (1<<MD_DISK_ACTIVE)|(1<<MD_DISK_SYNC);
				dinfo.major = MAJOR(dev);
				dinfo.minor = MINOR(dev);
				err = sys_ioctl(fd, ADD_NEW_DISK, (long)&dinfo);
			}
		} else {
			/* persistent */
			for (i = 0; i <= MD_SB_DISKS; i++) {
				dev = devices[i];
				if (!dev)
					break;
				dinfo.major = MAJOR(dev);
				dinfo.minor = MINOR(dev);
				sys_ioctl(fd, ADD_NEW_DISK, (long)&dinfo);
			}
		}
		if (!err)
			err = sys_ioctl(fd, RUN_ARRAY, 0);
		if (err)
			printk(KERN_WARNING "md: starting md%d failed\n", minor);
		else {
			/* reread the partition table.
			 * I (neilb) and not sure why this is needed, but I cannot
			 * boot a kernel with devfs compiled in from partitioned md
			 * array without it
			 */
			sys_close(fd);
			fd = sys_open(name, 0, 0);
			sys_ioctl(fd, BLKRRPART, 0);
		}
		sys_close(fd);
	}
}

static int __init raid_setup(char *str)
{
	int len, pos;

	len = strlen(str) + 1;
	pos = 0;

	while (pos < len) {
		char *comma = strchr(str+pos, ',');
		int wlen;
		if (comma)
			wlen = (comma-str)-pos;
		else	wlen = (len-1)-pos;

		if (!strncmp(str, "noautodetect", wlen))
			raid_noautodetect = 1;
		if (!strncmp(str, "autodetect", wlen))
			raid_noautodetect = 0;
		if (strncmp(str, "partitionable", wlen)==0)
			raid_autopart = 1;
		if (strncmp(str, "part", wlen)==0)
			raid_autopart = 1;
		pos += wlen+1;
	}
	return 1;
}

__setup("raid=", raid_setup);
__setup("md=", md_setup);

static void __init autodetect_raid(void)
{
	int fd;

	/*
	 * Since we don't want to detect and use half a raid array, we need to
	 * wait for the known devices to complete their probing
	 */
	printk(KERN_INFO "md: Waiting for all devices to be available before autodetect\n");
	printk(KERN_INFO "md: If you don't use raid, use raid=noautodetect\n");

	wait_for_device_probe();

	fd = sys_open("/dev/md0", 0, 0);
	if (fd >= 0) {
		sys_ioctl(fd, RAID_AUTORUN, raid_autopart);
		sys_close(fd);
	}
}

void __init md_run_setup(void)
{
	create_dev("/dev/md0", MKDEV(MD_MAJOR, 0));

	if (raid_noautodetect)
		printk(KERN_INFO "md: Skipping autodetection of RAID arrays. (raid=autodetect will force)\n");
	else
		autodetect_raid();
	md_setup_drive();
}