summaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* DO NOT MERGE - Merge Android 10 into master.HEADmasterXin Li2019-09-041-44/+53
| | | | | Bug: 140451723 Change-Id: I17b671cdb6375b57eb9364905b432d473f1b109e
* Add App Compat C-Suite project to manifestYuexi Ma2019-08-301-0/+1
| | | | | Bug: 140193734 Change-Id: Idc31a3e4dec37f65b86b493d355526ca7b9c2947
* Crosvm: add additional dependenciesJeff Vander Stoep2019-08-231-0/+4
| | | | | | Bug: 133498409 Test: repo sync, verify no errors Change-Id: I0a7f1da6a6e39d03c5c0d7fdeeb4c1900ba04e1d
* add external/kotlinx.coroutines to repo manifestSteve Elliott2019-08-221-0/+1
| | | | Change-Id: Ie71c6e38cdd70375b9f35d7f9dfb069c66ee6b39
* Remove build/katiDan Willemsen2019-08-211-1/+0
| | | | | | | | We've already got prebuilts of this in prebuilts/build-tools, we don't need the source in the tree as well. Test: treehugger Change-Id: I1e3087cd848bab9168d3dd34a240a8f2f5e930b4
* Add GWP-ASan to AOSP manifest.Elliott Hughes2019-08-201-0/+1
| | | | | | | Bug: 139531572 Bug: 135634846 Test: N/A Change-Id: I8e3a15cfb62faf274ecafbe4ce4cd303efdac559
* Add platform/tools/doc_generation project to masterTiem Song2019-08-141-0/+1
| | | | | Bug: 128540915 Test: N/A
* Remove unused frameworks/opt/datetimepickerNeil Fuller2019-08-131-1/+0
| | | | | | | | | | The code has Y2038 issues via android.text.format.Time. There are no users so it can be removed. Bug: 16550209 Test: build only Merged-In: Ic07eb1f810d5192d69b156fff6d64ff538471651 Change-Id: Ic07eb1f810d5192d69b156fff6d64ff538471651
* Add pdk to tools/platform-compat groups.atrost2019-08-071-1/+1
| | | | | | | | To follow libcore, which will depend on it. Bug: 138222363 Test: Treehugger only Merged-In: I30d35f022f1f7e7a292482e5db26e8adfe249ad7 Change-Id: I9065c512e2b4ae0dbd7b3a40e80a28ffc91e9e5d
* Add libfuse to masterPaul Lawrence2019-08-021-0/+1
| | | | Merged-In: I89781eb9948c4c02f91d415add2bfb162e24737c
* Add platform/external/mime-support to the AOSP master manifest.Tobias Thierer2019-07-311-0/+1
| | | | | | | Bug: 135431432 Test: N/A (Treehugger only) Change-Id: I4874374b465529ac99eed55667ee064f002bfdc0
* Add groups to project tools/platform-compat.atrost2019-07-301-1/+1
| | | | | | | | | As now a test in frameworks/base depends on a target in tools/platform-compat it needs to be present in the same groups as frameworks/base project. Example breakage: https://android-build.googleplex.com/builds/branches/partner-r-fs-release-generic-fs/grid?head=5765456&tail=5734200 Bug: 138222871
* Added packages/modules/DnsResolver.Xin Li2019-07-271-0/+1
| | | | | | Bug: 134997188 Merged-In: Ibfd1758b960d40cd8c2648b7a3cb11790f95da1e Change-Id: Ibfd1758b960d40cd8c2648b7a3cb11790f95da1e
* Reduce diff against internal manifest.Xin Li2019-07-251-4/+4
| | | | | | Bug: 134997188 Merged-In: Idd0e37954cedfb29f6569d73462eb5b49a01406d Change-Id: I961afbb92f86a19040eb8317e060d5ce38dbe481
* Add platform/external/OpenCSD to the manifest.Yabin Cui2019-07-231-0/+1
| | | | | | | | Bug: 135204414 Change-Id: I22dab695b185539432c81aeacbb59889793a6bcd Merged-In: Ia7bf2f7d7b63482b2dc082b95e37c28052049603 Merged-In: If777e6b4d91fd3fc0d94beb143ad74adbc48daab Merged-In: If0b8edabe011a90ba509082169c8ff486b242b0f
* Add new compat project tools/platform-compat to the manifest.atrost2019-07-181-0/+1
| | | | | | | Following the instructions in https://yaqs.googleplex.com/eng/q/5834446267744256 Change-Id: I80023003de9718346b2edfa72f8eed8f4d4bf0eb
* Remove external/perf_data_converter.Elliott Hughes2019-07-161-1/+0
| | | | | | | perfprofd is dead and gone. Test: builds Change-Id: Id6f05c85bc5bc404ca0ef3be31dfae692933208d
* Add libepoxy to aosp master manifestGreg Hartman2019-07-121-0/+1
| | | | | | | | Test: Local checkbuild BUG: 123765087 BUG: 123764798 (Milestone) BUG: 77276633 (OKR) Change-Id: Id1b653c310d75c03c95a368a98b6f67fd7625b7b
* Revert "Use the persistent-https URL for vendor blobs."Xin Li2019-06-241-1/+1
| | | | | | | | This reverts commit f7b6d016814dba76f1cac2bef3ef1bba93d536a2. Reason for revert: seems to break aosp-master-with-phones build Change-Id: Ib9615cdd9da09d40ae7102978e502c9ed0120077
* Build CrosVM for CuttlefishJeff Vander Stoep2019-06-211-0/+5
| | | | | | | | | | | | | | | | | | | | | | | CrosVM is a secure hypervisor which Cuttlefish [1] now uses instead of QEMU on GCE [2]. It is primarily written in Rust. CrosVM requires: -Two chromium projects: adhd [3] and crosvm [4]. -Three crates: byteorder [5], libc [6], and remain [7]. -A Rust toolchain prebuilt which we are building from [8]. [1] https://github.com/google/android-cuttlefish [2] https://cloud.google.com/compute/docs/ [3] https://chromium.googlesource.com/chromiumos/third_party/adhd/ [4] https://chromium.googlesource.com/chromiumos/platform/crosvm/ [5] https://github.com/BurntSushi/byteorder [6] https://crates.io/crates/libc [7] https://github.com/dtolnay/remain [8] https://static.rust-lang.org/dist/rustc-1.35.0-src.tar.gz Bug: 133498409 Test: repo init -b <manifest with this commit> repo sync -j20
* Use the persistent-https URL for vendor blobs.Xin Li2019-06-201-1/+1
| | | | Change-Id: I4072d09030bc176622f6355124a9aa3df78c5484
* Add path to bpfmt for global preuploadColin Cross2019-06-181-0/+1
| | | | | | | | | Add the path to bpfmt so that it can be enabled in individual projects. Don't enable it globally yet. Bug: 132785638 Test: manual Change-Id: Ib05950433ba5a0934853b9947324c7fe5c931b16
* Remove external/robolectricColin Cross2019-06-171-1/+0
| | | | | | | | All the code is in external/robolectric-shadows now. Fixes: 122331675 Test: m checkbuild Change-Id: I537398e89b46301ff7229420c6c6ea7a68353bc1
* Remove test kernel.Xin Li2019-06-131-2/+0
| | | | Change-Id: Ie21c33bf7d224e067bed3dfe7aece6a46aaa52b3
* Add system/tools/mkbootimg repoHridya Valsaraju2019-06-121-0/+1
| | | | | | Bug: 133171083 Test: make Change-Id: I2d9208af2952a3a538f2c1090b957d95d91aaf21
* Revert "Remove unused project external/fmtlib."Jiyong Park2019-06-111-0/+1
| | | | | | | | | | This reverts commit 47e9e995a19606813416f90ab251f4d08acfeb8d. fmtlib is needed again. Bug: 132145659 Test: repo sync Change-Id: I946592894b8f9f52747c9f0d213c2c065674bb4e
* Remove frameworks/opt/gamesdk from manifestHenry Daitx2019-06-071-1/+0
| | | | | Bug: 132164876 Merged-In: I1c5aa20b4855c626a6e25eba37256b1ffb6d3dde
* Add internal smartsync endpoint.Bill Napier2019-06-051-0/+2
| | | | | | | | DO NOT MERGE ANYWHERE BUG=75304981 Change-Id: I76466d3ef66ccf1330516a3d36e260662381c6ca
* Add platform/external/cpu_features to the manifest.Roland Levillain2019-06-031-0/+1
| | | | Bug: 122712425
* Added the following projects to manifest:Baligh Uddin2019-06-021-0/+4
| | | | | | | | | | - packages/modules/CaptivePortalLogin - packages/modules/ExtServices - packages/modules/NetworkPermissionConfig - packages/modules/NetworkStack Bug: 133225687 Change-Id: I02c60f7483b8aa605f8f5ba7bff083fd73d6b261
* Fix build break, until migration is doneBaligh Uddin2019-05-311-4/+0
|
* Add platform/external/lottie to manifest.Mariia Sandrikova2019-05-301-0/+1
| | | | | | | Third-party review: ag/6281574 Bug: 125468555 Change-Id: I829b6101e44a00af5aa64b68c9a16e87ee43790e
* Added the following projects to aosp-master manifest:Baligh Uddin2019-05-231-0/+4
| | | | | | | | | | | - platform/packages/modules/CaptivePortalLogin - platform/packages/modules/ExtServices - platform/packages/modules/NetworkPermissionConfig - platform/packages/modules/NetworkStack Bug: 133225687 Test: Sync locally Change-Id: I3c6ed5e4bb5d6479be123d4efe201825bd149e24
* Add igt-gpu-tools to manifestAlistair Strachan2019-05-211-0/+1
| | | | | Bug: 110963635 Change-Id: I55926b8ec4ec1ebabaf84587621aaf72c2941c35
* Remove external/spirv-llvm from the manifest.Stephen Hines2019-05-171-1/+0
| | | | | | Bug: http://b/118818878 Test: Builds. Change-Id: I86e94400104f89fe6aaa5a6fb1b5bf3f62aec024
* DO NOT MERGE - Merge Pie Bonito/Sargo into master.Xin Li2019-05-092-2/+19
| | | | | Bug: 131756210 Change-Id: I97892fee5b7a68ce3cc13262fce076c11733b2b4
* Walleye: Add custom kernel to fix lab testing.Ian Kasprzak2019-05-091-0/+2
| | | | | | | Bug: 132196666 Test: repo sync synced new project / path Change-Id: Ie66bfbe221e3cfeef8303fb8f0edb397b2c44dff
* Add platform/external/python/ipaddress to manifest.Kevin Cheng2019-05-071-0/+1
| | | | | Bug: 132083173 Test: None
* Add empty repo for mts to manifest.Chen Zhu2019-05-021-0/+1
| | | | | | | | | Bug: 131352186 Test: Manual test Merged-In: Ia598208edff4e06d1add91a16bc2ddd6eb3243a2 Change-Id: I3f6140ca6880ab7ee516c92cf01f6fe11b7a979d
* Create prebuilts/abi-dumps/platform to house abi references for opt-in ↵Andrew Hsieh2019-04-291-0/+1
| | | | | | | | | | | | shared libraries Shared libraries (other than vndk/[ll]ndk) can opt-in ABI stability enforcement by populating their dump in prebuilts/abi-dumps/platform See https://source.android.com/devices/architecture/vndk/abi-stability Bug: 79424996 Test: manual repo sync which shows prebuilts/abi-dumps/platform exists
* Add ukey2 to the PDKGreg Kaiser2019-04-191-1/+1
| | | | | | | | | We want platform/external/ukey2 in the Platform Development Kit because there are other packages we'll ship which use this project. Test: TreeHugger Change-Id: I72fbdfaa455ccc838420d04b41a0264359bf6194
* Add external/javapoetColin Cross2019-04-121-0/+1
| | | | | | | Bug: 130434382 Test: treehugger Merged-In: I6c68321600832c1a5e6a3589796d61aa17ab94ab Change-Id: Iaca23b8fa34aa925c27b3ef3803a843203709d54
* Delete external/libedit and prebuilts/libs/libeditColin Cross2019-04-031-2/+0
| | | | | | | | | | external/libedit is only used to update prebuilts/libs/libedit, and prebuilts/libs/libedit only contains host library prebuilt that is not used in the build. Fixes: 122331950 Test: m checkbuild Change-Id: Ibe57b7469b665391f9ebdec77ef8dc58f9e16d1d
* Remove unused frameworks/opt/net/lowpanDan Willemsen2019-04-021-1/+0
| | | | | | | | | This is no longer used on master. Change-Id: I19fdb45bf3e29533e7809de63d051c184e59d661 Fixes: 122331573 Test: codesearch Test: treehugger
* Add iperf3 to the manifest.Elliott Hughes2019-03-271-0/+1
| | | | | | Bug: http://b/123261826 Test: repo sync external/iperf3 Change-Id: Ib103d6083662d456c80b5b5a923ac7aeca356056
* Add in pyopenssl and it's dependencies to manifest.Kevin Cheng2019-03-251-0/+5
| | | | | | | | | | | | Added: - platform/external/python/asn1crypto - platform/external/python/cffi - platform/external/python/cryptography - platform/external/python/pycparser - platform/external/python/pyopenssl Bug: 122778810 Test: None
* Revert "Remove external/blktrace"Colin Cross2019-03-221-0/+1
| | | | | | | | This reverts commit 70d63873f198a1cb237138eedd578cb0ace8bfdd. Reason for revert: used internally Change-Id: I9f97765b55f7776feba3c6b1487d6c5f36329e60
* Remove external/blktraceColin Cross2019-03-221-1/+0
| | | | | | | | It hasn't been touched since 2009, the Makefiles are disabled, and it doesn't build when enabled. Test: none Change-Id: I4d380e837235a2b26c8c44842b0e75b7a560d93b
* Add external/neon_2_sse to default manifest.George Lu2019-03-211-0/+1
| | | | Bug: 80630324
* Remove platform/external/mmc-utilsBill Yi2019-03-191-1/+0
| | | | | | TEST: make checkbuild BUG:128626934 Change-Id: I8e5b221ae647472b37e359454d40ccb94b3ef474